/* * Many of the syscalls used in this file expect some of the arguments * to be __user pointers not __kernel pointers. To limit the sparse * noise, turn off sparse checking for this file. */ #ifdef __CHECKER__ #undef __CHECKER__ #warning "Sparse checking disabled for this file" #endif #include #include #include #include "do_mounts.h" /* * When md (and any require personalities) are compiled into the kernel * (not a module), arrays can be assembles are boot time using with AUTODETECT * where specially marked partitions are registered with md_autodetect_dev(), * and with MD_BOOT where devices to be collected are given on the boot line * with md=..... * The code for that is here. */ #ifdef CONFIG_MD_AUTODETECT static int __initdata raid_noautodetect; #else static int __initdata raid_noautodetect=1; #endif static int __initdata raid_autopart; static struct { int minor; int partitioned; int level; int chunk; char *device_names; } md_setup_args[256] __initdata; static int md_setup_ents __initdata; /* * Parse the command-line parameters given our kernel, but do not * actually try to invoke the MD device now; that is handled by * md_setup_drive after the low-level disk drivers have initialised. * * 27/11/1999: Fixed to work correctly with the 2.3 kernel (which * assigns the task of parsing integer arguments to the * invoked program now). Added ability to initialise all * the MD devices (by specifying multiple "md=" lines) * instead of just one. -- KTK * 18May2000: Added support for persistent-superblock arrays: * md=n,0,factor,fault,device-list uses RAID0 for device n * md=n,-1,factor,fault,device-list uses LINEAR for device n * md=n,device-list reads a RAID superblock from the devices * elements in device-list are read by name_to_kdev_t so can be * a hex number or something like /dev/hda1 /dev/sdb * 2001-06-03: Dave Cinege * Shifted name_to_kdev_t() and related operations to md_set_drive() * for later execution. Rewrote section to make devfs compatible. */ static int __init md_setup(char *str) { int minor, level, factor, fault, partitioned = 0; char *pername = ""; char *str1; int ent; if (*str == 'd') { partitioned = 1; str++; } if (get_option(&str, &minor) != 2) { /* MD Number */ printk(KERN_WARNING "md: Too few arguments supplied to md=.\n"); return 0; } str1 = str; for (ent=0 ; ent< md_setup_ents ; ent++) if (md_setup_args[ent].minor == minor && md_setup_args[ent].partitioned == partitioned) { printk(KERN_WARNING "md: md=%s%d, Specified more than once. " "Replacing previous definition.\n", partitioned?"d":"", minor); break; } if (ent >= ARRAY_SIZE(md_setup_args)) { printk(KERN_WARNING "md: md=%s%d - too many md initialisations\n", partitioned?"d":"", minor); return 0; } if (ent >= md_setup_ents) md_setup_ents++; switch (get_option(&str, &level)) { /* RAID level */ case 2: /* could be 0 or -1.. */ if (level == 0 || level == LEVEL_LINEAR) { if (get_option(&str, &factor) != 2 || /* Chunk Size */ get_option(&str, &fault) != 2) { printk(KERN_WARNING "md: Too few arguments supplied to md=.\n"); return 0; } md_setup_args[ent].level = level; md_setup_args[ent].chunk = 1 << (factor+12); if (level == LEVEL_LINEAR) pername = "linear"; else pername = "raid0"; break; } /* FALL THROUGH */ case 1: /* the first device is numeric */ str = str1; /* FALL THROUGH */ case 0: md_setup_args[ent].level = LEVEL_NONE; pername="super-block"; } printk(KERN_INFO "md: Will configure md%d (%s) from %s, below.\n", minor, pername, str); md_setup_args[ent].device_names = str; md_setup_args[ent].partitioned = partitioned; md_setup_args[ent].minor = minor; return 1; } static void __init md_setup_drive(void) { int minor, i, ent, partitioned; dev_t dev; dev_t devices[MD_SB_DISKS+1]; for (ent = 0; ent < md_setup_ents ; ent++) { int fd; int err = 0; char *devname; mdu_disk_info_t dinfo; char name[16]; minor = md_setup_args[ent].minor; partitioned = md_setup_args[ent].partitioned; devname = md_setup_args[ent].device_names; sprintf(name, "/dev/md%s%d", partitioned?"_d":"", minor); if (partitioned) dev = MKDEV(mdp_major, minor << MdpMinorShift); else dev = MKDEV(MD_MAJOR, minor); create_dev(name, dev); for (i = 0; i < MD_SB_DISKS && devname != NULL; i++) { char *p; char comp_name[64]; u32 rdev; p = strchr(devname, ','); if (p) *p++ = 0; dev = name_to_dev_t(devname); if (strncmp(devname, "/dev/", 5) == 0) devname += 5; snprintf(comp_name, 63, "/dev/%s", devname); rdev = bstat(comp_name); if (rdev) dev = new_decode_dev(rdev); if (!dev) { printk(KERN_WARNING "md: Unknown device name: %s\n", devname); break; } devices[i] = dev; devname = p; } devices[i] = 0; if (!i) continue; printk(KERN_INFO "md: Loading md%s%d: %s\n", partitioned ? "_d" : "", minor, md_setup_args[ent].device_names); fd = sys_open(name, 0, 0); if (fd < 0) { printk(KERN_ERR "md: open failed - cannot start " "array %s\n", name); continue; } if (sys_ioctl(fd, SET_ARRAY_INFO, 0) == -EBUSY) { printk(KERN_WARNING "md: Ignoring md=%d, already autodetected. (Use raid=noautodetect)\n", minor); sys_close(fd); continue; } if (md_setup_args[ent].level != LEVEL_NONE) { /* non-persistent */ mdu_array_info_t ainfo; ainfo.level = md_setup_args[ent].level; ainfo.size = 0; ainfo.nr_disks =0; ainfo.raid_disks =0; while (devices[ainfo.raid_disks]) ainfo.raid_disks++; ainfo.md_minor =minor; ainfo.not_persistent = 1; ainfo.state = (1 << MD_SB_CLEAN); ainfo.layout = 0; ainfo.chunk_size = md_setup_args[ent].chunk; err = sys_ioctl(fd, SET_ARRAY_INFO, (long)&ainfo); for (i = 0; !err && i <= MD_SB_DISKS; i++) { dev = devices[i]; if (!dev) break; dinfo.number = i; dinfo.raid_disk = i; dinfo.state = (1<= 0) { sys_ioctl(fd, RAID_AUTORUN, raid_autopart); sys_close(fd); } } void __init md_run_setup(void) { create_dev("/dev/md0", MKDEV(MD_MAJOR, 0)); if (raid_noautodetect) printk(KERN_INFO "md: Skipping autodetection of RAID arrays. (raid=autodetect will force)\n"); else autodetect_raid(); md_setup_drive(); }