aboutsummaryrefslogtreecommitdiffstats
blob: 84e27708ad973460bf8d644f26eb368c5c998238 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
/*
 * Copyright (C) 2001-2002 Sistina Software (UK) Limited.
 * Copyright (C) 2008 Red Hat, Inc. All rights reserved.
 *
 * Device-mapper snapshot exception store.
 *
 * This file is released under the GPL.
 */

#ifndef _LINUX_DM_EXCEPTION_STORE
#define _LINUX_DM_EXCEPTION_STORE

#include <linux/blkdev.h>
#include <linux/device-mapper.h>

/*
 * The snapshot code deals with largish chunks of the disk at a
 * time. Typically 32k - 512k.
 */
typedef sector_t chunk_t;

/*
 * An exception is used where an old chunk of data has been
 * replaced by a new one.
 * If chunk_t is 64 bits in size, the top 8 bits of new_chunk hold the number
 * of chunks that follow contiguously.  Remaining bits hold the number of the
 * chunk within the device.
 */
struct dm_exception {
	struct list_head hash_list;

	chunk_t old_chunk;
	chunk_t new_chunk;
};

/*
 * Abstraction to handle the meta/layout of exception stores (the
 * COW device).
 */
struct dm_exception_store;
struct dm_exception_store_type {
	const char *name;
	struct module *module;

	int (*ctr) (struct dm_exception_store *store,
		    unsigned argc, char **argv);

	/*
	 * Destroys this object when you've finished with it.
	 */
	void (*dtr) (struct dm_exception_store *store);

	/*
	 * The target shouldn't read the COW device until this is
	 * called.  As exceptions are read from the COW, they are
	 * reported back via the callback.
	 */
	int (*read_metadata) (struct dm_exception_store *store,
			      int (*callback)(void *callback_context,
					      chunk_t old, chunk_t new),
			      void *callback_context);

	/*
	 * Find somewhere to store the next exception.
	 */
	int (*prepare_exception) (struct dm_exception_store *store,
				  struct dm_exception *e);

	/*
	 * Update the metadata with this exception.
	 */
	void (*commit_exception) (struct dm_exception_store *store,
				  struct dm_exception *e, int valid,
				  void (*callback) (void *, int success),
				  void *callback_context);

	/*
	 * Returns 0 if the exception store is empty.
	 *
	 * If there are exceptions still to be merged, sets
	 * *last_old_chunk and *last_new_chunk to the most recent
	 * still-to-be-merged chunk and returns the number of
	 * consecutive previous ones.
	 */
	int (*prepare_merge) (struct dm_exception_store *store,
			      chunk_t *last_old_chunk, chunk_t *last_new_chunk);

	/*
	 * Clear the last n exceptions.
	 * nr_merged must be <= the value returned by prepare_merge.
	 */
	int (*commit_merge) (struct dm_exception_store *store, int nr_merged);

	/*
	 * The snapshot is invalid, note this in the metadata.
	 */
	void (*drop_snapshot) (struct dm_exception_store *store);

	unsigned (*status) (struct dm_exception_store *store,
			    status_type_t status, char *result,
			    unsigned maxlen);

	/*
	 * Return how full the snapshot is.
	 */
	void (*usage) (struct dm_exception_store *store,
		       sector_t *total_sectors, sector_t *sectors_allocated,
		       sector_t *metadata_sectors);

	/* For internal device-mapper use only. */
	struct list_head list;
};

struct dm_snapshot;

struct dm_exception_store {
	struct dm_exception_store_type *type;
	struct dm_snapshot *snap;

	/* Size of data blocks saved - must be a power of 2 */
	unsigned chunk_size;
	unsigned chunk_mask;
	unsigned chunk_shift;

	void *context;
};

/*
 * Obtain the origin or cow device used by a given snapshot.
 */
struct dm_dev *dm_snap_origin(struct dm_snapshot *snap);
struct dm_dev *dm_snap_cow(struct dm_snapshot *snap);

/*
 * Funtions to manipulate consecutive chunks
 */
#  if defined(CONFIG_LBDAF) || (BITS_PER_LONG == 64)
#    define DM_CHUNK_CONSECUTIVE_BITS 8
#    define DM_CHUNK_NUMBER_BITS 56

static inline chunk_t dm_chunk_number(chunk_t chunk)
{
	return chunk & (chunk_t)((1ULL << DM_CHUNK_NUMBER_BITS) - 1ULL);
}

static inline unsigned dm_consecutive_chunk_count(struct dm_exception *e)
{
	return e->new_chunk >> DM_CHUNK_NUMBER_BITS;
}

static inline void dm_consecutive_chunk_count_inc(struct dm_exception *e)
{
	e->new_chunk += (1ULL << DM_CHUNK_NUMBER_BITS);

	BUG_ON(!dm_consecutive_chunk_count(e));
}

static inline void dm_consecutive_chunk_count_dec(struct dm_exception *e)
{
	BUG_ON(!dm_consecutive_chunk_count(e));

	e->new_chunk -= (1ULL << DM_CHUNK_NUMBER_BITS);
}

#  else
#    define DM_CHUNK_CONSECUTIVE_BITS 0

static inline chunk_t dm_chunk_number(chunk_t chunk)
{
	return chunk;
}

static inline unsigned dm_consecutive_chunk_count(struct dm_exception *e)
{
	return 0;
}

static inline void dm_consecutive_chunk_count_inc(struct dm_exception *e)
{
}

static inline void dm_consecutive_chunk_count_dec(struct dm_exception *e)
{
}

#  endif

/*
 * Return the number of sectors in the device.
 */
static inline sector_t get_dev_size(struct block_device *bdev)
{
	return i_size_read(bdev->bd_inode) >> SECTOR_SHIFT;
}

static inline chunk_t sector_to_chunk(struct dm_exception_store *store,
				      sector_t sector)
{
	return sector >> store->chunk_shift;
}

int dm_exception_store_type_register(struct dm_exception_store_type *type);
int dm_exception_store_type_unregister(struct dm_exception_store_type *type);

int dm_exception_store_set_chunk_size(struct dm_exception_store *store,
				      unsigned chunk_size,
				      char **error);

int dm_exception_store_create(struct dm_target *ti, int argc, char **argv,
			      struct dm_snapshot *snap,
			      unsigned *args_used,
			      struct dm_exception_store **store);
void dm_exception_store_destroy(struct dm_exception_store *store);

int dm_exception_store_init(void);
void dm_exception_store_exit(void);

/*
 * Two exception store implementations.
 */
int dm_persistent_snapshot_init(void);
void dm_persistent_snapshot_exit(void);

int dm_transient_snapshot_init(void);
void dm_transient_snapshot_exit(void);

#endif /* _LINUX_DM_EXCEPTION_STORE */