1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
424
425
426
427
428
429
430
431
432
433
434
435
436
437
438
439
440
441
442
443
444
445
446
447
448
449
450
451
452
453
454
455
456
457
458
459
460
461
462
463
464
465
466
467
468
469
470
471
472
473
474
475
476
477
478
479
480
481
482
483
484
485
486
487
488
489
490
491
492
493
494
495
496
497
498
499
500
501
502
503
504
505
506
507
508
509
510
511
512
513
514
515
516
517
518
519
520
521
522
523
524
525
526
527
528
529
530
531
532
533
534
535
536
537
538
539
540
541
542
543
544
545
546
547
548
549
550
551
552
553
554
555
556
557
558
559
560
561
562
563
564
565
566
567
568
569
570
571
572
573
574
575
576
577
578
579
580
581
582
583
584
585
586
587
588
589
590
591
592
593
594
595
596
597
598
599
600
601
602
603
604
605
606
607
608
609
610
611
612
613
614
615
616
617
618
619
620
621
622
623
624
625
626
627
628
629
630
631
632
633
634
635
636
637
638
639
640
641
642
643
644
645
646
647
648
649
650
651
652
653
654
655
656
657
658
659
660
661
662
663
664
665
666
667
668
669
670
671
672
673
674
675
676
677
678
679
680
681
682
683
684
685
686
687
688
689
690
691
692
693
694
695
696
697
698
699
700
701
702
703
704
705
706
707
708
709
710
711
712
713
714
715
716
717
718
719
720
721
722
723
724
725
726
727
728
729
730
731
732
733
734
735
736
737
738
739
740
741
742
743
744
745
746
747
748
749
750
751
752
753
754
755
756
757
758
759
760
761
762
763
764
765
766
767
768
769
770
771
772
773
774
775
776
777
778
779
780
781
782
783
784
785
786
787
788
789
790
791
792
793
794
795
796
797
798
799
800
801
802
803
804
|
/*
* drivers/pci/pcie/aer/aerdrv_core.c
*
* This file is subject to the terms and conditions of the GNU General Public
* License. See the file "COPYING" in the main directory of this archive
* for more details.
*
* This file implements the core part of PCI-Express AER. When an pci-express
* error is delivered, an error message will be collected and printed to
* console, then, an error recovery procedure will be executed by following
* the pci error recovery rules.
*
* Copyright (C) 2006 Intel Corp.
* Tom Long Nguyen (tom.l.nguyen@intel.com)
* Zhang Yanmin (yanmin.zhang@intel.com)
*
*/
#include <linux/module.h>
#include <linux/pci.h>
#include <linux/kernel.h>
#include <linux/errno.h>
#include <linux/pm.h>
#include <linux/suspend.h>
#include <linux/delay.h>
#include <linux/slab.h>
#include <linux/kfifo.h>
#include "aerdrv.h"
static bool forceload;
static bool nosourceid;
module_param(forceload, bool, 0);
module_param(nosourceid, bool, 0);
#define PCI_EXP_AER_FLAGS (PCI_EXP_DEVCTL_CERE | PCI_EXP_DEVCTL_NFERE | \
PCI_EXP_DEVCTL_FERE | PCI_EXP_DEVCTL_URRE)
int pci_enable_pcie_error_reporting(struct pci_dev *dev)
{
if (pcie_aer_get_firmware_first(dev))
return -EIO;
if (!pci_find_ext_capability(dev, PCI_EXT_CAP_ID_ERR))
return -EIO;
return pcie_capability_set_word(dev, PCI_EXP_DEVCTL, PCI_EXP_AER_FLAGS);
}
EXPORT_SYMBOL_GPL(pci_enable_pcie_error_reporting);
int pci_disable_pcie_error_reporting(struct pci_dev *dev)
{
if (pcie_aer_get_firmware_first(dev))
return -EIO;
return pcie_capability_clear_word(dev, PCI_EXP_DEVCTL,
PCI_EXP_AER_FLAGS);
}
EXPORT_SYMBOL_GPL(pci_disable_pcie_error_reporting);
int pci_cleanup_aer_uncorrect_error_status(struct pci_dev *dev)
{
int pos;
u32 status;
pos = pci_find_ext_capability(dev, PCI_EXT_CAP_ID_ERR);
if (!pos)
return -EIO;
pci_read_config_dword(dev, pos + PCI_ERR_UNCOR_STATUS, &status);
if (status)
pci_write_config_dword(dev, pos + PCI_ERR_UNCOR_STATUS, status);
return 0;
}
EXPORT_SYMBOL_GPL(pci_cleanup_aer_uncorrect_error_status);
/**
* add_error_device - list device to be handled
* @e_info: pointer to error info
* @dev: pointer to pci_dev to be added
*/
static int add_error_device(struct aer_err_info *e_info, struct pci_dev *dev)
{
if (e_info->error_dev_num < AER_MAX_MULTI_ERR_DEVICES) {
e_info->dev[e_info->error_dev_num] = dev;
e_info->error_dev_num++;
return 0;
}
return -ENOSPC;
}
/**
* is_error_source - check whether the device is source of reported error
* @dev: pointer to pci_dev to be checked
* @e_info: pointer to reported error info
*/
static bool is_error_source(struct pci_dev *dev, struct aer_err_info *e_info)
{
int pos;
u32 status, mask;
u16 reg16;
/*
* When bus id is equal to 0, it might be a bad id
* reported by root port.
*/
if (!nosourceid && (PCI_BUS_NUM(e_info->id) != 0)) {
/* Device ID match? */
if (e_info->id == ((dev->bus->number << 8) | dev->devfn))
return true;
/* Continue id comparing if there is no multiple error */
if (!e_info->multi_error_valid)
return false;
}
/*
* When either
* 1) nosourceid==y;
* 2) bus id is equal to 0. Some ports might lose the bus
* id of error source id;
* 3) There are multiple errors and prior id comparing fails;
* We check AER status registers to find possible reporter.
*/
if (atomic_read(&dev->enable_cnt) == 0)
return false;
/* Check if AER is enabled */
pcie_capability_read_word(dev, PCI_EXP_DEVCTL, ®16);
if (!(reg16 & PCI_EXP_AER_FLAGS))
return false;
pos = pci_find_ext_capability(dev, PCI_EXT_CAP_ID_ERR);
if (!pos)
return false;
/* Check if error is recorded */
if (e_info->severity == AER_CORRECTABLE) {
pci_read_config_dword(dev, pos + PCI_ERR_COR_STATUS, &status);
pci_read_config_dword(dev, pos + PCI_ERR_COR_MASK, &mask);
} else {
pci_read_config_dword(dev, pos + PCI_ERR_UNCOR_STATUS, &status);
pci_read_config_dword(dev, pos + PCI_ERR_UNCOR_MASK, &mask);
}
if (status & ~mask)
return true;
return false;
}
static int find_device_iter(struct pci_dev *dev, void *data)
{
struct aer_err_info *e_info = (struct aer_err_info *)data;
if (is_error_source(dev, e_info)) {
/* List this device */
if (add_error_device(e_info, dev)) {
/* We cannot handle more... Stop iteration */
/* TODO: Should print error message here? */
return 1;
}
/* If there is only a single error, stop iteration */
if (!e_info->multi_error_valid)
return 1;
}
return 0;
}
/**
* find_source_device - search through device hierarchy for source device
* @parent: pointer to Root Port pci_dev data structure
* @e_info: including detailed error information such like id
*
* Return true if found.
*
* Invoked by DPC when error is detected at the Root Port.
* Caller of this function must set id, severity, and multi_error_valid of
* struct aer_err_info pointed by @e_info properly. This function must fill
* e_info->error_dev_num and e_info->dev[], based on the given information.
*/
static bool find_source_device(struct pci_dev *parent,
struct aer_err_info *e_info)
{
struct pci_dev *dev = parent;
int result;
/* Must reset in this function */
e_info->error_dev_num = 0;
/* Is Root Port an agent that sends error message? */
result = find_device_iter(dev, e_info);
if (result)
return true;
pci_walk_bus(parent->subordinate, find_device_iter, e_info);
if (!e_info->error_dev_num) {
dev_printk(KERN_DEBUG, &parent->dev,
"can't find device of ID%04x\n",
e_info->id);
return false;
}
return true;
}
static int report_error_detected(struct pci_dev *dev, void *data)
{
pci_ers_result_t vote;
const struct pci_error_handlers *err_handler;
struct aer_broadcast_data *result_data;
result_data = (struct aer_broadcast_data *) data;
device_lock(&dev->dev);
dev->error_state = result_data->state;
if (!dev->driver ||
!dev->driver->err_handler ||
!dev->driver->err_handler->error_detected) {
if (result_data->state == pci_channel_io_frozen &&
!(dev->hdr_type & PCI_HEADER_TYPE_BRIDGE)) {
/*
* In case of fatal recovery, if one of down-
* stream device has no driver. We might be
* unable to recover because a later insmod
* of a driver for this device is unaware of
* its hw state.
*/
dev_printk(KERN_DEBUG, &dev->dev, "device has %s\n",
dev->driver ?
"no AER-aware driver" : "no driver");
}
/*
* If there's any device in the subtree that does not
* have an error_detected callback, returning
* PCI_ERS_RESULT_NO_AER_DRIVER prevents calling of
* the subsequent mmio_enabled/slot_reset/resume
* callbacks of "any" device in the subtree. All the
* devices in the subtree are left in the error state
* without recovery.
*/
if (!(dev->hdr_type & PCI_HEADER_TYPE_BRIDGE))
vote = PCI_ERS_RESULT_NO_AER_DRIVER;
else
vote = PCI_ERS_RESULT_NONE;
} else {
err_handler = dev->driver->err_handler;
vote = err_handler->error_detected(dev, result_data->state);
}
result_data->result = merge_result(result_data->result, vote);
device_unlock(&dev->dev);
return 0;
}
static int report_mmio_enabled(struct pci_dev *dev, void *data)
{
pci_ers_result_t vote;
const struct pci_error_handlers *err_handler;
struct aer_broadcast_data *result_data;
result_data = (struct aer_broadcast_data *) data;
device_lock(&dev->dev);
if (!dev->driver ||
!dev->driver->err_handler ||
!dev->driver->err_handler->mmio_enabled)
goto out;
err_handler = dev->driver->err_handler;
vote = err_handler->mmio_enabled(dev);
result_data->result = merge_result(result_data->result, vote);
out:
device_unlock(&dev->dev);
return 0;
}
static int report_slot_reset(struct pci_dev *dev, void *data)
{
pci_ers_result_t vote;
const struct pci_error_handlers *err_handler;
struct aer_broadcast_data *result_data;
result_data = (struct aer_broadcast_data *) data;
device_lock(&dev->dev);
if (!dev->driver ||
!dev->driver->err_handler ||
!dev->driver->err_handler->slot_reset)
goto out;
err_handler = dev->driver->err_handler;
vote = err_handler->slot_reset(dev);
result_data->result = merge_result(result_data->result, vote);
out:
device_unlock(&dev->dev);
return 0;
}
static int report_resume(struct pci_dev *dev, void *data)
{
const struct pci_error_handlers *err_handler;
device_lock(&dev->dev);
dev->error_state = pci_channel_io_normal;
if (!dev->driver ||
!dev->driver->err_handler ||
!dev->driver->err_handler->resume)
goto out;
err_handler = dev->driver->err_handler;
err_handler->resume(dev);
out:
device_unlock(&dev->dev);
return 0;
}
/**
* broadcast_error_message - handle message broadcast to downstream drivers
* @dev: pointer to from where in a hierarchy message is broadcasted down
* @state: error state
* @error_mesg: message to print
* @cb: callback to be broadcasted
*
* Invoked during error recovery process. Once being invoked, the content
* of error severity will be broadcasted to all downstream drivers in a
* hierarchy in question.
*/
static pci_ers_result_t broadcast_error_message(struct pci_dev *dev,
enum pci_channel_state state,
char *error_mesg,
int (*cb)(struct pci_dev *, void *))
{
struct aer_broadcast_data result_data;
dev_printk(KERN_DEBUG, &dev->dev, "broadcast %s message\n", error_mesg);
result_data.state = state;
if (cb == report_error_detected)
result_data.result = PCI_ERS_RESULT_CAN_RECOVER;
else
result_data.result = PCI_ERS_RESULT_RECOVERED;
if (dev->hdr_type & PCI_HEADER_TYPE_BRIDGE) {
/*
* If the error is reported by a bridge, we think this error
* is related to the downstream link of the bridge, so we
* do error recovery on all subordinates of the bridge instead
* of the bridge and clear the error status of the bridge.
*/
if (cb == report_error_detected)
dev->error_state = state;
pci_walk_bus(dev->subordinate, cb, &result_data);
if (cb == report_resume) {
pci_cleanup_aer_uncorrect_error_status(dev);
dev->error_state = pci_channel_io_normal;
}
} else {
/*
* If the error is reported by an end point, we think this
* error is related to the upstream link of the end point.
*/
pci_walk_bus(dev->bus, cb, &result_data);
}
return result_data.result;
}
/**
* default_reset_link - default reset function
* @dev: pointer to pci_dev data structure
*
* Invoked when performing link reset on a Downstream Port or a
* Root Port with no aer driver.
*/
static pci_ers_result_t default_reset_link(struct pci_dev *dev)
{
pci_reset_bridge_secondary_bus(dev);
dev_printk(KERN_DEBUG, &dev->dev, "downstream link has been reset\n");
return PCI_ERS_RESULT_RECOVERED;
}
static int find_aer_service_iter(struct device *device, void *data)
{
struct pcie_port_service_driver *service_driver, **drv;
drv = (struct pcie_port_service_driver **) data;
if (device->bus == &pcie_port_bus_type && device->driver) {
service_driver = to_service_driver(device->driver);
if (service_driver->service == PCIE_PORT_SERVICE_AER) {
*drv = service_driver;
return 1;
}
}
return 0;
}
static struct pcie_port_service_driver *find_aer_service(struct pci_dev *dev)
{
struct pcie_port_service_driver *drv = NULL;
device_for_each_child(&dev->dev, &drv, find_aer_service_iter);
return drv;
}
static pci_ers_result_t reset_link(struct pci_dev *dev)
{
struct pci_dev *udev;
pci_ers_result_t status;
struct pcie_port_service_driver *driver;
if (dev->hdr_type & PCI_HEADER_TYPE_BRIDGE) {
/* Reset this port for all subordinates */
udev = dev;
} else {
/* Reset the upstream component (likely downstream port) */
udev = dev->bus->self;
}
/* Use the aer driver of the component firstly */
driver = find_aer_service(udev);
if (driver && driver->reset_link) {
status = driver->reset_link(udev);
} else if (pci_pcie_type(udev) == PCI_EXP_TYPE_DOWNSTREAM ||
pci_pcie_type(udev) == PCI_EXP_TYPE_ROOT_PORT) {
status = default_reset_link(udev);
} else {
dev_printk(KERN_DEBUG, &dev->dev,
"no link-reset support at upstream device %s\n",
pci_name(udev));
return PCI_ERS_RESULT_DISCONNECT;
}
if (status != PCI_ERS_RESULT_RECOVERED) {
dev_printk(KERN_DEBUG, &dev->dev,
"link reset at upstream device %s failed\n",
pci_name(udev));
return PCI_ERS_RESULT_DISCONNECT;
}
return status;
}
/**
* do_recovery - handle nonfatal/fatal error recovery process
* @dev: pointer to a pci_dev data structure of agent detecting an error
* @severity: error severity type
*
* Invoked when an error is nonfatal/fatal. Once being invoked, broadcast
* error detected message to all downstream drivers within a hierarchy in
* question and return the returned code.
*/
static void do_recovery(struct pci_dev *dev, int severity)
{
pci_ers_result_t status, result = PCI_ERS_RESULT_RECOVERED;
enum pci_channel_state state;
if (severity == AER_FATAL)
state = pci_channel_io_frozen;
else
state = pci_channel_io_normal;
status = broadcast_error_message(dev,
state,
"error_detected",
report_error_detected);
if (severity == AER_FATAL) {
result = reset_link(dev);
if (result != PCI_ERS_RESULT_RECOVERED)
goto failed;
}
if (status == PCI_ERS_RESULT_CAN_RECOVER)
status = broadcast_error_message(dev,
state,
"mmio_enabled",
report_mmio_enabled);
if (status == PCI_ERS_RESULT_NEED_RESET) {
/*
* TODO: Should call platform-specific
* functions to reset slot before calling
* drivers' slot_reset callbacks?
*/
status = broadcast_error_message(dev,
state,
"slot_reset",
report_slot_reset);
}
if (status != PCI_ERS_RESULT_RECOVERED)
goto failed;
broadcast_error_message(dev,
state,
"resume",
report_resume);
dev_info(&dev->dev, "AER: Device recovery successful\n");
return;
failed:
/* TODO: Should kernel panic here? */
dev_info(&dev->dev, "AER: Device recovery failed\n");
}
/**
* handle_error_source - handle logging error into an event log
* @aerdev: pointer to pcie_device data structure of the root port
* @dev: pointer to pci_dev data structure of error source device
* @info: comprehensive error information
*
* Invoked when an error being detected by Root Port.
*/
static void handle_error_source(struct pcie_device *aerdev,
struct pci_dev *dev,
struct aer_err_info *info)
{
int pos;
if (info->severity == AER_CORRECTABLE) {
/*
* Correctable error does not need software intervention.
* No need to go through error recovery process.
*/
pos = pci_find_ext_capability(dev, PCI_EXT_CAP_ID_ERR);
if (pos)
pci_write_config_dword(dev, pos + PCI_ERR_COR_STATUS,
info->status);
} else
do_recovery(dev, info->severity);
}
#ifdef CONFIG_ACPI_APEI_PCIEAER
static void aer_recover_work_func(struct work_struct *work);
#define AER_RECOVER_RING_ORDER 4
#define AER_RECOVER_RING_SIZE (1 << AER_RECOVER_RING_ORDER)
struct aer_recover_entry
{
u8 bus;
u8 devfn;
u16 domain;
int severity;
struct aer_capability_regs *regs;
};
static DEFINE_KFIFO(aer_recover_ring, struct aer_recover_entry,
AER_RECOVER_RING_SIZE);
/*
* Mutual exclusion for writers of aer_recover_ring, reader side don't
* need lock, because there is only one reader and lock is not needed
* between reader and writer.
*/
static DEFINE_SPINLOCK(aer_recover_ring_lock);
static DECLARE_WORK(aer_recover_work, aer_recover_work_func);
void aer_recover_queue(int domain, unsigned int bus, unsigned int devfn,
int severity, struct aer_capability_regs *aer_regs)
{
unsigned long flags;
struct aer_recover_entry entry = {
.bus = bus,
.devfn = devfn,
.domain = domain,
.severity = severity,
.regs = aer_regs,
};
spin_lock_irqsave(&aer_recover_ring_lock, flags);
if (kfifo_put(&aer_recover_ring, entry))
schedule_work(&aer_recover_work);
else
pr_err("AER recover: Buffer overflow when recovering AER for %04x:%02x:%02x:%x\n",
domain, bus, PCI_SLOT(devfn), PCI_FUNC(devfn));
spin_unlock_irqrestore(&aer_recover_ring_lock, flags);
}
EXPORT_SYMBOL_GPL(aer_recover_queue);
static void aer_recover_work_func(struct work_struct *work)
{
struct aer_recover_entry entry;
struct pci_dev *pdev;
while (kfifo_get(&aer_recover_ring, &entry)) {
pdev = pci_get_domain_bus_and_slot(entry.domain, entry.bus,
entry.devfn);
if (!pdev) {
pr_err("AER recover: Can not find pci_dev for %04x:%02x:%02x:%x\n",
entry.domain, entry.bus,
PCI_SLOT(entry.devfn), PCI_FUNC(entry.devfn));
continue;
}
cper_print_aer(pdev, entry.severity, entry.regs);
do_recovery(pdev, entry.severity);
pci_dev_put(pdev);
}
}
#endif
/**
* get_device_error_info - read error status from dev and store it to info
* @dev: pointer to the device expected to have a error record
* @info: pointer to structure to store the error record
*
* Return 1 on success, 0 on error.
*
* Note that @info is reused among all error devices. Clear fields properly.
*/
static int get_device_error_info(struct pci_dev *dev, struct aer_err_info *info)
{
int pos, temp;
/* Must reset in this function */
info->status = 0;
info->tlp_header_valid = 0;
pos = pci_find_ext_capability(dev, PCI_EXT_CAP_ID_ERR);
/* The device might not support AER */
if (!pos)
return 1;
if (info->severity == AER_CORRECTABLE) {
pci_read_config_dword(dev, pos + PCI_ERR_COR_STATUS,
&info->status);
pci_read_config_dword(dev, pos + PCI_ERR_COR_MASK,
&info->mask);
if (!(info->status & ~info->mask))
return 0;
} else if (dev->hdr_type & PCI_HEADER_TYPE_BRIDGE ||
info->severity == AER_NONFATAL) {
/* Link is still healthy for IO reads */
pci_read_config_dword(dev, pos + PCI_ERR_UNCOR_STATUS,
&info->status);
pci_read_config_dword(dev, pos + PCI_ERR_UNCOR_MASK,
&info->mask);
if (!(info->status & ~info->mask))
return 0;
/* Get First Error Pointer */
pci_read_config_dword(dev, pos + PCI_ERR_CAP, &temp);
info->first_error = PCI_ERR_CAP_FEP(temp);
if (info->status & AER_LOG_TLP_MASKS) {
info->tlp_header_valid = 1;
pci_read_config_dword(dev,
pos + PCI_ERR_HEADER_LOG, &info->tlp.dw0);
pci_read_config_dword(dev,
pos + PCI_ERR_HEADER_LOG + 4, &info->tlp.dw1);
pci_read_config_dword(dev,
pos + PCI_ERR_HEADER_LOG + 8, &info->tlp.dw2);
pci_read_config_dword(dev,
pos + PCI_ERR_HEADER_LOG + 12, &info->tlp.dw3);
}
}
return 1;
}
static inline void aer_process_err_devices(struct pcie_device *p_device,
struct aer_err_info *e_info)
{
int i;
/* Report all before handle them, not to lost records by reset etc. */
for (i = 0; i < e_info->error_dev_num && e_info->dev[i]; i++) {
if (get_device_error_info(e_info->dev[i], e_info))
aer_print_error(e_info->dev[i], e_info);
}
for (i = 0; i < e_info->error_dev_num && e_info->dev[i]; i++) {
if (get_device_error_info(e_info->dev[i], e_info))
handle_error_source(p_device, e_info->dev[i], e_info);
}
}
/**
* aer_isr_one_error - consume an error detected by root port
* @p_device: pointer to error root port service device
* @e_src: pointer to an error source
*/
static void aer_isr_one_error(struct pcie_device *p_device,
struct aer_err_source *e_src)
{
struct aer_err_info *e_info;
/* struct aer_err_info might be big, so we allocate it with slab */
e_info = kmalloc(sizeof(struct aer_err_info), GFP_KERNEL);
if (!e_info) {
dev_printk(KERN_DEBUG, &p_device->port->dev,
"Can't allocate mem when processing AER errors\n");
return;
}
/*
* There is a possibility that both correctable error and
* uncorrectable error being logged. Report correctable error first.
*/
if (e_src->status & PCI_ERR_ROOT_COR_RCV) {
e_info->id = ERR_COR_ID(e_src->id);
e_info->severity = AER_CORRECTABLE;
if (e_src->status & PCI_ERR_ROOT_MULTI_COR_RCV)
e_info->multi_error_valid = 1;
else
e_info->multi_error_valid = 0;
aer_print_port_info(p_device->port, e_info);
if (find_source_device(p_device->port, e_info))
aer_process_err_devices(p_device, e_info);
}
if (e_src->status & PCI_ERR_ROOT_UNCOR_RCV) {
e_info->id = ERR_UNCOR_ID(e_src->id);
if (e_src->status & PCI_ERR_ROOT_FATAL_RCV)
e_info->severity = AER_FATAL;
else
e_info->severity = AER_NONFATAL;
if (e_src->status & PCI_ERR_ROOT_MULTI_UNCOR_RCV)
e_info->multi_error_valid = 1;
else
e_info->multi_error_valid = 0;
aer_print_port_info(p_device->port, e_info);
if (find_source_device(p_device->port, e_info))
aer_process_err_devices(p_device, e_info);
}
kfree(e_info);
}
/**
* get_e_source - retrieve an error source
* @rpc: pointer to the root port which holds an error
* @e_src: pointer to store retrieved error source
*
* Return 1 if an error source is retrieved, otherwise 0.
*
* Invoked by DPC handler to consume an error.
*/
static int get_e_source(struct aer_rpc *rpc, struct aer_err_source *e_src)
{
unsigned long flags;
/* Lock access to Root error producer/consumer index */
spin_lock_irqsave(&rpc->e_lock, flags);
if (rpc->prod_idx == rpc->cons_idx) {
spin_unlock_irqrestore(&rpc->e_lock, flags);
return 0;
}
*e_src = rpc->e_sources[rpc->cons_idx];
rpc->cons_idx++;
if (rpc->cons_idx == AER_ERROR_SOURCES_MAX)
rpc->cons_idx = 0;
spin_unlock_irqrestore(&rpc->e_lock, flags);
return 1;
}
/**
* aer_isr - consume errors detected by root port
* @work: definition of this work item
*
* Invoked, as DPC, when root port records new detected error
*/
void aer_isr(struct work_struct *work)
{
struct aer_rpc *rpc = container_of(work, struct aer_rpc, dpc_handler);
struct pcie_device *p_device = rpc->rpd;
struct aer_err_source uninitialized_var(e_src);
mutex_lock(&rpc->rpc_mutex);
while (get_e_source(rpc, &e_src))
aer_isr_one_error(p_device, &e_src);
mutex_unlock(&rpc->rpc_mutex);
}
/**
* aer_init - provide AER initialization
* @dev: pointer to AER pcie device
*
* Invoked when AER service driver is loaded.
*/
int aer_init(struct pcie_device *dev)
{
if (forceload) {
dev_printk(KERN_DEBUG, &dev->device,
"aerdrv forceload requested.\n");
pcie_aer_force_firmware_first(dev->port, 0);
}
return 0;
}
|