1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
|
/*
* include/linux/ion.h
*
* Copyright (C) 2011 Google, Inc.
*
* This software is licensed under the terms of the GNU General Public
* License version 2, as published by the Free Software Foundation, and
* may be copied, distributed, and modified under those terms.
*
* This program is distributed in the hope that it will be useful,
* but WITHOUT ANY WARRANTY; without even the implied warranty of
* MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
* GNU General Public License for more details.
*
*/
#ifndef _LINUX_ION_H
#define _LINUX_ION_H
#include <linux/types.h>
struct ion_handle;
/**
* enum ion_heap_types - list of all possible types of heaps
* @ION_HEAP_TYPE_SYSTEM: memory allocated via vmalloc
* @ION_HEAP_TYPE_SYSTEM_CONTIG: memory allocated via kmalloc
* @ION_HEAP_TYPE_CARVEOUT: memory allocated from a prereserved
* carveout heap, allocations are physically
* contiguous
* @ION_NUM_HEAPS: helper for iterating over heaps, a bit mask
* is used to identify the heaps, so only 32
* total heap types are supported
*/
enum ion_heap_type {
ION_HEAP_TYPE_SYSTEM,
ION_HEAP_TYPE_SYSTEM_CONTIG,
ION_HEAP_TYPE_CARVEOUT,
ION_HEAP_TYPE_CHUNK,
ION_HEAP_TYPE_CUSTOM, /* must be last so device specific heaps always
are at the end of this enum */
ION_NUM_HEAPS = 16,
};
#define ION_HEAP_SYSTEM_MASK (1 << ION_HEAP_TYPE_SYSTEM)
#define ION_HEAP_SYSTEM_CONTIG_MASK (1 << ION_HEAP_TYPE_SYSTEM_CONTIG)
#define ION_HEAP_CARVEOUT_MASK (1 << ION_HEAP_TYPE_CARVEOUT)
#define ION_NUM_HEAP_IDS sizeof(unsigned int) * 8
/**
* heap flags - the lower 16 bits are used by core ion, the upper 16
* bits are reserved for use by the heaps themselves.
*/
#define ION_FLAG_CACHED 1 /* mappings of this buffer should be
cached, ion will do cache
maintenance when the buffer is
mapped for dma */
#define ION_FLAG_CACHED_NEEDS_SYNC 2 /* mappings of this buffer will created
at mmap time, if this is set
caches must be managed manually */
#ifdef __KERNEL__
struct ion_device;
struct ion_heap;
struct ion_mapper;
struct ion_client;
struct ion_buffer;
/* This should be removed some day when phys_addr_t's are fully
plumbed in the kernel, and all instances of ion_phys_addr_t should
be converted to phys_addr_t. For the time being many kernel interfaces
do not accept phys_addr_t's that would have to */
#define ion_phys_addr_t unsigned long
/**
* struct ion_platform_heap - defines a heap in the given platform
* @type: type of the heap from ion_heap_type enum
* @id: unique identifier for heap. When allocating higher numbers
* will be allocated from first. At allocation these are passed
* as a bit mask and therefore can not exceed ION_NUM_HEAP_IDS.
* @name: used for debug purposes
* @base: base address of heap in physical memory if applicable
* @size: size of the heap in bytes if applicable
* @align: required alignment in physical memory if applicable
* @priv: private info passed from the board file
*
* Provided by the board file.
*/
struct ion_platform_heap {
enum ion_heap_type type;
unsigned int id;
const char *name;
ion_phys_addr_t base;
size_t size;
ion_phys_addr_t align;
void *priv;
};
/**
* struct ion_platform_data - array of platform heaps passed from board file
* @nr: number of structures in the array
* @heaps: array of platform_heap structions
*
* Provided by the board file in the form of platform data to a platform device.
*/
struct ion_platform_data {
int nr;
struct ion_platform_heap heaps[];
};
/**
* ion_reserve() - reserve memory for ion heaps if applicable
* @data: platform data specifying starting physical address and
* size
*
* Calls memblock reserve to set aside memory for heaps that are
* located at specific memory addresses or of specfic sizes not
* managed by the kernel
*/
void ion_reserve(struct ion_platform_data *data);
/**
* ion_client_create() - allocate a client and returns it
* @dev: the global ion device
* @heap_type_mask: mask of heaps this client can allocate from
* @name: used for debugging
*/
struct ion_client *ion_client_create(struct ion_device *dev,
const char *name);
/**
* ion_client_destroy() - free's a client and all it's handles
* @client: the client
*
* Free the provided client and all it's resources including
* any handles it is holding.
*/
void ion_client_destroy(struct ion_client *client);
/**
* ion_alloc - allocate ion memory
* @client: the client
* @len: size of the allocation
* @align: requested allocation alignment, lots of hardware blocks
* have alignment requirements of some kind
* @heap_id_mask: mask of heaps to allocate from, if multiple bits are set
* heaps will be tried in order from highest to lowest
* id
* @flags: heap flags, the low 16 bits are consumed by ion, the
* high 16 bits are passed on to the respective heap and
* can be heap custom
*
* Allocate memory in one of the heaps provided in heap mask and return
* an opaque handle to it.
*/
struct ion_handle *ion_alloc(struct ion_client *client, size_t len,
size_t align, unsigned int heap_id_mask,
unsigned int flags);
/**
* ion_free - free a handle
* @client: the client
* @handle: the handle to free
*
* Free the provided handle.
*/
void ion_free(struct ion_client *client, struct ion_handle *handle);
/**
* ion_phys - returns the physical address and len of a handle
* @client: the client
* @handle: the handle
* @addr: a pointer to put the address in
* @len: a pointer to put the length in
*
* This function queries the heap for a particular handle to get the
* handle's physical address. It't output is only correct if
* a heap returns physically contiguous memory -- in other cases
* this api should not be implemented -- ion_sg_table should be used
* instead. Returns -EINVAL if the handle is invalid. This has
* no implications on the reference counting of the handle --
* the returned value may not be valid if the caller is not
* holding a reference.
*/
int ion_phys(struct ion_client *client, struct ion_handle *handle,
ion_phys_addr_t *addr, size_t *len);
/**
* ion_map_dma - return an sg_table describing a handle
* @client: the client
* @handle: the handle
*
* This function returns the sg_table describing
* a particular ion handle.
*/
struct sg_table *ion_sg_table(struct ion_client *client,
struct ion_handle *handle);
/**
* ion_map_kernel - create mapping for the given handle
* @client: the client
* @handle: handle to map
*
* Map the given handle into the kernel and return a kernel address that
* can be used to access this address.
*/
void *ion_map_kernel(struct ion_client *client, struct ion_handle *handle);
/**
* ion_unmap_kernel() - destroy a kernel mapping for a handle
* @client: the client
* @handle: handle to unmap
*/
void ion_unmap_kernel(struct ion_client *client, struct ion_handle *handle);
/**
* ion_share_dma_buf() - given an ion client, create a dma-buf fd
* @client: the client
* @handle: the handle
*/
int ion_share_dma_buf(struct ion_client *client, struct ion_handle *handle);
/**
* ion_import_dma_buf() - given an dma-buf fd from the ion exporter get handle
* @client: the client
* @fd: the dma-buf fd
*
* Given an dma-buf fd that was allocated through ion via ion_share_dma_buf,
* import that fd and return a handle representing it. If a dma-buf from
* another exporter is passed in this function will return ERR_PTR(-EINVAL)
*/
struct ion_handle *ion_import_dma_buf(struct ion_client *client, int fd);
#endif /* __KERNEL__ */
/**
* DOC: Ion Userspace API
*
* create a client by opening /dev/ion
* most operations handled via following ioctls
*
*/
/**
* struct ion_allocation_data - metadata passed from userspace for allocations
* @len: size of the allocation
* @align: required alignment of the allocation
* @heap_id_mask: mask of heap ids to allocate from
* @flags: flags passed to heap
* @handle: pointer that will be populated with a cookie to use to
* refer to this allocation
*
* Provided by userspace as an argument to the ioctl
*/
struct ion_allocation_data {
size_t len;
size_t align;
unsigned int heap_id_mask;
unsigned int flags;
struct ion_handle *handle;
};
/**
* struct ion_fd_data - metadata passed to/from userspace for a handle/fd pair
* @handle: a handle
* @fd: a file descriptor representing that handle
*
* For ION_IOC_SHARE or ION_IOC_MAP userspace populates the handle field with
* the handle returned from ion alloc, and the kernel returns the file
* descriptor to share or map in the fd field. For ION_IOC_IMPORT, userspace
* provides the file descriptor and the kernel returns the handle.
*/
struct ion_fd_data {
struct ion_handle *handle;
int fd;
};
/**
* struct ion_handle_data - a handle passed to/from the kernel
* @handle: a handle
*/
struct ion_handle_data {
struct ion_handle *handle;
};
/**
* struct ion_custom_data - metadata passed to/from userspace for a custom ioctl
* @cmd: the custom ioctl function to call
* @arg: additional data to pass to the custom ioctl, typically a user
* pointer to a predefined structure
*
* This works just like the regular cmd and arg fields of an ioctl.
*/
struct ion_custom_data {
unsigned int cmd;
unsigned long arg;
};
#define ION_IOC_MAGIC 'I'
/**
* DOC: ION_IOC_ALLOC - allocate memory
*
* Takes an ion_allocation_data struct and returns it with the handle field
* populated with the opaque handle for the allocation.
*/
#define ION_IOC_ALLOC _IOWR(ION_IOC_MAGIC, 0, \
struct ion_allocation_data)
/**
* DOC: ION_IOC_FREE - free memory
*
* Takes an ion_handle_data struct and frees the handle.
*/
#define ION_IOC_FREE _IOWR(ION_IOC_MAGIC, 1, struct ion_handle_data)
/**
* DOC: ION_IOC_MAP - get a file descriptor to mmap
*
* Takes an ion_fd_data struct with the handle field populated with a valid
* opaque handle. Returns the struct with the fd field set to a file
* descriptor open in the current address space. This file descriptor
* can then be used as an argument to mmap.
*/
#define ION_IOC_MAP _IOWR(ION_IOC_MAGIC, 2, struct ion_fd_data)
/**
* DOC: ION_IOC_SHARE - creates a file descriptor to use to share an allocation
*
* Takes an ion_fd_data struct with the handle field populated with a valid
* opaque handle. Returns the struct with the fd field set to a file
* descriptor open in the current address space. This file descriptor
* can then be passed to another process. The corresponding opaque handle can
* be retrieved via ION_IOC_IMPORT.
*/
#define ION_IOC_SHARE _IOWR(ION_IOC_MAGIC, 4, struct ion_fd_data)
/**
* DOC: ION_IOC_IMPORT - imports a shared file descriptor
*
* Takes an ion_fd_data struct with the fd field populated with a valid file
* descriptor obtained from ION_IOC_SHARE and returns the struct with the handle
* filed set to the corresponding opaque handle.
*/
#define ION_IOC_IMPORT _IOWR(ION_IOC_MAGIC, 5, struct ion_fd_data)
/**
* DOC: ION_IOC_SYNC - syncs a shared file descriptors to memory
*
* Deprecated in favor of using the dma_buf api's correctly (syncing
* will happend automatically when the buffer is mapped to a device).
* If necessary should be used after touching a cached buffer from the cpu,
* this will make the buffer in memory coherent.
*/
#define ION_IOC_SYNC _IOWR(ION_IOC_MAGIC, 7, struct ion_fd_data)
/**
* DOC: ION_IOC_CUSTOM - call architecture specific ion ioctl
*
* Takes the argument of the architecture specific ioctl to call and
* passes appropriate userdata for that ioctl
*/
#define ION_IOC_CUSTOM _IOWR(ION_IOC_MAGIC, 6, struct ion_custom_data)
#endif /* _LINUX_ION_H */
|