aboutsummaryrefslogtreecommitdiffstats
blob: e0cc0146ae622a0f48060ccefc53ada28e299c59 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
/*
 * lib/textsearch.c	Generic text search interface
 *
 *		This program is free software; you can redistribute it and/or
 *		modify it under the terms of the GNU General Public License
 *		as published by the Free Software Foundation; either version
 *		2 of the License, or (at your option) any later version.
 *
 * Authors:	Thomas Graf <tgraf@suug.ch>
 * 		Pablo Neira Ayuso <pablo@netfilter.org>
 *
 * ==========================================================================
 *
 * INTRODUCTION
 *
 *   The textsearch infrastructure provides text searching facilities for
 *   both linear and non-linear data. Individual search algorithms are
 *   implemented in modules and chosen by the user.
 *
 * ARCHITECTURE
 *
 *      User
 *     +----------------+
 *     |        finish()|<--------------(6)-----------------+
 *     |get_next_block()|<--------------(5)---------------+ |
 *     |                |                     Algorithm   | |
 *     |                |                    +------------------------------+
 *     |                |                    |  init()   find()   destroy() |
 *     |                |                    +------------------------------+
 *     |                |       Core API           ^       ^          ^
 *     |                |      +---------------+  (2)     (4)        (8)
 *     |             (1)|----->| prepare()     |---+       |          |
 *     |             (3)|----->| find()/next() |-----------+          |
 *     |             (7)|----->| destroy()     |----------------------+
 *     +----------------+      +---------------+
 *  
 *   (1) User configures a search by calling _prepare() specifying the
 *       search parameters such as the pattern and algorithm name.
 *   (2) Core requests the algorithm to allocate and initialize a search
 *       configuration according to the specified parameters.
 *   (3) User starts the search(es) by calling _find() or _next() to
 *       fetch subsequent occurrences. A state variable is provided
 *       to the algorithm to store persistent variables.
 *   (4) Core eventually resets the search offset and forwards the find()
 *       request to the algorithm.
 *   (5) Algorithm calls get_next_block() provided by the user continuously
 *       to fetch the data to be searched in block by block.
 *   (6) Algorithm invokes finish() after the last call to get_next_block
 *       to clean up any leftovers from get_next_block. (Optional)
 *   (7) User destroys the configuration by calling _destroy().
 *   (8) Core notifies the algorithm to destroy algorithm specific
 *       allocations. (Optional)
 *
 * USAGE
 *
 *   Before a search can be performed, a configuration must be created
 *   by calling textsearch_prepare() specifying the searching algorithm,
 *   the pattern to look for and flags. As a flag, you can set TS_IGNORECASE
 *   to perform case insensitive matching. But it might slow down
 *   performance of algorithm, so you should use it at own your risk.
 *   The returned configuration may then be used for an arbitrary
 *   amount of times and even in parallel as long as a separate struct
 *   ts_state variable is provided to every instance.
 *
 *   The actual search is performed by either calling textsearch_find_-
 *   continuous() for linear data or by providing an own get_next_block()
 *   implementation and calling textsearch_find(). Both functions return
 *   the position of the first occurrence of the pattern or UINT_MAX if
 *   no match was found. Subsequent occurrences can be found by calling
 *   textsearch_next() regardless of the linearity of the data.
 *
 *   Once you're done using a configuration it must be given back via
 *   textsearch_destroy.
 *
 * EXAMPLE
 *
 *   int pos;
 *   struct ts_config *conf;
 *   struct ts_state state;
 *   const char *pattern = "chicken";
 *   const char *example = "We dance the funky chicken";
 *
 *   conf = textsearch_prepare("kmp", pattern, strlen(pattern),
 *                             GFP_KERNEL, TS_AUTOLOAD);
 *   if (IS_ERR(conf)) {
 *       err = PTR_ERR(conf);
 *       goto errout;
 *   }
 *
 *   pos = textsearch_find_continuous(conf, &state, example, strlen(example));
 *   if (pos != UINT_MAX)
 *       panic("Oh my god, dancing chickens at %d\n", pos);
 *
 *   textsearch_destroy(conf);
 * ==========================================================================
 */

#include <linux/module.h>
#include <linux/types.h>
#include <linux/string.h>
#include <linux/init.h>
#include <linux/rculist.h>
#include <linux/rcupdate.h>
#include <linux/err.h>
#include <linux/textsearch.h>
#include <linux/slab.h>

static LIST_HEAD(ts_ops);
static DEFINE_SPINLOCK(ts_mod_lock);

static inline struct ts_ops *lookup_ts_algo(const char *name)
{
	struct ts_ops *o;

	rcu_read_lock();
	list_for_each_entry_rcu(o, &ts_ops, list) {
		if (!strcmp(name, o->name)) {
			if (!try_module_get(o->owner))
				o = NULL;
			rcu_read_unlock();
			return o;
		}
	}
	rcu_read_unlock();

	return NULL;
}

/**
 * textsearch_register - register a textsearch module
 * @ops: operations lookup table
 *
 * This function must be called by textsearch modules to announce
 * their presence. The specified &@ops must have %name set to a
 * unique identifier and the callbacks find(), init(), get_pattern(),
 * and get_pattern_len() must be implemented.
 *
 * Returns 0 or -EEXISTS if another module has already registered
 * with same name.
 */
int textsearch_register(struct ts_ops *ops)
{
	int err = -EEXIST;
	struct ts_ops *o;

	if (ops->name == NULL || ops->find == NULL || ops->init == NULL ||
	    ops->get_pattern == NULL || ops->get_pattern_len == NULL)
		return -EINVAL;

	spin_lock(&ts_mod_lock);
	list_for_each_entry(o, &ts_ops, list) {
		if (!strcmp(ops->name, o->name))
			goto errout;
	}

	list_add_tail_rcu(&ops->list, &ts_ops);
	err = 0;
errout:
	spin_unlock(&ts_mod_lock);
	return err;
}

/**
 * textsearch_unregister - unregister a textsearch module
 * @ops: operations lookup table
 *
 * This function must be called by textsearch modules to announce
 * their disappearance for examples when the module gets unloaded.
 * The &ops parameter must be the same as the one during the
 * registration.
 *
 * Returns 0 on success or -ENOENT if no matching textsearch
 * registration was found.
 */
int textsearch_unregister(struct ts_ops *ops)
{
	int err = 0;
	struct ts_ops *o;

	spin_lock(&ts_mod_lock);
	list_for_each_entry(o, &ts_ops, list) {
		if (o == ops) {
			list_del_rcu(&o->list);
			goto out;
		}
	}

	err = -ENOENT;
out:
	spin_unlock(&ts_mod_lock);
	return err;
}

struct ts_linear_state
{
	unsigned int	len;
	const void	*data;
};

static unsigned int get_linear_data(unsigned int consumed, const u8 **dst,
				    struct ts_config *conf,
				    struct ts_state *state)
{
	struct ts_linear_state *st = (struct ts_linear_state *) state->cb;

	if (likely(consumed < st->len)) {
		*dst = st->data + consumed;
		return st->len - consumed;
	}

	return 0;
}

/**
 * textsearch_find_continuous - search a pattern in continuous/linear data
 * @conf: search configuration
 * @state: search state
 * @data: data to search in
 * @len: length of data
 *
 * A simplified version of textsearch_find() for continuous/linear data.
 * Call textsearch_next() to retrieve subsequent matches.
 *
 * Returns the position of first occurrence of the pattern or
 * %UINT_MAX if no occurrence was found.
 */ 
unsigned int textsearch_find_continuous(struct ts_config *conf,
					struct ts_state *state,
					const void *data, unsigned int len)
{
	struct ts_linear_state *st = (struct ts_linear_state *) state->cb;

	conf->get_next_block = get_linear_data;
	st->data = data;
	st->len = len;

	return textsearch_find(conf, state);
}

/**
 * textsearch_prepare - Prepare a search
 * @algo: name of search algorithm
 * @pattern: pattern data
 * @len: length of pattern
 * @gfp_mask: allocation mask
 * @flags: search flags
 *
 * Looks up the search algorithm module and creates a new textsearch
 * configuration for the specified pattern. Upon completion all
 * necessary refcnts are held and the configuration must be put back
 * using textsearch_put() after usage.
 *
 * Note: The format of the pattern may not be compatible between
 *       the various search algorithms.
 *
 * Returns a new textsearch configuration according to the specified
 * parameters or a ERR_PTR(). If a zero length pattern is passed, this
 * function returns EINVAL.
 */
struct ts_config *textsearch_prepare(const char *algo, const void *pattern,
				     unsigned int len, gfp_t gfp_mask, int flags)
{
	int err = -ENOENT;
	struct ts_config *conf;
	struct ts_ops *ops;
	
	if (len == 0)
		return ERR_PTR(-EINVAL);

	ops = lookup_ts_algo(algo);
#ifdef CONFIG_MODULES
	/*
	 * Why not always autoload you may ask. Some users are
	 * in a situation where requesting a module may deadlock,
	 * especially when the module is located on a NFS mount.
	 */
	if (ops == NULL && flags & TS_AUTOLOAD) {
		request_module("ts_%s", algo);
		ops = lookup_ts_algo(algo);
	}
#endif

	if (ops == NULL)
		goto errout;

	conf = ops->init(pattern, len, gfp_mask, flags);
	if (IS_ERR(conf)) {
		err = PTR_ERR(conf);
		goto errout;
	}

	conf->ops = ops;
	return conf;

errout:
	if (ops)
		module_put(ops->owner);
		
	return ERR_PTR(err);
}

/**
 * textsearch_destroy - destroy a search configuration
 * @conf: search configuration
 *
 * Releases all references of the configuration and frees
 * up the memory.
 */
void textsearch_destroy(struct ts_config *conf)
{
	if (conf->ops) {
		if (conf->ops->destroy)
			conf->ops->destroy(conf);
		module_put(conf->ops->owner);
	}

	kfree(conf);
}

EXPORT_SYMBOL(textsearch_register);
EXPORT_SYMBOL(textsearch_unregister);
EXPORT_SYMBOL(textsearch_prepare);
EXPORT_SYMBOL(textsearch_find_continuous);
EXPORT_SYMBOL(textsearch_destroy);