blob: 1d89f7919e8ceae7732db5d883a1766c3215a0b2 (
plain) (
tree)
|
|
/* config.h. Generated from config.h.in by configure. */
/* config.h.in. Generated from configure.ac by autoheader. */
/* Define to one of `_getb67', `GETB67', `getb67' for Cray-2 and Cray-YMP
systems. This function is required for `alloca.c' support on those systems.
*/
/* #undef CRAY_STACKSEG_END */
/* Define to 1 if using `alloca.c'. */
/* #undef C_ALLOCA */
/* Define to 1 if you have `alloca', as a function or macro. */
#define HAVE_ALLOCA 1
/* Define to 1 if you have <alloca.h> and it should be used (not on Ultrix).
*/
#define HAVE_ALLOCA_H 1
/* Have cairo support */
/* #undef HAVE_CAIRO */
/* Define to 1 if you have the `clock_gettime' function. */
/* #undef HAVE_CLOCK_GETTIME */
/* Define to 1 if you have the <dlfcn.h> header file. */
#define HAVE_DLFCN_H 1
/* Define to 1 if you have the <inttypes.h> header file. */
#define HAVE_INTTYPES_H 1
/* Enable if your compiler supports the Intel __sync_* atomic primitives */
#define HAVE_LIBDRM_ATOMIC_PRIMITIVES 1
/* Have libudev support */
/* #undef HAVE_LIBUDEV */
/* Enable if you have libatomic-ops-dev installed */
/* #undef HAVE_LIB_ATOMIC_OPS */
/* Define to 1 if you have the <memory.h> header file. */
#define HAVE_MEMORY_H 1
/* Have nouveau (nvidia) support */
/* #undef HAVE_NOUVEAU */
/* Have OMAP support */
#define HAVE_OMAP 1
/* Define to 1 if you have the `open_memstream' function. */
#define HAVE_OPEN_MEMSTREAM 1
/* Have radeon support */
/* #undef HAVE_RADEON */
/* Define to 1 if you have the <stdint.h> header file. */
#define HAVE_STDINT_H 1
/* Define to 1 if you have the <stdlib.h> header file. */
#define HAVE_STDLIB_H 1
/* Define to 1 if you have the <strings.h> header file. */
#define HAVE_STRINGS_H 1
/* Define to 1 if you have the <string.h> header file. */
#define HAVE_STRING_H 1
/* Define to 1 if you have the <sys/stat.h> header file. */
#define HAVE_SYS_STAT_H 1
/* Define to 1 if you have the <sys/types.h> header file. */
#define HAVE_SYS_TYPES_H 1
/* Define to 1 if you have the <unistd.h> header file. */
#define HAVE_UNISTD_H 1
/* Use valgrind intrinsics to suppress false warnings */
/* #undef HAVE_VALGRIND */
/* Have vmwgfx kernel headers */
/* #undef HAVE_VMWGFX */
/* Define to the sub-directory in which libtool stores uninstalled libraries.
*/
#define LT_OBJDIR ".libs/"
/* Name of package */
#define PACKAGE "libdrm"
/* Define to the address where bug reports for this package should be sent. */
#define PACKAGE_BUGREPORT "https://bugs.freedesktop.org/enter_bug.cgi?product=DRI"
/* Define to the full name of this package. */
#define PACKAGE_NAME "libdrm"
/* Define to the full name and version of this package. */
#define PACKAGE_STRING "libdrm 2.4.33"
/* Define to the one symbol short name of this package. */
#define PACKAGE_TARNAME "libdrm"
/* Define to the home page for this package. */
#define PACKAGE_URL ""
/* Define to the version of this package. */
#define PACKAGE_VERSION "2.4.33"
/* If using the C implementation of alloca, define if you know the
direction of stack growth for your system; otherwise it will be
automatically deduced at runtime.
STACK_DIRECTION > 0 => grows toward higher addresses
STACK_DIRECTION < 0 => grows toward lower addresses
STACK_DIRECTION = 0 => direction of growth unknown */
/* #undef STACK_DIRECTION */
/* Define to 1 if you have the ANSI C header files. */
#define STDC_HEADERS 1
/* Have UDEV support */
/* #undef UDEV */
/* Enable extensions on AIX 3, Interix. */
#ifndef _ALL_SOURCE
# define _ALL_SOURCE 1
#endif
/* Enable GNU extensions on systems that have them. */
#ifndef _GNU_SOURCE
# define _GNU_SOURCE 1
#endif
/* Enable threading extensions on Solaris. */
#ifndef _POSIX_PTHREAD_SEMANTICS
# define _POSIX_PTHREAD_SEMANTICS 1
#endif
/* Enable extensions on HP NonStop. */
#ifndef _TANDEM_SOURCE
# define _TANDEM_SOURCE 1
#endif
/* Enable general extensions on Solaris. */
#ifndef __EXTENSIONS__
# define __EXTENSIONS__ 1
#endif
/* Version number of package */
#define VERSION "2.4.33"
/* Number of bits in a file offset, on hosts where this is settable. */
/* #undef _FILE_OFFSET_BITS */
/* Define for large files, on AIX-style hosts. */
/* #undef _LARGE_FILES */
/* Define to 1 if on MINIX. */
/* #undef _MINIX */
/* Define to 2 if the system does not provide POSIX.1 features except with
this defined. */
/* #undef _POSIX_1_SOURCE */
/* Define to 1 if you need to in order for `stat' and other things to work. */
/* #undef _POSIX_SOURCE */
/* Define to `unsigned int' if <sys/types.h> does not define. */
/* #undef size_t */
|