aboutsummaryrefslogtreecommitdiffstats
blob: a031fbc14c7a282c390f52284f75d7df5606edb2 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
Working on bionic
=================

What are the big pieces of bionic?
----------------------------------

#### libc/ --- libc.so, libc.a

The C library. Stuff like `fopen(3)` and `kill(2)`.

#### libm/ --- libm.so, libm.a

The math library. Traditionally Unix systems kept stuff like `sin(3)` and
`cos(3)` in a separate library to save space in the days before shared
libraries.

#### libdl/ --- libdl.so

The dynamic linker interface library. This is actually just a bunch of stubs
that the dynamic linker replaces with pointers to its own implementation at
runtime. This is where stuff like `dlopen(3)` lives.

#### libstdc++/ --- libstdc++.so

The C++ ABI support functions. The C++ compiler doesn't know how to implement
thread-safe static initialization and the like, so it just calls functions that
are supplied by the system. Stuff like `__cxa_guard_acquire` and
`__cxa_pure_virtual` live here.

#### linker/ --- /system/bin/linker and /system/bin/linker64

The dynamic linker. When you run a dynamically-linked executable, its ELF file
has a `DT_INTERP` entry that says "use the following program to start me".  On
Android, that's either `linker` or `linker64` (depending on whether it's a
32-bit or 64-bit executable). It's responsible for loading the ELF executable
into memory and resolving references to symbols (so that when your code tries to
jump to `fopen(3)`, say, it lands in the right place).

#### tests/ --- unit tests

The `tests/` directory contains unit tests. Roughly arranged as one file per
publicly-exported header file.

#### benchmarks/ --- benchmarks

The `benchmarks/` directory contains benchmarks.


What's in libc/?
----------------

<pre>
libc/
  arch-arm/
  arch-arm64/
  arch-common/
  arch-mips/
  arch-mips64/
  arch-x86/
  arch-x86_64/
    # Each architecture has its own subdirectory for stuff that isn't shared
    # because it's architecture-specific. There will be a .mk file in here that
    # drags in all the architecture-specific files.
    bionic/
      # Every architecture needs a handful of machine-specific assembler files.
      # They live here.
    include/
      machine/
        # The majority of header files are actually in libc/include/, but many
        # of them pull in a <machine/something.h> for things like limits,
        # endianness, and how floating point numbers are represented. Those
        # headers live here.
    string/
      # Most architectures have a handful of optional assembler files
      # implementing optimized versions of various routines. The <string.h>
      # functions are particular favorites.
    syscalls/
      # The syscalls directories contain script-generated assembler files.
      # See 'Adding system calls' later.

  include/
    # The public header files on everyone's include path. These are a mixture of
    # files written by us and files taken from BSD.

  kernel/
    # The kernel uapi header files. These are scrubbed copies of the originals
    # in external/kernel-headers/. These files must not be edited directly. The
    # generate_uapi_headers.sh script should be used to go from a kernel tree to
    # external/kernel-headers/ --- this takes care of the architecture-specific
    # details. The update_all.py script should be used to regenerate bionic's
    # scrubbed headers from external/kernel-headers/.

  private/
    # These are private header files meant for use within bionic itself.

  dns/
    # Contains the DNS resolver (originates from NetBSD code).

  upstream-dlmalloc/
  upstream-freebsd/
  upstream-netbsd/
  upstream-openbsd/
    # These directories contain unmolested upstream source. Any time we can
    # just use a BSD implementation of something unmodified, we should.
    # The structure under these directories mimics the upstream tree,
    # but there's also...
    android/
      include/
        # This is where we keep the hacks necessary to build BSD source
        # in our world. The *-compat.h files are automatically included
        # using -include, but we also provide equivalents for missing
        # header/source files needed by the BSD implementation.

  bionic/
    # This is the biggest mess. The C++ files are files we own, typically
    # because the Linux kernel interface is sufficiently different that we
    # can't use any of the BSD implementations. The C files are usually
    # legacy mess that needs to be sorted out, either by replacing it with
    # current upstream source in one of the upstream directories or by
    # switching the file to C++ and cleaning it up.

  stdio/
    # These are legacy files of dubious provenance. We're working to clean
    # this mess up, and this directory should disappear.

  tools/
    # Various tools used to maintain bionic.

  tzcode/
    # A modified superset of the IANA tzcode. Most of the modifications relate
    # to Android's use of a single file (with corresponding index) to contain
    # time zone data.
  zoneinfo/
    # Android-format time zone data.
    # See 'Updating tzdata' later.
</pre>


Adding system calls
-------------------

Adding a system call usually involves:

  1. Add entries to SYSCALLS.TXT.
     See SYSCALLS.TXT itself for documentation on the format.
  2. Run the gensyscalls.py script.
  3. Add constants (and perhaps types) to the appropriate header file.
     Note that you should check to see whether the constants are already in
     kernel uapi header files, in which case you just need to make sure that
     the appropriate POSIX header file in libc/include/ includes the
     relevant file or files.
  4. Add function declarations to the appropriate header file.
  5. Add at least basic tests. Even a test that deliberately supplies
     an invalid argument helps check that we're generating the right symbol
     and have the right declaration in the header file. (And strace(1) can
     confirm that the correct system call is being made.)


Updating kernel header files
----------------------------

As mentioned above, this is currently a two-step process:

  1. Use generate_uapi_headers.sh to go from a Linux source tree to appropriate
     contents for external/kernel-headers/.
  2. Run update_all.py to scrub those headers and import them into bionic.


Updating tzdata
---------------

This is fully automated:

  1. Run update-tzdata.py.


Verifying changes
-----------------

If you make a change that is likely to have a wide effect on the tree (such as a
libc header change), you should run `make checkbuild`. A regular `make` will
_not_ build the entire tree; just the minimum number of projects that are
required for the device. Tests, additional developer tools, and various other
modules will not be built. Note that `make checkbuild` will not be complete
either, as `make tests` covers a few additional modules, but generally speaking
`make checkbuild` is enough.


Running the tests
-----------------

The tests are all built from the tests/ directory.

### Device tests

    $ mma
    $ adb sync
    $ adb shell /data/nativetest/bionic-unit-tests/bionic-unit-tests32
    $ adb shell \
        /data/nativetest/bionic-unit-tests-static/bionic-unit-tests-static32
    # Only for 64-bit targets
    $ adb shell /data/nativetest/bionic-unit-tests/bionic-unit-tests64
    $ adb shell \
        /data/nativetest/bionic-unit-tests-static/bionic-unit-tests-static64

### Host tests

The host tests require that you have `lunch`ed either an x86 or x86_64 target.

    $ mma
    # 64-bit tests for 64-bit targets, 32-bit otherwise.
    $ mm bionic-unit-tests-run-on-host
    # Only exists for 64-bit targets.
    $ mm bionic-unit-tests-run-on-host32

### Against glibc

As a way to check that our tests do in fact test the correct behavior (and not
just the behavior we think is correct), it is possible to run the tests against
the host's glibc.

    $ mma
    $ bionic-unit-tests-glibc32 # already in your path
    $ bionic-unit-tests-glibc64


Gathering test coverage
-----------------------

For either host or target coverage, you must first:

 * `$ export NATIVE_COVERAGE=true`
     * Note that the build system is ignorant to this flag being toggled, i.e. if
       you change this flag, you will have to manually rebuild bionic.
 * Set `bionic_coverage=true` in `libc/Android.mk` and `libm/Android.mk`.

### Coverage from device tests

    $ mma
    $ adb sync
    $ adb shell \
        GCOV_PREFIX=/data/local/tmp/gcov \
        GCOV_PREFIX_STRIP=`echo $ANDROID_BUILD_TOP | grep -o / | wc -l` \
        /data/nativetest/bionic-unit-tests/bionic-unit-tests32
    $ acov

`acov` will pull all coverage information from the device, push it to the right
directories, run `lcov`, and open the coverage report in your browser.

### Coverage from host tests

First, build and run the host tests as usual (see above).

    $ croot
    $ lcov -c -d $ANDROID_PRODUCT_OUT -o coverage.info
    $ genhtml -o covreport coverage.info # or lcov --list coverage.info

The coverage report is now available at `covreport/index.html`.