1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
|
/*
* Copyright (C) 2008 The Android Open Source Project
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in
* the documentation and/or other materials provided with the
* distribution.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
* "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
* LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS
* FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE
* COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT,
* INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING,
* BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS
* OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED
* AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY,
* OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT
* OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF
* SUCH DAMAGE.
*/
#include <pthread.h>
#include <errno.h>
#include <sys/mman.h>
#include <unistd.h>
#include "pthread_internal.h"
#include "private/bionic_macros.h"
#include "private/bionic_ssp.h"
#include "private/bionic_tls.h"
#include "private/libc_logging.h"
#include "private/ErrnoRestorer.h"
#include "private/ScopedPthreadMutexLocker.h"
// x86 uses segment descriptors rather than a direct pointer to TLS.
#if __i386__
#include <asm/ldt.h>
extern "C" __LIBC_HIDDEN__ void __init_user_desc(struct user_desc*, int, void*);
#endif
extern "C" int __isthreaded;
// This code is used both by each new pthread and the code that initializes the main thread.
void __init_tls(pthread_internal_t* thread) {
if (thread->user_allocated_stack()) {
// We don't know where the user got their stack, so assume the worst and zero the TLS area.
memset(&thread->tls[0], 0, BIONIC_TLS_SLOTS * sizeof(void*));
}
// Slot 0 must point to itself. The x86 Linux kernel reads the TLS from %fs:0.
thread->tls[TLS_SLOT_SELF] = thread->tls;
thread->tls[TLS_SLOT_THREAD_ID] = thread;
// GCC looks in the TLS for the stack guard on x86, so copy it there from our global.
thread->tls[TLS_SLOT_STACK_GUARD] = (void*) __stack_chk_guard;
}
void __init_alternate_signal_stack(pthread_internal_t* thread) {
// Create and set an alternate signal stack.
stack_t ss;
ss.ss_sp = mmap(NULL, SIGSTKSZ, PROT_READ|PROT_WRITE, MAP_PRIVATE|MAP_ANONYMOUS, -1, 0);
if (ss.ss_sp != MAP_FAILED) {
ss.ss_size = SIGSTKSZ;
ss.ss_flags = 0;
sigaltstack(&ss, NULL);
thread->alternate_signal_stack = ss.ss_sp;
}
}
int __init_thread(pthread_internal_t* thread, bool add_to_thread_list) {
int error = 0;
// Set the scheduling policy/priority of the thread.
if (thread->attr.sched_policy != SCHED_NORMAL) {
sched_param param;
param.sched_priority = thread->attr.sched_priority;
if (sched_setscheduler(thread->tid, thread->attr.sched_policy, ¶m) == -1) {
#if __LP64__
// For backwards compatibility reasons, we only report failures on 64-bit devices.
error = errno;
#endif
__libc_format_log(ANDROID_LOG_WARN, "libc",
"pthread_create sched_setscheduler call failed: %s", strerror(errno));
}
}
thread->cleanup_stack = NULL;
if (add_to_thread_list) {
_pthread_internal_add(thread);
}
return error;
}
static void* __create_thread_stack(pthread_internal_t* thread) {
// Create a new private anonymous map.
int prot = PROT_READ | PROT_WRITE;
int flags = MAP_PRIVATE | MAP_ANONYMOUS | MAP_NORESERVE;
void* stack = mmap(NULL, thread->attr.stack_size, prot, flags, -1, 0);
if (stack == MAP_FAILED) {
__libc_format_log(ANDROID_LOG_WARN,
"libc",
"pthread_create failed: couldn't allocate %zd-byte stack: %s",
thread->attr.stack_size, strerror(errno));
return NULL;
}
// Set the guard region at the end of the stack to PROT_NONE.
if (mprotect(stack, thread->attr.guard_size, PROT_NONE) == -1) {
__libc_format_log(ANDROID_LOG_WARN, "libc",
"pthread_create failed: couldn't mprotect PROT_NONE %zd-byte stack guard region: %s",
thread->attr.guard_size, strerror(errno));
munmap(stack, thread->attr.stack_size);
return NULL;
}
return stack;
}
static int __pthread_start(void* arg) {
pthread_internal_t* thread = reinterpret_cast<pthread_internal_t*>(arg);
// Wait for our creating thread to release us. This lets it have time to
// notify gdb about this thread before we start doing anything.
// This also provides the memory barrier needed to ensure that all memory
// accesses previously made by the creating thread are visible to us.
pthread_mutex_lock(&thread->startup_handshake_mutex);
pthread_mutex_destroy(&thread->startup_handshake_mutex);
__init_alternate_signal_stack(thread);
void* result = thread->start_routine(thread->start_routine_arg);
pthread_exit(result);
return 0;
}
// A dummy start routine for pthread_create failures where we've created a thread but aren't
// going to run user code on it. We swap out the user's start routine for this and take advantage
// of the regular thread teardown to free up resources.
static void* __do_nothing(void*) {
return NULL;
}
int pthread_create(pthread_t* thread_out, pthread_attr_t const* attr,
void* (*start_routine)(void*), void* arg) {
ErrnoRestorer errno_restorer;
// Inform the rest of the C library that at least one thread was created.
__isthreaded = 1;
pthread_internal_t* thread = __create_thread_struct();
if (thread == NULL) {
return EAGAIN;
}
if (attr == NULL) {
pthread_attr_init(&thread->attr);
} else {
thread->attr = *attr;
attr = NULL; // Prevent misuse below.
}
// Make sure the stack size and guard size are multiples of PAGE_SIZE.
thread->attr.stack_size = BIONIC_ALIGN(thread->attr.stack_size, PAGE_SIZE);
thread->attr.guard_size = BIONIC_ALIGN(thread->attr.guard_size, PAGE_SIZE);
if (thread->attr.stack_base == NULL) {
// The caller didn't provide a stack, so allocate one.
thread->attr.stack_base = __create_thread_stack(thread);
if (thread->attr.stack_base == NULL) {
__free_thread_struct(thread);
return EAGAIN;
}
} else {
// The caller did provide a stack, so remember we're not supposed to free it.
thread->attr.flags |= PTHREAD_ATTR_FLAG_USER_ALLOCATED_STACK;
}
// Make room for the TLS area.
// The child stack is the same address, just growing in the opposite direction.
// At offsets >= 0, we have the TLS slots.
// At offsets < 0, we have the child stack.
thread->tls = reinterpret_cast<void**>(reinterpret_cast<uint8_t*>(thread->attr.stack_base) +
thread->attr.stack_size - BIONIC_ALIGN(BIONIC_TLS_SLOTS * sizeof(void*), 16));
void* child_stack = thread->tls;
__init_tls(thread);
// Create a mutex for the thread in TLS to wait on once it starts so we can keep
// it from doing anything until after we notify the debugger about it
//
// This also provides the memory barrier we need to ensure that all
// memory accesses previously performed by this thread are visible to
// the new thread.
pthread_mutex_init(&thread->startup_handshake_mutex, NULL);
pthread_mutex_lock(&thread->startup_handshake_mutex);
thread->start_routine = start_routine;
thread->start_routine_arg = arg;
thread->set_cached_pid(getpid());
int flags = CLONE_VM | CLONE_FS | CLONE_FILES | CLONE_SIGHAND | CLONE_THREAD | CLONE_SYSVSEM |
CLONE_SETTLS | CLONE_PARENT_SETTID | CLONE_CHILD_CLEARTID;
void* tls = thread->tls;
#if defined(__i386__)
// On x86 (but not x86-64), CLONE_SETTLS takes a pointer to a struct user_desc rather than
// a pointer to the TLS itself.
user_desc tls_descriptor;
__init_user_desc(&tls_descriptor, false, tls);
tls = &tls_descriptor;
#endif
int rc = clone(__pthread_start, child_stack, flags, thread, &(thread->tid), tls, &(thread->tid));
if (rc == -1) {
int clone_errno = errno;
// We don't have to unlock the mutex at all because clone(2) failed so there's no child waiting to
// be unblocked, but we're about to unmap the memory the mutex is stored in, so this serves as a
// reminder that you can't rewrite this function to use a ScopedPthreadMutexLocker.
pthread_mutex_unlock(&thread->startup_handshake_mutex);
if (!thread->user_allocated_stack()) {
munmap(thread->attr.stack_base, thread->attr.stack_size);
}
__free_thread_struct(thread);
__libc_format_log(ANDROID_LOG_WARN, "libc", "pthread_create failed: clone failed: %s", strerror(errno));
return clone_errno;
}
int init_errno = __init_thread(thread, true);
if (init_errno != 0) {
// Mark the thread detached and replace its start_routine with a no-op.
// Letting the thread run is the easiest way to clean up its resources.
thread->attr.flags |= PTHREAD_ATTR_FLAG_DETACHED;
thread->start_routine = __do_nothing;
pthread_mutex_unlock(&thread->startup_handshake_mutex);
return init_errno;
}
// Publish the pthread_t and unlock the mutex to let the new thread start running.
*thread_out = reinterpret_cast<pthread_t>(thread);
pthread_mutex_unlock(&thread->startup_handshake_mutex);
return 0;
}
|