diff options
author | Saurabh Bipin Chandra | 2013-04-22 11:42:19 -0500 |
---|---|---|
committer | Saurabh Bipin Chandra | 2013-04-26 09:14:28 -0500 |
commit | 6647d1f16d70b9d867ce5b7aef92705939aa5975 (patch) | |
tree | 73b154f99e7ceff809c8a98be6489e4ee11d0877 /dce_rpc.h | |
download | repo-libdce-6647d1f16d70b9d867ce5b7aef92705939aa5975.tar.gz repo-libdce-6647d1f16d70b9d867ce5b7aef92705939aa5975.tar.xz repo-libdce-6647d1f16d70b9d867ce5b7aef92705939aa5975.zip |
[libDCE] Add IPC 3.x Adapted code to Repository3.00.01.00
This patch adds libdce code to the repository.
LibDCE has been adapted to use the MmRpc layer
of IPC 3.x. This version of LibDCE is expected to
work on QNX.
Patchset 2 adds/modifies:
1. Removes Tiler 2D allocation/free for now.
2. Corrects memplugin_free() for Tiler 1D.
3. Modifies dce_test app to dump output till 30 frames.
4. Renamed dce.h to libdce.h.
5. Corrected header files across all files.
6. Build configuration for QNX
7. Removes build warnings.
8. Add README for Build instructions
9. Takes care of comments of Buddy and Pradeep.
Patchset 3 adds/modifies:
1. Reduced Stack usage of each function.
2. Add ptr check in memplugin and remove from libdce.
3. Add DCE_Assert macros.
4. Add DCE_error_status enum.
5. Comments Cleanup
6. Make some functions static.
7. process() cleanup including removing reply_buf.
8. Add else if (for codec_type == Encoder type)
9. Converted Macros to Inline functions.
10.Converted init and deinit to dce_init and dce_deinit functions.
11. Removed dce_init() and dce_deinit() declarations
Patchset 4 adds/modifies:
1. Assert Input function arguments.
2. Correct copyright year.
3. Correct memplugin_free for Shared memory.
4. Create dce_priv.h and move trace and assert macros to the header.
5. Redeclare mem_type enum and add mem_error_status enum in
memplugin.h and make corresponding changes.
6. Add asserts in memplugin.
Intention of some of the changes above is to move towards
delinking Libdce and Memplugin.
Patchset 5:
1. Missed to add dce_priv.h file.
Patchset 6:
1. Take care Pradeep's comment.
Change-Id: I6e5e37b7088362e7bad66200fc3454bb828e0eff
Signed-off-by: Saurabh Bipin Chandra <a0131926@ti.com>
Diffstat (limited to 'dce_rpc.h')
-rw-r--r-- | dce_rpc.h | 145 |
1 files changed, 145 insertions, 0 deletions
diff --git a/dce_rpc.h b/dce_rpc.h new file mode 100644 index 0000000..8082d76 --- /dev/null +++ b/dce_rpc.h | |||
@@ -0,0 +1,145 @@ | |||
1 | /* | ||
2 | * Copyright (c) 2013, Texas Instruments Incorporated | ||
3 | * All rights reserved. | ||
4 | * | ||
5 | * Redistribution and use in source and binary forms, with or without | ||
6 | * modification, are permitted provided that the following conditions | ||
7 | * are met: | ||
8 | * | ||
9 | * * Redistributions of source code must retain the above copyright | ||
10 | * notice, this list of conditions and the following disclaimer. | ||
11 | * | ||
12 | * * Redistributions in binary form must reproduce the above copyright | ||
13 | * notice, this list of conditions and the following disclaimer in the | ||
14 | * documentation and/or other materials provided with the distribution. | ||
15 | * | ||
16 | * * Neither the name of Texas Instruments Incorporated nor the names of | ||
17 | * its contributors may be used to endorse or promote products derived | ||
18 | * from this software without specific prior written permission. | ||
19 | * | ||
20 | * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" | ||
21 | * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, | ||
22 | * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR | ||
23 | * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR | ||
24 | * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, | ||
25 | * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, | ||
26 | * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; | ||
27 | * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, | ||
28 | * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR | ||
29 | * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, | ||
30 | * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. | ||
31 | */ | ||
32 | |||
33 | #ifndef __DCE_RPC_H__ | ||
34 | #define __DCE_RPC_H__ | ||
35 | |||
36 | /* RPC layer types.. these define the payload of messages between IPUMM | ||
37 | * and MPU. This should be kept in sync between firmware build and | ||
38 | * driver. | ||
39 | * | ||
40 | * TODO: xxx_control(XDM_GETVERSION) is a bit awkward to deal with, because | ||
41 | * this seems to be the one special case where status->data is used.. | ||
42 | * possibly we should define a special ioctl and msg to handle this case. | ||
43 | */ | ||
44 | |||
45 | #define DCE_DEVICE_NAME "rpmsg-dce" | ||
46 | |||
47 | /* Message-Ids: | ||
48 | */ | ||
49 | //#define DCE_RPC_CONNECT (0x80000000 | 00) Connect not needed anymore. | ||
50 | typedef enum dce_rpc_call { | ||
51 | DCE_RPC_ENGINE_OPEN = 0, | ||
52 | DCE_RPC_ENGINE_CLOSE, | ||
53 | DCE_RPC_CODEC_CREATE, | ||
54 | DCE_RPC_CODEC_CONTROL, | ||
55 | DCE_RPC_CODEC_GET_VERSION, | ||
56 | DCE_RPC_CODEC_PROCESS, | ||
57 | DCE_RPC_CODEC_DELETE | ||
58 | } dce_rpc_call; | ||
59 | |||
60 | |||
61 | typedef enum dce_codec_type { | ||
62 | OMAP_DCE_VIDENC2 = 1, | ||
63 | OMAP_DCE_VIDDEC3 = 2 | ||
64 | } dce_codec_type; | ||
65 | |||
66 | /* Structures of RPC */ | ||
67 | typedef struct dce_connect { | ||
68 | uint32_t chipset_id; | ||
69 | uint32_t debug; | ||
70 | } dce_connect; | ||
71 | |||
72 | typedef struct dce_engine_open { | ||
73 | char name[32]; /* engine name (in) */ | ||
74 | Engine_Error error_code; /* error code (out) */ | ||
75 | Engine_Handle eng_handle; /* engine handle (out) */ | ||
76 | } dce_engine_open; | ||
77 | |||
78 | typedef struct dce_engine_close { | ||
79 | Engine_Handle eng_handle; /* engine handle (in) */ | ||
80 | } dce_engine_close; | ||
81 | |||
82 | typedef struct dce_codec_create { | ||
83 | Engine_Handle engine; | ||
84 | char codec_name[32]; | ||
85 | void *static_params; | ||
86 | dce_codec_type codec_id; | ||
87 | void *codec_handle; | ||
88 | } dce_codec_create; | ||
89 | |||
90 | typedef struct dce_codec_control { | ||
91 | void *codec_handle; | ||
92 | uint32_t cmd_id; | ||
93 | void *dyn_params; | ||
94 | void *status; | ||
95 | dce_codec_type codec_id; | ||
96 | int32_t result; | ||
97 | } dce_codec_control; | ||
98 | |||
99 | typedef struct dce_codec_get_version { | ||
100 | void *codec_handle; | ||
101 | void *dyn_params; | ||
102 | void *status; | ||
103 | void *version; | ||
104 | dce_codec_type codec_id; | ||
105 | int32_t result; | ||
106 | } dce_codec_get_version; | ||
107 | |||
108 | typedef struct dce_codec_delete { | ||
109 | void *codec_handle; | ||
110 | dce_codec_type codec_id; | ||
111 | } dce_codec_delete; | ||
112 | |||
113 | /* ---------------------- For GLP DCE -----------------------------*/ | ||
114 | /* NOTE: CODEC_PROCESS does somewhat more than the other ioctls, in that it | ||
115 | * handles buffer mapping/unmapping. So the inBufs/outBufs are copied inline | ||
116 | * (with translated addresses in the copy sent inline with codec_process_req). | ||
117 | * Since we need the inputID from inArgs, and it is a small struct, it is also | ||
118 | * copied inline. | ||
119 | * | ||
120 | * Therefore, the variable length data[] section has the format: | ||
121 | * uint8_t reloc[reloc_length * 4]; | ||
122 | * uint8_t inargs[in_args_length * 4]; | ||
123 | * uint8_t outbufs[in_bufs_length * 4]; | ||
124 | * uint8_t inbufs[in_bufs_length * 4]; | ||
125 | */ | ||
126 | |||
127 | #define MAX_INPUT_BUF 2 // Need to confirm for interlaced YUVs for Encoders | ||
128 | #define MAX_OUTPUT_BUF 2 | ||
129 | #define MAX_TOTAl_BUF (MAX_INPUT_BUF + MAX_OUTPUT_BUF) | ||
130 | |||
131 | /* Struct to be used if approach [3] of Mmrpc call is followed */ | ||
132 | typedef struct dce_codec_process { | ||
133 | void *codec_handle; | ||
134 | void *inBufs; | ||
135 | void *outBufs; | ||
136 | void *inArgs; | ||
137 | void *outArgs; | ||
138 | int32_t input_Buf[MAX_INPUT_BUF]; | ||
139 | int32_t output_Buf[MAX_OUTPUT_BUF]; | ||
140 | dce_codec_type codec_id; | ||
141 | int32_t result; | ||
142 | } dce_codec_process; | ||
143 | |||
144 | #endif /* __DCE_RPC_H__ */ | ||
145 | |||