aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorAngela Stegmaier2016-12-09 16:14:09 -0600
committerAngela Stegmaier2017-01-17 14:46:27 -0600
commit5fd7da53b505e1bc80a0c9d116fe31e5cd177d74 (patch)
tree53fc0f5585beb0ad879797e59889ba3f31a8bbab /libdce.h
parentc51f144b079836afb868bff44afe7308248a0217 (diff)
downloadrepo-libdce-5fd7da53b505e1bc80a0c9d116fe31e5cd177d74.tar.gz
repo-libdce-5fd7da53b505e1bc80a0c9d116fe31e5cd177d74.tar.xz
repo-libdce-5fd7da53b505e1bc80a0c9d116fe31e5cd177d74.zip
libdce[Android]: Add dce_ipc_recover API
In case of remote core recovery due to remote core crash, the rpmsg-dce handle needs to be closed and re-opened since any handles that were open when the crash happened are marked as stale in the driver. This patch adds a new API that the user can call to close the rpmsg-dce handle so that recovery can happen. In case the user receives notification of a remote core crash, it can call the dce_ipc_recover() API to make sure that the rpmsg-dce handle that is opened during dce_buf_lock is closed so that a new one can be opened the next time. Change-Id: I8ebc19e308ffe7431b57c31cfecd469e171777f6 Signed-off-by: Angela Stegmaier <angelabaker@ti.com>
Diffstat (limited to 'libdce.h')
-rw-r--r--libdce.h6
1 files changed, 6 insertions, 0 deletions
diff --git a/libdce.h b/libdce.h
index f17422e..bbc7c13 100644
--- a/libdce.h
+++ b/libdce.h
@@ -132,6 +132,12 @@ int dce_ipc_init(int core);
132 */ 132 */
133void dce_ipc_deinit(int core, int tableIdx); 133void dce_ipc_deinit(int core, int tableIdx);
134 134
135/*===============================================================*/
136/** dce_ipc_recover : Recover the DCE IPC in case of
137 * remote core crash.
138 */
139void dce_ipc_recover(void);
140
135/************************ Input/Output Buffer Lock/Unlock APIs ************************/ 141/************************ Input/Output Buffer Lock/Unlock APIs ************************/
136/*=====================================================================================*/ 142/*=====================================================================================*/
137/** dce_buf_lock : Pin or lock Tiler Buffers which would be used by the IVAHD codec 143/** dce_buf_lock : Pin or lock Tiler Buffers which would be used by the IVAHD codec