aboutsummaryrefslogtreecommitdiffstats
path: root/README
Commit message (Collapse)AuthorAgeFilesLines
* libdce: Updated JpegEncoder interface fileVeeranna Hanchinal2017-02-071-2/+2
| | | | | | | | Updated MJPEGE header file due to MJPEGE codec update to 01.00.17.01 version. Change-Id: Id820f9cf3c66e1659564ba297cc469a30dc55732 Signed-off-by: Veeranna Hanchinal <veeranna.hanchinal@ti.com>
* libdce: add JPEG encoderHongmei Gou2016-11-091-0/+1
| | | | | Change-Id: I0136abd43fe8c1af3fedc5013dae578c8f6c7537 Signed-off-by: Hongmei Gou <h-gou@ti.com>
* Updated README on FC version for MMIP 3.00.08.023.00.09.003.00.08.02Buddy Liong2015-08-171-1/+1
| | | | | | | | | For MMIP 3.00.08.02, the firmware requires FC to be updated to version 3.40.01.04 which solves the issue with FC_suspend() crashes if alg contains > 10 resources. Change-Id: If30a183f29746cd43204a1a4f0cbea5481004467 Signed-off-by: Buddy Liong <buddy.budiono@ti.com>
* README update for MMIP 3.00.08.013.00.08.01Buddy Liong2015-05-261-2/+2
| | | | | | | Update README to correspond the IVAHD codecs version. Change-Id: I351ae4cb24668caac7f35a7574da8d0e33f2053a Signed-off-by: Buddy Liong <buddy.budiono@ti.com>
* README update for MMIP 3.00.08.003.00.08.00Buddy Liong2015-05-111-8/+7
| | | | | | | | Update README to correspond the correct build tools and IVAHD codecs version. Change-Id: I051f314ab42694dbf0c7991f717b0bb99bfb1e1e Signed-off-by: Buddy Liong <buddy.budiono@ti.com>
* Integration based on IPC 3.30.01.12Buddy Liong2014-11-191-18/+18
| | | | | | | | | | Integration with IPC 3.30.01.12 requires build tool update on XDC tool version to 3_30_xx_xx. Using the latest XDC Tools of 3_30_05_60_core Copying the header files used from 3_30_05_60 version. Change-Id: I648bfa945bcc0d8a43b4653d8f303cd9c18ee03f Signed-off-by: Buddy Liong <buddy.budiono@ti.com>
* README update3.00.06.00Buddy Liong2014-08-201-1/+1
| | | | | | | | | Integration with IPC 3.23.00.01 requires build tool update on XDC tool version to 3_25_06_96 Copying the header files used from 3_25_06_90 version. Change-Id: Ie1e6e167a9cfb42fde706fa06ba4dd5900db7483 Signed-off-by: Buddy Liong <buddy.budiono@ti.com>
* README update3.00.05.01buddy.liong2014-07-171-3/+3
| | | | | | | | | | | Updating README note on the codec version used for MMIP 3.00.05.01 VC1 decoder codec version 01.00.00.13 MPEG2 decoder codec version 01.00.14.01 H.264 encoder codec version 02.00.08.01 Change-Id: Iccaf4895398d514d0710794d4e9d9773468669b8 Signed-off-by: buddy.liong <buddy.budiono@ti.com>
* [Linux] Add automatic search path for IPC headersPradeep Venkatasubbarao2014-07-161-1/+1
| | | | | | | | Adds the automatic search header mechanism using pkg-config for libmmrpc. Change-Id: If4aa61cb598567455a1342be358338e4adfcc3e0 Signed-off-by: Pradeep Venkatasubbarao <pradeepv@ti.com>
* README update3.00.04.02buddy.liong2014-04-101-1/+1
| | | | | | | | Updating README note on the VC1 codec version update from 01.00.00.11 to 01.00.00.12 on the IPUMM side. Change-Id: Ib02274fd0ac1c86f6e7978e4e82ac618603159b1 Signed-off-by: buddy.liong <buddy.budiono@ti.com>
* Updating README3.00.04.01buddy.liong2014-03-251-88/+6
| | | | | | | | | | | | | The command to build libdce on QNX requires additional information. Instead of "make clean" and "make install", due to the renaming of Makefile to Makefile.qnx, the command becomes "make -f Makefile.qnx clean" and "make -f Makefile.qnx install". Updates the "Supported API Information" to point to the header files instead of listed it again here. Change-Id: Ied47d812eb8b0a6c9a9bb0cace3f6241f91d7325 Signed-off-by: buddy.liong <buddy.budiono@ti.com>
* [LIBDCE] Updating README3.00.04.00buddy.liong2014-03-061-1/+1
| | | | | | | XDCTOOLS version is updated from 3.25.04.88 to 3.25.05.94. Change-Id: I94842de37a268d38cd6e32d09339a57ebbd9f7a4 Signed-off-by: buddy.liong <buddy.budiono@ti.com>
* [LIBDCE] Clean up README and unsupported header files.buddy.liong2013-12-181-31/+30
| | | | | | | | | | | Updating README on the version information of headers included in the packages folder. Removal of h264svcenc, h264svcvdec, and vc1enc header files since it is not supported in the current IPUMM. Change-Id: I2bb140604a7c7d6e4ba7482a11ac43bc5076d9f6 Signed-off-by: buddy.liong <buddy.budiono@ti.com>
* [LIBDCE]: Changes to make Encoder and Decoder co-exist on AndroidSunita Nadampalli2013-12-111-4/+7
| | | | | | | | | | | | | | | | | | | In the current design omx video decoder is sending ptr for inbufs and dma_buf_fd for the outbufs to the dce client. In order to co-exist with encoder the inbufs/outbufs interpretation is unified between encoder and decoder. this is achieved by passing the memheader for both inbufs and outbufs for both encoder and decoders. This patch modified the process function to handle memheader for all Android scenarios (inbufs/outbufs for encoder/decoder) With this unified buf interpretation, the process function simplified for Android. Note# This patch has should be merged along with the omx patch: http://review.omapzoom.org/#/c/34414/ Change-Id: Ia89ef9785ddf702bca986ce6b4a91983fb8bcc11 Signed-off-by: Sunita Nadampalli <sunitan@ti.com>
* [LIBDCE] Add Android specific changesSunita Nadampalli2013-09-131-1/+14
| | | | | | | | | This patch adds changes specific to Android OS: (1) Semaphore handling (2) Input buffer offset handling Change-Id: Id6232e0b90e638fd1268ccbfafb51c6ca916fad2 Signed-off-by: Sunita Nadampalli <sunitan@ti.com>
* [DOC] Update ReadMe3.00.02.00Saurabh Bipin Chandra2013-09-061-8/+429
| | | | | | | | | | | | | ReadMe now contains: 1. Build Information for QNX 2. Build Information for Linux 3. API Information 4. API call flow 5. Version Info of headers in packages folder. Change-Id: If76f6bae18bfac0cb9c6d918d365f5263c539d0d Signed-off-by: Saurabh Bipin Chandra <a0131926@ti.com>
* [DOC] Renamed README.txt as READMEPradeep Venkatasubbarao2013-09-061-0/+73
Change-Id: Ie4209ef72aa8e10d246e7b523678dd42350535d8 Signed-off-by: Pradeep Venkatasubbarao <pradeepv@ti.com>