aboutsummaryrefslogtreecommitdiffstats
Commit message (Collapse)AuthorAgeFilesLines
* libdce: Increase the concurrent engine handle countHEAD3.00.13.00masterSunita Nadampalli2017-02-071-1/+1
| | | | | | | | Increase the MAX_INSTANCES count for the concurrent engine handles to match the DCE server definitions. Change-Id: If29de276b9a173e114ad6df9b1358b4842e86b49 Signed-off-by: Sunita Nadampalli <sunitan@ti.com>
* get_rproc_info: Introduce new API to query remoteprocBuddy Liong2016-06-171-1/+2
| | | | | | | | | | | | | | | | | | | | | | This is the initial implementation of an extensible API that allows the user to query various remote core parameters. Currently, there are three query parameters that are supported: 1. CPU Load 2. Total configured heap size 3. Available heap size The intent of this API is to programmatically call the API and feed it in various other tools that can be developed on top of this (for example: soc performance visualization etc.) NOTE: This will require the implementation on ipumm-fw and/or dspdce-fw. Change-Id: I94c309221dbce24162a4f31166890d3acdb2d049 Signed-off-by: Karthik Ramanan <a0393906@ti.com> Signed-off-by: Buddy Liong <buddy.liong@ti.com>
* H.264 low latency with IVIDEO_NUMROWSBuddy Liong2016-03-011-0/+6
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | H.264 codec user guide describes the functionality of low latency. This functionality allows user to encode/decode a sub-frame level data communications. Without low latency, user can only encode/decode a complete/full frame only. More information about H264 low latency can be found in codec release package: * H.264 Encoder 2.0 on HDVICP2 and Media Controller Based Platform User's Guide (SPRUHG3), Appendix G - Low Latency / Sub Frame Level Synchronization * H.264 Decoder 2.0 on HDVICP2 and Media Controller Based Platform User's Guide (SPRUHF9), Appendix I - Low Latency / Sub Frame Level Synchronization This commit is only implemented low latency with IVIDEO_NUMROWS. H.264 encoder handles inputDataMode = IVIDEO_NUMROWS with getDataFxn as callback to get the numRows being filled into the inputBuffer pointer passed at process call. From H.264 encoder user guide Appendix G, more details can be found in sec. G2 H.264 Encoder Input with sub frame level synchronization H.264 decoder handles outputDataMode = IVIDEO_NUMROWS with putDataFxn as callback to notify client on the numRows/numBlocks being filled by codec into the outputBuffer pointer passed at process call. From H.264 decoder user guide Appendix I, more details can be found in sec. I.2 Details of using Sub Frame Level data sync at output side. The update is only valid on video codec on IVA-HD. This changes depend on the changes done on IPUMM DCE server. No low latency update is performed on video codec on DSP. This commit has dependencies on: IPC 3.42.00.02 or latest IPUMM commit ids: commit e37750cc921a9442c48e7212824b28850ac3aaa7 - H.264 low latency - IVIDEO_NUMROWS commit 266749c0b6a2584d563625f881f998c3d78ca873 - Handling when MPU crashes, eg. CTRL-C on MPU side. commit 030572aaa1964bb50a903852fab0ecc0149b6b7e - H.264 Low Latency - sync put_DataFxn to MPU side Change-Id: I308bc74a879099f38705df6e6dda4a86b6645986 Signed-off-by: Buddy Liong <buddy.liong@ti.com>
* [LINUX] Manage Tiler Pinning for dce DRM buffersPradeep Venkatasubbarao2014-03-251-6/+0
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | Applications using dce_alloc/dce_free calls to manage memory, leaked memory because on non-closure of the created dmabuf fds. Additionally, all memory allocated from Tiler/DMM via DRM need to be explictly pinned to tiler using dce_buf_lock/dce_buf_unlock calls. Hence in the earlier implementation, every call to dce_alloc/free had to be followed by a lock/unlock call to pin/unpin it to tiler. In order, to insulate the applications from the internal details of DRM memory management and for ease of use of alloc and free calls, dce_alloc now takes care of creating the dmabuf and pinning it to tiler while dce_free takes care of tiler unpinning and closure of dmabuf fd. Applications can continue to use dce_alloc and dce_free calls as before thus maintiaining backward compatibility. On the other hand, since the same interfaces are used for multiple remote core targets, like IPU and DSP, MemHeader struture is upgraded to hold the core for which the block of memory belongs to, to keep track of the core. Hence all applications/Remote cores using this version of libdce should recompile with the new MemHeader for proper functioning. Dependent IPUMM patch: https://gerrit.ext.ti.com/gerrit/omap/#/c/12994/ Change-Id: If09a1039b5b16f3cc5ff0e9c6c598932d8a2ce3e Signed-off-by: Pradeep Venkatasubbarao <pradeepv@ti.com> Signed-off-by: Amarinder Bindra <a-bindra@ti.com> Signed-off-by: Karthik Ramanan <a0393906@ti.com>
* Added VIDDEC2 interfaces for DSP codecsPradeep Venkatasubbarao2013-12-031-3/+12
| | | | | | | | | | | This patch adds VIDDEC2 interfaces and libdce now supports both VIDDEC2 and VIDDEC3 interfaces. It initializes ipc based on the server name(IVA or DSP). Provisions are made to handle multiple instances of IPU and DSP codecs. Change-Id: Ie1869e626423a6250983711114dc9d0854022309 Signed-off-by: Pradeep Venkatasubbarao <pradeepv@ti.com>
* [DCE] Modify approach to pass parameters to IPCSaurabh Bipin Chandra2013-08-271-69/+8
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Three approaches were followed for IPC MmRpc calls. 1. All the parameters which need to be sent and received to/from IPU are coupled in a struct allocated from Shared/Tiler Memory. Only the adrress of the struct is passed to MmRpc as a pointer argument. This approach is useful as MmRpc in some cases to avoid multiple translations. This approach is followed for : Engine_open(), Engine_close(), create(), control(), delete() 2. All the parameters which need to be sent are given as separate arguments to MmRpc. This approach is needed when you need to translate an address which is ofsetted from a pointer which in itself needs to be translated. This apporach is followed for : process() For understanding, take the example of inbufs argument in process call(). Inbufs allocated in Shared memory and needs to be translated, has the address of Input buffer (allocated from Tiler). It is not possible to give the Input buffer as an argument to Mmrpc for translation until inbufs is given as a parameter to Mmrpc. Therefore inbuf can't be populated inside another Shared/Tiler memory struct. 3. This approach is a workaround to use approach [1] by solving the issue posed by [2]. This approach is followed for : get_version() Taking the example of inbufs to explain, the Input buffer address will be one of the parameters of the struct (explained in [1]) along with inbufs address. Therefore the Input buffer address will get translated here. At the IPU, this address needs to be copied back to inbufs. This patch aligns all DCE calls except Engine_Open to use Approach [2]. Engine_open still follows Approach [1] because: 1. Engine open takes in pointers to Engine_attrs and Error_code structures. The client may set both, none or either one of them to NULL (as allowed by CE). So that implies either I'll have to pass NULL as param_pointer to IPU or decide not to pass them at all. In the second case, I'll have to pass extra arguments to inform IPU that I have not passed Attrs or ErrorCode or both. I tried passing NULL but mmrpc_write failed. Dependent on ipumm patch: https://gerrit.ext.ti.com/gerrit/omap/#/c/12773 Change-Id: Ic770aaa99a56ea559efe9446e6e98d70726cc7c5 Signed-off-by: Saurabh Bipin Chandra <a0131926@ti.com>
* [libDCE] Add IPC 3.x Adapted code to Repository3.00.01.00Saurabh Bipin Chandra2013-04-261-0/+145
This patch adds libdce code to the repository. LibDCE has been adapted to use the MmRpc layer of IPC 3.x. This version of LibDCE is expected to work on QNX. Patchset 2 adds/modifies: 1. Removes Tiler 2D allocation/free for now. 2. Corrects memplugin_free() for Tiler 1D. 3. Modifies dce_test app to dump output till 30 frames. 4. Renamed dce.h to libdce.h. 5. Corrected header files across all files. 6. Build configuration for QNX 7. Removes build warnings. 8. Add README for Build instructions 9. Takes care of comments of Buddy and Pradeep. Patchset 3 adds/modifies: 1. Reduced Stack usage of each function. 2. Add ptr check in memplugin and remove from libdce. 3. Add DCE_Assert macros. 4. Add DCE_error_status enum. 5. Comments Cleanup 6. Make some functions static. 7. process() cleanup including removing reply_buf. 8. Add else if (for codec_type == Encoder type) 9. Converted Macros to Inline functions. 10.Converted init and deinit to dce_init and dce_deinit functions. 11. Removed dce_init() and dce_deinit() declarations Patchset 4 adds/modifies: 1. Assert Input function arguments. 2. Correct copyright year. 3. Correct memplugin_free for Shared memory. 4. Create dce_priv.h and move trace and assert macros to the header. 5. Redeclare mem_type enum and add mem_error_status enum in memplugin.h and make corresponding changes. 6. Add asserts in memplugin. Intention of some of the changes above is to move towards delinking Libdce and Memplugin. Patchset 5: 1. Missed to add dce_priv.h file. Patchset 6: 1. Take care Pradeep's comment. Change-Id: I6e5e37b7088362e7bad66200fc3454bb828e0eff Signed-off-by: Saurabh Bipin Chandra <a0131926@ti.com>