aboutsummaryrefslogtreecommitdiffstats
Commit message (Collapse)AuthorAgeFilesLines
* [LINUX] Fix for make installSathishkumar2013-09-051-1/+1
| | | | | | | | | | | | This patch fixes make install. All the required headers are copied to $(includedir)/dce on make install. Unused variables(X11 and WAYLAND) are removed in Makefile.am and pkg-config on libmmrpc is removed as no libmmrpc.pc is available. xdc_target_types__=gnu/targets/std.h is added to libdce.h, so that applications need not do it when using libdce.h. Change-Id: I8cc70aa2102becdbdc4c6b1e38e2aaa91739c4cc Signed-off-by: Sathishkumar <x0203598@ti.com>
* [GLP] Libdce linux implementationSathishkumar2013-08-271-0/+11
make install & libdce.c issue fix 1. make install has been fixed. libdce.h will be installed in /usr/include, libdce.so files in /usr/lib and libdce.pc in /usr/lib/pkgconfig on using --prefix=/usr. By default the prefix is /usr/local. 2. init and deinit calls are removed from libdce.h 3. dce_set_fd and dce_get_fd calls are implemented in libdce.c 4. configure.ac checks for libmmrpc and makefile.am modified to link with libmmrpc. configure.ac and makefile.am modified 1. Codec_engine,xdctolls,framework_components,ipc,xdctools and xdaias paths needs to be exported. Configure.ac checks for the exported paths. 2. Makefile.am is modified to have the exported paths in the include directories list for the compiler. Modifications done after review 1. Comments added in memplugin_linux.c. White spaces removed manually and cleaned up libdce.c, memplugin.h. dce_priv.h is modified to have File and line number in the logs. linux/dce.h file is removed. Libdce modifications for linux Linux Specific libdce functionality added. 1. memplugin calls specific to linux are added in memplugin_linux.c 2. Error and debug logs implementation for linux in dce_priv.h 3. xll and wayland specific files are moved to linux folder Change-Id: Ib41e6a52d902376cdabbb939dee7585944720d92 Signed-off-by: Saurabh Bipin Chandra <a0131926@ti.com> Signed-off-by: Sathishkumar <x0203598@ti.com>