aboutsummaryrefslogtreecommitdiffstats
Commit message (Collapse)AuthorAgeFilesLines
* libdce: Updated JpegEncoder interface fileVeeranna Hanchinal2017-02-071-40/+43
| | | | | | | | Updated MJPEGE header file due to MJPEGE codec update to 01.00.17.01 version. Change-Id: Id820f9cf3c66e1659564ba297cc469a30dc55732 Signed-off-by: Veeranna Hanchinal <veeranna.hanchinal@ti.com>
* libdce: add JPEG encoderHongmei Gou2016-11-092-1/+822
| | | | | Change-Id: I0136abd43fe8c1af3fedc5013dae578c8f6c7537 Signed-off-by: Hongmei Gou <h-gou@ti.com>
* Integration based on IPC 3.30.01.12Buddy Liong2014-11-192-3/+8
| | | | | | | | | | Integration with IPC 3.30.01.12 requires build tool update on XDC tool version to 3_30_xx_xx. Using the latest XDC Tools of 3_30_05_60_core Copying the header files used from 3_30_05_60 version. Change-Id: I648bfa945bcc0d8a43b4653d8f303cd9c18ee03f Signed-off-by: Buddy Liong <buddy.budiono@ti.com>
* README update3.00.06.00Buddy Liong2014-08-205-21/+21
| | | | | | | | | Integration with IPC 3.23.00.01 requires build tool update on XDC tool version to 3_25_06_96 Copying the header files used from 3_25_06_90 version. Change-Id: Ie1e6e167a9cfb42fde706fa06ba4dd5900db7483 Signed-off-by: Buddy Liong <buddy.budiono@ti.com>
* [LIBDCE] Clean up README and unsupported header files.buddy.liong2013-12-183-1830/+0
| | | | | | | | | | | Updating README on the version information of headers included in the packages folder. Removal of h264svcenc, h264svcvdec, and vc1enc header files since it is not supported in the current IPUMM. Change-Id: I2bb140604a7c7d6e4ba7482a11ac43bc5076d9f6 Signed-off-by: buddy.liong <buddy.budiono@ti.com>
* Added VIDDEC2 interfaces for DSP codecsPradeep Venkatasubbarao2013-12-034-0/+1033
| | | | | | | | | | | This patch adds VIDDEC2 interfaces and libdce now supports both VIDDEC2 and VIDDEC3 interfaces. It initializes ipc based on the server name(IVA or DSP). Provisions are made to handle multiple instances of IPU and DSP codecs. Change-Id: Ie1869e626423a6250983711114dc9d0854022309 Signed-off-by: Pradeep Venkatasubbarao <pradeepv@ti.com>
* [Linux] Makefile updated to export xdais/fc header3.00.03.02Chandramohan2013-09-271-0/+2
| | | | | | | | Makefile changes to export the framework component and xdais header files. Change-Id: I789c53d96ff43ed91bb70e0f774af5078a041365 Signed-off-by: Chandramohan <chandramohan.c@ti.com>
* [LIBDCE] Add TI License Header for the codec headersSunita Nadampalli2013-09-1310-0/+321
| | | | | Change-Id: I906358240c9e72529f80a1d13822cb0205d66caf Signed-off-by: Sunita Nadampalli <sunitan@ti.com>
* [LIBDCE] Update packages with XDAIS, FC HeadersSaurabh Bipin Chandra2013-09-054-0/+868
| | | | | | | | | This patch adds XDAIS, FC headers included by the codec header files and makes necessary build changes to include them. Change-Id: I6de3988291e6f4fa229b47a119431d83be1025c2 Signed-off-by: Saurabh Bipin Chandra <a0131926@ti.com>
* [LINUX] Fix for make installSathishkumar2013-09-054-0/+44
| | | | | | | | | | | | This patch fixes make install. All the required headers are copied to $(includedir)/dce on make install. Unused variables(X11 and WAYLAND) are removed in Makefile.am and pkg-config on libmmrpc is removed as no libmmrpc.pc is available. xdc_target_types__=gnu/targets/std.h is added to libdce.h, so that applications need not do it when using libdce.h. Change-Id: I8cc70aa2102becdbdc4c6b1e38e2aaa91739c4cc Signed-off-by: Sathishkumar <x0203598@ti.com>
* [QNX-MAKE] Include XDC, CE, XDAIS, IVAHD Headers from packagesSaurabh Bipin Chandra2013-09-051-0/+82
| | | | | | | | | | | This patch adds std.h from GNU and it directs the build system to include Codec Engine, XDCTools, XDAIS and IVAHD Codec Header files from the packages/ folder. This removes the need for libdce users to install these tools. Change-Id: I368a5aaff4c1edeaf6eae794bea9971787e036e3 Signed-off-by: Saurabh Bipin Chandra <a0131926@ti.com>
* [LIBDCE] Added codec, xdais and xdctools headersSunita Nadampalli2013-09-0529-0/+22088
This patch adds codec,xdais and xdctools headers for libdce compilation at HLOS level. Since HLOS code doesn't refer to the tools directly, this patch provides copy for all the required headers. Note# These headers need to be updated for every release if the tools versions are changed. Version Info of the added Headers: Tools: XDC version : xdctools_3_25_02_70 CE version : codec_engine_3_24_00_08 XDAIS version : xdais_7_24_00_04 IVAHD_Codecs: H.264 Dec : 02.00.13.00 MJPEG Dec : 01.00.11.01 MPEG-4 Dec : 01.00.13.00 VC-1 Dec : 01.00.00.11 MPEG-2 Dec : 01.00.12.00 SVC Dec : 00.06.00.00 H.264 Enc : 02.00.06.01 MJPEG Enc : 01.00.02.01 SVC Enc : 00.02.00.05 Change-Id: Id2307e2376d3ba0c13464c1b21cdba53d8f997f2 Signed-off-by: Sunita Nadampalli <sunitan@ti.com>