/* * Copyright (c) 2013, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ /* ********************************** Notes ****************************************** ******* ********************************* Memory ***************************************** * ******* ********************************* IPC 3.x ***************************************** * Two approaches are followed for IPC MmRpc calls. * 1. All the parameters which need to be sent and received to/from IPU are coupled in a struct * allocated from Shared Memory. Only the adrress of the struct is passed to MmRpc * as a pointer argument. This approach is useful as MmRpc in some cases to avoid multiple * translations. * This approach is followed for : * Engine_open(), Engine_close(), create(), control(), delete() * For understanding refer to the Mmrpc_test.c in IPC 3.x * 2. All the parameters which need to be sent are given as separate arguments to * MmRpc. This appraoch is needed when you need to translate an address which is * ofsetted from a pointer which in itself needs to be translated. * This apporach is followed for : process() * For understanding, take the example of inbufs argument in process call(). Inbufs * allocated in Shared memory and needs to be translated, has the address of Input * buffer (allocated from Tiler). It is not possible to give the Input buffer as an argument * to Mmrpc for translation until inbufs is given as a parameter to Mmrpc. Therefore inbuf * can't be populated inside another Shared memory struct. * 3. This approach is a workaround to use approach [1] by solving the issue posed by [2]. * This approach is followed for : get_version() * Taking the example of inbufs to explain, the Input buffer address will be one of the * parameters of the struct (explained in [1]) along with inbufs address. Therefore the * Input buffer address will get translated here. At the IPU, this address needs to be * copied back to inbufs. ********************************************************************************* */ #include #include #include #include #include #include #if defined(BUILDOS_GLP) #include #include #include #include #endif /* BUILDOS_GLP */ /* IPC Headers */ #include /*DCE Headers */ #include "libdce.h" #include "dce_rpc.h" #include "dce_priv.h" #include "memplugin.h" #if defined(BUILDOS_GLP) #ifdef GLP_X11 int dce_auth_x11(int *fd); #endif /* GLP_X11 */ #ifdef GLP_WAYLAND int dce_auth_wayland(int *fd); #endif /* GLP_WAYLAND */ static int fd = -1; static struct omap_device *dev; static int ioctl_base; #define CMD(name) (ioctl_base + DRM_OMAP_DCE_##name) uint32_t dce_debug = 3; #endif /* BUILDOS_GLP */ /********************* GLOBALS ***********************/ /* Hande used for Remote Communication */ static MmRpc_Handle MmRpcHandle = NULL; static pthread_mutex_t mutex = PTHREAD_MUTEX_INITIALIZER; static int count = 0; /****************** INLINE FUNCTIONS ********************/ static inline void Fill_MmRpc_fxnCtx(MmRpc_FxnCtx *fxnCtx, int fxn_id, int num_params, int num_xlts, MmRpc_Xlt *xltAry) { fxnCtx->fxn_id = fxn_id; fxnCtx->num_params = num_params; fxnCtx->num_xlts = num_xlts; fxnCtx->xltAry = xltAry; } static inline void Fill_MmRpc_fxnCtx_Ptr_Params(MmRpc_Param *mmrpc_params, int size, void *addr, void *handle) { mmrpc_params->type = MmRpc_ParamType_Ptr; mmrpc_params->param.ptr.size = size; mmrpc_params->param.ptr.addr = (size_t)addr; mmrpc_params->param.ptr.handle = (size_t)handle; } static inline void Fill_MmRpc_fxnCtx_Scalar_Params(MmRpc_Param *mmrpc_params, int size, int data) { mmrpc_params->type = MmRpc_ParamType_Scalar; mmrpc_params->param.scalar.size = size; mmrpc_params->param.scalar.data = (size_t)data; } static inline void Fill_MmRpc_fxnCtx_Xlt_Array(MmRpc_Xlt *mmrpc_xlt, int index, int32_t base, int32_t addr, void *handle) { /* index : index of params filled in FxnCtx */ /* offset : calculated from address of index */ mmrpc_xlt->index = index; mmrpc_xlt->offset = MmRpc_OFFSET(base, addr); mmrpc_xlt->handle = (size_t)handle; } /************************ FUNCTIONS **************************/ /* Interface for QNX for parameter buffer allocation */ /* These interfaces are implemented to maintain Backward Compatability */ void *dce_alloc(int sz) { return (memplugin_alloc(sz, 0, TILER_1D_BUFFER)); } void dce_free(void *ptr) { memplugin_free(ptr, TILER_1D_BUFFER); } /*************** Startup/Shutdown Functions ***********************/ static int dce_init(void) { dce_error_status eError = DCE_EOK; MmRpc_Params args; printf(" >> dce_init\n"); pthread_mutex_lock(&mutex); count++; /* Check if already Initialized */ _ASSERT(count == 1, DCE_EOK); /* Create remote server insance */ MmRpc_Params_init(&args); eError = MmRpc_create(DCE_DEVICE_NAME, &args, &MmRpcHandle); _ASSERT_AND_EXECUTE(eError == DCE_EOK, DCE_EIPC_CREATE_FAIL, count--); printf("open(/dev/" DCE_DEVICE_NAME ") -> 0x%x\n", (int)MmRpcHandle); EXIT: pthread_mutex_unlock(&mutex); return (eError); } static void dce_deinit(void) { pthread_mutex_lock(&mutex); count--; if( count > 0 ) { goto EXIT; } if( MmRpcHandle != NULL ) { MmRpc_delete(&MmRpcHandle); } MmRpcHandle = NULL; EXIT: pthread_mutex_unlock(&mutex); return; } /*===============================================================*/ /** Engine_open : Open Codec Engine. * * @ param attrs [in] : Engine Attributes. This param is not passed to Remote core. * @ param name [in] : Name of Encoder or Decoder codec. * @ param ec [out] : Error returned by Codec Engine. * @ return : Codec Engine Handle is returned to be used to create codec. * In case of error, NULL is returned as Engine Handle. */ Engine_Handle Engine_open(String name, Engine_Attrs *attrs, Engine_Error *ec) { MmRpc_FxnCtx fxnCtx; int32_t fxnRet; dce_error_status eError = DCE_EOK; dce_engine_open *engine_open_msg = NULL; Engine_Handle eng_handle = NULL; _ASSERT(name != '\0', DCE_EINVALID_INPUT); /* Initialize DCE and IPC. In case of Error Deinitialize them */ _ASSERT_AND_EXECUTE(dce_init() == DCE_EOK, DCE_EIPC_CREATE_FAIL, dce_deinit()); printf(">> Engine_open Params::name = %s size = %d\n", name, strlen(name)); /* Allocate Shared memory for the engine_open rpc msg structure*/ /* Tiler Memory preferred for now for First level testing */ engine_open_msg = memplugin_alloc(sizeof(dce_engine_open), 0, TILER_1D_BUFFER); _ASSERT_AND_EXECUTE(engine_open_msg != NULL, DCE_EOUT_OF_MEMORY, eng_handle = NULL); /* Populating the msg structure with all the params */ /* Populating all params into a struct avoid individual address translations of name, ec */ strncpy(engine_open_msg->name, name, strlen(name)); engine_open_msg->eng_handle = NULL; /* Marshall function arguments into the send buffer */ Fill_MmRpc_fxnCtx(&fxnCtx, DCE_RPC_ENGINE_OPEN, 1, 0, NULL); Fill_MmRpc_fxnCtx_Ptr_Params(fxnCtx.params, sizeof(dce_engine_open), engine_open_msg, NULL); /* Invoke the Remote function through MmRpc */ eError = MmRpc_call(MmRpcHandle, &fxnCtx, &fxnRet); /* In case of Error, the Application will get a NULL Engine Handle */ _ASSERT_AND_EXECUTE(eError == DCE_EOK, DCE_EIPC_CALL_FAIL, eng_handle = NULL); /* Populate return arguments */ eng_handle = engine_open_msg->eng_handle; ec[0] = engine_open_msg->error_code; EXIT: memplugin_free(engine_open_msg, TILER_1D_BUFFER); return (eng_handle); } /*===============================================================*/ /** Engine_close : Close Engine. * * @ param engine [in] : Engine Handle obtained in Engine_open() call. */ Void Engine_close(Engine_Handle engine) { MmRpc_FxnCtx fxnCtx; int32_t fxnRet; dce_error_status eError = DCE_EOK; dce_engine_close *engine_close_msg = NULL; _ASSERT(engine != NULL, DCE_EINVALID_INPUT); /* Allocate Shared/Tiler memory for the engine_close rpc msg structure*/ engine_close_msg = memplugin_alloc(sizeof(dce_engine_close), 0, TILER_1D_BUFFER); _ASSERT(engine_close_msg != NULL, DCE_EOUT_OF_MEMORY); /* Populating the msg structure with all the params */ engine_close_msg->eng_handle = engine; /* Marshall function arguments into the send buffer */ Fill_MmRpc_fxnCtx(&fxnCtx, DCE_RPC_ENGINE_CLOSE, 1, 0, NULL); Fill_MmRpc_fxnCtx_Ptr_Params(fxnCtx.params, sizeof(dce_engine_close), engine_close_msg, NULL); /* Invoke the Remote function through MmRpc */ eError = MmRpc_call(MmRpcHandle, &fxnCtx, &fxnRet); _ASSERT(eError == DCE_EOK, DCE_EIPC_CALL_FAIL); EXIT: memplugin_free(engine_close_msg, TILER_1D_BUFFER); dce_deinit(); return; } /*===============================================================*/ /** Functions create(), control(), get_version(), process(), delete() are common codec * glue function signatures which are same for both encoder and decoder */ /*===============================================================*/ /** create : Create Encoder/Decoder codec. * * @ param engine [in] : Engine Handle obtained in Engine_open() call. * @ param name [in] : Name of Encoder or Decoder codec. * @ param params [in] : Static parameters of codec. * @ param codec_id [in] : To differentiate between Encoder and Decoder codecs. * @ return : Codec Handle is returned to be used for control, process, delete calls. * In case of error, NULL is returned. */ static void *create(Engine_Handle engine, String name, void *params, dce_codec_type codec_id) { MmRpc_FxnCtx fxnCtx; MmRpc_Xlt xltAry; int32_t fxnRet; dce_error_status eError = DCE_EOK; dce_codec_create *codec_create_msg = NULL; void *codec_handle = NULL; _ASSERT(name != '\0', DCE_EINVALID_INPUT); _ASSERT(engine != NULL, DCE_EINVALID_INPUT); _ASSERT(params != NULL, DCE_EINVALID_INPUT); /* Allocate Shared/Tiler memory for the codec_create rpc msg structure*/ codec_create_msg = memplugin_alloc(sizeof(dce_codec_create), 0, TILER_1D_BUFFER); _ASSERT_AND_EXECUTE(codec_create_msg != NULL, DCE_EOUT_OF_MEMORY, codec_handle = NULL); /* Populating the msg structure with all the params */ codec_create_msg->engine = engine; strncpy(codec_create_msg->codec_name, name, strlen(name)); codec_create_msg->codec_id = codec_id; codec_create_msg->codec_handle = NULL; codec_create_msg->static_params = params; /* Marshall function arguments into the send buffer */ Fill_MmRpc_fxnCtx(&fxnCtx, DCE_RPC_CODEC_CREATE, 1, 1, &xltAry); Fill_MmRpc_fxnCtx_Ptr_Params(&(fxnCtx.params[0]), sizeof(dce_codec_create), codec_create_msg, NULL); /* Mention the virtual pointers that need translation */ /* Allocations through dce_alloc need translation */ /* In this case the static params buffer need translation */ Fill_MmRpc_fxnCtx_Xlt_Array(fxnCtx.xltAry, 0, (int32_t)codec_create_msg, (int32_t)&(codec_create_msg->static_params), NULL); /* Invoke the Remote function through MmRpc */ eError = MmRpc_call(MmRpcHandle, &fxnCtx, &fxnRet); /* In case of Error, the Application will get a NULL Codec Handle */ _ASSERT_AND_EXECUTE(eError == DCE_EOK, DCE_EIPC_CALL_FAIL, codec_handle = NULL); codec_handle = codec_create_msg->codec_handle; EXIT: memplugin_free(codec_create_msg, TILER_1D_BUFFER); return (codec_handle); } /*===============================================================*/ /** control : Codec control call. * * @ param codec [in] : Codec Handle obtained in create() call. * @ param id [in] : Command id for XDM control operation. * @ param dynParams [in] : Dynamic input parameters to Codec. * @ param status [out] : Codec returned status parameters. * @ param codec_id [in] : To differentiate between Encoder and Decoder codecs. * @ return : Status of control() call is returned. * #XDM_EOK [0] : Success. * #XDM_EFAIL [-1] : Failure. * #IPC_FAIL [-2] : MmRpc Call failed. * #XDM_EUNSUPPORTED [-3] : Unsupported request. * #OUT_OF_MEMORY [-4] : Out of Shared Memory. */ static XDAS_Int32 control(void *codec, int id, void *dynParams, void *status, dce_codec_type codec_id) { MmRpc_FxnCtx fxnCtx; MmRpc_Xlt xltAry[2]; int32_t fxnRet; dce_error_status eError = DCE_EOK; dce_codec_control *codec_control_msg = NULL; _ASSERT(codec != NULL, DCE_EINVALID_INPUT); _ASSERT(dynParams != NULL, DCE_EINVALID_INPUT); _ASSERT(status != NULL, DCE_EINVALID_INPUT); /* Allocate Shared/Tiler memory for the codec_control rpc msg structure*/ codec_control_msg = memplugin_alloc(sizeof(dce_codec_control), 0, TILER_1D_BUFFER); _ASSERT(codec_control_msg != NULL, DCE_EOUT_OF_MEMORY); /* Populating the msg structure with all the params */ codec_control_msg->codec_handle = codec; codec_control_msg->cmd_id = id; codec_control_msg->codec_id = codec_id; codec_control_msg->dyn_params = dynParams; codec_control_msg->status = status; /* Marshall function arguments into the send buffer */ Fill_MmRpc_fxnCtx(&fxnCtx, DCE_RPC_CODEC_CONTROL, 1, 2, xltAry); Fill_MmRpc_fxnCtx_Ptr_Params(fxnCtx.params, sizeof(dce_codec_control), codec_control_msg, NULL); /* Dynamic and status params buffer need translation */ Fill_MmRpc_fxnCtx_Xlt_Array(fxnCtx.xltAry, 0, (int32_t)codec_control_msg, (int32_t)&(codec_control_msg->dyn_params), NULL); Fill_MmRpc_fxnCtx_Xlt_Array(&(fxnCtx.xltAry[1]), 0, (int32_t)codec_control_msg, (int32_t)&(codec_control_msg->status), NULL); /* Invoke the Remote function through MmRpc */ eError = MmRpc_call(MmRpcHandle, &fxnCtx, &fxnRet); _ASSERT(eError == DCE_EOK, DCE_EIPC_CALL_FAIL); eError = codec_control_msg->result; EXIT: memplugin_free(codec_control_msg, TILER_1D_BUFFER); return (eError); } /*===============================================================*/ /** get_version : Codec control call to get the codec version. This call has been made * separate from control call because it involves an additional version * buffer translation. * * @ param codec [in] : Codec Handle obtained in create() call. * @ param id [in] : Command id for XDM control operation. * @ param dynParams [in] : Dynamic input parameters to Codec. * @ param status [out] : Codec returned status parameters. * @ param codec_id [in] : To differentiate between Encoder and Decoder codecs. * @ return : Status of control() call is returned. * #XDM_EOK [0] : Success. * #XDM_EFAIL [-1] : Failure. * #IPC_FAIL [-2] : MmRpc Call failed. * #XDM_EUNSUPPORTED [-3] : Unsupported request. * #OUT_OF_MEMORY [-4] : Out of Shared Memory. */ static XDAS_Int32 get_version(void *codec, void *dynParams, void *status, dce_codec_type codec_id) { MmRpc_FxnCtx fxnCtx; MmRpc_Xlt xltAry[3]; int32_t fxnRet; dce_error_status eError = DCE_EOK; dce_codec_get_version *codec_get_version_msg = NULL; _ASSERT(codec != NULL, DCE_EINVALID_INPUT); _ASSERT(dynParams != NULL, DCE_EINVALID_INPUT); _ASSERT(status != NULL, DCE_EINVALID_INPUT); /* Allocate Shared/Tiler memory for the codec_get_version rpc msg structure*/ codec_get_version_msg = memplugin_alloc(sizeof(dce_codec_get_version), 0, TILER_1D_BUFFER); _ASSERT(codec_get_version_msg != NULL, DCE_EOUT_OF_MEMORY); /* Populating the msg structure with all the params */ codec_get_version_msg->codec_handle = codec; codec_get_version_msg->codec_id = codec_id; codec_get_version_msg->dyn_params = dynParams; codec_get_version_msg->status = status; if( codec_id == OMAP_DCE_VIDDEC3 ) { codec_get_version_msg->version = ((IVIDDEC3_Status *)status)->data.buf; } else if( codec_id == OMAP_DCE_VIDENC2 ) { codec_get_version_msg->version = ((IVIDDEC3_Status *)status)->data.buf; } /* Marshall function arguments into the send buffer */ Fill_MmRpc_fxnCtx(&fxnCtx, DCE_RPC_CODEC_CONTROL, 1, 3, xltAry); Fill_MmRpc_fxnCtx_Ptr_Params(fxnCtx.params, sizeof(dce_codec_get_version), codec_get_version_msg, NULL); /* Dynamic, status params and version info buffer need translation */ Fill_MmRpc_fxnCtx_Xlt_Array(fxnCtx.xltAry, 0, (int32_t)codec_get_version_msg, (int32_t)&(codec_get_version_msg->dyn_params), NULL); Fill_MmRpc_fxnCtx_Xlt_Array(&(fxnCtx.xltAry[1]), 0, (int32_t)codec_get_version_msg, (int32_t)&(codec_get_version_msg->status), NULL); Fill_MmRpc_fxnCtx_Xlt_Array(&(fxnCtx.xltAry[2]), 0, (int32_t)codec_get_version_msg, (int32_t)&(codec_get_version_msg->version), NULL); /* Invoke the Remote function through MmRpc */ eError = MmRpc_call(MmRpcHandle, &fxnCtx, &fxnRet); _ASSERT(eError == DCE_EOK, DCE_EIPC_CALL_FAIL); eError = codec_get_version_msg->result; EXIT: memplugin_free(codec_get_version_msg, TILER_1D_BUFFER); return (eError); } typedef enum process_call_params { CODEC_HANDLE_INDEX = 0, INBUFS_INDEX, OUTBUFS_INDEX, INARGS_INDEX, OUTARGS_INDEX, CODEC_ID_INDEX } process_call_params; /*===============================================================*/ /** process : Encode/Decode process. * * @ param codec [in] : Codec Handle obtained in create() call. * @ param inBufs [in] : Input buffer details. * @ param outBufs [in] : Output buffer details. * @ param inArgs [in] : Input arguments. * @ param outArgs [out] : Output arguments. * @ param codec_id [in] : To differentiate between Encoder and Decoder codecs. * @ return : Status of the process call. * #XDM_EOK [0] : Success. * #XDM_EFAIL [-1] : Failure. * #IPC_FAIL [-2] : MmRpc Call failed. * #XDM_EUNSUPPORTED [-3] : Unsupported request. */ static XDAS_Int32 process(void *codec, void *inBufs, void *outBufs, void *inArgs, void *outArgs, dce_codec_type codec_id) { MmRpc_FxnCtx fxnCtx; MmRpc_Xlt xltAry[MAX_TOTAl_BUF]; int fxnRet, count, total_count, numInBufs = 0, numOutBufs = 0, sz[5] = { 0 }; dce_error_status eError = DCE_EOK; _ASSERT(codec != NULL, DCE_EINVALID_INPUT); _ASSERT(inBufs != NULL, DCE_EINVALID_INPUT); _ASSERT(outBufs != NULL, DCE_EINVALID_INPUT); _ASSERT(inArgs != NULL, DCE_EINVALID_INPUT); _ASSERT(outArgs != NULL, DCE_EINVALID_INPUT); if( codec_id == OMAP_DCE_VIDDEC3 ) { numInBufs = ((XDM2_BufDesc *)inBufs)->numBufs; numOutBufs = ((XDM2_BufDesc *)outBufs)->numBufs; sz[INBUFS_INDEX] = sizeof(XDM2_BufDesc); sz[OUTBUFS_INDEX] = sizeof(XDM2_BufDesc); sz[INARGS_INDEX] = sizeof(VIDDEC3_InArgs); sz[OUTARGS_INDEX] = sizeof(VIDDEC3_OutArgs); } else if( codec_id == OMAP_DCE_VIDENC2 ) { numInBufs = ((IVIDEO2_BufDesc *)inBufs)->numPlanes; numOutBufs = ((XDM2_BufDesc *)outBufs)->numBufs; sz[INBUFS_INDEX] = sizeof(IVIDEO2_BufDesc); sz[OUTBUFS_INDEX] = sizeof(XDM2_BufDesc); sz[INARGS_INDEX] = sizeof(VIDENC2_InArgs); sz[OUTARGS_INDEX] = sizeof(VIDENC2_OutArgs); } /* marshall function arguments into the send buffer */ /* Approach [2] as explained in "Notes" used for process */ Fill_MmRpc_fxnCtx(&fxnCtx, DCE_RPC_CODEC_PROCESS, 6, numInBufs + numOutBufs, xltAry); Fill_MmRpc_fxnCtx_Scalar_Params(&(fxnCtx.params[CODEC_HANDLE_INDEX]), sizeof(int32_t), (int32_t)codec); Fill_MmRpc_fxnCtx_Ptr_Params(&(fxnCtx.params[INBUFS_INDEX]), sz[INBUFS_INDEX], inBufs, NULL); Fill_MmRpc_fxnCtx_Ptr_Params(&(fxnCtx.params[OUTBUFS_INDEX]), sz[OUTBUFS_INDEX], outBufs, NULL); Fill_MmRpc_fxnCtx_Ptr_Params(&(fxnCtx.params[INARGS_INDEX]), sz[INARGS_INDEX], inArgs, NULL); Fill_MmRpc_fxnCtx_Ptr_Params(&(fxnCtx.params[OUTARGS_INDEX]), sz[OUTARGS_INDEX], outArgs, NULL); Fill_MmRpc_fxnCtx_Scalar_Params(&(fxnCtx.params[CODEC_ID_INDEX]), sizeof(int32_t), codec_id); /* InBufs, OutBufs, InArgs, OutArgs buffer need translation but since they have been */ /* individually mentioned as fxnCtx Params, they need not be mentioned below again */ /* Input and Output Buffers have to be mentioned for translation */ for( count = 0, total_count = 0; count < numInBufs; count++, total_count++ ) { if( codec_id == OMAP_DCE_VIDDEC3 ) { Fill_MmRpc_fxnCtx_Xlt_Array(&(fxnCtx.xltAry[total_count]), INBUFS_INDEX, (int32_t)inBufs, (int32_t)&(((XDM2_BufDesc *)inBufs)->descs[count].buf), NULL); } else if( codec_id == OMAP_DCE_VIDENC2 ) { Fill_MmRpc_fxnCtx_Xlt_Array(&(fxnCtx.xltAry[total_count]), INBUFS_INDEX, (int32_t)inBufs, (int32_t)&(((IVIDEO2_BufDesc *)inBufs)->planeDesc[count].buf), NULL); } } for( count = 0; count < numOutBufs; count++, total_count++ ) { Fill_MmRpc_fxnCtx_Xlt_Array(&(fxnCtx.xltAry[total_count]), OUTBUFS_INDEX, (int32_t)outBufs, (int32_t)&(((XDM2_BufDesc *)outBufs)->descs[count].buf), NULL); } /* Invoke the Remote function through MmRpc */ eError = MmRpc_call(MmRpcHandle, &fxnCtx, &fxnRet); _ASSERT(eError == DCE_EOK, DCE_EIPC_CALL_FAIL); eError = (dce_error_status)(fxnRet); EXIT: return (eError); } /*===============================================================*/ /** delete : Delete Encode/Decode codec instance. * * @ param codec [in] : Codec Handle obtained in create() call. * @ param codec_id [in] : To differentiate between Encoder and Decoder codecs. * @ return : NIL. */ static void delete(void *codec, dce_codec_type codec_id) { MmRpc_FxnCtx fxnCtx; int32_t fxnRet; dce_error_status eError = DCE_EOK; dce_codec_delete *codec_delete_msg = NULL; _ASSERT(codec != NULL, DCE_EINVALID_INPUT); /* Allocate Shared/Tiler memory for the codec_delete rpc msg structure*/ codec_delete_msg = memplugin_alloc(sizeof(dce_codec_delete), 0, TILER_1D_BUFFER); _ASSERT(codec_delete_msg != NULL, DCE_EOUT_OF_MEMORY); /* Populating the msg structure with all the params */ codec_delete_msg->codec_handle = codec; codec_delete_msg->codec_id = codec_id; /* Marshall function arguments into the send buffer */ Fill_MmRpc_fxnCtx(&fxnCtx, DCE_RPC_CODEC_DELETE, 1, 0, NULL); Fill_MmRpc_fxnCtx_Ptr_Params(fxnCtx.params, sizeof(dce_codec_delete), codec_delete_msg, NULL); /* Invoke the Remote function through MmRpc */ eError = MmRpc_call(MmRpcHandle, &fxnCtx, &fxnRet); _ASSERT(eError == DCE_EOK, DCE_EIPC_CALL_FAIL); EXIT: memplugin_free(codec_delete_msg, TILER_1D_BUFFER); return; } /*************** Deocder Codec Engine Functions ***********************/ VIDDEC3_Handle VIDDEC3_create(Engine_Handle engine, String name, VIDDEC3_Params *params) { VIDDEC3_Handle codec; DEBUG(">> engine=%p, name=%s, params=%p", engine, name, params); codec = create(engine, name, params, OMAP_DCE_VIDDEC3); DEBUG("<< codec=%p", codec); return (codec); } XDAS_Int32 VIDDEC3_control(VIDDEC3_Handle codec, VIDDEC3_Cmd id, VIDDEC3_DynamicParams *dynParams, VIDDEC3_Status *status) { XDAS_Int32 ret; DEBUG(">> codec=%p, id=%d, dynParams=%p, status=%p", codec, id, dynParams, status); if( id == XDM_GETVERSION ) { ret = get_version(codec, dynParams, status, OMAP_DCE_VIDDEC3); } else { ret = control(codec, id, dynParams, status, OMAP_DCE_VIDDEC3); } DEBUG("<< ret=%d", ret); return (ret); } XDAS_Int32 VIDDEC3_process(VIDDEC3_Handle codec, XDM2_BufDesc *inBufs, XDM2_BufDesc *outBufs, VIDDEC3_InArgs *inArgs, VIDDEC3_OutArgs *outArgs) { XDAS_Int32 ret; DEBUG(">> codec=%p, inBufs=%p, outBufs=%p, inArgs=%p, outArgs=%p", codec, inBufs, outBufs, inArgs, outArgs); ret = process(codec, inBufs, outBufs, inArgs, outArgs, OMAP_DCE_VIDDEC3); DEBUG("<< ret=%d", ret); return (ret); } Void VIDDEC3_delete(VIDDEC3_Handle codec) { DEBUG(">> codec=%p", codec); delete(codec, OMAP_DCE_VIDDEC3); DEBUG("<<"); } /*************** Enocder Codec Engine Functions ***********************/ VIDENC2_Handle VIDENC2_create(Engine_Handle engine, String name, VIDENC2_Params *params) { VIDENC2_Handle codec; DEBUG(">> engine=%p, name=%s, params=%p", engine, name, params); codec = create(engine, name, params, OMAP_DCE_VIDENC2); DEBUG("<< codec=%p", codec); return (codec); } XDAS_Int32 VIDENC2_control(VIDENC2_Handle codec, VIDENC2_Cmd id, VIDENC2_DynamicParams *dynParams, VIDENC2_Status *status) { XDAS_Int32 ret; DEBUG(">> codec=%p, id=%d, dynParams=%p, status=%p", codec, id, dynParams, status); ret = control(codec, id, dynParams, status, OMAP_DCE_VIDENC2); DEBUG("<< ret=%d", ret); return (ret); } XDAS_Int32 VIDENC2_process(VIDENC2_Handle codec, IVIDEO2_BufDesc *inBufs, XDM2_BufDesc *outBufs, VIDENC2_InArgs *inArgs, VIDENC2_OutArgs *outArgs) { XDAS_Int32 ret; DEBUG(">> codec=%p, inBufs=%p, outBufs=%p, inArgs=%p, outArgs=%p", codec, inBufs, outBufs, inArgs, outArgs); ret = process(codec, inBufs, outBufs, inArgs, outArgs, OMAP_DCE_VIDENC2); DEBUG("<< ret=%d", ret); return (ret); } Void VIDENC2_delete(VIDENC2_Handle codec) { DEBUG(">> codec=%p", codec); delete(codec, OMAP_DCE_VIDENC2); DEBUG("<<"); }