/*
* (C) Copyright 2000-2009
* Wolfgang Denk, DENX Software Engineering, wd@denx.de.
*
* See file CREDITS for list of people who contributed to this
* project.
*
* This program is free software; you can redistribute it and/or
* modify it under the terms of the GNU General Public License as
* published by the Free Software Foundation; either version 2 of
* the License, or (at your option) any later version.
*
* This program is distributed in the hope that it will be useful,
* but WITHOUT ANY WARRANTY; without even the implied warranty of
* MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
* GNU General Public License for more details.
*
* You should have received a copy of the GNU General Public License
* along with this program; if not, write to the Free Software
* Foundation, Inc., 59 Temple Place, Suite 330, Boston,
* MA 02111-1307 USA
*/
/*
* Definitions for Command Processor
*/
#ifndef __COMMAND_H
#define __COMMAND_H
#include <config.h>
#include <linker_lists.h>
#ifndef NULL
#define NULL 0
#endif
/* Default to a width of 8 characters for help message command width */
#ifndef CONFIG_SYS_HELP_CMD_WIDTH
#define CONFIG_SYS_HELP_CMD_WIDTH 8
#endif
#ifndef __ASSEMBLY__
/*
* Monitor Command Table
*/
struct cmd_tbl_s {
char *name; /* Command Name */
int maxargs; /* maximum number of arguments */
int repeatable; /* autorepeat allowed? */
/* Implementation function */
int (*cmd)(struct cmd_tbl_s *, int, int, char * const []);
char *usage; /* Usage message (short) */
#ifdef CONFIG_SYS_LONGHELP
char *help; /* Help message (long) */
#endif
#ifdef CONFIG_AUTO_COMPLETE
/* do auto completion on the arguments */
int (*complete)(int argc, char * const argv[], char last_char, int maxv, char *cmdv[]);
#endif
};
typedef struct cmd_tbl_s cmd_tbl_t;
#if defined(CONFIG_CMD_RUN)
extern int do_run(cmd_tbl_t *cmdtp, int flag, int argc, char * const argv[]);
#endif
/* common/command.c */
int _do_help (cmd_tbl_t *cmd_start, int cmd_items, cmd_tbl_t * cmdtp, int
flag, int argc, char * const argv[]);
cmd_tbl_t *find_cmd(const char *cmd);
cmd_tbl_t *find_cmd_tbl (const char *cmd, cmd_tbl_t *table, int table_len);
extern int cmd_usage(const cmd_tbl_t *cmdtp);
#ifdef CONFIG_AUTO_COMPLETE
extern int var_complete(int argc, char * const argv[], char last_char, int maxv, char *cmdv[]);
extern int cmd_auto_complete(const char *const prompt, char *buf, int *np, int *colp);
#endif
/*
* Monitor Command
*
* All commands use a common argument format:
*
* void function (cmd_tbl_t *cmdtp, int flag, int argc, char * const argv[]);
*/
#if defined(CONFIG_CMD_MEMORY) \
|| defined(CONFIG_CMD_I2C) \
|| defined(CONFIG_CMD_ITEST) \
|| defined(CONFIG_CMD_PCI) \
|| defined(CONFIG_CMD_PORTIO)
#define CMD_DATA_SIZE
extern int cmd_get_data_size(char* arg, int default_size);
#endif
#ifdef CONFIG_CMD_BOOTD
extern int do_bootd(cmd_tbl_t *cmdtp, int flag, int argc, char * const argv[]);
#endif
#ifdef CONFIG_CMD_BOOTM
extern int do_bootm(cmd_tbl_t *cmdtp, int flag, int argc, char * const argv[]);
extern int bootm_maybe_autostart(cmd_tbl_t *cmdtp, const char *cmd);
#else
static inline int bootm_maybe_autostart(cmd_tbl_t *cmdtp, const char *cmd)
{
return 0;
}
#endif
extern int common_diskboot(cmd_tbl_t *cmdtp, const char *intf, int argc,
char *const argv[]);
extern int do_reset(cmd_tbl_t *cmdtp, int flag, int argc, char * const argv[]);
/*
* Error codes that commands return to cmd_process(). We use the standard 0
* and 1 for success and failure, but add one more case - failure with a
* request to call cmd_usage(). But the cmd_process() function handles
* CMD_RET_USAGE itself and after calling cmd_usage() it will return 1.
* This is just a convenience for commands to avoid them having to call
* cmd_usage() all over the place.
*/
enum command_ret_t {
CMD_RET_SUCCESS, /* 0 = Success */
CMD_RET_FAILURE, /* 1 = Failure */
CMD_RET_USAGE = -1, /* Failure, please report 'usage' error */
};
/**
* Process a command with arguments. We look up the command and execute it
* if valid. Otherwise we print a usage message.
*
* @param flag Some flags normally 0 (see CMD_FLAG_.. above)
* @param argc Number of arguments (arg 0 must be the command text)
* @param argv Arguments
* @param repeatable This function sets this to 0 if the command is not
* repeatable. If the command is repeatable, the value
* is left unchanged.
* @param ticks If ticks is not null, this function set it to the
* number of ticks the command took to complete.
* @return 0 if the command succeeded, 1 if it failed
*/
int cmd_process(int flag, int argc, char * const argv[],
int *repeatable, unsigned long *ticks);
#endif /* __ASSEMBLY__ */
/*
* Command Flags:
*/
#define CMD_FLAG_REPEAT 0x0001 /* repeat last command */
#define CMD_FLAG_BOOTD 0x0002 /* command is from bootd */
#ifdef CONFIG_AUTO_COMPLETE
# define _CMD_COMPLETE(x) x,
#else
# define _CMD_COMPLETE(x)
#endif
#ifdef CONFIG_SYS_LONGHELP
# define _CMD_HELP(x) x,
#else
# define _CMD_HELP(x)
#endif
#define U_BOOT_CMD_MKENT_COMPLETE(_name, _maxargs, _rep, _cmd, \
_usage, _help, _comp) \
{ #_name, _maxargs, _rep, _cmd, _usage, \
_CMD_HELP(_help) _CMD_COMPLETE(_comp) }
#define U_BOOT_CMD_MKENT(_name, _maxargs, _rep, _cmd, _usage, _help) \
U_BOOT_CMD_MKENT_COMPLETE(_name, _maxargs, _rep, _cmd, \
_usage, _help, NULL)
#define U_BOOT_CMD_COMPLETE(_name, _maxargs, _rep, _cmd, _usage, _help, _comp) \
ll_entry_declare(cmd_tbl_t, _name, cmd) = \
U_BOOT_CMD_MKENT_COMPLETE(_name, _maxargs, _rep, _cmd, \
_usage, _help, _comp);
#define U_BOOT_CMD(_name, _maxargs, _rep, _cmd, _usage, _help) \
U_BOOT_CMD_COMPLETE(_name, _maxargs, _rep, _cmd, _usage, _help, NULL)
#if defined(CONFIG_NEEDS_MANUAL_RELOC)
void fixup_cmdtable(cmd_tbl_t *cmdtp, int size);
#endif
#endif /* __COMMAND_H */