aboutsummaryrefslogblamecommitdiffstats
blob: 5ba99e35a2e1a66a8d773ad4f1c11c22b0f74031 (plain) (tree)





































































                                                                                              

                                                                         



                                                                                     

                                                                          







                                                                         
                                                                 


                                                                                            
                                                                               





























                                                                                
/*
 *	include/linux/pc_keyb.h
 *
 *	PC Keyboard And Keyboard Controller
 *
 *	(c) 1997 Martin Mares <mj@atrey.karlin.mff.cuni.cz>
 */

/*
 *	Configuration Switches
 */
#undef KBD_REPORT_ERR			/* Report keyboard errors */
#define KBD_REPORT_UNKN			/* Report unknown scan codes */
#define KBD_REPORT_TIMEOUTS		/* Report keyboard timeouts */
#undef KBD_IS_FOCUS_9000		/* We have the brain-damaged FOCUS-9000 keyboard */
#undef INITIALIZE_MOUSE			/* Define if your PS/2 mouse needs initialization. */

#define KBD_INIT_TIMEOUT 1000		/* Timeout in ms for initializing the keyboard */
#define KBC_TIMEOUT 250			/* Timeout in ms for sending to keyboard controller */
#define KBD_TIMEOUT 1000		/* Timeout in ms for keyboard command acknowledge */

/*
 *	Internal variables of the driver
 */
extern unsigned char pckbd_read_mask;
extern unsigned char aux_device_present;

/*
 *	Keyboard Controller Registers on normal PCs.
 */
#define KBD_STATUS_REG		0x64	/* Status register (R) */
#define KBD_CNTL_REG		0x64	/* Controller command register (W) */
#define KBD_DATA_REG		0x60	/* Keyboard data register (R/W) */

/*
 *	Keyboard Controller Commands
 */
#define KBD_CCMD_READ_MODE	0x20	/* Read mode bits */
#define KBD_CCMD_WRITE_MODE	0x60	/* Write mode bits */
#define KBD_CCMD_GET_VERSION	0xA1	/* Get controller version */
#define KBD_CCMD_MOUSE_DISABLE	0xA7	/* Disable mouse interface */
#define KBD_CCMD_MOUSE_ENABLE	0xA8	/* Enable mouse interface */
#define KBD_CCMD_TEST_MOUSE	0xA9	/* Mouse interface test */
#define KBD_CCMD_SELF_TEST	0xAA	/* Controller self test */
#define KBD_CCMD_KBD_TEST	0xAB	/* Keyboard interface test */
#define KBD_CCMD_KBD_DISABLE	0xAD	/* Keyboard interface disable */
#define KBD_CCMD_KBD_ENABLE	0xAE	/* Keyboard interface enable */
#define KBD_CCMD_WRITE_AUX_OBUF	0xD3    /* Write to output buffer as if
					   initiated by the auxiliary device */
#define KBD_CCMD_WRITE_MOUSE	0xD4	/* Write the following byte to the mouse */

/*
 *	Keyboard Commands
 */
#define KBD_CMD_SET_LEDS	0xED	/* Set keyboard leds */
#define KBD_CMD_SET_RATE	0xF3	/* Set typematic rate */
#define KBD_CMD_ENABLE		0xF4	/* Enable scanning */
#define KBD_CMD_DISABLE		0xF5	/* Disable scanning */
#define KBD_CMD_RESET		0xFF	/* Reset */

/*
 *	Keyboard Replies
 */
#define KBD_REPLY_POR		0xAA	/* Power on reset */
#define KBD_REPLY_ACK		0xFA	/* Command ACK */
#define KBD_REPLY_RESEND	0xFE	/* Command NACK, send the cmd again */

/*
 *	Status Register Bits
 */
#define KBD_STAT_OBF		0x01	/* Keyboard output buffer full */
#define KBD_STAT_IBF		0x02	/* Keyboard input buffer full */
#define KBD_STAT_SELFTEST	0x04	/* Self test successful */
#define KBD_STAT_CMD		0x08	/* Last write was a command write (0=data) */
#define KBD_STAT_UNLOCKED	0x10	/* Zero if keyboard locked */
#define KBD_STAT_MOUSE_OBF	0x20	/* Mouse output buffer full */
#define KBD_STAT_GTO		0x40	/* General receive/xmit timeout */
#define KBD_STAT_PERR		0x80	/* Parity error */

#define AUX_STAT_OBF (KBD_STAT_OBF | KBD_STAT_MOUSE_OBF)

/*
 *	Controller Mode Register Bits
 */
#define KBD_MODE_KBD_INT	0x01	/* Keyboard data generate IRQ1 */
#define KBD_MODE_MOUSE_INT	0x02	/* Mouse data generate IRQ12 */
#define KBD_MODE_SYS		0x04	/* The system flag (?) */
#define KBD_MODE_NO_KEYLOCK	0x08	/* The keylock doesn't affect the keyboard if set */
#define KBD_MODE_DISABLE_KBD	0x10	/* Disable keyboard interface */
#define KBD_MODE_DISABLE_MOUSE	0x20	/* Disable mouse interface */
#define KBD_MODE_KCC		0x40	/* Scan code conversion to PC format */
#define KBD_MODE_RFU		0x80

/*
 *	Mouse Commands
 */
#define AUX_SET_RES		0xE8	/* Set resolution */
#define AUX_SET_SCALE11		0xE6	/* Set 1:1 scaling */
#define AUX_SET_SCALE21		0xE7	/* Set 2:1 scaling */
#define AUX_GET_SCALE		0xE9	/* Get scaling factor */
#define AUX_SET_STREAM		0xEA	/* Set stream mode */
#define AUX_SET_SAMPLE		0xF3	/* Set sample rate */
#define AUX_ENABLE_DEV		0xF4	/* Enable aux device */
#define AUX_DISABLE_DEV		0xF5	/* Disable aux device */
#define AUX_RESET		0xFF	/* Reset aux device */
#define AUX_ACK			0xFA	/* Command byte ACK. */

#define AUX_BUF_SIZE		2048	/* This might be better divisible by
					   three to make overruns stay in sync
					   but then the read function would need
					   a lock etc - ick */

#if 0
struct aux_queue {
	unsigned long head;
	unsigned long tail;
	wait_queue_head_t proc_list;
	struct fasync_struct *fasync;
	unsigned char buf[AUX_BUF_SIZE];
};
#endif