/*
* Copyright (c) 2012, The Chromium Authors
*
* See file CREDITS for list of people who contributed to this
* project.
*
* This program is free software; you can redistribute it and/or
* modify it under the terms of the GNU General Public License as
* published by the Free Software Foundation; either version 2 of
* the License, or (at your option) any later version.
*
* This program is distributed in the hope that it will be useful,
* but WITHOUT ANY WARRANTY; without even the implied warranty of
* MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
* GNU General Public License for more details.
*
* You should have received a copy of the GNU General Public License
* along with this program; if not, write to the Free Software
* Foundation, Inc., 59 Temple Place, Suite 330, Boston,
* MA 02111-1307 USA
*/
#define DEBUG
#include <common.h>
static const char test_cmd[] = "setenv list 1\n setenv list ${list}2; "
"setenv list ${list}3\0"
"setenv list ${list}4";
static int do_ut_cmd(cmd_tbl_t *cmdtp, int flag, int argc, char * const argv[])
{
printf("%s: Testing commands\n", __func__);
run_command("env default -f", 0);
/* run a single command */
run_command("setenv single 1", 0);
assert(!strcmp("1", getenv("single")));
/* make sure that compound statements work */
#ifdef CONFIG_SYS_HUSH_PARSER
run_command("if test -n ${single} ; then setenv check 1; fi", 0);
assert(!strcmp("1", getenv("check")));
run_command("setenv check", 0);
#endif
/* commands separated by ; */
run_command_list("setenv list 1; setenv list ${list}1", -1, 0);
assert(!strcmp("11", getenv("list")));
/* commands separated by \n */
run_command_list("setenv list 1\n setenv list ${list}1", -1, 0);
assert(!strcmp("11", getenv("list")));
/* command followed by \n and nothing else */
run_command_list("setenv list 1${list}\n", -1, 0);
assert(!strcmp("111", getenv("list")));
/* three commands in a row */
run_command_list("setenv list 1\n setenv list ${list}2; "
"setenv list ${list}3", -1, 0);
assert(!strcmp("123", getenv("list")));
/* a command string with \0 in it. Stuff after \0 should be ignored */
run_command("setenv list", 0);
run_command_list(test_cmd, sizeof(test_cmd), 0);
assert(!strcmp("123", getenv("list")));
/*
* a command list where we limit execution to only the first command
* using the length parameter.
*/
run_command_list("setenv list 1\n setenv list ${list}2; "
"setenv list ${list}3", strlen("setenv list 1"), 0);
assert(!strcmp("1", getenv("list")));
printf("%s: Everything went swimmingly\n", __func__);
return 0;
}
U_BOOT_CMD(
ut_cmd, 5, 1, do_ut_cmd,
"Very basic test of command parsers",
""
);