aboutsummaryrefslogtreecommitdiffstats
path: root/api/api.c
blob: 1ee7c68f7afc64b74263e51c611e2604f91b291f (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
424
425
426
427
428
429
430
431
432
433
434
435
436
437
438
439
440
441
442
443
444
445
446
447
448
449
450
451
452
453
454
455
456
457
458
459
460
461
462
463
464
465
466
467
468
469
470
471
472
473
474
475
476
477
478
479
480
481
482
483
484
485
486
487
488
489
490
491
492
493
494
495
496
497
498
499
500
501
502
503
504
505
506
507
508
509
510
511
512
513
514
515
516
517
518
519
520
521
522
523
524
525
526
527
528
529
530
531
532
533
534
535
536
537
538
539
540
541
542
543
544
545
546
547
548
549
550
551
552
553
554
555
556
557
558
559
560
561
562
563
564
565
566
567
568
569
570
571
572
573
574
575
576
577
578
579
580
581
582
583
584
585
586
587
588
589
590
591
592
593
594
595
596
597
598
599
600
601
602
603
604
605
606
607
608
609
610
611
612
613
614
615
616
617
618
619
620
621
622
623
624
625
626
627
628
629
630
631
632
633
634
635
636
637
638
639
640
641
642
643
644
645
646
647
648
649
650
651
652
653
654
655
656
657
658
659
660
661
662
663
664
665
666
667
668
669
670
/*
 * (C) Copyright 2007 Semihalf
 *
 * Written by: Rafal Jaworowski <raj@semihalf.com>
 *
 * See file CREDITS for list of people who contributed to this
 * project.
 *
 * This program is free software; you can redistribute it and/or
 * modify it under the terms of the GNU General Public License as
 * published by the Free Software Foundation; either version 2 of
 * the License, or (at your option) any later version.
 *
 * This program is distributed in the hope that it will be useful,
 * but WITHOUT ANY WARRANTY; without even the implied warranty of
 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
 * GNU General Public License for more details.
 *
 * You should have received a copy of the GNU General Public License
 * along with this program; if not, write to the Free Software
 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
 * MA 02111-1307 USA
 *
 */

#include <config.h>

#if defined(CONFIG_API)

#include <command.h>
#include <common.h>
#include <malloc.h>
#include <linux/types.h>
#include <api_public.h>

#include "api_private.h"

#define DEBUG
#undef DEBUG

/* U-Boot routines needed */
extern int do_reset (cmd_tbl_t *cmdtp, int flag, int argc, char *argv[]);
extern uchar (*env_get_char)(int);
extern uchar *env_get_addr(int);

/*****************************************************************************
 *
 * This is the API core.
 *
 * API_ functions are part of U-Boot code and constitute the lowest level
 * calls:
 *
 *  - they know what values they need as arguments
 *  - their direct return value pertains to the API_ "shell" itself (0 on
 *    success, some error code otherwise)
 *  - if the call returns a value it is buried within arguments
 *
 ****************************************************************************/

#ifdef DEBUG
#define debugf(fmt, args...) do { printf("%s(): ", __func__); printf(fmt, ##args); } while (0)
#else
#define debugf(fmt, args...)
#endif

typedef	int (*cfp_t)(va_list argp);

static int calls_no;

/*
 * pseudo signature:
 *
 * int API_getc(int *c)
 */
static int API_getc(va_list ap)
{
	int *c;

	if ((c = (int *)va_arg(ap, u_int32_t)) == NULL)
		return API_EINVAL;

	*c = getc();
	return 0;
}

/*
 * pseudo signature:
 *
 * int API_tstc(int *c)
 */
static int API_tstc(va_list ap)
{
	int *t;

	if ((t = (int *)va_arg(ap, u_int32_t)) == NULL)
		return API_EINVAL;

	*t = tstc();
	return 0;
}

/*
 * pseudo signature:
 *
 * int API_putc(char *ch)
 */
static int API_putc(va_list ap)
{
	char *c;

	if ((c = (char *)va_arg(ap, u_int32_t)) == NULL)
		return API_EINVAL;

	putc(*c);
	return 0;
}

/*
 * pseudo signature:
 *
 * int API_puts(char **s)
 */
static int API_puts(va_list ap)
{
	char *s;

	if ((s = (char *)va_arg(ap, u_int32_t)) == NULL)
		return API_EINVAL;

	puts(s);
	return 0;
}

/*
 * pseudo signature:
 *
 * int API_reset(void)
 */
static int API_reset(va_list ap)
{
	do_reset(NULL, 0, 0, NULL);

	/* NOT REACHED */
	return 0;
}

/*
 * pseudo signature:
 *
 * int API_get_sys_info(struct sys_info *si)
 *
 * fill out the sys_info struct containing selected parameters about the
 * machine
 */
static int API_get_sys_info(va_list ap)
{
	struct sys_info *si;

	si = (struct sys_info *)va_arg(ap, u_int32_t);
	if (si == NULL)
		return API_ENOMEM;

	return (platform_sys_info(si)) ? 0 : API_ENODEV;
}

/*
 * pseudo signature:
 *
 * int API_udelay(unsigned long *udelay)
 */
static int API_udelay(va_list ap)
{
	unsigned long *d;

	if ((d = (unsigned long *)va_arg(ap, u_int32_t)) == NULL)
		return API_EINVAL;

	udelay(*d);
	return 0;
}

/*
 * pseudo signature:
 *
 * int API_get_timer(unsigned long *current, unsigned long *base)
 */
static int API_get_timer(va_list ap)
{
	unsigned long *base, *cur;

	cur = (unsigned long *)va_arg(ap, u_int32_t);
	if (cur == NULL)
		return API_EINVAL;

	base = (unsigned long *)va_arg(ap, u_int32_t);
	if (base == NULL)
		return API_EINVAL;

	*cur = get_timer(*base);
	return 0;
}


/*****************************************************************************
 *
 * pseudo signature:
 *
 * int API_dev_enum(struct device_info *)
 *
 *
 * cookies uniqely identify the previously enumerated device instance and
 * provide a hint for what to inspect in current enum iteration:
 *
 *   - net: &eth_device struct address from list pointed to by eth_devices
 *
 *   - storage: block_dev_desc_t struct address from &ide_dev_desc[n],
 *     &scsi_dev_desc[n] and similar tables
 *
 ****************************************************************************/

static int API_dev_enum(va_list ap)
{
	struct device_info *di;

	/* arg is ptr to the device_info struct we are going to fill out */
	di = (struct device_info *)va_arg(ap, u_int32_t);
	if (di == NULL)
		return API_EINVAL;

	if (di->cookie == NULL) {
		/* start over - clean up enumeration */
		dev_enum_reset();	/* XXX shouldn't the name contain 'stor'? */
		debugf("RESTART ENUM\n");

		/* net device enumeration first */
		if (dev_enum_net(di))
			return 0;
	}

	/*
	 * The hidden assumption is there can only be one active network
	 * device and it is identified upon enumeration (re)start, so there's
	 * no point in trying to find network devices in other cases than the
	 * (re)start and hence the 'next' device can only be storage
	 */
	if (!dev_enum_storage(di))
		/* make sure we mark there are no more devices */
		di->cookie = NULL;

	return 0;
}


static int API_dev_open(va_list ap)
{
	struct device_info *di;
	int err = 0;

	/* arg is ptr to the device_info struct */
	di = (struct device_info *)va_arg(ap, u_int32_t);
	if (di == NULL)
		return API_EINVAL;

	/* Allow only one consumer of the device at a time */
	if (di->state == DEV_STA_OPEN)
		return API_EBUSY;

	if (di->cookie == NULL)
		return API_ENODEV;

	if (di->type & DEV_TYP_STOR)
		err = dev_open_stor(di->cookie);

	else if (di->type & DEV_TYP_NET)
		err = dev_open_net(di->cookie);
	else
		err = API_ENODEV;

	if (!err)
		di->state = DEV_STA_OPEN;

	return err;
}


static int API_dev_close(va_list ap)
{
	struct device_info *di;
	int err = 0;

	/* arg is ptr to the device_info struct */
	di = (struct device_info *)va_arg(ap, u_int32_t);
	if (di == NULL)
		return API_EINVAL;

	if (di->state == DEV_STA_CLOSED)
		return 0;

	if (di->cookie == NULL)
		return API_ENODEV;

	if (di->type & DEV_TYP_STOR)
		err = dev_close_stor(di->cookie);

	else if (di->type & DEV_TYP_NET)
		err = dev_close_net(di->cookie);
	else
		/*
		 * In case of unknown device we cannot change its state, so
		 * only return error code
		 */
		err = API_ENODEV;

	if (!err)
		di->state = DEV_STA_CLOSED;

	return err;
}


/*
 * Notice: this is for sending network packets only, as U-Boot does not
 * support writing to storage at the moment (12.2007)
 *
 * pseudo signature:
 *
 * int API_dev_write(
 *	struct device_info *di,
 *	void *buf,
 *	int *len
 * )
 *
 * buf:	ptr to buffer from where to get the data to send
 *
 * len: length of packet to be sent (in bytes)
 *
 */
static int API_dev_write(va_list ap)
{
	struct device_info *di;
	void *buf;
	int *len;
	int err = 0;

	/* 1. arg is ptr to the device_info struct */
	di = (struct device_info *)va_arg(ap, u_int32_t);
	if (di == NULL)
		return API_EINVAL;

	/* XXX should we check if device is open? i.e. the ->state ? */

	if (di->cookie == NULL)
		return API_ENODEV;

	/* 2. arg is ptr to buffer from where to get data to write */
	buf = (void *)va_arg(ap, u_int32_t);
	if (buf == NULL)
		return API_EINVAL;

	/* 3. arg is length of buffer */
	len = (int *)va_arg(ap, u_int32_t);
	if (len == NULL)
		return API_EINVAL;
	if (*len <= 0)
		return API_EINVAL;

	if (di->type & DEV_TYP_STOR)
		/*
		 * write to storage is currently not supported by U-Boot:
		 * no storage device implements block_write() method
		 */
		return API_ENODEV;

	else if (di->type & DEV_TYP_NET)
		err = dev_write_net(di->cookie, buf, *len);
	else
		err = API_ENODEV;

	return err;
}


/*
 * pseudo signature:
 *
 * int API_dev_read(
 *	struct device_info *di,
 *	void *buf,
 *	size_t *len,
 *	unsigned long *start
 *	size_t *act_len
 * )
 *
 * buf:	ptr to buffer where to put the read data
 *
 * len: ptr to length to be read
 *      - network: len of packet to read (in bytes)
 *      - storage: # of blocks to read (can vary in size depending on define)
 *
 * start: ptr to start block (only used for storage devices, ignored for
 *        network)
 *
 * act_len: ptr to where to put the len actually read
 */
static int API_dev_read(va_list ap)
{
	struct device_info *di;
	void *buf;
	lbasize_t *len_stor, *act_len_stor;
	lbastart_t *start;
	int *len_net, *act_len_net;

	/* 1. arg is ptr to the device_info struct */
	di = (struct device_info *)va_arg(ap, u_int32_t);
	if (di == NULL)
		return API_EINVAL;

	/* XXX should we check if device is open? i.e. the ->state ? */

	if (di->cookie == NULL)
		return API_ENODEV;

	/* 2. arg is ptr to buffer from where to put the read data */
	buf = (void *)va_arg(ap, u_int32_t);
	if (buf == NULL)
		return API_EINVAL;

	if (di->type & DEV_TYP_STOR) {
		/* 3. arg - ptr to var with # of blocks to read */
		len_stor = (lbasize_t *)va_arg(ap, u_int32_t);
		if (!len_stor)
			return API_EINVAL;
		if (*len_stor <= 0)
			return API_EINVAL;

		/* 4. arg - ptr to var with start block */
		start = (lbastart_t *)va_arg(ap, u_int32_t);

		/* 5. arg - ptr to var where to put the len actually read */
		act_len_stor = (lbasize_t *)va_arg(ap, u_int32_t);
		if (!act_len_stor)
			return API_EINVAL;

		*act_len_stor = dev_read_stor(di->cookie, buf, *len_stor, *start);

	} else if (di->type & DEV_TYP_NET) {

		/* 3. arg points to the var with length of packet to read */
		len_net = (int *)va_arg(ap, u_int32_t);
		if (!len_net)
			return API_EINVAL;
		if (*len_net <= 0)
			return API_EINVAL;

		/* 4. - ptr to var where to put the len actually read */
		act_len_net = (int *)va_arg(ap, u_int32_t);
		if (!act_len_net)
			return API_EINVAL;

		*act_len_net = dev_read_net(di->cookie, buf, *len_net);

	} else
		return API_ENODEV;

	return 0;
}


/*
 * pseudo signature:
 *
 * int API_env_get(const char *name, char **value)
 *
 * name: ptr to name of env var
 */
static int API_env_get(va_list ap)
{
	char *name, **value;

	if ((name = (char *)va_arg(ap, u_int32_t)) == NULL)
		return API_EINVAL;
	if ((value = (char **)va_arg(ap, u_int32_t)) == NULL)
		return API_EINVAL;

	*value = getenv(name);

	return 0;
}

/*
 * pseudo signature:
 *
 * int API_env_set(const char *name, const char *value)
 *
 * name: ptr to name of env var
 *
 * value: ptr to value to be set
 */
static int API_env_set(va_list ap)
{
	char *name, *value;

	if ((name = (char *)va_arg(ap, u_int32_t)) == NULL)
		return API_EINVAL;
	if ((value = (char *)va_arg(ap, u_int32_t)) == NULL)
		return API_EINVAL;

	setenv(name, value);

	return 0;
}

/*
 * pseudo signature:
 *
 * int API_env_enum(const char *last, char **next)
 *
 * last: ptr to name of env var found in last iteration
 */
static int API_env_enum(va_list ap)
{
	int i, n;
	char *last, **next;

	last = (char *)va_arg(ap, u_int32_t);

	if ((next = (char **)va_arg(ap, u_int32_t)) == NULL)
		return API_EINVAL;

	if (last == NULL)
		/* start over */
		*next = ((char *)env_get_addr(0));
	else {
		*next = last;

		for (i = 0; env_get_char(i) != '\0'; i = n + 1) {
			for (n = i; env_get_char(n) != '\0'; ++n) {
				if (n >= CFG_ENV_SIZE) {
					/* XXX shouldn't we set *next = NULL?? */
					return 0;
				}
			}

			if (envmatch((uchar *)last, i) < 0)
				continue;

			/* try to get next name */
			i = n + 1;
			if (env_get_char(i) == '\0') {
				/* no more left */
				*next = NULL;
				return 0;
			}

			*next = ((char *)env_get_addr(i));
			return 0;
		}
	}

	return 0;
}

static cfp_t calls_table[API_MAXCALL] = { NULL, };

/*
 * The main syscall entry point - this is not reentrant, only one call is
 * serviced until finished.
 *
 * e.g. syscall(1, int *, u_int32_t, u_int32_t, u_int32_t, u_int32_t);
 *
 * call:	syscall number
 *
 * retval:	points to the return value placeholder, this is the place the
 *		syscall puts its return value, if NULL the caller does not
 *		expect a return value
 *
 * ...		syscall arguments (variable number)
 *
 * returns:	0 if the call not found, 1 if serviced
 */
int syscall(int call, int *retval, ...)
{
	va_list	ap;
	int rv;

	if (call < 0 || call >= calls_no) {
		debugf("invalid call #%d\n", call);
		return 0;
	}

	if (calls_table[call] == NULL) {
		debugf("syscall #%d does not have a handler\n", call);
		return 0;
	}

	va_start(ap, retval);
	rv = calls_table[call](ap);
	if (retval != NULL)
		*retval = rv;

	return 1;
}

void api_init(void)
{
	struct api_signature *sig = NULL;

	/* TODO put this into linker set one day... */
	calls_table[API_RSVD] = NULL;
	calls_table[API_GETC] = &API_getc;
	calls_table[API_PUTC] = &API_putc;
	calls_table[API_TSTC] = &API_tstc;
	calls_table[API_PUTS] = &API_puts;
	calls_table[API_RESET] = &API_reset;
	calls_table[API_GET_SYS_INFO] = &API_get_sys_info;
	calls_table[API_UDELAY] = &API_udelay;
	calls_table[API_GET_TIMER] = &API_get_timer;
	calls_table[API_DEV_ENUM] = &API_dev_enum;
	calls_table[API_DEV_OPEN] = &API_dev_open;
	calls_table[API_DEV_CLOSE] = &API_dev_close;
	calls_table[API_DEV_READ] = &API_dev_read;
	calls_table[API_DEV_WRITE] = &API_dev_write;
	calls_table[API_ENV_GET] = &API_env_get;
	calls_table[API_ENV_SET] = &API_env_set;
	calls_table[API_ENV_ENUM] = &API_env_enum;
	calls_no = API_MAXCALL;

	debugf("API initialized with %d calls\n", calls_no);

	dev_stor_init();

	/*
	 * Produce the signature so the API consumers can find it
	 */
	sig = malloc(sizeof(struct api_signature));
	if (sig == NULL) {
		printf("API: could not allocate memory for the signature!\n");
		return;
	}

	debugf("API sig @ 0x%08x\n", sig);
	memcpy(sig->magic, API_SIG_MAGIC, 8);
	sig->version = API_SIG_VERSION;
	sig->syscall = &syscall;
	sig->checksum = 0;
	sig->checksum = crc32(0, (unsigned char *)sig,
			      sizeof(struct api_signature));
	debugf("syscall entry: 0x%08x\n", sig->syscall);
}

void platform_set_mr(struct sys_info *si, unsigned long start, unsigned long size,
			int flags)
{
	int i;

	if (!si->mr || !size || (flags == 0))
		return;

	/* find free slot */
	for (i = 0; i < si->mr_no; i++)
		if (si->mr[i].flags == 0) {
			/* insert new mem region */
			si->mr[i].start = start;
			si->mr[i].size = size;
			si->mr[i].flags = flags;
			return;
		}
}

#endif /* CONFIG_API */