aboutsummaryrefslogtreecommitdiffstats
blob: 5642dd33bc32c71265e1d470e767c214d821cf1d (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
/*
 * (C) Copyright 2007-2008 Semihalf
 *
 * Written by: Rafal Jaworowski <raj@semihalf.com>
 *
 * See file CREDITS for list of people who contributed to this
 * project.
 *
 * This program is free software; you can redistribute it and/or
 * modify it under the terms of the GNU General Public License as
 * published by the Free Software Foundation; either version 2 of
 * the License, or (at your option) any later version.
 *
 * This program is distributed in the hope that it will be useful,
 * but WITHOUT ANY WARRANTY; without even the implied warranty of
 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
 * GNU General Public License for more details.
 *
 * You should have received a copy of the GNU General Public License
 * along with this program; if not, write to the Free Software
 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
 * MA 02111-1307 USA
 *
 */

#include <config.h>

#if defined(CONFIG_API)

#include <common.h>
#include <api_public.h>

#if defined(CONFIG_CMD_USB) && defined(CONFIG_USB_STORAGE)
#include <usb.h>
#endif

#define DEBUG
#undef DEBUG

#ifdef DEBUG
#define debugf(fmt, args...) do { printf("%s(): ", __func__); printf(fmt, ##args); } while (0)
#else
#define debugf(fmt, args...)
#endif

#define errf(fmt, args...) do { printf("ERROR @ %s(): ", __func__); printf(fmt, ##args); } while (0)


#define ENUM_IDE	0
#define ENUM_USB	1
#define ENUM_SCSI	2
#define ENUM_MMC	3
#define ENUM_SATA	4
#define ENUM_MAX	5

struct stor_spec {
	int		max_dev;
	int		enum_started;
	int		enum_ended;
	int		type;		/* "external" type: DT_STOR_{IDE,USB,etc} */
	char		*name;
};

static struct stor_spec specs[ENUM_MAX] = { { 0, 0, 0, 0, "" }, };


void dev_stor_init(void)
{
#if defined(CONFIG_CMD_IDE)
	specs[ENUM_IDE].max_dev = CFG_IDE_MAXDEVICE;
	specs[ENUM_IDE].enum_started = 0;
	specs[ENUM_IDE].enum_ended = 0;
	specs[ENUM_IDE].type = DEV_TYP_STOR | DT_STOR_IDE;
	specs[ENUM_IDE].name = "ide";
#endif
#if defined(CONFIG_CMD_MMC)
	specs[ENUM_MMC].max_dev = CFG_MMC_MAX_DEVICE;
	specs[ENUM_MMC].enum_started = 0;
	specs[ENUM_MMC].enum_ended = 0;
	specs[ENUM_MMC].type = DEV_TYP_STOR | DT_STOR_MMC;
	specs[ENUM_MMC].name = "mmc";
#endif
#if defined(CONFIG_CMD_SATA)
	specs[ENUM_SATA].max_dev = CFG_SATA_MAX_DEVICE;
	specs[ENUM_SATA].enum_started = 0;
	specs[ENUM_SATA].enum_ended = 0;
	specs[ENUM_SATA].type = DEV_TYP_STOR | DT_STOR_SATA;
	specs[ENUM_SATA].name = "sata";
#endif
#if defined(CONFIG_CMD_SCSI)
	specs[ENUM_SCSI].max_dev = CFG_SCSI_MAX_DEVICE;
	specs[ENUM_SCSI].enum_started = 0;
	specs[ENUM_SCSI].enum_ended = 0;
	specs[ENUM_SCSI].type = DEV_TYP_STOR | DT_STOR_SCSI;
	specs[ENUM_SCSI].name = "scsi";
#endif
#if defined(CONFIG_CMD_USB) && defined(CONFIG_USB_STORAGE)
	specs[ENUM_USB].max_dev = USB_MAX_STOR_DEV;
	specs[ENUM_USB].enum_started = 0;
	specs[ENUM_USB].enum_ended = 0;
	specs[ENUM_USB].type = DEV_TYP_STOR | DT_STOR_USB;
	specs[ENUM_USB].name = "usb";
#endif
}

/*
 * Finds next available device in the storage group
 *
 * type:	storage group type - ENUM_IDE, ENUM_SCSI etc.
 *
 * first:	if 1 the first device in the storage group is returned (if
 *              exists), if 0 the next available device is searched
 *
 * more:	returns 0/1 depending if there are more devices in this group
 *		available (for future iterations)
 *
 * returns:	0/1 depending if device found in this iteration
 */
static int dev_stor_get(int type, int first, int *more, struct device_info *di)
{
	int found = 0;
	*more = 0;

	int i;

	block_dev_desc_t *dd;

	if (first) {
		di->cookie = (void *)get_dev(specs[type].name, 0);
		if (di->cookie == NULL)
			return 0;
		else
			found = 1;

	} else {
		for (i = 0; i < specs[type].max_dev; i++)
			if (di->cookie == (void *)get_dev(specs[type].name, i)) {
				/* previous cookie found -- advance to the
				 * next device, if possible */

				if (++i >= specs[type].max_dev) {
					/* out of range, no more to enum */
					di->cookie = NULL;
					break;
				}

				di->cookie = (void *)get_dev(specs[type].name, i);
				if (di->cookie == NULL)
					return 0;
				else
					found = 1;

				/* provide hint if there are more devices in
				 * this group to enumerate */
				if ((i + 1) < specs[type].max_dev)
					*more = 1;

				break;
			}
	}

	if (found) {
		di->type = specs[type].type;

		if (di->cookie != NULL) {
			dd = (block_dev_desc_t *)di->cookie;
			if (dd->type == DEV_TYPE_UNKNOWN) {
				debugf("device instance exists, but is not active..");
				found = 0;
			} else {
				di->di_stor.block_count = dd->lba;
				di->di_stor.block_size = dd->blksz;
			}
		}

	} else
		di->cookie = NULL;

	return found;
}


/*
 * returns:	ENUM_IDE, ENUM_USB etc. based on block_dev_desc_t
 */
static int dev_stor_type(block_dev_desc_t *dd)
{
	int i, j;

	for (i = ENUM_IDE; i < ENUM_MAX; i++)
		for (j = 0; j < specs[i].max_dev; j++)
			if (dd == get_dev(specs[i].name, j))
				return i;

	return ENUM_MAX;
}


/*
 * returns:	0/1 whether cookie points to some device in this group
 */
static int dev_is_stor(int type, struct device_info *di)
{
	return (dev_stor_type(di->cookie) == type) ? 1 : 0;
}


static int dev_enum_stor(int type, struct device_info *di)
{
	int found = 0, more = 0;

	debugf("called, type %d\n", type);

	/*
	 * Formulae for enumerating storage devices:
	 * 1. if cookie (hint from previous enum call) is NULL we start again
	 *    with enumeration, so return the first available device, done.
	 *
	 * 2. if cookie is not NULL, check if it identifies some device in
	 *    this group:
	 *
	 * 2a. if cookie is a storage device from our group (IDE, USB etc.),
	 *     return next available (if exists) in this group
	 *
	 * 2b. if it isn't device from our group, check if such devices were
	 *     ever enumerated before:
	 *     - if not, return the first available device from this group
	 *     - else return 0
	 */

	if (di->cookie == NULL) {

		debugf("group%d - enum restart\n", type);

		/*
		 * 1. Enumeration (re-)started: take the first available
		 * device, if exists
		 */
		found = dev_stor_get(type, 1, &more, di);
		specs[type].enum_started = 1;

	} else if (dev_is_stor(type, di)) {

		debugf("group%d - enum continued for the next device\n", type);

		if (specs[type].enum_ended) {
			debugf("group%d - nothing more to enum!\n", type);
			return 0;
		}

		/* 2a. Attempt to take a next available device in the group */
		found = dev_stor_get(type, 0, &more, di);

	} else {

		if (specs[type].enum_ended) {
			debugf("group %d - already enumerated, skipping\n", type);
			return 0;
		}

		debugf("group%d - first time enum\n", type);

		if (specs[type].enum_started == 0) {
			/*
			 * 2b.  If enumerating devices in this group did not
			 * happen before, it means the cookie pointed to a
			 * device frome some other group (another storage
			 * group, or network); in this case try to take the
			 * first available device from our group
			 */
			specs[type].enum_started = 1;

			/*
			 * Attempt to take the first device in this group:
			 *'first element' flag is set
			 */
			found = dev_stor_get(type, 1, &more, di);

		} else {
			errf("group%d - out of order iteration\n", type);
			found = 0;
			more = 0;
		}
	}

	/*
	 * If there are no more devices in this group, consider its
	 * enumeration finished
	 */
	specs[type].enum_ended = (!more) ? 1 : 0;

	if (found)
		debugf("device found, returning cookie 0x%08x\n",
			(u_int32_t)di->cookie);
	else
		debugf("no device found\n");

	return found;
}

void dev_enum_reset(void)
{
	int i;

	for (i = 0; i < ENUM_MAX; i ++) {
		specs[i].enum_started = 0;
		specs[i].enum_ended = 0;
	}
}

int dev_enum_storage(struct device_info *di)
{
	int i;

	/*
	 * check: ide, usb, scsi, mmc
	 */
	for (i = ENUM_IDE; i < ENUM_MAX; i ++) {
		if (dev_enum_stor(i, di))
			return 1;
	}

	return 0;
}

static int dev_stor_is_valid(int type, block_dev_desc_t *dd)
{
	int i;

	for (i = 0; i < specs[type].max_dev; i++)
		if (dd == get_dev(specs[type].name, i))
			if (dd->type != DEV_TYPE_UNKNOWN)
				return 1;

	return 0;
}


int dev_open_stor(void *cookie)
{
	int type = dev_stor_type(cookie);

	if (type == ENUM_MAX)
		return API_ENODEV;

	if (dev_stor_is_valid(type, (block_dev_desc_t *)cookie))
		return 0;

	return API_ENODEV;
}


int dev_close_stor(void *cookie)
{
	/*
	 * Not much to do as we actually do not alter storage devices upon
	 * close
	 */
	return 0;
}


static int dev_stor_index(block_dev_desc_t *dd)
{
	int i, type;

	type = dev_stor_type(dd);
	for (i = 0; i < specs[type].max_dev; i++)
		if (dd == get_dev(specs[type].name, i))
			return i;

	return (specs[type].max_dev);
}


lbasize_t dev_read_stor(void *cookie, void *buf, lbasize_t len, lbastart_t start)
{
	int type;
	block_dev_desc_t *dd = (block_dev_desc_t *)cookie;

	if ((type = dev_stor_type(dd)) == ENUM_MAX)
		return 0;

	if (!dev_stor_is_valid(type, dd))
		return 0;

	if ((dd->block_read) == NULL) {
		debugf("no block_read() for device 0x%08x\n", cookie);
		return 0;
	}

	return (dd->block_read(dev_stor_index(dd), start, len, buf));
}

#endif /* CONFIG_API */