aboutsummaryrefslogtreecommitdiffstats
blob: 039a1f2604f84794c535e767f432e1a65c7de387 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
/*
 * (C) Copyright 2010
 * Texas Instruments, <www.ti.com>
 *
 * This program is free software; you can redistribute it and/or
 * modify it under the terms of the GNU General Public License as
 * published by the Free Software Foundation; either version 2 of
 * the License, or (at your option) any later version.
 *
 * This program is distributed in the hope that it will be useful,
 * but WITHOUT ANY WARRANTY; without even the implied warranty of
 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
 * GNU General Public License for more details.
 *
 * You should have received a copy of the GNU General Public License
 * along with this program; if not, write to the Free Software
 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
 * MA 02111-1307 USA
 */

#ifndef _SYS_PROTO_H_
#define _SYS_PROTO_H_

#include <asm/arch/omap.h>
#include <asm/arch/clocks.h>
#include <asm/io.h>
#include <asm/omap_common.h>
#include <asm/arch/mux_omap4.h>

DECLARE_GLOBAL_DATA_PTR;

struct omap_sysinfo {
	char *board_string;
};
extern const struct omap_sysinfo sysinfo;

void gpmc_init(void);
void watchdog_init(void);
u32 get_device_type(void);
void do_set_mux(u32 base, struct pad_conf_entry const *array, int size);
void set_muxconf_regs_essential(void);
void set_muxconf_regs_non_essential(void);
void sr32(void *, u32, u32, u32);
u32 wait_on_value(u32, u32, void *, u32);
void sdelay(unsigned long);
void set_pl310_ctrl_reg(u32 val);
void setup_clocks_for_console(void);
void prcm_init(void);
void bypass_dpll(u32 const base);
void freq_update_core(void);
u32 get_sys_clk_freq(void);
u32 omap4_ddr_clk(void);
void cancel_out(u32 *num, u32 *den, u32 den_limit);
void sdram_init(void);
u32 omap_sdram_size(void);
u32 cortex_rev(void);
void init_omap_revision(void);
void do_io_settings(void);
void omap_vc_init(u16 speed_khz);
int omap_vc_bypass_send_value(u8 sa, u8 reg_addr, u8 reg_data);
u32 warm_reset(void);
void force_emif_self_refresh(void);
void setup_warmreset_time(void);

static inline u32 running_from_sdram(void)
{
	u32 pc;
	asm volatile ("mov %0, pc" : "=r" (pc));
	return ((pc >= OMAP44XX_DRAM_ADDR_SPACE_START) &&
	    (pc < OMAP44XX_DRAM_ADDR_SPACE_END));
}

static inline u8 uboot_loaded_by_spl(void)
{
	/*
	 * u-boot can be running from sdram either because of configuration
	 * Header or by SPL. If because of CH, then the romcode sets the
	 * CHSETTINGS executed bit to true in the boot parameter structure that
	 * it passes to the bootloader.This parameter is stored in the ch_flags
	 * variable by both SPL and u-boot.Check out for CHSETTINGS, which is a
	 * mandatory section if CH is present.
	 */
	if ((gd->arch.omap_boot_params.ch_flags) & (CH_FLAGS_CHSETTINGS))
		return 0;
	else
		return running_from_sdram();
}
/*
 * The basic hardware init of OMAP(s_init()) can happen in 4
 * different contexts:
 *  1. SPL running from SRAM
 *  2. U-Boot running from FLASH
 *  3. Non-XIP U-Boot loaded to SDRAM by SPL
 *  4. Non-XIP U-Boot loaded to SDRAM by ROM code using the
 *     Configuration Header feature
 *
 * This function finds this context.
 * Defining as inline may help in compiling out unused functions in SPL
 */
static inline u32 omap_hw_init_context(void)
{
#ifdef CONFIG_SPL_BUILD
	return OMAP_INIT_CONTEXT_SPL;
#else
	if (uboot_loaded_by_spl())
		return OMAP_INIT_CONTEXT_UBOOT_AFTER_SPL;
	else if (running_from_sdram())
		return OMAP_INIT_CONTEXT_UBOOT_AFTER_CH;
	else
		return OMAP_INIT_CONTEXT_UBOOT_FROM_NOR;
#endif
}

#endif