aboutsummaryrefslogtreecommitdiffstats
blob: e6aa89bdd00d9729d5bbe99038dc9c2d86a97885 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
/*
 * (C) Copyright 2010
 * Texas Instruments, <www.ti.com>
 *
 * Aneesh V <aneesh@ti.com>
 *
 * See file CREDITS for list of people who contributed to this
 * project.
 *
 * This program is free software; you can redistribute it and/or
 * modify it under the terms of the GNU General Public License as
 * published by the Free Software Foundation; either version 2 of
 * the License, or (at your option) any later version.
 *
 * This program is distributed in the hope that it will be useful,
 * but WITHOUT ANY WARRANTY; without even the implied warranty of
 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
 * GNU General Public License for more details.
 *
 * You should have received a copy of the GNU General Public License
 * along with this program; if not, write to the Free Software
 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
 * MA 02111-1307 USA
 */
#include <common.h>
#include <spl.h>
#include <asm/u-boot.h>
#include <nand.h>
#include <fat.h>
#include <version.h>
#include <i2c.h>
#include <image.h>
#include <malloc.h>
#include <linux/compiler.h>

DECLARE_GLOBAL_DATA_PTR;

#ifndef CONFIG_SYS_UBOOT_START
#define CONFIG_SYS_UBOOT_START	CONFIG_SYS_TEXT_BASE
#endif
#ifndef CONFIG_SYS_MONITOR_LEN
#define CONFIG_SYS_MONITOR_LEN	(200 * 1024)
#endif

u32 *boot_params_ptr = NULL;
struct spl_image_info spl_image;

/* Define board data structure */
static bd_t bdata __attribute__ ((section(".data")));

inline void hang(void)
{
	puts("### ERROR ### Please RESET the board ###\n");
	for (;;)
		;
}

/*
 * Default function to determine if u-boot or the OS should
 * be started. This implementation always returns 1.
 *
 * Please implement your own board specific funcion to do this.
 *
 * RETURN
 * 0 to not start u-boot
 * positive if u-boot should start
 */
#ifdef CONFIG_SPL_OS_BOOT
__weak int spl_start_uboot(void)
{
	puts("SPL: Please implement spl_start_uboot() for your board\n");
	puts("SPL: Direct Linux boot not active!\n");
	return 1;
}
#endif

/*
 * Weak default function for board specific cleanup/preparation before
 * Linux boot. Some boards/platforms might not need it, so just provide
 * an empty stub here.
 */
__weak void spl_board_prepare_for_linux(void)
{
	/* Nothing to do! */
}

void spl_parse_image_header(const struct image_header *header)
{
	u32 header_size = sizeof(struct image_header);

	if (image_get_magic(header) == IH_MAGIC) {
		if (spl_image.flags & SPL_COPY_PAYLOAD_ONLY) {
			/*
			 * On some system (e.g. powerpc), the load-address and
			 * entry-point is located at address 0. We can't load
			 * to 0-0x40. So skip header in this case.
			 */
			spl_image.load_addr = image_get_load(header);
			spl_image.entry_point = image_get_ep(header);
			spl_image.size = image_get_data_size(header);
		} else {
			spl_image.entry_point = image_get_load(header);
			/* Load including the header */
			spl_image.load_addr = spl_image.entry_point -
				header_size;
			spl_image.size = image_get_data_size(header) +
				header_size;
		}
		spl_image.os = image_get_os(header);
		spl_image.name = image_get_name(header);
		debug("spl: payload image: %s load addr: 0x%x size: %d\n",
			spl_image.name, spl_image.load_addr, spl_image.size);
	} else {
		/* Signature not found - assume u-boot.bin */
		debug("mkimage signature not found - ih_magic = %x\n",
			header->ih_magic);
		/* Let's assume U-Boot will not be more than 200 KB */
		spl_image.size = CONFIG_SYS_MONITOR_LEN;
		spl_image.entry_point = CONFIG_SYS_UBOOT_START;
		spl_image.load_addr = CONFIG_SYS_TEXT_BASE;
		spl_image.os = IH_OS_U_BOOT;
		spl_image.name = "U-Boot";
	}
}

__weak void __noreturn jump_to_image_no_args(struct spl_image_info *spl_image)
{
	typedef void __noreturn (*image_entry_noargs_t)(void);

	image_entry_noargs_t image_entry =
			(image_entry_noargs_t) spl_image->entry_point;

	debug("image entry point: 0x%X\n", spl_image->entry_point);
	image_entry();
}

#ifdef CONFIG_SPL_RAM_DEVICE
static void spl_ram_load_image(void)
{
	const struct image_header *header;

	/*
	 * Get the header.  It will point to an address defined by handoff
	 * which will tell where the image located inside the flash. For
	 * now, it will temporary fixed to address pointed by U-Boot.
	 */
	header = (struct image_header *)
		(CONFIG_SYS_TEXT_BASE -	sizeof(struct image_header));

	spl_parse_image_header(header);
}
#endif

void board_init_r(gd_t *dummy1, ulong dummy2)
{
	u32 boot_device;
	debug(">>spl:board_init_r()\n");

#ifdef CONFIG_SYS_SPL_MALLOC_START
	mem_malloc_init(CONFIG_SYS_SPL_MALLOC_START,
			CONFIG_SYS_SPL_MALLOC_SIZE);
#endif

#ifndef CONFIG_PPC
	/*
	 * timer_init() does not exist on PPC systems. The timer is initialized
	 * and enabled (decrementer) in interrupt_init() here.
	 */
	timer_init();
#endif

#ifdef CONFIG_SPL_BOARD_INIT
	spl_board_init();
#endif

	boot_device = spl_boot_device();
	debug("boot device - %d\n", boot_device);
	switch (boot_device) {
#ifdef CONFIG_SPL_RAM_DEVICE
	case BOOT_DEVICE_RAM:
		spl_ram_load_image();
		break;
#endif
#ifdef CONFIG_SPL_MMC_SUPPORT
	case BOOT_DEVICE_MMC1:
	case BOOT_DEVICE_MMC2:
	case BOOT_DEVICE_MMC2_2:
		spl_mmc_load_image();
		break;
#endif
#ifdef CONFIG_SPL_NAND_SUPPORT
	case BOOT_DEVICE_NAND:
		spl_nand_load_image();
		break;
#endif
#ifdef CONFIG_SPL_ONENAND_SUPPORT
	case BOOT_DEVICE_ONENAND:
		spl_onenand_load_image();
		break;
#endif
#ifdef CONFIG_SPL_NOR_SUPPORT
	case BOOT_DEVICE_NOR:
		spl_nor_load_image();
		break;
#endif
#ifdef CONFIG_SPL_YMODEM_SUPPORT
	case BOOT_DEVICE_UART:
		spl_ymodem_load_image();
		break;
#endif
#ifdef CONFIG_SPL_SPI_SUPPORT
	case BOOT_DEVICE_SPI:
		spl_spi_load_image();
		break;
#endif
#ifdef CONFIG_SPL_ETH_SUPPORT
	case BOOT_DEVICE_CPGMAC:
#ifdef CONFIG_SPL_ETH_DEVICE
		spl_net_load_image(CONFIG_SPL_ETH_DEVICE);
#else
		spl_net_load_image(NULL);
#endif
		break;
#endif
#ifdef CONFIG_SPL_USBETH_SUPPORT
	case BOOT_DEVICE_USBETH:
		spl_net_load_image("usb_ether");
		break;
#endif
	default:
		debug("SPL: Un-supported Boot Device\n");
		hang();
	}

	switch (spl_image.os) {
	case IH_OS_U_BOOT:
		debug("Jumping to U-Boot\n");
		break;
#ifdef CONFIG_SPL_OS_BOOT
	case IH_OS_LINUX:
		debug("Jumping to Linux\n");
		spl_board_prepare_for_linux();
		jump_to_image_linux((void *)CONFIG_SYS_SPL_ARGS_ADDR);
#endif
	default:
		debug("Unsupported OS image.. Jumping nevertheless..\n");
	}
	jump_to_image_no_args(&spl_image);
}

/*
 * This requires UART clocks to be enabled.  In order for this to work the
 * caller must ensure that the gd pointer is valid.
 */
void preloader_console_init(void)
{
	gd->bd = &bdata;
	gd->baudrate = CONFIG_BAUDRATE;

	serial_init();		/* serial communications setup */

	gd->have_console = 1;

	puts("\nU-Boot SPL " PLAIN_VERSION " (" U_BOOT_DATE " - " \
			U_BOOT_TIME ")\n");
#ifdef CONFIG_SPL_DISPLAY_PRINT
	spl_display_print();
#endif
}