blob: d5ae9a9eb14d718f73eb9a6ab9cfc6c1c259ad30 (
plain) (
blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
|
This driver supports NE2000 compatible cards (those based on DP8390,
DP83902 and similar). It can be used with PCMCIA/CF cards provided
that the CCR is correctly initialized.
The code is based on sources from the Linux kernel (pcnet_cs.c,
8390.h) and eCOS(if_dp83902a.c, if_dp83902a.h). Both of these 2
wonderful world are GPL, so this is, of course, GPL.
I developed and tested this driver on a custom PXA255 based system and
with a billionton CF network card connected to the PCMCIA interface of
the micro (have a look at README.PXA_CF for the support of this port).
The options you have to specify in the config file are (with the
value for my board as an example):
#define CONFIG_DRIVER_NE2000
- Enables the driver
#define CONFIG_DRIVER_NE2000_BASE (0x20000000+0x300)
- Address where the board is mapped
#define CONFIG_DRIVER_NE2000_CCR (0x28000000+0x3f8)
- Address of the CCR (card configuration register). It could be found
by enabling DEBUG in cmd_pcmcia.c. If this is not defined nothing is
done as far as PCMCIA support is concerned.
#define CONFIG_DRIVER_NE2000_VAL (0x20)
- The value to be written in the CCR. It selects among different I/O
spaces that could be used by the card.
Enjoy!
Christian Pellegrin <chri@ascensit.com>
|