aboutsummaryrefslogtreecommitdiffstats
blob: 6a2cf93db123a43728c82d67ffe0dc3e7742d617 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
/*
 * Porting to U-Boot:
 *
 * (C) Copyright 2010
 * Stefano Babic, DENX Software Engineering, sbabic@denx.de.
 *
 * Lattice's ispVME Embedded Tool to load Lattice's FPGA:
 *
 * Lattice Semiconductor Corp. Copyright 2009
 *
 * See file CREDITS for list of people who contributed to this
 * project.
 *
 * This program is free software; you can redistribute it and/or
 * modify it under the terms of the GNU General Public License as
 * published by the Free Software Foundation; either version 2 of
 * the License, or (at your option) any later version.
 *
 * This program is distributed in the hope that it will be useful,
 * but WITHOUT ANY WARRANTY; without even the implied warranty of
 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
 * GNU General Public License for more details.
 *
 * You should have received a copy of the GNU General Public License
 * along with this program; if not, write to the Free Software
 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
 * MA 02111-1307 USA
 *
 */

#ifndef _VME_OPCODE_H
#define _VME_OPCODE_H

#define VME_VERSION_NUMBER "12.1"

/* Maximum declarations. */

#define VMEHEXMAX	60000L	/* The hex file is split 60K per file. */
#define SCANMAX		64000L	/* The maximum SDR/SIR burst. */

/*
 *
 * Supported JTAG state transitions.
 *
 */

#define RESET		0x00
#define IDLE		0x01
#define IRPAUSE		0x02
#define DRPAUSE		0x03
#define SHIFTIR		0x04
#define SHIFTDR		0x05
/* 11/15/05 Nguyen changed to support DRCAPTURE*/
#define DRCAPTURE	0x06

/*
 * Flow control register bit definitions.  A set bit indicates
 * that the register currently exhibits the corresponding mode.
 */

#define INTEL_PRGM	0x0001	/* Intelligent programming is in effect. */
#define CASCADE		0x0002	/* Currently splitting large SDR. */
#define REPEATLOOP	0x0008	/* Currently executing a repeat loop. */
#define SHIFTRIGHT	0x0080	/* The next data stream needs a right shift. */
#define SHIFTLEFT	0x0100	/* The next data stream needs a left shift. */
#define VERIFYUES	0x0200	/* Continue if fail is in effect. */

/*
 * DataType register bit definitions.  A set bit indicates
 * that the register currently holds the corresponding type of data.
 */

#define EXPRESS		0x0001    /* Simultaneous program and verify. */
#define SIR_DATA	0x0002    /* SIR is the active SVF command. */
#define SDR_DATA	0x0004    /* SDR is the active SVF command. */
#define COMPRESS	0x0008    /* Data is compressed. */
#define TDI_DATA	0x0010    /* TDI data is present. */
#define TDO_DATA	0x0020    /* TDO data is present. */
#define MASK_DATA	0x0040    /* MASK data is present. */
#define HEAP_IN		0x0080    /* Data is from the heap. */
#define LHEAP_IN	0x0200    /* Data is from intel data buffer. */
#define VARIABLE	0x0400    /* Data is from a declared variable. */
#define CRC_DATA	0x0800	 /* CRC data is pressent. */
#define CMASK_DATA	0x1000    /* CMASK data is pressent. */
#define RMASK_DATA	0x2000	 /* RMASK data is pressent. */
#define READ_DATA	0x4000    /* READ data is pressent. */
#define DMASK_DATA	0x8000	 /* DMASK data is pressent. */

/*
 *
 * Pin opcodes.
 *
 */

#define signalENABLE	0x1C    /* ispENABLE pin. */
#define signalTMS	0x1D    /* TMS pin. */
#define signalTCK	0x1E    /* TCK pin. */
#define signalTDI	0x1F    /* TDI pin. */
#define signalTRST	0x20    /* TRST pin. */

/*
 *
 * Supported vendors.
 *
 */

#define VENDOR		0x56
#define LATTICE		0x01
#define ALTERA		0x02
#define XILINX		0x03

/*
 * Opcode definitions.
 *
 * Note: opcodes must be unique.
 */

#define ENDDATA		0x00	/* The end of the current SDR data stream. */
#define RUNTEST		0x01	/* The duration to stay at the stable state. */
#define ENDDR		0x02	/* The stable state after SDR. */
#define ENDIR		0x03	/* The stable state after SIR. */
#define ENDSTATE	0x04	/* The stable state after RUNTEST. */
#define TRST		0x05	/* Assert the TRST pin. */
#define HIR		0x06	/*
				 * The sum of the IR bits of the
				 * leading devices.
				 */
#define TIR		0x07	/*
				 * The sum of the IR bits of the trailing
				 * devices.
				 */
#define HDR		0x08	/* The number of leading devices. */
#define TDR		0x09	/* The number of trailing devices. */
#define ispEN		0x0A	/* Assert the ispEN pin. */
#define FREQUENCY	0x0B	/*
				 * The maximum clock rate to run the JTAG state
				 * machine.
				 */
#define STATE		0x10	/* Move to the next stable state. */
#define SIR		0x11	/* The instruction stream follows. */
#define SDR		0x12	/* The data stream follows. */
#define TDI		0x13	/* The following data stream feeds into
					the device. */
#define TDO		0x14	/*
				 * The following data stream is compared against
				 * the device.
				 */
#define MASK		0x15	/* The following data stream is used as mask. */
#define XSDR		0x16	/*
				 * The following data stream is for simultaneous
				 * program and verify.
				 */
#define XTDI		0x17	/* The following data stream is for shift in
				 * only. It must be stored for the next
				 * XSDR.
				 */
#define XTDO		0x18	/*
				 * There is not data stream.  The data stream
				 * was stored from the previous XTDI.
				 */
#define MEM		0x19	/*
				 * The maximum memory needed to allocate in
				 * order hold one row of data.
				 */
#define WAIT		0x1A	/* The duration of delay to observe. */
#define TCK		0x1B	/* The number of TCK pulses. */
#define SHR		0x23	/*
				 * Set the flow control register for
				 * right shift
				 */
#define SHL		0x24	/*
				 * Set the flow control register for left shift.
				 */
#define HEAP		0x32	/* The memory size needed to hold one loop. */
#define REPEAT		0x33	/* The beginning of the loop. */
#define LEFTPAREN	0x35	/* The beginning of data following the loop. */
#define VAR		0x55	/* Plac holder for loop data. */
#define SEC		0x1C	/*
				 * The delay time in seconds that must be
				 * observed.
				 */
#define SMASK		0x1D	/* The mask for TDI data. */
#define MAX_WAIT	0x1E	/* The absolute maximum wait time. */
#define ON		0x1F	/* Assert the targeted pin. */
#define OFF		0x20	/* Dis-assert the targeted pin. */
#define SETFLOW		0x30	/* Change the flow control register. */
#define RESETFLOW	0x31	/* Clear the flow control register. */

#define CRC		0x47	/*
				 * The following data stream is used for CRC
				 * calculation.
				 */
#define CMASK		0x48	/*
				 * The following data stream is used as mask
				 * for CRC calculation.
				 */
#define RMASK		0x49	/*
				 * The following data stream is used as mask
				 * for read and save.
				 */
#define READ		0x50	/*
				 * The following data stream is used for read
				 * and save.
				 */
#define ENDLOOP		0x59	/* The end of the repeat loop. */
#define SECUREHEAP	0x60	/* Used to secure the HEAP opcode. */
#define VUES		0x61	/* Support continue if fail. */
#define DMASK		0x62	/*
				 * The following data stream is used for dynamic
				 * I/O.
				 */
#define COMMENT		0x63	/* Support SVF comments in the VME file. */
#define HEADER		0x64	/* Support header in VME file. */
#define FILE_CRC	0x65	/* Support crc-protected VME file. */
#define LCOUNT		0x66	/* Support intelligent programming. */
#define LDELAY		0x67	/* Support intelligent programming. */
#define LSDR		0x68	/* Support intelligent programming. */
#define LHEAP		0x69	/*
				 * Memory needed to hold intelligent data
				 * buffer
				 */
#define CONTINUE	0x70	/* Allow continuation. */
#define LVDS		0x71	/* Support LVDS. */
#define ENDVME		0x7F	/* End of the VME file. */
#define ENDFILE		0xFF	/* End of file. */

/*
 *
 * ispVM Embedded Return Codes.
 *
 */

#define VME_VERIFICATION_FAILURE	-1
#define VME_FILE_READ_FAILURE		-2
#define VME_VERSION_FAILURE		-3
#define VME_INVALID_FILE		-4
#define VME_ARGUMENT_FAILURE		-5
#define VME_CRC_FAILURE			-6

#define g_ucPinTDI	0x01
#define g_ucPinTCK	0x02
#define g_ucPinTMS	0x04
#define g_ucPinENABLE	0x08
#define g_ucPinTRST	0x10

/*
 *
 * Type definitions.
 *
 */

/* Support LVDS */
typedef struct {
	unsigned short usPositiveIndex;
	unsigned short usNegativeIndex;
	unsigned char  ucUpdate;
} LVDSPair;

typedef enum {
	min_lattice_iface_type,		/* insert all new types after this */
	lattice_jtag_mode,		/* jtag/tap  */
	max_lattice_iface_type		/* insert all new types before this */
} Lattice_iface;

typedef enum {
	min_lattice_type,
	Lattice_XP2,			/* Lattice XP2 Family */
	max_lattice_type		/* insert all new types before this */
} Lattice_Family;

typedef struct {
	Lattice_Family	family;	/* part type */
	Lattice_iface	iface;	/* interface type */
	size_t		size;	/* bytes of data part can accept */
	void		*iface_fns; /* interface function table */
	void		*base;	/* base interface address */
	int		cookie;	/* implementation specific cookie */
	char		*desc;	/* description string */
} Lattice_desc;			/* end, typedef Altera_desc */

/* Lattice Model Type */
#define CONFIG_SYS_XP2		CONFIG_SYS_FPGA_DEV(0x1)

/* Board specific implementation specific function types */
typedef void (*Lattice_jtag_init)(void);
typedef void (*Lattice_jtag_set_tdi)(int v);
typedef void (*Lattice_jtag_set_tms)(int v);
typedef void (*Lattice_jtag_set_tck)(int v);
typedef int (*Lattice_jtag_get_tdo)(void);

typedef struct {
	Lattice_jtag_init	jtag_init;
	Lattice_jtag_set_tdi	jtag_set_tdi;
	Lattice_jtag_set_tms	jtag_set_tms;
	Lattice_jtag_set_tck	jtag_set_tck;
	Lattice_jtag_get_tdo	jtag_get_tdo;
} lattice_board_specific_func;

void writePort(unsigned char pins, unsigned char value);
unsigned char readPort(void);
void sclock(void);
void ispVMDelay(unsigned short int a_usMicroSecondDelay);
void calibration(void);

int lattice_load(Lattice_desc *desc, const void *buf, size_t bsize);
int lattice_dump(Lattice_desc *desc, const void *buf, size_t bsize);
int lattice_info(Lattice_desc *desc);

void ispVMStart(void);
void ispVMEnd(void);
extern void ispVMFreeMem(void);
signed char ispVMCode(void);
void ispVMDelay(unsigned short int a_usMicroSecondDelay);
void ispVMCalculateCRC32(unsigned char a_ucData);
unsigned char GetByte(void);
void writePort(unsigned char pins, unsigned char value);
unsigned char readPort(void);
void sclock(void);
#endif