summaryrefslogtreecommitdiffstats
path: root/audio
Commit message (Collapse)AuthorAgeFilesLines
* audio: primary: Allocate temporary buffer for resamplingMisael Lopez Cruz2017-01-171-19/+23
| | | | | | | | | | | | | Resampling and remixing requires a temporary buffer to read audio frames at native format (i.e. stereo, 44.1kHz). This temporary buffer was being allocated for remixing but not for resampling. The buffer is now being allocated for the worst case, which is when resampling and remixing are both required. Change-Id: I0e5eb0a45906067f04bd93313cd51e8cdc0d1a9a Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
* Set product files and packages for APPE based audioPraneeth Bajjuri2017-01-171-0/+6
| | | | | | | | | | | | | | | | The APPE HAL and the previous primary HAL cannot coexist, so the APPE HAL must become the primary HAL when the APPE_AUDIO feature is enabled. Similarly, some product files are specific to APPE and replace those used by the previous primary and JAMR3 HALs. Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com> [move to am57xevm but do not enable APPE/JAMR changes as they might be not applicable on this EVM] Signed-off-by: Praneeth Bajjuri <praneeth@ti.com> Change-Id: I2911e58fcefb4c8dd5e8bbda1ff01f816aa57f31
* AM57xevm: Initial Device project baselinePraneeth Bajjuri2016-04-279-0/+3273
Initial commit based on jacinto6evm board Signed-off-by: Praneeth Bajjuri <praneeth@ti.com>