diff options
Diffstat (limited to 'overlay/frameworks/base/core/res/res/values/config.xml')
-rw-r--r-- | overlay/frameworks/base/core/res/res/values/config.xml | 107 |
1 files changed, 107 insertions, 0 deletions
diff --git a/overlay/frameworks/base/core/res/res/values/config.xml b/overlay/frameworks/base/core/res/res/values/config.xml new file mode 100644 index 0000000..15ddf65 --- /dev/null +++ b/overlay/frameworks/base/core/res/res/values/config.xml | |||
@@ -0,0 +1,107 @@ | |||
1 | <?xml version="1.0" encoding="utf-8"?> | ||
2 | <!-- | ||
3 | /* | ||
4 | ** Copyright 2011, The Android Open Source Project | ||
5 | ** | ||
6 | ** Licensed under the Apache License, Version 2.0 (the "License"); | ||
7 | ** you may not use this file except in compliance with the License. | ||
8 | ** You may obtain a copy of the License at | ||
9 | ** | ||
10 | ** http://www.apache.org/licenses/LICENSE-2.0 | ||
11 | ** | ||
12 | ** Unless required by applicable law or agreed to in writing, software | ||
13 | ** distributed under the License is distributed on an "AS IS" BASIS, | ||
14 | ** WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. | ||
15 | ** See the License for the specific language governing permissions and | ||
16 | ** limitations under the License. | ||
17 | */ | ||
18 | --> | ||
19 | |||
20 | <!-- These resources are around just to allow their values to be customized | ||
21 | for different hardware and product builds. --> | ||
22 | <resources> | ||
23 | |||
24 | <!-- Enable multi-user. --> | ||
25 | <bool name="config_enableMultiUserUI">true</bool> | ||
26 | <!-- Arbitrary max 8 users. --> | ||
27 | <integer name="config_multiuserMaximumUsers">8</integer> | ||
28 | |||
29 | <!-- This device is not "voice capable"; it's data-only. --> | ||
30 | <bool name="config_voice_capable">false</bool> | ||
31 | |||
32 | <!-- This device does not allow sms service. --> | ||
33 | <bool name="config_sms_capable">false</bool> | ||
34 | |||
35 | <!-- List of regexpressions describing the interface (if any) that represent tetherable | ||
36 | Wifi interfaces. If the device doesn't want to support tethering over Wifi this | ||
37 | should be empty. An example would be "softap.*" --> | ||
38 | <string-array translatable="false" name="config_tether_wifi_regexs"> | ||
39 | </string-array> | ||
40 | |||
41 | <!-- Array of ConnectivityManager.TYPE_xxxx values allowable for tethering --> | ||
42 | <!-- [1,7,9] for TYPE_WIFI, TYPE_BLUETOOTH and TYPE_ETHERNET--> | ||
43 | <integer-array translatable="false" name="config_tether_upstream_types"> | ||
44 | <item>9</item> | ||
45 | </integer-array> | ||
46 | |||
47 | <!-- This string array should be overridden by the device to present a list of network | ||
48 | attributes. This is used by the connectivity manager to decide which networks can coexist | ||
49 | based on the hardware --> | ||
50 | <!-- An Array of "[Connection name],[ConnectivityManager connection type], | ||
51 | [associated radio-type],[priority],[restoral-timer(ms)],[dependencyMet] --> | ||
52 | <!-- the 5th element "resore-time" indicates the number of milliseconds to delay | ||
53 | before automatically restore the default connection. Set -1 if the connection | ||
54 | does not require auto-restore. --> | ||
55 | <!-- the 6th element indicates boot-time dependency-met value. --> | ||
56 | <string-array translatable="false" name="networkAttributes"> | ||
57 | <item>"ethernet,9,9,0,-1,true"</item> | ||
58 | </string-array> | ||
59 | |||
60 | <!-- This string array should be overridden by the device to present a list of radio | ||
61 | attributes. This is used by the connectivity manager to decide which networks can coexist | ||
62 | based on the hardware --> | ||
63 | <!-- An Array of "[ConnectivityManager connectionType], | ||
64 | [# simultaneous connection types]" --> | ||
65 | <string-array translatable="false" name="radioAttributes"> | ||
66 | <item>"9,1"</item> | ||
67 | </string-array> | ||
68 | |||
69 | <!-- Boolean indicating whether the wifi chipset has dual frequency band support --> | ||
70 | <bool translatable="false" name="config_wifi_dual_band_support">true</bool> | ||
71 | |||
72 | <!-- List of regexpressions describing the interface (if any) that represent tetherable | ||
73 | bluetooth interfaces. If the device doesn't want to support tethering over bluetooth this | ||
74 | should be empty. --> | ||
75 | <string-array translatable="false" name="config_tether_bluetooth_regexs"> | ||
76 | </string-array> | ||
77 | |||
78 | <!-- Separate software navigation bar required on this device. --> | ||
79 | <bool name="config_showNavigationBar">true</bool> | ||
80 | |||
81 | <!-- Whether WiFi display is supported by this device. | ||
82 | There are many prerequisites for this feature to work correctly. | ||
83 | Here are a few of them: | ||
84 | * The WiFi radio must support WiFi P2P. | ||
85 | * The WiFi radio must support concurrent connections to the WiFi display and | ||
86 | to an access point. | ||
87 | * The Audio Flinger audio_policy.conf file must specify a rule for the "r_submix" | ||
88 | remote submix module. This module is used to record and stream system | ||
89 | audio output to the WiFi display encoder in the media server. | ||
90 | * The remote submix module "audio.r_submix.default" must be installed on the device. | ||
91 | * The device must be provisioned with HDCP keys (for protected content). | ||
92 | --> | ||
93 | <bool name="config_enableWifiDisplay">false</bool> | ||
94 | |||
95 | <!-- Default list of files pinned by the Pinner Service --> | ||
96 | <string-array translatable="false" name="config_defaultPinnerServiceFiles"> | ||
97 | <item>"/system/framework/arm/boot-framework.oat"</item> | ||
98 | <item>"/system/framework/arm/boot-framework.vdex"</item> | ||
99 | <item>"/system/framework/oat/arm/services.odex"</item> | ||
100 | <item>"/system/framework/oat/arm/services.vdex"</item> | ||
101 | <item>"/system/framework/arm/boot.oat"</item> | ||
102 | <item>"/system/framework/arm/boot.vdex"</item> | ||
103 | <item>"/system/framework/arm/boot-core-libart.oat"</item> | ||
104 | <item>"/system/framework/arm/boot-core-libart.vdex"</item> | ||
105 | </string-array> | ||
106 | |||
107 | </resources> | ||