diff options
Diffstat (limited to 'overlay/frameworks/base/core/res/res/values/config.xml')
-rw-r--r-- | overlay/frameworks/base/core/res/res/values/config.xml | 102 |
1 files changed, 89 insertions, 13 deletions
diff --git a/overlay/frameworks/base/core/res/res/values/config.xml b/overlay/frameworks/base/core/res/res/values/config.xml index 7cc17c1..53bf751 100644 --- a/overlay/frameworks/base/core/res/res/values/config.xml +++ b/overlay/frameworks/base/core/res/res/values/config.xml | |||
@@ -1,31 +1,107 @@ | |||
1 | <?xml version="1.0" encoding="utf-8"?> | 1 | <?xml version="1.0" encoding="utf-8"?> |
2 | <!-- | 2 | <!-- |
3 | Copyright (C) 2018 Texas Instruments Incorporated - http://www.ti.com/ | 3 | /* |
4 | 4 | ** Copyright 2018, The Android Open Source Project | |
5 | Licensed under the Apache License, Version 2.0 (the "License"); | 5 | ** |
6 | you may not use this file except in compliance with the License. | 6 | ** Licensed under the Apache License, Version 2.0 (the "License"); |
7 | You may obtain a copy of the License at | 7 | ** you may not use this file except in compliance with the License. |
8 | 8 | ** You may obtain a copy of the License at | |
9 | http://www.apache.org/licenses/LICENSE-2.0 | 9 | ** |
10 | 10 | ** http://www.apache.org/licenses/LICENSE-2.0 | |
11 | Unless required by applicable law or agreed to in writing, software | 11 | ** |
12 | distributed under the License is distributed on an "AS IS" BASIS, | 12 | ** Unless required by applicable law or agreed to in writing, software |
13 | WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. | 13 | ** distributed under the License is distributed on an "AS IS" BASIS, |
14 | See the License for the specific language governing permissions and | 14 | ** WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. |
15 | limitations under the License. | 15 | ** See the License for the specific language governing permissions and |
16 | ** limitations under the License. | ||
17 | */ | ||
16 | --> | 18 | --> |
17 | 19 | ||
18 | <!-- These resources are around just to allow their values to be customized | 20 | <!-- These resources are around just to allow their values to be customized |
19 | for different hardware and product builds. --> | 21 | for different hardware and product builds. --> |
20 | <resources> | 22 | <resources> |
21 | 23 | ||
24 | <!-- Enable multi-user. --> | ||
25 | <bool name="config_enableMultiUserUI">true</bool> | ||
26 | <!-- Arbitrary max 8 users. --> | ||
27 | <integer name="config_multiuserMaximumUsers">8</integer> | ||
28 | |||
22 | <!-- This device is not "voice capable"; it's data-only. --> | 29 | <!-- This device is not "voice capable"; it's data-only. --> |
23 | <bool name="config_voice_capable">false</bool> | 30 | <bool name="config_voice_capable">false</bool> |
24 | 31 | ||
25 | <!-- This device does not allow sms service. --> | 32 | <!-- This device does not allow sms service. --> |
26 | <bool name="config_sms_capable">false</bool> | 33 | <bool name="config_sms_capable">false</bool> |
27 | 34 | ||
35 | <!-- List of regexpressions describing the interface (if any) that represent tetherable | ||
36 | Wifi interfaces. If the device doesn't want to support tethering over Wifi this | ||
37 | should be empty. An example would be "softap.*" --> | ||
38 | <string-array translatable="false" name="config_tether_wifi_regexs"> | ||
39 | </string-array> | ||
40 | |||
41 | <!-- Array of ConnectivityManager.TYPE_xxxx values allowable for tethering --> | ||
42 | <!-- [1,7,9] for TYPE_WIFI, TYPE_BLUETOOTH and TYPE_ETHERNET--> | ||
43 | <integer-array translatable="false" name="config_tether_upstream_types"> | ||
44 | <item>9</item> | ||
45 | </integer-array> | ||
46 | |||
47 | <!-- This string array should be overridden by the device to present a list of network | ||
48 | attributes. This is used by the connectivity manager to decide which networks can coexist | ||
49 | based on the hardware --> | ||
50 | <!-- An Array of "[Connection name],[ConnectivityManager connection type], | ||
51 | [associated radio-type],[priority],[restoral-timer(ms)],[dependencyMet] --> | ||
52 | <!-- the 5th element "resore-time" indicates the number of milliseconds to delay | ||
53 | before automatically restore the default connection. Set -1 if the connection | ||
54 | does not require auto-restore. --> | ||
55 | <!-- the 6th element indicates boot-time dependency-met value. --> | ||
56 | <string-array translatable="false" name="networkAttributes"> | ||
57 | <item>"ethernet,9,9,0,-1,true"</item> | ||
58 | </string-array> | ||
59 | |||
60 | <!-- This string array should be overridden by the device to present a list of radio | ||
61 | attributes. This is used by the connectivity manager to decide which networks can coexist | ||
62 | based on the hardware --> | ||
63 | <!-- An Array of "[ConnectivityManager connectionType], | ||
64 | [# simultaneous connection types]" --> | ||
65 | <string-array translatable="false" name="radioAttributes"> | ||
66 | <item>"9,1"</item> | ||
67 | </string-array> | ||
68 | |||
69 | <!-- Boolean indicating whether the wifi chipset has dual frequency band support --> | ||
70 | <bool translatable="false" name="config_wifi_dual_band_support">true</bool> | ||
71 | |||
72 | <!-- List of regexpressions describing the interface (if any) that represent tetherable | ||
73 | bluetooth interfaces. If the device doesn't want to support tethering over bluetooth this | ||
74 | should be empty. --> | ||
75 | <string-array translatable="false" name="config_tether_bluetooth_regexs"> | ||
76 | </string-array> | ||
77 | |||
28 | <!-- Separate software navigation bar required on this device. --> | 78 | <!-- Separate software navigation bar required on this device. --> |
29 | <bool name="config_showNavigationBar">true</bool> | 79 | <bool name="config_showNavigationBar">true</bool> |
30 | 80 | ||
81 | <!-- Whether WiFi display is supported by this device. | ||
82 | There are many prerequisites for this feature to work correctly. | ||
83 | Here are a few of them: | ||
84 | * The WiFi radio must support WiFi P2P. | ||
85 | * The WiFi radio must support concurrent connections to the WiFi display and | ||
86 | to an access point. | ||
87 | * The Audio Flinger audio_policy.conf file must specify a rule for the "r_submix" | ||
88 | remote submix module. This module is used to record and stream system | ||
89 | audio output to the WiFi display encoder in the media server. | ||
90 | * The remote submix module "audio.r_submix.default" must be installed on the device. | ||
91 | * The device must be provisioned with HDCP keys (for protected content). | ||
92 | --> | ||
93 | <bool name="config_enableWifiDisplay">false</bool> | ||
94 | |||
95 | <!-- Default list of files pinned by the Pinner Service --> | ||
96 | <string-array translatable="false" name="config_defaultPinnerServiceFiles"> | ||
97 | <item>"/system/framework/arm/boot-framework.oat"</item> | ||
98 | <item>"/system/framework/arm/boot-framework.vdex"</item> | ||
99 | <item>"/system/framework/oat/arm/services.odex"</item> | ||
100 | <item>"/system/framework/oat/arm/services.vdex"</item> | ||
101 | <item>"/system/framework/arm/boot.oat"</item> | ||
102 | <item>"/system/framework/arm/boot.vdex"</item> | ||
103 | <item>"/system/framework/arm/boot-core-libart.oat"</item> | ||
104 | <item>"/system/framework/arm/boot-core-libart.vdex"</item> | ||
105 | </string-array> | ||
106 | |||
31 | </resources> | 107 | </resources> |