diff options
Diffstat (limited to 'utils/kmstest.cpp')
-rw-r--r-- | utils/kmstest.cpp | 94 |
1 files changed, 91 insertions, 3 deletions
diff --git a/utils/kmstest.cpp b/utils/kmstest.cpp index fee3070..0f763c0 100644 --- a/utils/kmstest.cpp +++ b/utils/kmstest.cpp | |||
@@ -4,6 +4,8 @@ | |||
4 | #include <regex> | 4 | #include <regex> |
5 | #include <set> | 5 | #include <set> |
6 | #include <chrono> | 6 | #include <chrono> |
7 | #include <cstdint> | ||
8 | #include <cinttypes> | ||
7 | 9 | ||
8 | #include <sys/select.h> | 10 | #include <sys/select.h> |
9 | 11 | ||
@@ -16,6 +18,13 @@ | |||
16 | using namespace std; | 18 | using namespace std; |
17 | using namespace kms; | 19 | using namespace kms; |
18 | 20 | ||
21 | struct PropInfo { | ||
22 | PropInfo(Property *p, uint64_t v) : prop(p), val(v) {} | ||
23 | |||
24 | Property *prop; | ||
25 | uint64_t val; | ||
26 | }; | ||
27 | |||
19 | struct PlaneInfo | 28 | struct PlaneInfo |
20 | { | 29 | { |
21 | Plane* plane; | 30 | Plane* plane; |
@@ -31,6 +40,8 @@ struct PlaneInfo | |||
31 | unsigned view_h; | 40 | unsigned view_h; |
32 | 41 | ||
33 | vector<Framebuffer*> fbs; | 42 | vector<Framebuffer*> fbs; |
43 | |||
44 | vector<PropInfo> props; | ||
34 | }; | 45 | }; |
35 | 46 | ||
36 | struct OutputInfo | 47 | struct OutputInfo |
@@ -44,6 +55,9 @@ struct OutputInfo | |||
44 | vector<Framebuffer*> fbs; | 55 | vector<Framebuffer*> fbs; |
45 | 56 | ||
46 | vector<PlaneInfo> planes; | 57 | vector<PlaneInfo> planes; |
58 | |||
59 | vector<PropInfo> conn_props; | ||
60 | vector<PropInfo> crtc_props; | ||
47 | }; | 61 | }; |
48 | 62 | ||
49 | static bool s_use_dmt; | 63 | static bool s_use_dmt; |
@@ -267,6 +281,23 @@ static void parse_plane(ResourceManager& resman, Card& card, const string& plane | |||
267 | pinfo.y = output.mode.vdisplay / 2 - pinfo.h / 2; | 281 | pinfo.y = output.mode.vdisplay / 2 - pinfo.h / 2; |
268 | } | 282 | } |
269 | 283 | ||
284 | static void parse_prop(Card& card, const string& prop_str, vector<PropInfo> &props, const DrmPropObject* propobj) | ||
285 | { | ||
286 | string name, val; | ||
287 | Property* prop; | ||
288 | |||
289 | size_t split = prop_str.find("="); | ||
290 | |||
291 | if (split == string::npos) | ||
292 | EXIT("Equal sign ('=') not found in %s", prop_str.c_str()); | ||
293 | |||
294 | name = prop_str.substr(0, split); | ||
295 | val = prop_str.substr(split+1); | ||
296 | prop = propobj->get_prop(name); | ||
297 | |||
298 | props.push_back(PropInfo(prop, stoull(val, 0, 0))); | ||
299 | } | ||
300 | |||
270 | static vector<Framebuffer*> get_default_fb(Card& card, unsigned width, unsigned height) | 301 | static vector<Framebuffer*> get_default_fb(Card& card, unsigned width, unsigned height) |
271 | { | 302 | { |
272 | vector<Framebuffer*> v; | 303 | vector<Framebuffer*> v; |
@@ -336,6 +367,7 @@ static const char* usage_str = | |||
336 | " -p, --plane=PLANE PLANE is [<plane>:][<x>,<y>-]<w>x<h>\n" | 367 | " -p, --plane=PLANE PLANE is [<plane>:][<x>,<y>-]<w>x<h>\n" |
337 | " -f, --fb=FB FB is [<w>x<h>][-][<4cc>]\n" | 368 | " -f, --fb=FB FB is [<w>x<h>][-][<4cc>]\n" |
338 | " -v, --view=VIEW VIEW is <x>,<y>-<w>x<h>\n" | 369 | " -v, --view=VIEW VIEW is <x>,<y>-<w>x<h>\n" |
370 | " -P, --property=PROP=VAL Set PROP to VAL in the previous DRM object\n" | ||
339 | " --dmt Search for the given mode from DMT tables\n" | 371 | " --dmt Search for the given mode from DMT tables\n" |
340 | " --cea Search for the given mode from CEA tables\n" | 372 | " --cea Search for the given mode from CEA tables\n" |
341 | " --cvt=CVT Create videomode with CVT. CVT is 'v1', 'v2' or 'v2o'\n" | 373 | " --cvt=CVT Create videomode with CVT. CVT is 'v1', 'v2' or 'v2o'\n" |
@@ -378,6 +410,7 @@ enum class ArgType | |||
378 | Plane, | 410 | Plane, |
379 | Framebuffer, | 411 | Framebuffer, |
380 | View, | 412 | View, |
413 | Property, | ||
381 | }; | 414 | }; |
382 | 415 | ||
383 | struct Arg | 416 | struct Arg |
@@ -419,6 +452,10 @@ static vector<Arg> parse_cmdline(int argc, char **argv) | |||
419 | { | 452 | { |
420 | args.push_back(Arg { ArgType::View, s }); | 453 | args.push_back(Arg { ArgType::View, s }); |
421 | }), | 454 | }), |
455 | Option("P|property=", [&](string s) | ||
456 | { | ||
457 | args.push_back(Arg { ArgType::Property, s }); | ||
458 | }), | ||
422 | Option("|dmt", []() | 459 | Option("|dmt", []() |
423 | { | 460 | { |
424 | s_use_dmt = true; | 461 | s_use_dmt = true; |
@@ -590,6 +627,28 @@ static vector<OutputInfo> setups_to_outputs(Card& card, ResourceManager& resman, | |||
590 | parse_view(arg.arg, *current_plane); | 627 | parse_view(arg.arg, *current_plane); |
591 | break; | 628 | break; |
592 | } | 629 | } |
630 | |||
631 | case ArgType::Property: | ||
632 | { | ||
633 | if (!current_output) | ||
634 | EXIT("No object to which set the property"); | ||
635 | |||
636 | if (current_plane) | ||
637 | parse_prop(card, arg.arg, current_plane->props, | ||
638 | current_plane->plane); | ||
639 | else if (current_output->crtc) | ||
640 | parse_prop(card, arg.arg, | ||
641 | current_output->crtc_props, | ||
642 | current_output->crtc); | ||
643 | else if (current_output->connector) | ||
644 | parse_prop(card, arg.arg, | ||
645 | current_output->conn_props, | ||
646 | current_output->connector); | ||
647 | else | ||
648 | EXIT("no object"); | ||
649 | |||
650 | break; | ||
651 | } | ||
593 | } | 652 | } |
594 | } | 653 | } |
595 | 654 | ||
@@ -631,9 +690,19 @@ static void print_outputs(const vector<OutputInfo>& outputs) | |||
631 | for (unsigned i = 0; i < outputs.size(); ++i) { | 690 | for (unsigned i = 0; i < outputs.size(); ++i) { |
632 | const OutputInfo& o = outputs[i]; | 691 | const OutputInfo& o = outputs[i]; |
633 | 692 | ||
634 | printf("Connector %u/@%u: %s\n", o.connector->idx(), o.connector->id(), | 693 | printf("Connector %u/@%u: %s", o.connector->idx(), o.connector->id(), |
635 | o.connector->fullname().c_str()); | 694 | o.connector->fullname().c_str()); |
636 | printf(" Crtc %u/@%u", o.crtc->idx(), o.crtc->id()); | 695 | |
696 | for (const PropInfo &prop: o.conn_props) | ||
697 | printf(" %s=%" PRIu64, prop.prop->name().c_str(), | ||
698 | prop.val); | ||
699 | |||
700 | printf("\n Crtc %u/@%u", o.crtc->idx(), o.crtc->id()); | ||
701 | |||
702 | for (const PropInfo &prop: o.crtc_props) | ||
703 | printf(" %s=%" PRIu64, prop.prop->name().c_str(), | ||
704 | prop.val); | ||
705 | |||
637 | if (o.primary_plane) | 706 | if (o.primary_plane) |
638 | printf(" (plane %u/@%u)", o.primary_plane->idx(), o.primary_plane->id()); | 707 | printf(" (plane %u/@%u)", o.primary_plane->idx(), o.primary_plane->id()); |
639 | printf(": %s\n", videomode_to_string(o.mode).c_str()); | 708 | printf(": %s\n", videomode_to_string(o.mode).c_str()); |
@@ -646,8 +715,13 @@ static void print_outputs(const vector<OutputInfo>& outputs) | |||
646 | for (unsigned j = 0; j < o.planes.size(); ++j) { | 715 | for (unsigned j = 0; j < o.planes.size(); ++j) { |
647 | const PlaneInfo& p = o.planes[j]; | 716 | const PlaneInfo& p = o.planes[j]; |
648 | auto fb = p.fbs[0]; | 717 | auto fb = p.fbs[0]; |
649 | printf(" Plane %u/@%u: %u,%u-%ux%u\n", p.plane->idx(), p.plane->id(), | 718 | printf(" Plane %u/@%u: %u,%u-%ux%u", p.plane->idx(), p.plane->id(), |
650 | p.x, p.y, p.w, p.h); | 719 | p.x, p.y, p.w, p.h); |
720 | for (const PropInfo &prop: p.props) | ||
721 | printf(" %s=%" PRIu64, prop.prop->name().c_str(), | ||
722 | prop.val); | ||
723 | printf("\n"); | ||
724 | |||
651 | printf(" Fb %u %ux%u-%s\n", fb->id(), fb->width(), fb->height(), | 725 | printf(" Fb %u %ux%u-%s\n", fb->id(), fb->width(), fb->height(), |
652 | PixelFormatToFourCC(fb->format()).c_str()); | 726 | PixelFormatToFourCC(fb->format()).c_str()); |
653 | } | 727 | } |
@@ -680,6 +754,9 @@ static void set_crtcs_n_planes_legacy(Card& card, const vector<OutputInfo>& outp | |||
680 | auto conn = o.connector; | 754 | auto conn = o.connector; |
681 | auto crtc = o.crtc; | 755 | auto crtc = o.crtc; |
682 | 756 | ||
757 | if (!o.conn_props.empty() || !o.crtc_props.empty()) | ||
758 | printf("WARNING: properties not set without atomic modesetting"); | ||
759 | |||
683 | if (!o.fbs.empty()) { | 760 | if (!o.fbs.empty()) { |
684 | auto fb = o.fbs[0]; | 761 | auto fb = o.fbs[0]; |
685 | int r = crtc->set_mode(conn, *fb, o.mode); | 762 | int r = crtc->set_mode(conn, *fb, o.mode); |
@@ -696,6 +773,8 @@ static void set_crtcs_n_planes_legacy(Card& card, const vector<OutputInfo>& outp | |||
696 | if (r) | 773 | if (r) |
697 | printf("crtc->set_plane() failed for plane %u: %s\n", | 774 | printf("crtc->set_plane() failed for plane %u: %s\n", |
698 | p.plane->id(), strerror(-r)); | 775 | p.plane->id(), strerror(-r)); |
776 | if (!p.props.empty()) | ||
777 | printf("WARNING: properties not set without atomic modesetting"); | ||
699 | } | 778 | } |
700 | } | 779 | } |
701 | } | 780 | } |
@@ -752,11 +831,17 @@ static void set_crtcs_n_planes_atomic(Card& card, const vector<OutputInfo>& outp | |||
752 | { "CRTC_ID", crtc->id() }, | 831 | { "CRTC_ID", crtc->id() }, |
753 | }); | 832 | }); |
754 | 833 | ||
834 | for (const PropInfo &prop: o.conn_props) | ||
835 | req.add(conn, prop.prop, prop.val); | ||
836 | |||
755 | req.add(crtc, { | 837 | req.add(crtc, { |
756 | { "ACTIVE", 1 }, | 838 | { "ACTIVE", 1 }, |
757 | { "MODE_ID", mode_blob->id() }, | 839 | { "MODE_ID", mode_blob->id() }, |
758 | }); | 840 | }); |
759 | 841 | ||
842 | for (const PropInfo &prop: o.crtc_props) | ||
843 | req.add(crtc, prop.prop, prop.val); | ||
844 | |||
760 | if (!o.fbs.empty()) { | 845 | if (!o.fbs.empty()) { |
761 | auto fb = o.fbs[0]; | 846 | auto fb = o.fbs[0]; |
762 | 847 | ||
@@ -789,6 +874,9 @@ static void set_crtcs_n_planes_atomic(Card& card, const vector<OutputInfo>& outp | |||
789 | { "CRTC_W", p.w }, | 874 | { "CRTC_W", p.w }, |
790 | { "CRTC_H", p.h }, | 875 | { "CRTC_H", p.h }, |
791 | }); | 876 | }); |
877 | |||
878 | for (const PropInfo &prop: p.props) | ||
879 | req.add(p.plane, prop.prop, prop.val); | ||
792 | } | 880 | } |
793 | } | 881 | } |
794 | 882 | ||