/*
* Copyright © 2008 Jérôme Glisse
* All Rights Reserved.
*
* Permission is hereby granted, free of charge, to any person obtaining
* a copy of this software and associated documentation files (the
* "Software"), to deal in the Software without restriction, including
* without limitation the rights to use, copy, modify, merge, publish,
* distribute, sub license, and/or sell copies of the Software, and to
* permit persons to whom the Software is furnished to do so, subject to
* the following conditions:
*
* THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND,
* EXPRESS OR IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES
* OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE AND
* NON-INFRINGEMENT. IN NO EVENT SHALL THE COPYRIGHT HOLDERS, AUTHORS
* AND/OR ITS SUPPLIERS BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER
* LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR OTHERWISE,
* ARISING FROM, OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE
* USE OR OTHER DEALINGS IN THE SOFTWARE.
*
* The above copyright notice and this permission notice (including the
* next paragraph) shall be included in all copies or substantial portions
* of the Software.
*/
/*
* Authors:
* Aapo Tahkola <aet@rasterburn.org>
* Nicolai Haehnle <prefect_@gmx.net>
* Jérôme Glisse <glisse@freedesktop.org>
*/
#include <assert.h>
#include <errno.h>
#include <stdlib.h>
#include <string.h>
#include <pthread.h>
#include <sys/mman.h>
#include <sys/ioctl.h>
#include "radeon_cs.h"
#include "radeon_cs_int.h"
#include "radeon_bo_int.h"
#include "radeon_cs_gem.h"
#include "radeon_bo_gem.h"
#include "drm.h"
#include "xf86drm.h"
#include "xf86atomic.h"
#include "radeon_drm.h"
#include "bof.h"
#define CS_BOF_DUMP 0
struct radeon_cs_manager_gem {
struct radeon_cs_manager base;
uint32_t device_id;
unsigned nbof;
};
#pragma pack(1)
struct cs_reloc_gem {
uint32_t handle;
uint32_t read_domain;
uint32_t write_domain;
uint32_t flags;
};
#pragma pack()
#define RELOC_SIZE (sizeof(struct cs_reloc_gem) / sizeof(uint32_t))
struct cs_gem {
struct radeon_cs_int base;
struct drm_radeon_cs cs;
struct drm_radeon_cs_chunk chunks[2];
unsigned nrelocs;
uint32_t *relocs;
struct radeon_bo_int **relocs_bo;
};
static pthread_mutex_t id_mutex = PTHREAD_MUTEX_INITIALIZER;
static uint32_t cs_id_source = 0;
/**
* result is undefined if called with ~0
*/
static uint32_t get_first_zero(const uint32_t n)
{
/* __builtin_ctz returns number of trailing zeros. */
return 1 << __builtin_ctz(~n);
}
/**
* Returns a free id for cs.
* If there is no free id we return zero
**/
static uint32_t generate_id(void)
{
uint32_t r = 0;
pthread_mutex_lock( &id_mutex );
/* check for free ids */
if (cs_id_source != ~r) {
/* find first zero bit */
r = get_first_zero(cs_id_source);
/* set id as reserved */
cs_id_source |= r;
}
pthread_mutex_unlock( &id_mutex );
return r;
}
/**
* Free the id for later reuse
**/
static void free_id(uint32_t id)
{
pthread_mutex_lock( &id_mutex );
cs_id_source &= ~id;
pthread_mutex_unlock( &id_mutex );
}
static struct radeon_cs_int *cs_gem_create(struct radeon_cs_manager *csm,
uint32_t ndw)
{
struct cs_gem *csg;
/* max cmd buffer size is 64Kb */
if (ndw > (64 * 1024 / 4)) {
return NULL;
}
csg = (struct cs_gem*)calloc(1, sizeof(struct cs_gem));
if (csg == NULL) {
return NULL;
}
csg->base.csm = csm;
csg->base.ndw = 64 * 1024 / 4;
csg->base.packets = (uint32_t*)calloc(1, 64 * 1024);
if (csg->base.packets == NULL) {
free(csg);
return NULL;
}
csg->base.relocs_total_size = 0;
csg->base.crelocs = 0;
csg->base.id = generate_id();
csg->nrelocs = 4096 / (4 * 4) ;
csg->relocs_bo = (struct radeon_bo_int**)calloc(1,
csg->nrelocs*sizeof(void*));
if (csg->relocs_bo == NULL) {
free(csg->base.packets);
free(csg);
return NULL;
}
csg->base.relocs = csg->relocs = (uint32_t*)calloc(1, 4096);
if (csg->relocs == NULL) {
free(csg->relocs_bo);
free(csg->base.packets);
free(csg);
return NULL;
}
csg->chunks[0].chunk_id = RADEON_CHUNK_ID_IB;
csg->chunks[0].length_dw = 0;
csg->chunks[0].chunk_data = (uint64_t)(uintptr_t)csg->base.packets;
csg->chunks[1].chunk_id = RADEON_CHUNK_ID_RELOCS;
csg->chunks[1].length_dw = 0;
csg->chunks[1].chunk_data = (uint64_t)(uintptr_t)csg->relocs;
return (struct radeon_cs_int*)csg;
}
static int cs_gem_write_reloc(struct radeon_cs_int *cs,
struct radeon_bo *bo,
uint32_t read_domain,
uint32_t write_domain,
uint32_t flags)
{
struct radeon_bo_int *boi = (struct radeon_bo_int *)bo;
struct cs_gem *csg = (struct cs_gem*)cs;
struct cs_reloc_gem *reloc;
uint32_t idx;
unsigned i;
assert(boi->space_accounted);
/* check domains */
if ((read_domain && write_domain) || (!read_domain && !write_domain)) {
/* in one CS a bo can only be in read or write domain but not
* in read & write domain at the same sime
*/
return -EINVAL;
}
if (read_domain == RADEON_GEM_DOMAIN_CPU) {
return -EINVAL;
}
if (write_domain == RADEON_GEM_DOMAIN_CPU) {
return -EINVAL;
}
/* use bit field hash function to determine
if this bo is for sure not in this cs.*/
if ((atomic_read((atomic_t *)radeon_gem_get_reloc_in_cs(bo)) & cs->id)) {
/* check if bo is already referenced.
* Scanning from end to begin reduces cycles with mesa because
* it often relocates same shared dma bo again. */
for(i = cs->crelocs; i != 0;) {
--i;
idx = i * RELOC_SIZE;
reloc = (struct cs_reloc_gem*)&csg->relocs[idx];
if (reloc->handle == bo->handle) {
/* Check domains must be in read or write. As we check already
* checked that in argument one of the read or write domain was
* set we only need to check that if previous reloc as the read
* domain set then the read_domain should also be set for this
* new relocation.
*/
/* the DDX expects to read and write from same pixmap */
if (write_domain && (reloc->read_domain & write_domain)) {
reloc->read_domain = 0;
reloc->write_domain = write_domain;
} else if (read_domain & reloc->write_domain) {
reloc->read_domain = 0;
} else {
if (write_domain != reloc->write_domain)
return -EINVAL;
if (read_domain != reloc->read_domain)
return -EINVAL;
}
reloc->read_domain |= read_domain;
reloc->write_domain |= write_domain;
/* update flags */
reloc->flags |= (flags & reloc->flags);
/* write relocation packet */
radeon_cs_write_dword((struct radeon_cs *)cs, 0xc0001000);
radeon_cs_write_dword((struct radeon_cs *)cs, idx);
return 0;
}
}
}
/* new relocation */
if (csg->base.crelocs >= csg->nrelocs) {
/* allocate more memory (TODO: should use a slab allocatore maybe) */
uint32_t *tmp, size;
size = ((csg->nrelocs + 1) * sizeof(struct radeon_bo*));
tmp = (uint32_t*)realloc(csg->relocs_bo, size);
if (tmp == NULL) {
return -ENOMEM;
}
csg->relocs_bo = (struct radeon_bo_int **)tmp;
size = ((csg->nrelocs + 1) * RELOC_SIZE * 4);
tmp = (uint32_t*)realloc(csg->relocs, size);
if (tmp == NULL) {
return -ENOMEM;
}
cs->relocs = csg->relocs = tmp;
csg->nrelocs += 1;
csg->chunks[1].chunk_data = (uint64_t)(uintptr_t)csg->relocs;
}
csg->relocs_bo[csg->base.crelocs] = boi;
idx = (csg->base.crelocs++) * RELOC_SIZE;
reloc = (struct cs_reloc_gem*)&csg->relocs[idx];
reloc->handle = bo->handle;
reloc->read_domain = read_domain;
reloc->write_domain = write_domain;
reloc->flags = flags;
csg->chunks[1].length_dw += RELOC_SIZE;
radeon_bo_ref(bo);
/* bo might be referenced from another context so have to use atomic opertions */
atomic_add((atomic_t *)radeon_gem_get_reloc_in_cs(bo), cs->id);
cs->relocs_total_size += boi->size;
radeon_cs_write_dword((struct radeon_cs *)cs, 0xc0001000);
radeon_cs_write_dword((struct radeon_cs *)cs, idx);
return 0;
}
static int cs_gem_begin(struct radeon_cs_int *cs,
uint32_t ndw,
const char *file,
const char *func,
int line)
{
if (cs->section_ndw) {
fprintf(stderr, "CS already in a section(%s,%s,%d)\n",
cs->section_file, cs->section_func, cs->section_line);
fprintf(stderr, "CS can't start section(%s,%s,%d)\n",
file, func, line);
return -EPIPE;
}
cs->section_ndw = ndw;
cs->section_cdw = 0;
cs->section_file = file;
cs->section_func = func;
cs->section_line = line;
if (cs->cdw + ndw > cs->ndw) {
uint32_t tmp, *ptr;
/* round up the required size to a multiple of 1024 */
tmp = (cs->cdw + ndw + 0x3FF) & (~0x3FF);
ptr = (uint32_t*)realloc(cs->packets, 4 * tmp);
if (ptr == NULL) {
return -ENOMEM;
}
cs->packets = ptr;
cs->ndw = tmp;
}
return 0;
}
static int cs_gem_end(struct radeon_cs_int *cs,
const char *file,
const char *func,
int line)
{
if (!cs->section_ndw) {
fprintf(stderr, "CS no section to end at (%s,%s,%d)\n",
file, func, line);
return -EPIPE;
}
if (cs->section_ndw != cs->section_cdw) {
fprintf(stderr, "CS section size missmatch start at (%s,%s,%d) %d vs %d\n",
cs->section_file, cs->section_func, cs->section_line, cs->section_ndw, cs->section_cdw);
fprintf(stderr, "CS section end at (%s,%s,%d)\n",
file, func, line);
/* We must reset the section even when there is error. */
cs->section_ndw = 0;
return -EPIPE;
}
cs->section_ndw = 0;
return 0;
}
#if CS_BOF_DUMP
static void cs_gem_dump_bof(struct radeon_cs_int *cs)
{
struct cs_gem *csg = (struct cs_gem*)cs;
struct radeon_cs_manager_gem *csm;
bof_t *bcs, *blob, *array, *bo, *size, *handle, *device_id, *root;
char tmp[256];
unsigned i;
csm = (struct radeon_cs_manager_gem *)cs->csm;
root = device_id = bcs = blob = array = bo = size = handle = NULL;
root = bof_object();
if (root == NULL)
goto out_err;
device_id = bof_int32(csm->device_id);
if (device_id == NULL)
return;
if (bof_object_set(root, "device_id", device_id))
goto out_err;
bof_decref(device_id);
device_id = NULL;
/* dump relocs */
blob = bof_blob(csg->nrelocs * 16, csg->relocs);
if (blob == NULL)
goto out_err;
if (bof_object_set(root, "reloc", blob))
goto out_err;
bof_decref(blob);
blob = NULL;
/* dump cs */
blob = bof_blob(cs->cdw * 4, cs->packets);
if (blob == NULL)
goto out_err;
if (bof_object_set(root, "pm4", blob))
goto out_err;
bof_decref(blob);
blob = NULL;
/* dump bo */
array = bof_array();
if (array == NULL)
goto out_err;
for (i = 0; i < csg->base.crelocs; i++) {
bo = bof_object();
if (bo == NULL)
goto out_err;
size = bof_int32(csg->relocs_bo[i]->size);
if (size == NULL)
goto out_err;
if (bof_object_set(bo, "size", size))
goto out_err;
bof_decref(size);
size = NULL;
handle = bof_int32(csg->relocs_bo[i]->handle);
if (handle == NULL)
goto out_err;
if (bof_object_set(bo, "handle", handle))
goto out_err;
bof_decref(handle);
handle = NULL;
radeon_bo_map((struct radeon_bo*)csg->relocs_bo[i], 0);
blob = bof_blob(csg->relocs_bo[i]->size, csg->relocs_bo[i]->ptr);
radeon_bo_unmap((struct radeon_bo*)csg->relocs_bo[i]);
if (blob == NULL)
goto out_err;
if (bof_object_set(bo, "data", blob))
goto out_err;
bof_decref(blob);
blob = NULL;
if (bof_array_append(array, bo))
goto out_err;
bof_decref(bo);
bo = NULL;
}
if (bof_object_set(root, "bo", array))
goto out_err;
sprintf(tmp, "d-0x%04X-%08d.bof", csm->device_id, csm->nbof++);
bof_dump_file(root, tmp);
out_err:
bof_decref(blob);
bof_decref(array);
bof_decref(bo);
bof_decref(size);
bof_decref(handle);
bof_decref(device_id);
bof_decref(root);
}
#endif
static int cs_gem_emit(struct radeon_cs_int *cs)
{
struct cs_gem *csg = (struct cs_gem*)cs;
uint64_t chunk_array[2];
unsigned i;
int r;
while (cs->cdw & 7)
radeon_cs_write_dword((struct radeon_cs *)cs, 0x80000000);
#if CS_BOF_DUMP
cs_gem_dump_bof(cs);
#endif
csg->chunks[0].length_dw = cs->cdw;
chunk_array[0] = (uint64_t)(uintptr_t)&csg->chunks[0];
chunk_array[1] = (uint64_t)(uintptr_t)&csg->chunks[1];
csg->cs.num_chunks = 2;
csg->cs.chunks = (uint64_t)(uintptr_t)chunk_array;
r = drmCommandWriteRead(cs->csm->fd, DRM_RADEON_CS,
&csg->cs, sizeof(struct drm_radeon_cs));
for (i = 0; i < csg->base.crelocs; i++) {
csg->relocs_bo[i]->space_accounted = 0;
/* bo might be referenced from another context so have to use atomic opertions */
atomic_dec((atomic_t *)radeon_gem_get_reloc_in_cs((struct radeon_bo*)csg->relocs_bo[i]), cs->id);
radeon_bo_unref((struct radeon_bo *)csg->relocs_bo[i]);
csg->relocs_bo[i] = NULL;
}
cs->csm->read_used = 0;
cs->csm->vram_write_used = 0;
cs->csm->gart_write_used = 0;
return r;
}
static int cs_gem_destroy(struct radeon_cs_int *cs)
{
struct cs_gem *csg = (struct cs_gem*)cs;
free_id(cs->id);
free(csg->relocs_bo);
free(cs->relocs);
free(cs->packets);
free(cs);
return 0;
}
static int cs_gem_erase(struct radeon_cs_int *cs)
{
struct cs_gem *csg = (struct cs_gem*)cs;
unsigned i;
if (csg->relocs_bo) {
for (i = 0; i < csg->base.crelocs; i++) {
if (csg->relocs_bo[i]) {
/* bo might be referenced from another context so have to use atomic opertions */
atomic_dec((atomic_t *)radeon_gem_get_reloc_in_cs((struct radeon_bo*)csg->relocs_bo[i]), cs->id);
radeon_bo_unref((struct radeon_bo *)csg->relocs_bo[i]);
csg->relocs_bo[i] = NULL;
}
}
}
cs->relocs_total_size = 0;
cs->cdw = 0;
cs->section_ndw = 0;
cs->crelocs = 0;
csg->chunks[0].length_dw = 0;
csg->chunks[1].length_dw = 0;
return 0;
}
static int cs_gem_need_flush(struct radeon_cs_int *cs)
{
return 0; //(cs->relocs_total_size > (32*1024*1024));
}
static void cs_gem_print(struct radeon_cs_int *cs, FILE *file)
{
struct radeon_cs_manager_gem *csm;
unsigned int i;
csm = (struct radeon_cs_manager_gem *)cs->csm;
fprintf(file, "VENDORID:DEVICEID 0x%04X:0x%04X\n", 0x1002, csm->device_id);
for (i = 0; i < cs->cdw; i++) {
fprintf(file, "0x%08X\n", cs->packets[i]);
}
}
static struct radeon_cs_funcs radeon_cs_gem_funcs = {
cs_gem_create,
cs_gem_write_reloc,
cs_gem_begin,
cs_gem_end,
cs_gem_emit,
cs_gem_destroy,
cs_gem_erase,
cs_gem_need_flush,
cs_gem_print,
};
static int radeon_get_device_id(int fd, uint32_t *device_id)
{
struct drm_radeon_info info = {};
int r;
*device_id = 0;
info.request = RADEON_INFO_DEVICE_ID;
info.value = (uintptr_t)device_id;
r = drmCommandWriteRead(fd, DRM_RADEON_INFO, &info,
sizeof(struct drm_radeon_info));
return r;
}
struct radeon_cs_manager *radeon_cs_manager_gem_ctor(int fd)
{
struct radeon_cs_manager_gem *csm;
csm = calloc(1, sizeof(struct radeon_cs_manager_gem));
if (csm == NULL) {
return NULL;
}
csm->base.funcs = &radeon_cs_gem_funcs;
csm->base.fd = fd;
radeon_get_device_id(fd, &csm->device_id);
return &csm->base;
}
void radeon_cs_manager_gem_dtor(struct radeon_cs_manager *csm)
{
free(csm);
}