/* i915_dma.c -- DMA support for the I915 -*- linux-c -*-
*/
/*
* Copyright 2003 Tungsten Graphics, Inc., Cedar Park, Texas.
* All Rights Reserved.
*
* Permission is hereby granted, free of charge, to any person obtaining a
* copy of this software and associated documentation files (the
* "Software"), to deal in the Software without restriction, including
* without limitation the rights to use, copy, modify, merge, publish,
* distribute, sub license, and/or sell copies of the Software, and to
* permit persons to whom the Software is furnished to do so, subject to
* the following conditions:
*
* The above copyright notice and this permission notice (including the
* next paragraph) shall be included in all copies or substantial portions
* of the Software.
*
* THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS
* OR IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF
* MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE AND NON-INFRINGEMENT.
* IN NO EVENT SHALL TUNGSTEN GRAPHICS AND/OR ITS SUPPLIERS BE LIABLE FOR
* ANY CLAIM, DAMAGES OR OTHER LIABILITY, WHETHER IN AN ACTION OF CONTRACT,
* TORT OR OTHERWISE, ARISING FROM, OUT OF OR IN CONNECTION WITH THE
* SOFTWARE OR THE USE OR OTHER DEALINGS IN THE SOFTWARE.
*
*/
#include "drmP.h"
#include "drm.h"
#include "i915_drm.h"
#include "i915_drv.h"
/* Really want an OS-independent resettable timer. Would like to have
* this loop run for (eg) 3 sec, but have the timer reset every time
* the head pointer changes, so that EBUSY only happens if the ring
* actually stalls for (eg) 3 seconds.
*/
int i915_wait_ring(struct drm_device * dev, int n, const char *caller)
{
drm_i915_private_t *dev_priv = dev->dev_private;
drm_i915_ring_buffer_t *ring = &(dev_priv->ring);
u32 last_head = I915_READ(LP_RING + RING_HEAD) & HEAD_ADDR;
int i;
for (i = 0; i < 10000; i++) {
ring->head = I915_READ(LP_RING + RING_HEAD) & HEAD_ADDR;
ring->space = ring->head - (ring->tail + 8);
if (ring->space < 0)
ring->space += ring->Size;
if (ring->space >= n)
return 0;
if (ring->head != last_head)
i = 0;
last_head = ring->head;
DRM_UDELAY(1);
}
return -EBUSY;
}
void i915_kernel_lost_context(struct drm_device * dev)
{
drm_i915_private_t *dev_priv = dev->dev_private;
drm_i915_ring_buffer_t *ring = &(dev_priv->ring);
ring->head = I915_READ(LP_RING + RING_HEAD) & HEAD_ADDR;
ring->tail = I915_READ(LP_RING + RING_TAIL) & TAIL_ADDR;
ring->space = ring->head - (ring->tail + 8);
if (ring->space < 0)
ring->space += ring->Size;
}
static int i915_dma_cleanup(struct drm_device * dev)
{
drm_i915_private_t *dev_priv = dev->dev_private;
/* Make sure interrupts are disabled here because the uninstall ioctl
* may not have been called from userspace and after dev_private
* is freed, it's too late.
*/
if (dev->irq)
drm_irq_uninstall(dev);
if (dev_priv->ring.virtual_start) {
drm_core_ioremapfree(&dev_priv->ring.map, dev);
dev_priv->ring.virtual_start = 0;
dev_priv->ring.map.handle = 0;
dev_priv->ring.map.size = 0;
}
if (dev_priv->status_page_dmah) {
drm_pci_free(dev, dev_priv->status_page_dmah);
dev_priv->status_page_dmah = NULL;
/* Need to rewrite hardware status page */
I915_WRITE(0x02080, 0x1ffff000);
}
if (dev_priv->status_gfx_addr) {
dev_priv->status_gfx_addr = 0;
drm_core_ioremapfree(&dev_priv->hws_map, dev);
I915_WRITE(0x02080, 0x1ffff000);
}
return 0;
}
#define DRI2_SAREA_BLOCK_TYPE(b) ((b) >> 16)
#define DRI2_SAREA_BLOCK_SIZE(b) ((b) & 0xffff)
#define DRI2_SAREA_BLOCK_NEXT(p) \
((void *) ((unsigned char *) (p) + \
DRI2_SAREA_BLOCK_SIZE(*(unsigned int *) p)))
#define DRI2_SAREA_BLOCK_END 0x0000
#define DRI2_SAREA_BLOCK_LOCK 0x0001
#define DRI2_SAREA_BLOCK_EVENT_BUFFER 0x0002
static int
setup_dri2_sarea(struct drm_device * dev,
struct drm_file *file_priv,
drm_i915_init_t * init)
{
drm_i915_private_t *dev_priv = dev->dev_private;
int ret;
unsigned int *p, *end, *next;
mutex_lock(&dev->struct_mutex);
dev_priv->sarea_bo =
drm_lookup_buffer_object(file_priv,
init->sarea_handle, 1);
mutex_unlock(&dev->struct_mutex);
if (!dev_priv->sarea_bo) {
DRM_ERROR("did not find sarea bo\n");
return -EINVAL;
}
ret = drm_bo_kmap(dev_priv->sarea_bo, 0,
dev_priv->sarea_bo->num_pages,
&dev_priv->sarea_kmap);
if (ret) {
DRM_ERROR("could not map sarea bo\n");
return ret;
}
p = dev_priv->sarea_kmap.virtual;
end = (void *) p + (dev_priv->sarea_bo->num_pages << PAGE_SHIFT);
while (p < end && DRI2_SAREA_BLOCK_TYPE(*p) != DRI2_SAREA_BLOCK_END) {
switch (DRI2_SAREA_BLOCK_TYPE(*p)) {
case DRI2_SAREA_BLOCK_LOCK:
dev->lock.hw_lock = (void *) (p + 1);
dev->sigdata.lock = dev->lock.hw_lock;
break;
}
next = DRI2_SAREA_BLOCK_NEXT(p);
if (next <= p || end < next) {
DRM_ERROR("malformed dri2 sarea: next is %p should be within %p-%p\n",
next, p, end);
return -EINVAL;
}
p = next;
}
return 0;
}
static int i915_initialize(struct drm_device * dev,
struct drm_file *file_priv,
drm_i915_init_t * init)
{
drm_i915_private_t *dev_priv = dev->dev_private;
int ret;
dev_priv->sarea = drm_getsarea(dev);
if (!dev_priv->sarea) {
DRM_ERROR("can not find sarea!\n");
i915_dma_cleanup(dev);
return -EINVAL;
}
if (init->mmio_offset != 0)
dev_priv->mmio_map = drm_core_findmap(dev, init->mmio_offset);
if (!dev_priv->mmio_map) {
i915_dma_cleanup(dev);
DRM_ERROR("can not find mmio map!\n");
return -EINVAL;
}
#ifdef I915_HAVE_BUFFER
dev_priv->max_validate_buffers = I915_MAX_VALIDATE_BUFFERS;
#endif
if (init->sarea_priv_offset)
dev_priv->sarea_priv = (drm_i915_sarea_t *)
((u8 *) dev_priv->sarea->handle +
init->sarea_priv_offset);
else {
/* No sarea_priv for you! */
dev_priv->sarea_priv = NULL;
}
dev_priv->ring.Start = init->ring_start;
dev_priv->ring.End = init->ring_end;
dev_priv->ring.Size = init->ring_size;
dev_priv->ring.tail_mask = dev_priv->ring.Size - 1;
dev_priv->ring.map.offset = init->ring_start;
dev_priv->ring.map.size = init->ring_size;
dev_priv->ring.map.type = 0;
dev_priv->ring.map.flags = 0;
dev_priv->ring.map.mtrr = 0;
drm_core_ioremap(&dev_priv->ring.map, dev);
if (dev_priv->ring.map.handle == NULL) {
i915_dma_cleanup(dev);
DRM_ERROR("can not ioremap virtual address for"
" ring buffer\n");
return -ENOMEM;
}
dev_priv->ring.virtual_start = dev_priv->ring.map.handle;
dev_priv->cpp = init->cpp;
if (dev_priv->sarea_priv)
dev_priv->sarea_priv->pf_current_page = 0;
/* We are using separate values as placeholders for mechanisms for
* private backbuffer/depthbuffer usage.
*/
dev_priv->use_mi_batchbuffer_start = 0;
if (IS_I965G(dev)) /* 965 doesn't support older method */
dev_priv->use_mi_batchbuffer_start = 1;
/* Allow hardware batchbuffers unless told otherwise.
*/
dev_priv->allow_batchbuffer = 1;
/* Enable vblank on pipe A for older X servers
*/
dev_priv->vblank_pipe = DRM_I915_VBLANK_PIPE_A;
/* Program Hardware Status Page */
if (!I915_NEED_GFX_HWS(dev)) {
dev_priv->status_page_dmah =
drm_pci_alloc(dev, PAGE_SIZE, PAGE_SIZE, 0xffffffff);
if (!dev_priv->status_page_dmah) {
i915_dma_cleanup(dev);
DRM_ERROR("Can not allocate hardware status page\n");
return -ENOMEM;
}
dev_priv->hw_status_page = dev_priv->status_page_dmah->vaddr;
dev_priv->dma_status_page = dev_priv->status_page_dmah->busaddr;
memset(dev_priv->hw_status_page, 0, PAGE_SIZE);
I915_WRITE(0x02080, dev_priv->dma_status_page);
}
DRM_DEBUG("Enabled hardware status page\n");
#ifdef I915_HAVE_BUFFER
mutex_init(&dev_priv->cmdbuf_mutex);
#endif
if (init->func == I915_INIT_DMA2) {
ret = setup_dri2_sarea(dev, file_priv, init);
if (ret) {
i915_dma_cleanup(dev);
DRM_ERROR("could not set up dri2 sarea\n");
return ret;
}
}
return 0;
}
static int i915_dma_resume(struct drm_device * dev)
{
drm_i915_private_t *dev_priv = (drm_i915_private_t *) dev->dev_private;
DRM_DEBUG("\n");
if (!dev_priv->sarea) {
DRM_ERROR("can not find sarea!\n");
return -EINVAL;
}
if (!dev_priv->mmio_map) {
DRM_ERROR("can not find mmio map!\n");
return -EINVAL;
}
if (dev_priv->ring.map.handle == NULL) {
DRM_ERROR("can not ioremap virtual address for"
" ring buffer\n");
return -ENOMEM;
}
/* Program Hardware Status Page */
if (!dev_priv->hw_status_page) {
DRM_ERROR("Can not find hardware status page\n");
return -EINVAL;
}
DRM_DEBUG("hw status page @ %p\n", dev_priv->hw_status_page);
if (dev_priv->status_gfx_addr != 0)
I915_WRITE(0x02080, dev_priv->status_gfx_addr);
else
I915_WRITE(0x02080, dev_priv->dma_status_page);
DRM_DEBUG("Enabled hardware status page\n");
return 0;
}
static int i915_dma_init(struct drm_device *dev, void *data,
struct drm_file *file_priv)
{
drm_i915_init_t *init = data;
int retcode = 0;
switch (init->func) {
case I915_INIT_DMA:
case I915_INIT_DMA2:
retcode = i915_initialize(dev, file_priv, init);
break;
case I915_CLEANUP_DMA:
retcode = i915_dma_cleanup(dev);
break;
case I915_RESUME_DMA:
retcode = i915_dma_resume(dev);
break;
default:
retcode = -EINVAL;
break;
}
return retcode;
}
/* Implement basically the same security restrictions as hardware does
* for MI_BATCH_NON_SECURE. These can be made stricter at any time.
*
* Most of the calculations below involve calculating the size of a
* particular instruction. It's important to get the size right as
* that tells us where the next instruction to check is. Any illegal
* instruction detected will be given a size of zero, which is a
* signal to abort the rest of the buffer.
*/
static int do_validate_cmd(int cmd)
{
switch (((cmd >> 29) & 0x7)) {
case 0x0:
switch ((cmd >> 23) & 0x3f) {
case 0x0:
return 1; /* MI_NOOP */
case 0x4:
return 1; /* MI_FLUSH */
default:
return 0; /* disallow everything else */
}
break;
case 0x1:
return 0; /* reserved */
case 0x2:
return (cmd & 0xff) + 2; /* 2d commands */
case 0x3:
if (((cmd >> 24) & 0x1f) <= 0x18)
return 1;
switch ((cmd >> 24) & 0x1f) {
case 0x1c:
return 1;
case 0x1d:
switch ((cmd >> 16) & 0xff) {
case 0x3:
return (cmd & 0x1f) + 2;
case 0x4:
return (cmd & 0xf) + 2;
default:
return (cmd & 0xffff) + 2;
}
case 0x1e:
if (cmd & (1 << 23))
return (cmd & 0xffff) + 1;
else
return 1;
case 0x1f:
if ((cmd & (1 << 23)) == 0) /* inline vertices */
return (cmd & 0x1ffff) + 2;
else if (cmd & (1 << 17)) /* indirect random */
if ((cmd & 0xffff) == 0)
return 0; /* unknown length, too hard */
else
return (((cmd & 0xffff) + 1) / 2) + 1;
else
return 2; /* indirect sequential */
default:
return 0;
}
default:
return 0;
}
return 0;
}
static int validate_cmd(int cmd)
{
int ret = do_validate_cmd(cmd);
/* printk("validate_cmd( %x ): %d\n", cmd, ret); */
return ret;
}
static int i915_emit_cmds(struct drm_device *dev, int __user *buffer,
int dwords)
{
drm_i915_private_t *dev_priv = dev->dev_private;
int i;
RING_LOCALS;
if ((dwords+1) * sizeof(int) >= dev_priv->ring.Size - 8)
return -EINVAL;
BEGIN_LP_RING((dwords+1)&~1);
for (i = 0; i < dwords;) {
int cmd, sz;
if (DRM_COPY_FROM_USER_UNCHECKED(&cmd, &buffer[i], sizeof(cmd)))
return -EINVAL;
if ((sz = validate_cmd(cmd)) == 0 || i + sz > dwords)
return -EINVAL;
OUT_RING(cmd);
while (++i, --sz) {
if (DRM_COPY_FROM_USER_UNCHECKED(&cmd, &buffer[i],
sizeof(cmd))) {
return -EINVAL;
}
OUT_RING(cmd);
}
}
if (dwords & 1)
OUT_RING(0);
ADVANCE_LP_RING();
return 0;
}
static int i915_emit_box(struct drm_device * dev,
struct drm_clip_rect __user * boxes,
int i, int DR1, int DR4)
{
drm_i915_private_t *dev_priv = dev->dev_private;
struct drm_clip_rect box;
RING_LOCALS;
if (DRM_COPY_FROM_USER_UNCHECKED(&box, &boxes[i], sizeof(box))) {
return -EFAULT;
}
if (box.y2 <= box.y1 || box.x2 <= box.x1 || box.y2 <= 0 || box.x2 <= 0) {
DRM_ERROR("Bad box %d,%d..%d,%d\n",
box.x1, box.y1, box.x2, box.y2);
return -EINVAL;
}
if (IS_I965G(dev)) {
BEGIN_LP_RING(4);
OUT_RING(GFX_OP_DRAWRECT_INFO_I965);
OUT_RING((box.x1 & 0xffff) | (box.y1 << 16));
OUT_RING(((box.x2 - 1) & 0xffff) | ((box.y2 - 1) << 16));
OUT_RING(DR4);
ADVANCE_LP_RING();
} else {
BEGIN_LP_RING(6);
OUT_RING(GFX_OP_DRAWRECT_INFO);
OUT_RING(DR1);
OUT_RING((box.x1 & 0xffff) | (box.y1 << 16));
OUT_RING(((box.x2 - 1) & 0xffff) | ((box.y2 - 1) << 16));
OUT_RING(DR4);
OUT_RING(0);
ADVANCE_LP_RING();
}
return 0;
}
/* XXX: Emitting the counter should really be moved to part of the IRQ
* emit. For now, do it in both places:
*/
void i915_emit_breadcrumb(struct drm_device *dev)
{
drm_i915_private_t *dev_priv = dev->dev_private;
RING_LOCALS;
if (++dev_priv->counter > BREADCRUMB_MASK) {
dev_priv->counter = 1;
DRM_DEBUG("Breadcrumb counter wrapped around\n");
}
if (dev_priv->sarea_priv)
dev_priv->sarea_priv->last_enqueue = dev_priv->counter;
BEGIN_LP_RING(4);
OUT_RING(CMD_STORE_DWORD_IDX);
OUT_RING(20);
OUT_RING(dev_priv->counter);
OUT_RING(0);
ADVANCE_LP_RING();
}
int i915_emit_mi_flush(struct drm_device *dev, uint32_t flush)
{
drm_i915_private_t *dev_priv = dev->dev_private;
uint32_t flush_cmd = CMD_MI_FLUSH;
RING_LOCALS;
flush_cmd |= flush;
i915_kernel_lost_context(dev);
BEGIN_LP_RING(4);
OUT_RING(flush_cmd);
OUT_RING(0);
OUT_RING(0);
OUT_RING(0);
ADVANCE_LP_RING();
return 0;
}
static int i915_dispatch_cmdbuffer(struct drm_device * dev,
drm_i915_cmdbuffer_t * cmd)
{
#ifdef I915_HAVE_FENCE
drm_i915_private_t *dev_priv = dev->dev_private;
#endif
int nbox = cmd->num_cliprects;
int i = 0, count, ret;
if (cmd->sz & 0x3) {
DRM_ERROR("alignment\n");
return -EINVAL;
}
i915_kernel_lost_context(dev);
count = nbox ? nbox : 1;
for (i = 0; i < count; i++) {
if (i < nbox) {
ret = i915_emit_box(dev, cmd->cliprects, i,
cmd->DR1, cmd->DR4);
if (ret)
return ret;
}
ret = i915_emit_cmds(dev, (int __user *)cmd->buf, cmd->sz / 4);
if (ret)
return ret;
}
i915_emit_breadcrumb(dev);
#ifdef I915_HAVE_FENCE
if (unlikely((dev_priv->counter & 0xFF) == 0))
drm_fence_flush_old(dev, 0, dev_priv->counter);
#endif
return 0;
}
int i915_dispatch_batchbuffer(struct drm_device * dev,
drm_i915_batchbuffer_t * batch)
{
drm_i915_private_t *dev_priv = dev->dev_private;
struct drm_clip_rect __user *boxes = batch->cliprects;
int nbox = batch->num_cliprects;
int i = 0, count;
RING_LOCALS;
if ((batch->start | batch->used) & 0x7) {
DRM_ERROR("alignment\n");
return -EINVAL;
}
i915_kernel_lost_context(dev);
count = nbox ? nbox : 1;
for (i = 0; i < count; i++) {
if (i < nbox) {
int ret = i915_emit_box(dev, boxes, i,
batch->DR1, batch->DR4);
if (ret)
return ret;
}
if (dev_priv->use_mi_batchbuffer_start) {
BEGIN_LP_RING(2);
if (IS_I965G(dev)) {
OUT_RING(MI_BATCH_BUFFER_START | (2 << 6) | MI_BATCH_NON_SECURE_I965);
OUT_RING(batch->start);
} else {
OUT_RING(MI_BATCH_BUFFER_START | (2 << 6));
OUT_RING(batch->start | MI_BATCH_NON_SECURE);
}
ADVANCE_LP_RING();
} else {
BEGIN_LP_RING(4);
OUT_RING(MI_BATCH_BUFFER);
OUT_RING(batch->start | MI_BATCH_NON_SECURE);
OUT_RING(batch->start + batch->used - 4);
OUT_RING(0);
ADVANCE_LP_RING();
}
}
i915_emit_breadcrumb(dev);
#ifdef I915_HAVE_FENCE
if (unlikely((dev_priv->counter & 0xFF) == 0))
drm_fence_flush_old(dev, 0, dev_priv->counter);
#endif
return 0;
}
static void i915_do_dispatch_flip(struct drm_device * dev, int plane, int sync)
{
drm_i915_private_t *dev_priv = dev->dev_private;
u32 num_pages, current_page, next_page, dspbase;
int shift = 2 * plane, x, y;
RING_LOCALS;
/* Calculate display base offset */
num_pages = dev_priv->sarea_priv->third_handle ? 3 : 2;
current_page = (dev_priv->sarea_priv->pf_current_page >> shift) & 0x3;
next_page = (current_page + 1) % num_pages;
switch (next_page) {
default:
case 0:
dspbase = dev_priv->sarea_priv->front_offset;
break;
case 1:
dspbase = dev_priv->sarea_priv->back_offset;
break;
case 2:
dspbase = dev_priv->sarea_priv->third_offset;
break;
}
if (plane == 0) {
x = dev_priv->sarea_priv->planeA_x;
y = dev_priv->sarea_priv->planeA_y;
} else {
x = dev_priv->sarea_priv->planeB_x;
y = dev_priv->sarea_priv->planeB_y;
}
dspbase += (y * dev_priv->sarea_priv->pitch + x) * dev_priv->cpp;
DRM_DEBUG("plane=%d current_page=%d dspbase=0x%x\n", plane, current_page,
dspbase);
BEGIN_LP_RING(4);
OUT_RING(sync ? 0 :
(MI_WAIT_FOR_EVENT | (plane ? MI_WAIT_FOR_PLANE_B_FLIP :
MI_WAIT_FOR_PLANE_A_FLIP)));
OUT_RING(CMD_OP_DISPLAYBUFFER_INFO | (sync ? 0 : ASYNC_FLIP) |
(plane ? DISPLAY_PLANE_B : DISPLAY_PLANE_A));
OUT_RING(dev_priv->sarea_priv->pitch * dev_priv->cpp);
OUT_RING(dspbase);
ADVANCE_LP_RING();
dev_priv->sarea_priv->pf_current_page &= ~(0x3 << shift);
dev_priv->sarea_priv->pf_current_page |= next_page << shift;
}
void i915_dispatch_flip(struct drm_device * dev, int planes, int sync)
{
drm_i915_private_t *dev_priv = dev->dev_private;
int i;
DRM_DEBUG("planes=0x%x pfCurrentPage=%d\n",
planes, dev_priv->sarea_priv->pf_current_page);
i915_emit_mi_flush(dev, MI_READ_FLUSH | MI_EXE_FLUSH);
for (i = 0; i < 2; i++)
if (planes & (1 << i))
i915_do_dispatch_flip(dev, i, sync);
i915_emit_breadcrumb(dev);
#ifdef I915_HAVE_FENCE
if (unlikely(!sync && ((dev_priv->counter & 0xFF) == 0)))
drm_fence_flush_old(dev, 0, dev_priv->counter);
#endif
}
int i915_quiescent(struct drm_device *dev)
{
drm_i915_private_t *dev_priv = dev->dev_private;
i915_kernel_lost_context(dev);
return i915_wait_ring(dev, dev_priv->ring.Size - 8, __FUNCTION__);
}
static int i915_flush_ioctl(struct drm_device *dev, void *data,
struct drm_file *file_priv)
{
LOCK_TEST_WITH_RETURN(dev, file_priv);
return i915_quiescent(dev);
}
static int i915_batchbuffer(struct drm_device *dev, void *data,
struct drm_file *file_priv)
{
drm_i915_private_t *dev_priv = (drm_i915_private_t *) dev->dev_private;
drm_i915_sarea_t *sarea_priv = (drm_i915_sarea_t *)
dev_priv->sarea_priv;
drm_i915_batchbuffer_t *batch = data;
int ret;
if (!dev_priv->allow_batchbuffer) {
DRM_ERROR("Batchbuffer ioctl disabled\n");
return -EINVAL;
}
DRM_DEBUG("i915 batchbuffer, start %x used %d cliprects %d\n",
batch->start, batch->used, batch->num_cliprects);
LOCK_TEST_WITH_RETURN(dev, file_priv);
if (batch->num_cliprects && DRM_VERIFYAREA_READ(batch->cliprects,
batch->num_cliprects *
sizeof(struct drm_clip_rect)))
return -EFAULT;
ret = i915_dispatch_batchbuffer(dev, batch);
sarea_priv->last_dispatch = READ_BREADCRUMB(dev_priv);
return ret;
}
static int i915_cmdbuffer(struct drm_device *dev, void *data,
struct drm_file *file_priv)
{
drm_i915_private_t *dev_priv = (drm_i915_private_t *) dev->dev_private;
drm_i915_sarea_t *sarea_priv = (drm_i915_sarea_t *)
dev_priv->sarea_priv;
drm_i915_cmdbuffer_t *cmdbuf = data;
int ret;
DRM_DEBUG("i915 cmdbuffer, buf %p sz %d cliprects %d\n",
cmdbuf->buf, cmdbuf->sz, cmdbuf->num_cliprects);
LOCK_TEST_WITH_RETURN(dev, file_priv);
if (cmdbuf->num_cliprects &&
DRM_VERIFYAREA_READ(cmdbuf->cliprects,
cmdbuf->num_cliprects *
sizeof(struct drm_clip_rect))) {
DRM_ERROR("Fault accessing cliprects\n");
return -EFAULT;
}
ret = i915_dispatch_cmdbuffer(dev, cmdbuf);
if (ret) {
DRM_ERROR("i915_dispatch_cmdbuffer failed\n");
return ret;
}
sarea_priv->last_dispatch = READ_BREADCRUMB(dev_priv);
return 0;
}
#if DRM_DEBUG_CODE
#define DRM_DEBUG_RELOCATION (drm_debug != 0)
#else
#define DRM_DEBUG_RELOCATION 0
#endif
static int i915_do_cleanup_pageflip(struct drm_device * dev)
{
drm_i915_private_t *dev_priv = dev->dev_private;
int i, planes, num_pages = dev_priv->sarea_priv->third_handle ? 3 : 2;
DRM_DEBUG("\n");
for (i = 0, planes = 0; i < 2; i++)
if (dev_priv->sarea_priv->pf_current_page & (0x3 << (2 * i))) {
dev_priv->sarea_priv->pf_current_page =
(dev_priv->sarea_priv->pf_current_page &
~(0x3 << (2 * i))) | ((num_pages - 1) << (2 * i));
planes |= 1 << i;
}
if (planes)
i915_dispatch_flip(dev, planes, 0);
return 0;
}
static int i915_flip_bufs(struct drm_device *dev, void *data, struct drm_file *file_priv)
{
drm_i915_flip_t *param = data;
DRM_DEBUG("\n");
LOCK_TEST_WITH_RETURN(dev, file_priv);
/* This is really planes */
if (param->pipes & ~0x3) {
DRM_ERROR("Invalid planes 0x%x, only <= 0x3 is valid\n",
param->pipes);
return -EINVAL;
}
i915_dispatch_flip(dev, param->pipes, 0);
return 0;
}
static int i915_getparam(struct drm_device *dev, void *data,
struct drm_file *file_priv)
{
drm_i915_private_t *dev_priv = dev->dev_private;
drm_i915_getparam_t *param = data;
int value;
if (!dev_priv) {
DRM_ERROR("called with no initialization\n");
return -EINVAL;
}
switch (param->param) {
case I915_PARAM_IRQ_ACTIVE:
value = dev->irq ? 1 : 0;
break;
case I915_PARAM_ALLOW_BATCHBUFFER:
value = dev_priv->allow_batchbuffer ? 1 : 0;
break;
case I915_PARAM_LAST_DISPATCH:
value = READ_BREADCRUMB(dev_priv);
break;
case I915_PARAM_CHIPSET_ID:
value = dev->pci_device;
break;
default:
DRM_ERROR("Unknown parameter %d\n", param->param);
return -EINVAL;
}
if (DRM_COPY_TO_USER(param->value, &value, sizeof(int))) {
DRM_ERROR("DRM_COPY_TO_USER failed\n");
return -EFAULT;
}
return 0;
}
static int i915_setparam(struct drm_device *dev, void *data,
struct drm_file *file_priv)
{
drm_i915_private_t *dev_priv = dev->dev_private;
drm_i915_setparam_t *param = data;
if (!dev_priv) {
DRM_ERROR("called with no initialization\n");
return -EINVAL;
}
switch (param->param) {
case I915_SETPARAM_USE_MI_BATCHBUFFER_START:
if (!IS_I965G(dev))
dev_priv->use_mi_batchbuffer_start = param->value;
break;
case I915_SETPARAM_TEX_LRU_LOG_GRANULARITY:
dev_priv->tex_lru_log_granularity = param->value;
break;
case I915_SETPARAM_ALLOW_BATCHBUFFER:
dev_priv->allow_batchbuffer = param->value;
break;
default:
DRM_ERROR("unknown parameter %d\n", param->param);
return -EINVAL;
}
return 0;
}
drm_i915_mmio_entry_t mmio_table[] = {
[MMIO_REGS_PS_DEPTH_COUNT] = {
I915_MMIO_MAY_READ|I915_MMIO_MAY_WRITE,
0x2350,
8
}
};
static int mmio_table_size = sizeof(mmio_table)/sizeof(drm_i915_mmio_entry_t);
static int i915_mmio(struct drm_device *dev, void *data,
struct drm_file *file_priv)
{
uint32_t buf[8];
drm_i915_private_t *dev_priv = dev->dev_private;
drm_i915_mmio_entry_t *e;
drm_i915_mmio_t *mmio = data;
void __iomem *base;
int i;
if (!dev_priv) {
DRM_ERROR("called with no initialization\n");
return -EINVAL;
}
if (mmio->reg >= mmio_table_size)
return -EINVAL;
e = &mmio_table[mmio->reg];
base = (u8 *) dev_priv->mmio_map->handle + e->offset;
switch (mmio->read_write) {
case I915_MMIO_READ:
if (!(e->flag & I915_MMIO_MAY_READ))
return -EINVAL;
for (i = 0; i < e->size / 4; i++)
buf[i] = I915_READ(e->offset + i * 4);
if (DRM_COPY_TO_USER(mmio->data, buf, e->size)) {
DRM_ERROR("DRM_COPY_TO_USER failed\n");
return -EFAULT;
}
break;
case I915_MMIO_WRITE:
if (!(e->flag & I915_MMIO_MAY_WRITE))
return -EINVAL;
if (DRM_COPY_FROM_USER(buf, mmio->data, e->size)) {
DRM_ERROR("DRM_COPY_TO_USER failed\n");
return -EFAULT;
}
for (i = 0; i < e->size / 4; i++)
I915_WRITE(e->offset + i * 4, buf[i]);
break;
}
return 0;
}
static int i915_set_status_page(struct drm_device *dev, void *data,
struct drm_file *file_priv)
{
drm_i915_private_t *dev_priv = dev->dev_private;
drm_i915_hws_addr_t *hws = data;
if (!I915_NEED_GFX_HWS(dev))
return -EINVAL;
if (!dev_priv) {
DRM_ERROR("called with no initialization\n");
return -EINVAL;
}
DRM_DEBUG("set status page addr 0x%08x\n", (u32)hws->addr);
dev_priv->status_gfx_addr = hws->addr & (0x1ffff<<12);
dev_priv->hws_map.offset = dev->agp->base + hws->addr;
dev_priv->hws_map.size = 4*1024;
dev_priv->hws_map.type = 0;
dev_priv->hws_map.flags = 0;
dev_priv->hws_map.mtrr = 0;
drm_core_ioremap(&dev_priv->hws_map, dev);
if (dev_priv->hws_map.handle == NULL) {
i915_dma_cleanup(dev);
dev_priv->status_gfx_addr = 0;
DRM_ERROR("can not ioremap virtual address for"
" G33 hw status page\n");
return -ENOMEM;
}
dev_priv->hw_status_page = dev_priv->hws_map.handle;
memset(dev_priv->hw_status_page, 0, PAGE_SIZE);
I915_WRITE(0x02080, dev_priv->status_gfx_addr);
DRM_DEBUG("load hws 0x2080 with gfx mem 0x%x\n",
dev_priv->status_gfx_addr);
DRM_DEBUG("load hws at %p\n", dev_priv->hw_status_page);
return 0;
}
int i915_driver_load(struct drm_device *dev, unsigned long flags)
{
struct drm_i915_private *dev_priv = dev->dev_private;
unsigned long base, size;
int ret = 0, mmio_bar = IS_I9XX(dev) ? 0 : 1;
/* i915 has 4 more counters */
dev->counters += 4;
dev->types[6] = _DRM_STAT_IRQ;
dev->types[7] = _DRM_STAT_PRIMARY;
dev->types[8] = _DRM_STAT_SECONDARY;
dev->types[9] = _DRM_STAT_DMA;
dev_priv = drm_alloc(sizeof(drm_i915_private_t), DRM_MEM_DRIVER);
if (dev_priv == NULL)
return -ENOMEM;
memset(dev_priv, 0, sizeof(drm_i915_private_t));
dev->dev_private = (void *)dev_priv;
/* Add register map (needed for suspend/resume) */
base = drm_get_resource_start(dev, mmio_bar);
size = drm_get_resource_len(dev, mmio_bar);
ret = drm_addmap(dev, base, size, _DRM_REGISTERS,
_DRM_KERNEL | _DRM_DRIVER, &dev_priv->mmio_map);
#ifdef __linux__
#if LINUX_VERSION_CODE < KERNEL_VERSION(2,6,25)
intel_init_chipset_flush_compat(dev);
#endif
#endif
return ret;
}
int i915_driver_unload(struct drm_device *dev)
{
struct drm_i915_private *dev_priv = dev->dev_private;
if (dev_priv->mmio_map)
drm_rmmap(dev, dev_priv->mmio_map);
drm_free(dev->dev_private, sizeof(drm_i915_private_t),
DRM_MEM_DRIVER);
#ifdef __linux__
#if LINUX_VERSION_CODE < KERNEL_VERSION(2,6,25)
intel_fini_chipset_flush_compat(dev);
#endif
#endif
return 0;
}
void i915_driver_lastclose(struct drm_device * dev)
{
drm_i915_private_t *dev_priv = dev->dev_private;
/* agp off can use this to get called before dev_priv */
if (!dev_priv)
return;
#ifdef I915_HAVE_BUFFER
if (dev_priv->val_bufs) {
vfree(dev_priv->val_bufs);
dev_priv->val_bufs = NULL;
}
#endif
if (drm_getsarea(dev) && dev_priv->sarea_priv)
i915_do_cleanup_pageflip(dev);
if (dev_priv->agp_heap)
i915_mem_takedown(&(dev_priv->agp_heap));
if (dev_priv->sarea_kmap.virtual) {
drm_bo_kunmap(&dev_priv->sarea_kmap);
dev_priv->sarea_kmap.virtual = NULL;
dev->lock.hw_lock = NULL;
dev->sigdata.lock = NULL;
}
if (dev_priv->sarea_bo) {
mutex_lock(&dev->struct_mutex);
drm_bo_usage_deref_locked(&dev_priv->sarea_bo);
mutex_unlock(&dev->struct_mutex);
dev_priv->sarea_bo = NULL;
}
i915_dma_cleanup(dev);
}
void i915_driver_preclose(struct drm_device * dev, struct drm_file *file_priv)
{
drm_i915_private_t *dev_priv = dev->dev_private;
i915_mem_release(dev, file_priv, dev_priv->agp_heap);
}
struct drm_ioctl_desc i915_ioctls[] = {
DRM_IOCTL_DEF(DRM_I915_INIT, i915_dma_init, DRM_AUTH|DRM_MASTER|DRM_ROOT_ONLY),
DRM_IOCTL_DEF(DRM_I915_FLUSH, i915_flush_ioctl, DRM_AUTH),
DRM_IOCTL_DEF(DRM_I915_FLIP, i915_flip_bufs, DRM_AUTH),
DRM_IOCTL_DEF(DRM_I915_BATCHBUFFER, i915_batchbuffer, DRM_AUTH),
DRM_IOCTL_DEF(DRM_I915_IRQ_EMIT, i915_irq_emit, DRM_AUTH),
DRM_IOCTL_DEF(DRM_I915_IRQ_WAIT, i915_irq_wait, DRM_AUTH),
DRM_IOCTL_DEF(DRM_I915_GETPARAM, i915_getparam, DRM_AUTH),
DRM_IOCTL_DEF(DRM_I915_SETPARAM, i915_setparam, DRM_AUTH|DRM_MASTER|DRM_ROOT_ONLY),
DRM_IOCTL_DEF(DRM_I915_ALLOC, i915_mem_alloc, DRM_AUTH),
DRM_IOCTL_DEF(DRM_I915_FREE, i915_mem_free, DRM_AUTH),
DRM_IOCTL_DEF(DRM_I915_INIT_HEAP, i915_mem_init_heap, DRM_AUTH|DRM_MASTER|DRM_ROOT_ONLY),
DRM_IOCTL_DEF(DRM_I915_CMDBUFFER, i915_cmdbuffer, DRM_AUTH),
DRM_IOCTL_DEF(DRM_I915_DESTROY_HEAP, i915_mem_destroy_heap, DRM_AUTH|DRM_MASTER|DRM_ROOT_ONLY ),
DRM_IOCTL_DEF(DRM_I915_SET_VBLANK_PIPE, i915_vblank_pipe_set, DRM_AUTH|DRM_MASTER|DRM_ROOT_ONLY ),
DRM_IOCTL_DEF(DRM_I915_GET_VBLANK_PIPE, i915_vblank_pipe_get, DRM_AUTH ),
DRM_IOCTL_DEF(DRM_I915_VBLANK_SWAP, i915_vblank_swap, DRM_AUTH),
DRM_IOCTL_DEF(DRM_I915_MMIO, i915_mmio, DRM_AUTH),
DRM_IOCTL_DEF(DRM_I915_HWS_ADDR, i915_set_status_page, DRM_AUTH),
#ifdef I915_HAVE_BUFFER
DRM_IOCTL_DEF(DRM_I915_EXECBUFFER, i915_execbuffer, DRM_AUTH),
#endif
};
int i915_max_ioctl = DRM_ARRAY_SIZE(i915_ioctls);
/**
* Determine if the device really is AGP or not.
*
* All Intel graphics chipsets are treated as AGP, even if they are really
* PCI-e.
*
* \param dev The device to be tested.
*
* \returns
* A value of 1 is always retured to indictate every i9x5 is AGP.
*/
int i915_driver_device_is_agp(struct drm_device * dev)
{
return 1;
}
int i915_driver_firstopen(struct drm_device *dev)
{
#ifdef I915_HAVE_BUFFER
drm_bo_driver_init(dev);
#endif
return 0;
}