diff options
author | Ben Skeggs | 2015-11-23 18:33:56 -0600 |
---|---|---|
committer | Ben Skeggs | 2015-12-21 21:22:20 -0600 |
commit | b845d61de93c762f73463a67a634ecb1ae8c4c35 (patch) | |
tree | 08845794f5825f2bb27b89e875d79fd955cf9573 | |
parent | f6b1b5b7c9cf6667d169bad3b33a73e4fe2bc14c (diff) | |
download | external-libdrm-b845d61de93c762f73463a67a634ecb1ae8c4c35.tar.gz external-libdrm-b845d61de93c762f73463a67a634ecb1ae8c4c35.tar.xz external-libdrm-b845d61de93c762f73463a67a634ecb1ae8c4c35.zip |
nouveau: introduce object to represent the kernel client
Because NVIF intentionally lacks some of the paths necessary to be
compatible with various mistakes we've made over the years, libdrm
needs to know whether a client has been updated and that it's safe
to make use of the new kernel interfaces.
Clients still using nouveau_device_open()/wrap() will be forced to
make use of ABI16 instead of NVIF.
v2.
- remove lib_version, nothing used it
- leave client-provided pointer unmodified on failure
Signed-off-by: Ben Skeggs <bskeggs@redhat.com>
Tested-by: Samuel Pitoiset <samuel.pitoiset@gmail.com>
Reviewed-by: Emil Velikov <emil.l.velikov@gmail.com>
-rwxr-xr-x | nouveau/nouveau-symbol-check | 2 | ||||
-rw-r--r-- | nouveau/nouveau.c | 35 | ||||
-rw-r--r-- | nouveau/nouveau.h | 18 |
3 files changed, 55 insertions, 0 deletions
diff --git a/nouveau/nouveau-symbol-check b/nouveau/nouveau-symbol-check index 38b6ec52..e360b92d 100755 --- a/nouveau/nouveau-symbol-check +++ b/nouveau/nouveau-symbol-check | |||
@@ -30,6 +30,8 @@ nouveau_device_del | |||
30 | nouveau_device_open | 30 | nouveau_device_open |
31 | nouveau_device_open_existing | 31 | nouveau_device_open_existing |
32 | nouveau_device_wrap | 32 | nouveau_device_wrap |
33 | nouveau_drm_del | ||
34 | nouveau_drm_new | ||
33 | nouveau_getparam | 35 | nouveau_getparam |
34 | nouveau_object_del | 36 | nouveau_object_del |
35 | nouveau_object_find | 37 | nouveau_object_find |
diff --git a/nouveau/nouveau.c b/nouveau/nouveau.c index 00173034..2b163513 100644 --- a/nouveau/nouveau.c +++ b/nouveau/nouveau.c | |||
@@ -195,6 +195,41 @@ nouveau_object_find(struct nouveau_object *obj, uint32_t pclass) | |||
195 | return obj; | 195 | return obj; |
196 | } | 196 | } |
197 | 197 | ||
198 | void | ||
199 | nouveau_drm_del(struct nouveau_drm **pdrm) | ||
200 | { | ||
201 | free(*pdrm); | ||
202 | *pdrm = NULL; | ||
203 | } | ||
204 | |||
205 | int | ||
206 | nouveau_drm_new(int fd, struct nouveau_drm **pdrm) | ||
207 | { | ||
208 | struct nouveau_drm *drm; | ||
209 | drmVersionPtr ver; | ||
210 | |||
211 | #ifdef DEBUG | ||
212 | debug_init(getenv("NOUVEAU_LIBDRM_DEBUG")); | ||
213 | #endif | ||
214 | |||
215 | if (!(drm = calloc(1, sizeof(*drm)))) | ||
216 | return -ENOMEM; | ||
217 | drm->fd = fd; | ||
218 | |||
219 | if (!(ver = drmGetVersion(fd))) { | ||
220 | nouveau_drm_del(&drm); | ||
221 | return -EINVAL; | ||
222 | } | ||
223 | *pdrm = drm; | ||
224 | |||
225 | drm->version = (ver->version_major << 24) | | ||
226 | (ver->version_minor << 8) | | ||
227 | ver->version_patchlevel; | ||
228 | drm->nvif = false; | ||
229 | drmFreeVersion(ver); | ||
230 | return 0; | ||
231 | } | ||
232 | |||
198 | /* this is the old libdrm's version of nouveau_device_wrap(), the symbol | 233 | /* this is the old libdrm's version of nouveau_device_wrap(), the symbol |
199 | * is kept here to prevent AIGLX from crashing if the DDX is linked against | 234 | * is kept here to prevent AIGLX from crashing if the DDX is linked against |
200 | * the new libdrm, but the DRI driver against the old | 235 | * the new libdrm, but the DRI driver against the old |
diff --git a/nouveau/nouveau.h b/nouveau/nouveau.h index 24cda6f1..2287eba8 100644 --- a/nouveau/nouveau.h +++ b/nouveau/nouveau.h | |||
@@ -22,6 +22,24 @@ struct nouveau_object { | |||
22 | void *data; | 22 | void *data; |
23 | }; | 23 | }; |
24 | 24 | ||
25 | struct nouveau_drm { | ||
26 | struct nouveau_object client; | ||
27 | int fd; | ||
28 | uint32_t version; | ||
29 | bool nvif; | ||
30 | }; | ||
31 | |||
32 | static inline struct nouveau_drm * | ||
33 | nouveau_drm(struct nouveau_object *obj) | ||
34 | { | ||
35 | while (obj && obj->parent) | ||
36 | obj = obj->parent; | ||
37 | return (struct nouveau_drm *)obj; | ||
38 | } | ||
39 | |||
40 | int nouveau_drm_new(int fd, struct nouveau_drm **); | ||
41 | void nouveau_drm_del(struct nouveau_drm **); | ||
42 | |||
25 | struct nouveau_fifo { | 43 | struct nouveau_fifo { |
26 | struct nouveau_object *object; | 44 | struct nouveau_object *object; |
27 | uint32_t channel; | 45 | uint32_t channel; |