diff options
author | Emil Velikov | 2012-04-27 13:20:53 -0500 |
---|---|---|
committer | Emil Velikov | 2014-09-01 10:06:02 -0500 |
commit | b26dc002f7834f49b99822a1608a99de2fbac74e (patch) | |
tree | 3d51dcd24d99a4a1ca5bccbe3a84313c755538bb /Android.mk | |
parent | 0a92953e7022a400fabe0407ff8b9bc67f423970 (diff) | |
download | external-libdrm-b26dc002f7834f49b99822a1608a99de2fbac74e.tar.gz external-libdrm-b26dc002f7834f49b99822a1608a99de2fbac74e.tar.xz external-libdrm-b26dc002f7834f49b99822a1608a99de2fbac74e.zip |
libdrm,intel: rework android header handling
Contains the following patches squashed in:
commit 99247a5bd724ddcf0f06a5518baad207c53f1e2b
Author: Haitao Huang <haitao.huang@intel.com>
Date: Fri, 27 Apr 2012 13:20:53 -0500
Android.mk: use LOCAL_COPY_HEADERS to export headers.
Export necessary header files used by other components for
Android, such as libva intel-driver, gralloc, hwcomposer, etc.
Change-Id: I2feabf6941379ef4d756e942f30eba059de641f1
Signed-off-by: Haitao Huang <haitao.huang@intel.com>
[chad: Fixed inconsistent indentation.]
Signed-off-by: Chad Versace <chad.versace@linux.intel.com>
commit 7d0b528cb69995d7ea4e29b2daa1e3b28a362f42
Author: Emil Velikov <emil.l.velikov@gmail.com>
Date: Sun, 27 Jul 2014 18:22:41 +0100
android: reuse headers lists, separate libdrm from intel headers
Rather than having a duplicate copy of the headers list(s),
reuse the existing one(s). Distinguish that the intel headers
should be copied when libdrm_intel is used.
v2 Rename the headers variable(s) to *_H_FILES.
Signed-off-by: Emil Velikov <emil.l.velikov@gmail.com>
commit 361de3ba4cadd5357596d1537bb3f216d281532b
Author: Piotr Luc <piotr.luc@intel.com>
Date: Fri, 14 Jun 2013 13:00:39 +0200
Export include dir from libdrm
BZ: 116218
Google introduced new method of specifying include path(s)
between modules. This allows a module to include header from a
library without directly specifyining by includer the path where
headers are located.
The method requires from library that holds headers to export
include path(s) in LOCAL_EXPORT_C_INCLUDE_DIRS variable.
These exported include path(s) are automatically added to
include path(s) of modules that have name of the library in the
LOCAL_SHARED_LIBRARIES or LOCAL_STATIC_LIBRARIES list.
This change sets LOCAL_EXPORT_C_INCLUDE_DIRS to folders that
contain headers file that used by other modules in order to
export these paths.
Change-Id: Id1ac885b31ef2efe194e0289fbcaecd9eb533df0
Signed-off-by: Piotr Luc <piotr.luc@intel.com>
Reviewed-on: http://android.intel.com:8080/113562
Reviewed-by: cactus <cactus@intel.com>
Reviewed-by: Luc, Piotr <Piotr.Luc@intel.com>
Reviewed-by: Purushothaman, Vijay A <vijay.a.purushothaman@intel.com>
Reviewed-by: Stimson, Dale B <dale.b.stimson@intel.com>
Tested-by: Stimson, Dale B <dale.b.stimson@intel.com>
Reviewed-by: buildbot <buildbot@intel.com>
Tested-by: buildbot <buildbot@intel.com>
commit 2bf22fcbd4cbb9e7c7764d5eff0bb4e75ab1a005
Author: Emil Velikov <emil.l.velikov@gmail.com>
Date: 27 Jul 2014 18:27:21 +0100
android: Separate libdrm and intel LOCAL_EXPORT_C_INCLUDE_DIRS
Signed-off-by: Emil Velikov <emil.l.velikov@gmail.com>
Diffstat (limited to 'Android.mk')
-rw-r--r-- | Android.mk | 15 |
1 files changed, 13 insertions, 2 deletions
@@ -1,5 +1,5 @@ | |||
1 | # | 1 | # |
2 | # Copyright © 2011 Intel Corporation | 2 | # Copyright © 2011-2012 Intel Corporation |
3 | # | 3 | # |
4 | # Permission is hereby granted, free of charge, to any person obtaining a | 4 | # Permission is hereby granted, free of charge, to any person obtaining a |
5 | # copy of this software and associated documentation files (the "Software"), | 5 | # copy of this software and associated documentation files (the "Software"), |
@@ -26,13 +26,18 @@ include $(CLEAR_VARS) | |||
26 | 26 | ||
27 | LIBDRM_TOP := $(LOCAL_PATH) | 27 | LIBDRM_TOP := $(LOCAL_PATH) |
28 | 28 | ||
29 | # Import variables LIBDRM_FILES, LIBDRM_HEADERS | 29 | # Import variables LIBDRM_FILES, LIBDRM_H_FILES |
30 | include $(LOCAL_PATH)/Makefile.sources | 30 | include $(LOCAL_PATH)/Makefile.sources |
31 | # Import variables LIBDRM_INCLUDE_H_FILES, LIBDRM_INCLUDE_VMWGFX_H_FILES | ||
32 | include $(LOCAL_PATH)/include/drm/Makefile.sources | ||
31 | 33 | ||
32 | LOCAL_MODULE := libdrm | 34 | LOCAL_MODULE := libdrm |
33 | LOCAL_MODULE_TAGS := optional | 35 | LOCAL_MODULE_TAGS := optional |
34 | 36 | ||
35 | LOCAL_SRC_FILES := $(LIBDRM_FILES) | 37 | LOCAL_SRC_FILES := $(LIBDRM_FILES) |
38 | LOCAL_EXPORT_C_INCLUDE_DIRS += \ | ||
39 | $(LOCAL_PATH) \ | ||
40 | $(LOCAL_PATH)/include/drm | ||
36 | 41 | ||
37 | LOCAL_C_INCLUDES := \ | 42 | LOCAL_C_INCLUDES := \ |
38 | $(LIBDRM_TOP)/include/drm | 43 | $(LIBDRM_TOP)/include/drm |
@@ -40,6 +45,12 @@ LOCAL_C_INCLUDES := \ | |||
40 | LOCAL_CFLAGS := \ | 45 | LOCAL_CFLAGS := \ |
41 | -DHAVE_LIBDRM_ATOMIC_PRIMITIVES=1 | 46 | -DHAVE_LIBDRM_ATOMIC_PRIMITIVES=1 |
42 | 47 | ||
48 | LOCAL_COPY_HEADERS := \ | ||
49 | $(LIBDRM_H_FILES) \ | ||
50 | $(addprefix include/drm/,$(LIBDRM_INCLUDE_H_FILES)) \ | ||
51 | $(addprefix include/drm/,$(LIBDRM_INCLUDE_VMWGFX_H_FILES)) | ||
52 | |||
53 | LOCAL_COPY_HEADERS_TO := libdrm | ||
43 | include $(BUILD_SHARED_LIBRARY) | 54 | include $(BUILD_SHARED_LIBRARY) |
44 | 55 | ||
45 | include $(LOCAL_PATH)/intel/Android.mk | 56 | include $(LOCAL_PATH)/intel/Android.mk |