aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorEmil Velikov2017-04-05 11:21:29 -0500
committerEmil Velikov2017-04-05 12:11:25 -0500
commit0010d312dbf0dae05652b75cdef7cd361f686623 (patch)
treefa19d1b32dadfddbe37d55f05d341b4515a5daff /configure.ac
parent10ca5e13a8357dfa5562102ae94b9fa7f535f4df (diff)
downloadexternal-libdrm-0010d312dbf0dae05652b75cdef7cd361f686623.tar.gz
external-libdrm-0010d312dbf0dae05652b75cdef7cd361f686623.tar.xz
external-libdrm-0010d312dbf0dae05652b75cdef7cd361f686623.zip
configure.ac: pthread-stubs is not a thing on GNU/kFreeBSD
As mentioned on the xcb mailing list, the platform uses the GLIBC forwarding mechanism. https://lists.freedesktop.org/archives/xcb/2016-November/010896.html Reported-by: Andreas Boll <andreas.boll.dev@gmail.com> Signed-off-by: Emil Velikov <emil.velikov@collabora.com> Reviewed-by: Eric Engestrom <eric.engestrom@imgtec.com> Reviewed-by: Andreas Boll <andreas.boll.dev@gmail.com>
Diffstat (limited to 'configure.ac')
-rw-r--r--configure.ac2
1 files changed, 1 insertions, 1 deletions
diff --git a/configure.ac b/configure.ac
index 036f65a2..7b9369be 100644
--- a/configure.ac
+++ b/configure.ac
@@ -64,7 +64,7 @@ LT_INIT([disable-static])
64dnl pthread-stubs is mandatory on BSD platforms, due to the nature of the 64dnl pthread-stubs is mandatory on BSD platforms, due to the nature of the
65dnl project. Even then there's a notable issue as described in the project README 65dnl project. Even then there's a notable issue as described in the project README
66case "$host_os" in 66case "$host_os" in
67linux* | cygwin* | darwin* | solaris* | gnu*) 67linux* | cygwin* | darwin* | solaris* | *-gnu* | gnu*)
68 pthread_stubs_possible="no" 68 pthread_stubs_possible="no"
69 ;; 69 ;;
70* ) 70* )