diff options
author | Eric Engestrom | 2017-05-31 07:48:53 -0500 |
---|---|---|
committer | Eric Engestrom | 2017-06-03 17:39:12 -0500 |
commit | 1b8db1777983b917384c2ed78ed5a2ab653d9e55 (patch) | |
tree | e14a70aef0c75263bf19fff1706a64fa7a3d5814 /include | |
parent | ce9e3ba6e2cc65e1e9e6e05a5f326c4dd25ab2c4 (diff) | |
download | external-libdrm-1b8db1777983b917384c2ed78ed5a2ab653d9e55.tar.gz external-libdrm-1b8db1777983b917384c2ed78ed5a2ab653d9e55.tar.xz external-libdrm-1b8db1777983b917384c2ed78ed5a2ab653d9e55.zip |
headers: sync drm_fourcc.h with airlied/drm-next
This adds a bunch of modifiers stuff, as well as a few new formats.
Includes the following changes:
ebbb0e5cfd2ceb1150b1 drm: add extern C guard for the UAPI headers
b9fb2a21ac8058965a6b drm_fourcc: Document linear modifier
af913418261d6d3e7a29 drm_fourcc: Fix DRM_FORMAT_MOD_LINEAR #define
fd056f05b9fcba35b77e drm: add fourcc codes for 16bit R and RG
73f1a5858bf82f3bf232 drm/fourcc: add vivante tiled layout format modifiers
ba2b5277dc52cc96944d drm: add RGB formats with separate alpha plane
5e91144dd702d068b22a drm/tegra: Add tiling FB modifiers
Generated using `make headers_install` from airlied/drm-next
at commit 2a1720376adda5ecf8e636fbfb05339c7dad1c55
Signed-off-by: Eric Engestrom <eric.engestrom@imgtec.com>
Reviewed-by: Emil Velikov <emil.velikov@collabora.com>
Diffstat (limited to 'include')
-rw-r--r-- | include/drm/drm_fourcc.h | 126 |
1 files changed, 126 insertions, 0 deletions
diff --git a/include/drm/drm_fourcc.h b/include/drm/drm_fourcc.h index 4d8da699..55e30104 100644 --- a/include/drm/drm_fourcc.h +++ b/include/drm/drm_fourcc.h | |||
@@ -26,6 +26,10 @@ | |||
26 | 26 | ||
27 | #include "drm.h" | 27 | #include "drm.h" |
28 | 28 | ||
29 | #if defined(__cplusplus) | ||
30 | extern "C" { | ||
31 | #endif | ||
32 | |||
29 | #define fourcc_code(a, b, c, d) ((__u32)(a) | ((__u32)(b) << 8) | \ | 33 | #define fourcc_code(a, b, c, d) ((__u32)(a) | ((__u32)(b) << 8) | \ |
30 | ((__u32)(c) << 16) | ((__u32)(d) << 24)) | 34 | ((__u32)(c) << 16) | ((__u32)(d) << 24)) |
31 | 35 | ||
@@ -37,10 +41,17 @@ | |||
37 | /* 8 bpp Red */ | 41 | /* 8 bpp Red */ |
38 | #define DRM_FORMAT_R8 fourcc_code('R', '8', ' ', ' ') /* [7:0] R */ | 42 | #define DRM_FORMAT_R8 fourcc_code('R', '8', ' ', ' ') /* [7:0] R */ |
39 | 43 | ||
44 | /* 16 bpp Red */ | ||
45 | #define DRM_FORMAT_R16 fourcc_code('R', '1', '6', ' ') /* [15:0] R little endian */ | ||
46 | |||
40 | /* 16 bpp RG */ | 47 | /* 16 bpp RG */ |
41 | #define DRM_FORMAT_RG88 fourcc_code('R', 'G', '8', '8') /* [15:0] R:G 8:8 little endian */ | 48 | #define DRM_FORMAT_RG88 fourcc_code('R', 'G', '8', '8') /* [15:0] R:G 8:8 little endian */ |
42 | #define DRM_FORMAT_GR88 fourcc_code('G', 'R', '8', '8') /* [15:0] G:R 8:8 little endian */ | 49 | #define DRM_FORMAT_GR88 fourcc_code('G', 'R', '8', '8') /* [15:0] G:R 8:8 little endian */ |
43 | 50 | ||
51 | /* 32 bpp RG */ | ||
52 | #define DRM_FORMAT_RG1616 fourcc_code('R', 'G', '3', '2') /* [31:0] R:G 16:16 little endian */ | ||
53 | #define DRM_FORMAT_GR1616 fourcc_code('G', 'R', '3', '2') /* [31:0] G:R 16:16 little endian */ | ||
54 | |||
44 | /* 8 bpp RGB */ | 55 | /* 8 bpp RGB */ |
45 | #define DRM_FORMAT_RGB332 fourcc_code('R', 'G', 'B', '8') /* [7:0] R:G:B 3:3:2 */ | 56 | #define DRM_FORMAT_RGB332 fourcc_code('R', 'G', 'B', '8') /* [7:0] R:G:B 3:3:2 */ |
46 | #define DRM_FORMAT_BGR233 fourcc_code('B', 'G', 'R', '8') /* [7:0] B:G:R 2:3:3 */ | 57 | #define DRM_FORMAT_BGR233 fourcc_code('B', 'G', 'R', '8') /* [7:0] B:G:R 2:3:3 */ |
@@ -103,6 +114,20 @@ | |||
103 | #define DRM_FORMAT_AYUV fourcc_code('A', 'Y', 'U', 'V') /* [31:0] A:Y:Cb:Cr 8:8:8:8 little endian */ | 114 | #define DRM_FORMAT_AYUV fourcc_code('A', 'Y', 'U', 'V') /* [31:0] A:Y:Cb:Cr 8:8:8:8 little endian */ |
104 | 115 | ||
105 | /* | 116 | /* |
117 | * 2 plane RGB + A | ||
118 | * index 0 = RGB plane, same format as the corresponding non _A8 format has | ||
119 | * index 1 = A plane, [7:0] A | ||
120 | */ | ||
121 | #define DRM_FORMAT_XRGB8888_A8 fourcc_code('X', 'R', 'A', '8') | ||
122 | #define DRM_FORMAT_XBGR8888_A8 fourcc_code('X', 'B', 'A', '8') | ||
123 | #define DRM_FORMAT_RGBX8888_A8 fourcc_code('R', 'X', 'A', '8') | ||
124 | #define DRM_FORMAT_BGRX8888_A8 fourcc_code('B', 'X', 'A', '8') | ||
125 | #define DRM_FORMAT_RGB888_A8 fourcc_code('R', '8', 'A', '8') | ||
126 | #define DRM_FORMAT_BGR888_A8 fourcc_code('B', '8', 'A', '8') | ||
127 | #define DRM_FORMAT_RGB565_A8 fourcc_code('R', '5', 'A', '8') | ||
128 | #define DRM_FORMAT_BGR565_A8 fourcc_code('B', '5', 'A', '8') | ||
129 | |||
130 | /* | ||
106 | * 2 plane YCbCr | 131 | * 2 plane YCbCr |
107 | * index 0 = Y plane, [7:0] Y | 132 | * index 0 = Y plane, [7:0] Y |
108 | * index 1 = Cr:Cb plane, [15:0] Cr:Cb little endian | 133 | * index 1 = Cr:Cb plane, [15:0] Cr:Cb little endian |
@@ -150,11 +175,13 @@ | |||
150 | 175 | ||
151 | /* Vendor Ids: */ | 176 | /* Vendor Ids: */ |
152 | #define DRM_FORMAT_MOD_NONE 0 | 177 | #define DRM_FORMAT_MOD_NONE 0 |
178 | #define DRM_FORMAT_MOD_VENDOR_NONE 0 | ||
153 | #define DRM_FORMAT_MOD_VENDOR_INTEL 0x01 | 179 | #define DRM_FORMAT_MOD_VENDOR_INTEL 0x01 |
154 | #define DRM_FORMAT_MOD_VENDOR_AMD 0x02 | 180 | #define DRM_FORMAT_MOD_VENDOR_AMD 0x02 |
155 | #define DRM_FORMAT_MOD_VENDOR_NV 0x03 | 181 | #define DRM_FORMAT_MOD_VENDOR_NV 0x03 |
156 | #define DRM_FORMAT_MOD_VENDOR_SAMSUNG 0x04 | 182 | #define DRM_FORMAT_MOD_VENDOR_SAMSUNG 0x04 |
157 | #define DRM_FORMAT_MOD_VENDOR_QCOM 0x05 | 183 | #define DRM_FORMAT_MOD_VENDOR_QCOM 0x05 |
184 | #define DRM_FORMAT_MOD_VENDOR_VIVANTE 0x06 | ||
158 | /* add more to the end as needed */ | 185 | /* add more to the end as needed */ |
159 | 186 | ||
160 | #define fourcc_mod_code(vendor, val) \ | 187 | #define fourcc_mod_code(vendor, val) \ |
@@ -168,6 +195,16 @@ | |||
168 | * authoritative source for all of these. | 195 | * authoritative source for all of these. |
169 | */ | 196 | */ |
170 | 197 | ||
198 | /* | ||
199 | * Linear Layout | ||
200 | * | ||
201 | * Just plain linear layout. Note that this is different from no specifying any | ||
202 | * modifier (e.g. not setting DRM_MODE_FB_MODIFIERS in the DRM_ADDFB2 ioctl), | ||
203 | * which tells the driver to also take driver-internal information into account | ||
204 | * and so might actually result in a tiled framebuffer. | ||
205 | */ | ||
206 | #define DRM_FORMAT_MOD_LINEAR fourcc_mod_code(NONE, 0) | ||
207 | |||
171 | /* Intel framebuffer modifiers */ | 208 | /* Intel framebuffer modifiers */ |
172 | 209 | ||
173 | /* | 210 | /* |
@@ -229,4 +266,93 @@ | |||
229 | */ | 266 | */ |
230 | #define DRM_FORMAT_MOD_SAMSUNG_64_32_TILE fourcc_mod_code(SAMSUNG, 1) | 267 | #define DRM_FORMAT_MOD_SAMSUNG_64_32_TILE fourcc_mod_code(SAMSUNG, 1) |
231 | 268 | ||
269 | /* Vivante framebuffer modifiers */ | ||
270 | |||
271 | /* | ||
272 | * Vivante 4x4 tiling layout | ||
273 | * | ||
274 | * This is a simple tiled layout using tiles of 4x4 pixels in a row-major | ||
275 | * layout. | ||
276 | */ | ||
277 | #define DRM_FORMAT_MOD_VIVANTE_TILED fourcc_mod_code(VIVANTE, 1) | ||
278 | |||
279 | /* | ||
280 | * Vivante 64x64 super-tiling layout | ||
281 | * | ||
282 | * This is a tiled layout using 64x64 pixel super-tiles, where each super-tile | ||
283 | * contains 8x4 groups of 2x4 tiles of 4x4 pixels (like above) each, all in row- | ||
284 | * major layout. | ||
285 | * | ||
286 | * For more information: see | ||
287 | * https://github.com/etnaviv/etna_viv/blob/master/doc/hardware.md#texture-tiling | ||
288 | */ | ||
289 | #define DRM_FORMAT_MOD_VIVANTE_SUPER_TILED fourcc_mod_code(VIVANTE, 2) | ||
290 | |||
291 | /* | ||
292 | * Vivante 4x4 tiling layout for dual-pipe | ||
293 | * | ||
294 | * Same as the 4x4 tiling layout, except every second 4x4 pixel tile starts at a | ||
295 | * different base address. Offsets from the base addresses are therefore halved | ||
296 | * compared to the non-split tiled layout. | ||
297 | */ | ||
298 | #define DRM_FORMAT_MOD_VIVANTE_SPLIT_TILED fourcc_mod_code(VIVANTE, 3) | ||
299 | |||
300 | /* | ||
301 | * Vivante 64x64 super-tiling layout for dual-pipe | ||
302 | * | ||
303 | * Same as the 64x64 super-tiling layout, except every second 4x4 pixel tile | ||
304 | * starts at a different base address. Offsets from the base addresses are | ||
305 | * therefore halved compared to the non-split super-tiled layout. | ||
306 | */ | ||
307 | #define DRM_FORMAT_MOD_VIVANTE_SPLIT_SUPER_TILED fourcc_mod_code(VIVANTE, 4) | ||
308 | |||
309 | |||
310 | /* NVIDIA Tegra frame buffer modifiers */ | ||
311 | |||
312 | /* | ||
313 | * Some modifiers take parameters, for example the number of vertical GOBs in | ||
314 | * a block. Reserve the lower 32 bits for parameters | ||
315 | */ | ||
316 | #define __fourcc_mod_tegra_mode_shift 32 | ||
317 | #define fourcc_mod_tegra_code(val, params) \ | ||
318 | fourcc_mod_code(NV, ((((__u64)val) << __fourcc_mod_tegra_mode_shift) | params)) | ||
319 | #define fourcc_mod_tegra_mod(m) \ | ||
320 | (m & ~((1ULL << __fourcc_mod_tegra_mode_shift) - 1)) | ||
321 | #define fourcc_mod_tegra_param(m) \ | ||
322 | (m & ((1ULL << __fourcc_mod_tegra_mode_shift) - 1)) | ||
323 | |||
324 | /* | ||
325 | * Tegra Tiled Layout, used by Tegra 2, 3 and 4. | ||
326 | * | ||
327 | * Pixels are arranged in simple tiles of 16 x 16 bytes. | ||
328 | */ | ||
329 | #define NV_FORMAT_MOD_TEGRA_TILED fourcc_mod_tegra_code(1, 0) | ||
330 | |||
331 | /* | ||
332 | * Tegra 16Bx2 Block Linear layout, used by TK1/TX1 | ||
333 | * | ||
334 | * Pixels are arranged in 64x8 Groups Of Bytes (GOBs). GOBs are then stacked | ||
335 | * vertically by a power of 2 (1 to 32 GOBs) to form a block. | ||
336 | * | ||
337 | * Within a GOB, data is ordered as 16B x 2 lines sectors laid in Z-shape. | ||
338 | * | ||
339 | * Parameter 'v' is the log2 encoding of the number of GOBs stacked vertically. | ||
340 | * Valid values are: | ||
341 | * | ||
342 | * 0 == ONE_GOB | ||
343 | * 1 == TWO_GOBS | ||
344 | * 2 == FOUR_GOBS | ||
345 | * 3 == EIGHT_GOBS | ||
346 | * 4 == SIXTEEN_GOBS | ||
347 | * 5 == THIRTYTWO_GOBS | ||
348 | * | ||
349 | * Chapter 20 "Pixel Memory Formats" of the Tegra X1 TRM describes this format | ||
350 | * in full detail. | ||
351 | */ | ||
352 | #define NV_FORMAT_MOD_TEGRA_16BX2_BLOCK(v) fourcc_mod_tegra_code(2, v) | ||
353 | |||
354 | #if defined(__cplusplus) | ||
355 | } | ||
356 | #endif | ||
357 | |||
232 | #endif /* DRM_FOURCC_H */ | 358 | #endif /* DRM_FOURCC_H */ |