diff options
Diffstat (limited to 'amdgpu')
-rw-r--r-- | amdgpu/amdgpu.h | 21 | ||||
-rw-r--r-- | amdgpu/amdgpu_device.c | 14 | ||||
-rw-r--r-- | amdgpu/amdgpu_internal.h | 1 |
3 files changed, 36 insertions, 0 deletions
diff --git a/amdgpu/amdgpu.h b/amdgpu/amdgpu.h index 2eb03bf1..928b2a68 100644 --- a/amdgpu/amdgpu.h +++ b/amdgpu/amdgpu.h | |||
@@ -94,6 +94,10 @@ enum amdgpu_gpu_va_range | |||
94 | amdgpu_gpu_va_range_general = 0 | 94 | amdgpu_gpu_va_range_general = 0 |
95 | }; | 95 | }; |
96 | 96 | ||
97 | enum amdgpu_sw_info { | ||
98 | amdgpu_sw_info_address32_hi = 0, | ||
99 | }; | ||
100 | |||
97 | /*--------------------------------------------------------------------------*/ | 101 | /*--------------------------------------------------------------------------*/ |
98 | /* -------------------------- Datatypes ----------------------------------- */ | 102 | /* -------------------------- Datatypes ----------------------------------- */ |
99 | /*--------------------------------------------------------------------------*/ | 103 | /*--------------------------------------------------------------------------*/ |
@@ -1086,6 +1090,23 @@ int amdgpu_query_info(amdgpu_device_handle dev, unsigned info_id, | |||
1086 | unsigned size, void *value); | 1090 | unsigned size, void *value); |
1087 | 1091 | ||
1088 | /** | 1092 | /** |
1093 | * Query hardware or driver information. | ||
1094 | * | ||
1095 | * The return size is query-specific and depends on the "info_id" parameter. | ||
1096 | * No more than "size" bytes is returned. | ||
1097 | * | ||
1098 | * \param dev - \c [in] Device handle. See #amdgpu_device_initialize() | ||
1099 | * \param info - \c [in] amdgpu_sw_info_* | ||
1100 | * \param value - \c [out] Pointer to the return value. | ||
1101 | * | ||
1102 | * \return 0 on success\n | ||
1103 | * <0 - Negative POSIX error code | ||
1104 | * | ||
1105 | */ | ||
1106 | int amdgpu_query_sw_info(amdgpu_device_handle dev, enum amdgpu_sw_info info, | ||
1107 | void *value); | ||
1108 | |||
1109 | /** | ||
1089 | * Query information about GDS | 1110 | * Query information about GDS |
1090 | * | 1111 | * |
1091 | * \param dev - \c [in] Device handle. See #amdgpu_device_initialize() | 1112 | * \param dev - \c [in] Device handle. See #amdgpu_device_initialize() |
diff --git a/amdgpu/amdgpu_device.c b/amdgpu/amdgpu_device.c index f34e27a9..6ee25a9e 100644 --- a/amdgpu/amdgpu_device.c +++ b/amdgpu/amdgpu_device.c | |||
@@ -275,6 +275,7 @@ int amdgpu_device_initialize(int fd, | |||
275 | max = MIN2(max, (start & ~0xffffffffULL) + 0x100000000ULL); | 275 | max = MIN2(max, (start & ~0xffffffffULL) + 0x100000000ULL); |
276 | amdgpu_vamgr_init(&dev->vamgr_32, start, max, | 276 | amdgpu_vamgr_init(&dev->vamgr_32, start, max, |
277 | dev->dev_info.virtual_address_alignment); | 277 | dev->dev_info.virtual_address_alignment); |
278 | dev->address32_hi = start >> 32; | ||
278 | 279 | ||
279 | start = max; | 280 | start = max; |
280 | if (dev->dev_info.high_va_offset && dev->dev_info.high_va_max) | 281 | if (dev->dev_info.high_va_offset && dev->dev_info.high_va_max) |
@@ -312,3 +313,16 @@ const char *amdgpu_get_marketing_name(amdgpu_device_handle dev) | |||
312 | { | 313 | { |
313 | return dev->marketing_name; | 314 | return dev->marketing_name; |
314 | } | 315 | } |
316 | |||
317 | int amdgpu_query_sw_info(amdgpu_device_handle dev, enum amdgpu_sw_info info, | ||
318 | void *value) | ||
319 | { | ||
320 | uint32_t *val32 = (uint32_t*)value; | ||
321 | |||
322 | switch (info) { | ||
323 | case amdgpu_sw_info_address32_hi: | ||
324 | *val32 = dev->address32_hi; | ||
325 | return 0; | ||
326 | } | ||
327 | return -EINVAL; | ||
328 | } | ||
diff --git a/amdgpu/amdgpu_internal.h b/amdgpu/amdgpu_internal.h index 75276a99..dd0c3a61 100644 --- a/amdgpu/amdgpu_internal.h +++ b/amdgpu/amdgpu_internal.h | |||
@@ -73,6 +73,7 @@ struct amdgpu_device { | |||
73 | int flink_fd; | 73 | int flink_fd; |
74 | unsigned major_version; | 74 | unsigned major_version; |
75 | unsigned minor_version; | 75 | unsigned minor_version; |
76 | uint32_t address32_hi; | ||
76 | 77 | ||
77 | char *marketing_name; | 78 | char *marketing_name; |
78 | /** List of buffer handles. Protected by bo_table_mutex. */ | 79 | /** List of buffer handles. Protected by bo_table_mutex. */ |