diff options
Diffstat (limited to 'configure.ac')
-rw-r--r-- | configure.ac | 4 |
1 files changed, 2 insertions, 2 deletions
diff --git a/configure.ac b/configure.ac index c9c4754c..68270004 100644 --- a/configure.ac +++ b/configure.ac | |||
@@ -65,10 +65,10 @@ AC_CHECK_HEADERS([sys/sysctl.h sys/select.h]) | |||
65 | LT_PREREQ([2.2]) | 65 | LT_PREREQ([2.2]) |
66 | LT_INIT([disable-static]) | 66 | LT_INIT([disable-static]) |
67 | 67 | ||
68 | dnl pthread-stubs is mandatory on BSD platforms, due to the nature of the | 68 | dnl pthread-stubs is mandatory on some BSD platforms, due to the nature of the |
69 | dnl project. Even then there's a notable issue as described in the project README | 69 | dnl project. Even then there's a notable issue as described in the project README |
70 | case "$host_os" in | 70 | case "$host_os" in |
71 | linux* | cygwin* | darwin* | solaris* | *-gnu* | gnu*) | 71 | linux* | cygwin* | darwin* | solaris* | *-gnu* | gnu* | openbsd*) |
72 | pthread_stubs_possible="no" | 72 | pthread_stubs_possible="no" |
73 | ;; | 73 | ;; |
74 | * ) | 74 | * ) |