aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
Diffstat (limited to 'intel/intel-symbol-check')
-rwxr-xr-xintel/intel-symbol-check2
1 files changed, 1 insertions, 1 deletions
diff --git a/intel/intel-symbol-check b/intel/intel-symbol-check
index 2aa2d819..4d30a4b1 100755
--- a/intel/intel-symbol-check
+++ b/intel/intel-symbol-check
@@ -3,7 +3,7 @@
3# The following symbols (past the first five) are taken from the public headers. 3# The following symbols (past the first five) are taken from the public headers.
4# A list of the latter should be available Makefile.sources/LIBDRM_INTEL_H_FILES 4# A list of the latter should be available Makefile.sources/LIBDRM_INTEL_H_FILES
5 5
6FUNCS=$(nm -D --format=bsd --defined-only ${1-.libs/libdrm_intel.so} | awk '{print $3}' | while read func; do 6FUNCS=$($NM -D --format=bsd --defined-only ${1-.libs/libdrm_intel.so} | awk '{print $3}' | while read func; do
7( grep -q "^$func$" || echo $func ) <<EOF 7( grep -q "^$func$" || echo $func ) <<EOF
8__bss_start 8__bss_start
9_edata 9_edata