aboutsummaryrefslogtreecommitdiffstats
Commit message (Collapse)AuthorAgeFilesLines
* Convert to Android.bpDan Willemsen2017-10-231-14/+0
| | | | | | | | | | | | See build/soong/README.md for more information about Soong. Removes BOARD_GPU_DRIVERS, which wasn't affecting anything, since none of the HAVE_* macros are defined. Even if they were, we'd prefer to compile all of them so that a single library can support multiple boards. Test: mmma external/libdrm Change-Id: Ie01736bce6cf41e3da5040fe5341ade0634b5111
* Build libdrm* modules with BOARD_VNDK_VERSIONJiyong Park2017-10-191-1/+1
| | | | | | | | | | | | | | | | | They are marked as vendor module since they all are depending on libdrm, which is a vendor lib. Also, libdrm_platform is newly introduced as the platform version of libdrm. Bug: 37342627 Bug: 63741047 Test: BOARD_VNDK_VERSION=current m -j libdrm_amdgpu libdrm_etnaviv libdrm_freedreno libdrm_intel libdrm_nouveau libdrm_radeon libdrm_rockchip libdrm_tegra libkms modetest atomictest planetest Change-Id: Ic1ff6fb616f406f1c5e005d3e6f6039758d62315 Merged-In: Ic1ff6fb616f406f1c5e005d3e6f6039758d62315
* android: introduce Android.common.mk to reduce boilerplateEmil Velikov2017-01-271-5/+2
| | | | | | | | | | | | | | | | ... across the makefiles. Currently this isn't much but that will change shortly. As an added bonus this fixes all present and future cases where we've forgotten to strip out the headers from LOCAL_SRC_FILES. In a couple of cases (the tests) we start setting LOCAL_EXPORT_C_INCLUDE_DIRS, which shouldn't be an issue. Cc: Chih-Wei Huang <cwhuang@android-x86.org> Cc: Rob Herring <robh@kernel.org> Signed-off-by: Emil Velikov <emil.l.velikov@gmail.com> Reviewed-by: Rob Herring <robh@kernel.org>
* android: remove LOCAL_MODULE_TAGS := optional tagEmil Velikov2017-01-271-1/+0
| | | | | | | | | | | | Seems to be the default option since ~2009 with commit 2f31293ba78 "auto import from //branches/cupcake/...@137197". Fleshed out from a larger commit in the AOSP repo/fork. Cc: Dan Willemsen <dwillemsen@google.com> Cc: Chih-Wei Huang <cwhuang@android-x86.org> Cc: Rob Herring <robh@kernel.org> Signed-off-by: Emil Velikov <emil.l.velikov@gmail.com> Reviewed-by: Rob Herring <robh@kernel.org>
* Android: strip out header files from sources listRob Herring2016-07-061-1/+1
| | | | | | | AOSP master now errors if LOCAL_SRC_FILES contains headers, so filter out header files from the source lists. Signed-off-by: Rob Herring <robh@kernel.org>
* amdgpu: add Android build supportMauro Rossi2015-08-201-0/+18
Reviewed-by: Alex Deucher <alexander.deucher@amd.com> Reviewed-by: Emil Velikov <emil.l.velikov@gmail.com>