| Commit message (Expand) | Author | Age | Files | Lines |
* | Fix dev->agp->base initialization on BSD, and fix addmap range check on Linux. | Eric Anholt | 2007-08-15 | 1 | -1/+11 |
* | BSD: Replace brief description in each file's first line with doxygen later on. | Eric Anholt | 2007-08-15 | 1 | -3/+4 |
* | Replace DRM_IOCTL_ARGS with (dev, data, file_priv) and remove DRM_DEVICE. | Eric Anholt | 2007-07-20 | 1 | -88/+59 |
* | Replace filp in ioctl arguments with drm_file *file_priv. | Eric Anholt | 2007-07-20 | 1 | -4/+4 |
* | Remove DRM_ERR OS macro. | Eric Anholt | 2007-07-20 | 1 | -42/+42 |
* | Core build fix for BSD. | Michel Dänzer | 2006-12-01 | 1 | -0/+3 |
* | Correct another LOR issue with resource allocation. This leaves the | Eric Anholt | 2005-11-08 | 1 | -1/+6 |
* | Initial port of savage to FreeBSD for the AGP and !ShadowStatus case. Adds | Eric Anholt | 2005-11-08 | 1 | -1/+1 |
* | Correct a LOR related to the PCI resource allocations by simply moving the | Eric Anholt | 2005-11-08 | 1 | -1/+1 |
* | Correct a recursion on non-recursive mutex in drm_addmap from radeon's | Eric Anholt | 2005-11-07 | 1 | -5/+6 |
* | - Don't try to allocate mappings of less than a PAGE_SIZE in MGA DMA code. | Eric Anholt | 2005-08-26 | 1 | -26/+47 |
* | Previously, drm_get_resource_start() and drm_get_resource_len() would | Eric Anholt | 2005-08-26 | 1 | -27/+28 |
* | [1] Fix BSD DRM for the nonroot changes. [2] Don't attempt to acquire the | Eric Anholt | 2005-08-25 | 1 | -7/+51 |
* | Rename the driver hooks in the DRM to something a little more | Eric Anholt | 2005-08-04 | 1 | -5/+5 |
* | Get the BSD DRM compiling again after MGA and mapping changes. Note that | Eric Anholt | 2005-06-28 | 1 | -103/+136 |
* | Add a few more bits of Tonnerre's NetBSD port (Still need to deal with the | Eric Anholt | 2005-06-06 | 1 | -1/+2 |
* | Convert BSD code to mostly use bus_dma, the dma abstraction for dealing | Eric Anholt | 2005-04-26 | 1 | -27/+18 |
* | Fix a panic on startup with non-initmapping drivers by assigning the | Eric Anholt | 2005-04-24 | 1 | -1/+1 |
* | Use /*- to begin license blocks in BSD code to reduce diffs against FreeBSD | Eric Anholt | 2005-04-15 | 1 | -1/+2 |
* | Fix build on FreeBSD-current, thanks to jhb@. | Eric Anholt | 2005-04-12 | 1 | -0/+5 |
* | Restore a debugging message to DRM_DEBUG instead of DRM_ERROR. | Eric Anholt | 2005-02-06 | 1 | -1/+1 |
* | - Implement drm_initmap, and extend it with the resource number to help | Eric Anholt | 2005-02-05 | 1 | -61/+193 |
* | Now that the memory debug code is gone, and all 3 BSDs have M_ZERO, stop | Eric Anholt | 2004-11-06 | 1 | -87/+57 |
* | Commit first pieces of port to OpenBSD, done by Martin Lexa (martin at | Eric Anholt | 2004-11-06 | 1 | -7/+6 |
* | Commit WIP of BSD conversion to core model. Compiles for r128, radeon, but | Eric Anholt | 2004-11-05 | 1 | -114/+79 |
* | Merged drmfntbl-0-0-1 | Dave Airlie | 2004-08-17 | 1 | -17/+6 |
* | Warning fixes. | Eric Anholt | 2004-05-09 | 1 | -1/+1 |
* | Fix some misuse of NULL where 0 is intended. | Eric Anholt | 2004-01-05 | 1 | -1/+1 |
* | Don't ioremap the framebuffer area. The ioremapped area wasn't used by | Eric Anholt | 2003-12-16 | 1 | -22/+17 |
* | Fix a locking nit, and add asserts in some things that should be called | Eric Anholt | 2003-11-12 | 1 | -1/+1 |
* | Return EBUSY when attempting to addmap a DRM_SHM area with a lock in it if | Eric Anholt | 2003-11-05 | 1 | -0/+10 |
* | Clean up BSD MTRR handling. The NetBSD code is untested, but it's my best | Eric Anholt | 2003-10-19 | 1 | -42/+11 |
* | - SMPng lock the DRM. This is only partial -- there are a few code paths | Eric Anholt | 2003-10-19 | 1 | -103/+58 |
* | Some code cleanups done while working on locking. Reduces always-true | Eric Anholt | 2003-10-03 | 1 | -82/+63 |
* | Stylistic preparation for SMPng locking work: DRM_LOCK/DRM_UNLOCK have side | Eric Anholt | 2003-10-03 | 1 | -24/+24 |
* | Mostly whitespace cleanups and style(9) fixes focused on "if(" -> "if (" | Eric Anholt | 2003-10-01 | 1 | -56/+49 |
* | Fix the debug build. | Eric Anholt | 2003-08-18 | 1 | -1/+1 |
* | - Remove $FreeBSD$ tags as they weren't too useful and merges are now being | Eric Anholt | 2003-08-18 | 1 | -1/+1 |
* | Support AGP bridges where the AGP aperture can't be accessed directly by | Michel Daenzer | 2003-05-16 | 1 | -1/+1 |
* | Add PCI DMA memory functions and make addbufs_pci and associated code use | Eric Anholt | 2003-04-26 | 1 | -56/+97 |
* | Merge from FreeBSD-current. | Eric Anholt | 2003-04-24 | 1 | -1/+1 |
* | Clean up the DRM_COPY_TO_USER()ing of DRM(infobufs), making it more | Eric Anholt | 2003-04-24 | 1 | -15/+9 |
* | Remove more gamma DMA infrastructure. Most of this code was copied straight | Eric Anholt | 2003-04-24 | 1 | -34/+2 |
* | Move some common code from addbufs_<type> to addbufs. Make buf_alloc be | Eric Anholt | 2003-04-24 | 1 | -113/+57 |
* | Remove DRM_DMA_HISTOGRAM and associated code. | Eric Anholt | 2003-04-23 | 1 | -19/+0 |
* | Add DRMFILE definitions and supply filp for BSD in the | Eric Anholt | 2003-03-28 | 1 | -9/+9 |
* | Merge back from FreeBSD-current, adding FreeBSD ID tags to aid future | Eric Anholt | 2003-03-11 | 1 | -0/+1 |
* | Merge from bsd-4-0-0-branch. | Eric Anholt | 2003-02-21 | 1 | -27/+31 |
* | Remove some noise being spit to the console. | Eric Anholt | 2002-09-29 | 1 | -2/+0 |
* | merged bsd-3-0-0-branch | Alan Hourihane | 2002-07-05 | 1 | -171/+217 |