aboutsummaryrefslogtreecommitdiffstats
Commit message (Collapse)AuthorAgeFilesLines
* meson,configure: include config.h automaticallyEric Engestrom2018-03-201-4/+0
| | | | | | | | | This will prevent any more missing `#include "config.h"` bug, at the cost of having to recompile some files that didn't need to be when changing build options. Signed-off-by: Eric Engestrom <eric.engestrom@imgtec.com> Reviewed-by: Emil Velikov <emil.velikov@collabora.com>
* drm: rename libdrm{,_macros}.hEmil Velikov2015-04-281-1/+1
| | | | | | Provide a more meaningful name, considering what it does. Signed-off-by: Emil Velikov <emil.l.velikov@gmail.com>
* libkms: annotate private symbolsEmil Velikov2015-04-281-7/+12
| | | | | Cc: Jakob Bornecrantz <jakob@vmware.com> Signed-off-by: Emil Velikov <emil.l.velikov@gmail.com>
* tests/kmstest: support exynosHyungwon Hwang2014-01-121-0/+2
| | | | | | | | In this patch, to support exynos for KMS, Exynos KMS driver is newly added. Also, Exynos is added to the list of kmstest supported modules. Signed-off-by: Hyungwon Hwang <human.hwang@samsung.com> Signed-off-by: Rob Clark <robclark@freedesktop.org>
* libkms: add dumb supportDave Airlie2011-03-031-0/+2
| | | | | this uses the drm cap interface to check if the dumb ioctl is supported.
* libkms/radeon: Add backendnobled2011-02-171-0/+2
| | | | | | Todo: What tiling should be set on scanout buffers? Haven't tested besides compiling it.
* libkms/nouveau: Add supportMarcin Koƛcielnicki2010-02-271-0/+2
|
* libkms: Use sysfs instead of udev to find driverJakob Bornecrantz2010-01-121-1/+1
| | | | Udev code is still there just commented out.
* libkms: Add intel backendJakob Bornecrantz2010-01-071-0/+2
|
* libkms: Pick driver backend via pci id that we get from udevJakob Bornecrantz2010-01-071-0/+2
|
* libkms: Add libkmsJakob Bornecrantz2009-12-041-0/+67