aboutsummaryrefslogtreecommitdiffstats
path: root/tests
Commit message (Expand)AuthorAgeFilesLines
* Move mmfs tests over to be drm tests.Eric Anholt2008-04-294-63/+50
* Add mmap ioctl to mmfs.Eric Anholt2008-04-232-1/+131
* Add pread/pwrite ioctls to mmfs.Eric Anholt2008-04-235-24/+162
* Extend the mmfs basic test to do a couple of ioctls.Eric Anholt2008-04-231-0/+66
* Move mmfs.h userland interface to shared-core.Eric Anholt2008-04-231-1/+0
* Initial add of mmfs module.Eric Anholt2008-04-232-1/+71
* Fix ttmtest.Thomas Hellstrom2007-11-132-19/+21
* Bug #12838: Fix lock test client vs. server master race and misplaced closes.Robert Noland2007-10-171-4/+5
* Fix a race in the auth test where client prevents server from being master.Robert Noland2007-10-171-2/+2
* Add a set of tests for DRM locking, exposing issues on BSD.Eric Anholt2007-08-152-0/+263
* Fix a bad error message in auth.c regression test.Eric Anholt2007-08-151-1/+1
* Require master in setversion test, since it requires auth.Eric Anholt2007-08-151-1/+1
* Add a regression test for the setversion interface.Eric Anholt2007-08-152-0/+85
* Add simple regression test for getstats (does it not crash the kernel?).Eric Anholt2007-08-152-0/+52
* Add a regression test for authentication.Eric Anholt2007-08-132-1/+139
* Add libdrm source dir, to build tests from a different build dirPatrice Mandin2007-08-021-2/+4
* Improve the drawable test to use multiple drawables.Eric Anholt2007-07-251-21/+42
* Add a test for drawable add, remove, and update.Eric Anholt2007-07-194-1/+168
* Fix the getclient test (Need this feature for future tests).Eric Anholt2007-07-191-2/+0
* Add some trivial regression tests, one of which fails.Eric Anholt2007-07-197-27/+249
* Checkpoint commit.Thomas Hellstrom2007-02-071-3/+3
* Make vm handle buffer objects instead of ttm objects.Thomas Hellstrom2007-02-021-1/+1
* Make the utility runnable also for normal users.Thomas Hellstrom2007-01-311-1/+1
* Indent according to xorg rules.Thomas Hellstrom2007-01-301-70/+54
* Add license header.Thomas Hellstrom2007-01-301-0/+31
* Add some relevant tests for the new buffer object interface.Thomas Hellstrom2007-01-301-1/+220
* Add the ttmtest test utility.Thomas Hellstrom2007-01-3012-0/+1372
* Bug #2567: Fix reversed memset arguments. (David Krause)Adam Jackson2005-02-181-1/+1
* use libdrm after it was updatedDave Airlie2005-01-241-1/+1
* Forgot to add the new MakefileJon Smirl2004-10-091-0/+27
* Make the test programs buildJon Smirl2004-10-092-7/+7
* Apply patch from Bryan Stine bugzilla #1227Dave Airlie2004-08-311-3/+12
* Targets for building dristat and drmstat.David Dawes2003-04-241-0/+9
* Minor cleanups for dri/drmstat test progs (Both still need targets for newLeif Delgass2003-04-242-7/+9
* Remove #if 0'd code and some unused string functionsKeith Whitwell2003-04-241-12/+0
* Implement drmOpen* without /proc dependence (Fallback to /proc is includedRik Faith2001-02-281-216/+23
* Merge mga-1-0-0-branch into trunk.Gareth Hughes2001-02-151-0/+473
* Merged glxmisc-3-0-0Brian Paul2000-06-081-2/+2
* Merged mga branch with trunkJeff Hartmann2000-04-041-1/+1
* Merge with 4.0Jeff Hartmann2000-03-151-2/+1
* Import of XFree86 3.9.18Kevin E Martin2000-02-221-20/+20
* Import of XFree86 3.9.17Rik Faith2000-01-061-19/+19
* Rename the device to be /dev/dri instead of /dev/dri to avoid a conflict.Daryll Strauss1999-12-181-18/+18
* Move Mesa to xc/extras Update to the latest Mesa 3.2 code Fix the Q3DemoDaryll Strauss1999-12-061-15/+15
* First DRI release of 3dfx driver.Daryll Strauss1999-12-051-0/+417