/* * Copyright 2014 Advanced Micro Devices, Inc. * * Permission is hereby granted, free of charge, to any person obtaining a * copy of this software and associated documentation files (the "Software"), * to deal in the Software without restriction, including without limitation * the rights to use, copy, modify, merge, publish, distribute, sublicense, * and/or sell copies of the Software, and to permit persons to whom the * Software is furnished to do so, subject to the following conditions: * * The above copyright notice and this permission notice shall be included in * all copies or substantial portions of the Software. * * THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR * IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY, * FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN NO EVENT SHALL * THE COPYRIGHT HOLDER(S) OR AUTHOR(S) BE LIABLE FOR ANY CLAIM, DAMAGES OR * OTHER LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, * ARISING FROM, OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE USE OR * OTHER DEALINGS IN THE SOFTWARE. * */ /** * \file amdgpu.h * * Declare public libdrm_amdgpu API * * This file define API exposed by libdrm_amdgpu library. * User wanted to use libdrm_amdgpu functionality must include * this file. * */ #ifndef _AMDGPU_H_ #define _AMDGPU_H_ #include #include #ifdef __cplusplus extern "C" { #endif struct drm_amdgpu_info_hw_ip; /*--------------------------------------------------------------------------*/ /* --------------------------- Defines ------------------------------------ */ /*--------------------------------------------------------------------------*/ /** * Define max. number of Command Buffers (IB) which could be sent to the single * hardware IP to accommodate CE/DE requirements * * \sa amdgpu_cs_ib_info */ #define AMDGPU_CS_MAX_IBS_PER_SUBMIT 4 /** * Special timeout value meaning that the timeout is infinite. */ #define AMDGPU_TIMEOUT_INFINITE 0xffffffffffffffffull /** * Used in amdgpu_cs_query_fence_status(), meaning that the given timeout * is absolute. */ #define AMDGPU_QUERY_FENCE_TIMEOUT_IS_ABSOLUTE (1 << 0) /*--------------------------------------------------------------------------*/ /* ----------------------------- Enums ------------------------------------ */ /*--------------------------------------------------------------------------*/ /** * Enum describing possible handle types * * \sa amdgpu_bo_import, amdgpu_bo_export * */ enum amdgpu_bo_handle_type { /** GEM flink name (needs DRM authentication, used by DRI2) */ amdgpu_bo_handle_type_gem_flink_name = 0, /** KMS handle which is used by all driver ioctls */ amdgpu_bo_handle_type_kms = 1, /** DMA-buf fd handle */ amdgpu_bo_handle_type_dma_buf_fd = 2 }; /** Define known types of GPU VM VA ranges */ enum amdgpu_gpu_va_range { /** Allocate from "normal"/general range */ amdgpu_gpu_va_range_general = 0 }; enum amdgpu_sw_info { amdgpu_sw_info_address32_hi = 0, }; /*--------------------------------------------------------------------------*/ /* -------------------------- Datatypes ----------------------------------- */ /*--------------------------------------------------------------------------*/ /** * Define opaque pointer to context associated with fd. * This context will be returned as the result of * "initialize" function and should be pass as the first * parameter to any API call */ typedef struct amdgpu_device *amdgpu_device_handle; /** * Define GPU Context type as pointer to opaque structure * Example of GPU Context is the "rendering" context associated * with OpenGL context (glCreateContext) */ typedef struct amdgpu_context *amdgpu_context_handle; /** * Define handle for amdgpu resources: buffer, GDS, etc. */ typedef struct amdgpu_bo *amdgpu_bo_handle; /** * Define handle for list of BOs */ typedef struct amdgpu_bo_list *amdgpu_bo_list_handle; /** * Define handle to be used to work with VA allocated ranges */ typedef struct amdgpu_va *amdgpu_va_handle; /** * Define handle for semaphore */ typedef struct amdgpu_semaphore *amdgpu_semaphore_handle; /*--------------------------------------------------------------------------*/ /* -------------------------- Structures ---------------------------------- */ /*--------------------------------------------------------------------------*/ /** * Structure describing memory allocation request * * \sa amdgpu_bo_alloc() * */ struct amdgpu_bo_alloc_request { /** Allocation request. It must be aligned correctly. */ uint64_t alloc_size; /** * It may be required to have some specific alignment requirements * for physical back-up storage (e.g. for displayable surface). * If 0 there is no special alignment requirement */ uint64_t phys_alignment; /** * UMD should specify where to allocate memory and how it * will be accessed by the CPU. */ uint32_t preferred_heap; /** Additional flags passed on allocation */ uint64_t flags; }; /** * Special UMD specific information associated with buffer. * * It may be need to pass some buffer charactersitic as part * of buffer sharing. Such information are defined UMD and * opaque for libdrm_amdgpu as well for kernel driver. * * \sa amdgpu_bo_set_metadata(), amdgpu_bo_query_info, * amdgpu_bo_import(), amdgpu_bo_export * */ struct amdgpu_bo_metadata { /** Special flag associated with surface */ uint64_t flags; /** * ASIC-specific tiling information (also used by DCE). * The encoding is defined by the AMDGPU_TILING_* definitions. */ uint64_t tiling_info; /** Size of metadata associated with the buffer, in bytes. */ uint32_t size_metadata; /** UMD specific metadata. Opaque for kernel */ uint32_t umd_metadata[64]; }; /** * Structure describing allocated buffer. Client may need * to query such information as part of 'sharing' buffers mechanism * * \sa amdgpu_bo_set_metadata(), amdgpu_bo_query_info(), * amdgpu_bo_import(), amdgpu_bo_export() */ struct amdgpu_bo_info { /** Allocated memory size */ uint64_t alloc_size; /** * It may be required to have some specific alignment requirements * for physical back-up storage. */ uint64_t phys_alignment; /** Heap where to allocate memory. */ uint32_t preferred_heap; /** Additional allocation flags. */ uint64_t alloc_flags; /** Metadata associated with buffer if any. */ struct amdgpu_bo_metadata metadata; }; /** * Structure with information about "imported" buffer * * \sa amdgpu_bo_import() * */ struct amdgpu_bo_import_result { /** Handle of memory/buffer to use */ amdgpu_bo_handle buf_handle; /** Buffer size */ uint64_t alloc_size; }; /** * * Structure to describe GDS partitioning information. * \note OA and GWS resources are asscoiated with GDS partition * * \sa amdgpu_gpu_resource_query_gds_info * */ struct amdgpu_gds_resource_info { uint32_t gds_gfx_partition_size; uint32_t compute_partition_size; uint32_t gds_total_size; uint32_t gws_per_gfx_partition; uint32_t gws_per_compute_partition; uint32_t oa_per_gfx_partition; uint32_t oa_per_compute_partition; }; /** * Structure describing CS fence * * \sa amdgpu_cs_query_fence_status(), amdgpu_cs_request, amdgpu_cs_submit() * */ struct amdgpu_cs_fence { /** In which context IB was sent to execution */ amdgpu_context_handle context; /** To which HW IP type the fence belongs */ uint32_t ip_type; /** IP instance index if there are several IPs of the same type. */ uint32_t ip_instance; /** Ring index of the HW IP */ uint32_t ring; /** Specify fence for which we need to check submission status.*/ uint64_t fence; }; /** * Structure describing IB * * \sa amdgpu_cs_request, amdgpu_cs_submit() * */ struct amdgpu_cs_ib_info { /** Special flags */ uint64_t flags; /** Virtual MC address of the command buffer */ uint64_t ib_mc_address; /** * Size of Command Buffer to be submitted. * - The size is in units of dwords (4 bytes). * - Could be 0 */ uint32_t size; }; /** * Structure describing fence information * * \sa amdgpu_cs_request, amdgpu_cs_query_fence, * amdgpu_cs_submit(), amdgpu_cs_query_fence_status() */ struct amdgpu_cs_fence_info { /** buffer object for the fence */ amdgpu_bo_handle handle; /** fence offset in the unit of sizeof(uint64_t) */ uint64_t offset; }; /** * Structure describing submission request * * \note We could have several IBs as packet. e.g. CE, CE, DE case for gfx * * \sa amdgpu_cs_submit() */ struct amdgpu_cs_request { /** Specify flags with additional information */ uint64_t flags; /** Specify HW IP block type to which to send the IB. */ unsigned ip_type; /** IP instance index if there are several IPs of the same type. */ unsigned ip_instance; /** * Specify ring index of the IP. We could have several rings * in the same IP. E.g. 0 for SDMA0 and 1 for SDMA1. */ uint32_t ring; /** * List handle with resources used by this request. */ amdgpu_bo_list_handle resources; /** * Number of dependencies this Command submission needs to * wait for before starting execution. */ uint32_t number_of_dependencies; /** * Array of dependencies which need to be met before * execution can start. */ struct amdgpu_cs_fence *dependencies; /** Number of IBs to submit in the field ibs. */ uint32_t number_of_ibs; /** * IBs to submit. Those IBs will be submit together as single entity */ struct amdgpu_cs_ib_info *ibs; /** * The returned sequence number for the command submission */ uint64_t seq_no; /** * The fence information */ struct amdgpu_cs_fence_info fence_info; }; /** * Structure which provide information about GPU VM MC Address space * alignments requirements * * \sa amdgpu_query_buffer_size_alignment */ struct amdgpu_buffer_size_alignments { /** Size alignment requirement for allocation in * local memory */ uint64_t size_local; /** * Size alignment requirement for allocation in remote memory */ uint64_t size_remote; }; /** * Structure which provide information about heap * * \sa amdgpu_query_heap_info() * */ struct amdgpu_heap_info { /** Theoretical max. available memory in the given heap */ uint64_t heap_size; /** * Number of bytes allocated in the heap. This includes all processes * and private allocations in the kernel. It changes when new buffers * are allocated, freed, and moved. It cannot be larger than * heap_size. */ uint64_t heap_usage; /** * Theoretical possible max. size of buffer which * could be allocated in the given heap */ uint64_t max_allocation; }; /** * Describe GPU h/w info needed for UMD correct initialization * * \sa amdgpu_query_gpu_info() */ struct amdgpu_gpu_info { /** Asic id */ uint32_t asic_id; /** Chip revision */ uint32_t chip_rev; /** Chip external revision */ uint32_t chip_external_rev; /** Family ID */ uint32_t family_id; /** Special flags */ uint64_t ids_flags; /** max engine clock*/ uint64_t max_engine_clk; /** max memory clock */ uint64_t max_memory_clk; /** number of shader engines */ uint32_t num_shader_engines; /** number of shader arrays per engine */ uint32_t num_shader_arrays_per_engine; /** Number of available good shader pipes */ uint32_t avail_quad_shader_pipes; /** Max. number of shader pipes.(including good and bad pipes */ uint32_t max_quad_shader_pipes; /** Number of parameter cache entries per shader quad pipe */ uint32_t cache_entries_per_quad_pipe; /** Number of available graphics context */ uint32_t num_hw_gfx_contexts; /** Number of render backend pipes */ uint32_t rb_pipes; /** Enabled render backend pipe mask */ uint32_t enabled_rb_pipes_mask; /** Frequency of GPU Counter */ uint32_t gpu_counter_freq; /** CC_RB_BACKEND_DISABLE.BACKEND_DISABLE per SE */ uint32_t backend_disable[4]; /** Value of MC_ARB_RAMCFG register*/ uint32_t mc_arb_ramcfg; /** Value of GB_ADDR_CONFIG */ uint32_t gb_addr_cfg; /** Values of the GB_TILE_MODE0..31 registers */ uint32_t gb_tile_mode[32]; /** Values of GB_MACROTILE_MODE0..15 registers */ uint32_t gb_macro_tile_mode[16]; /** Value of PA_SC_RASTER_CONFIG register per SE */ uint32_t pa_sc_raster_cfg[4]; /** Value of PA_SC_RASTER_CONFIG_1 register per SE */ uint32_t pa_sc_raster_cfg1[4]; /* CU info */ uint32_t cu_active_number; uint32_t cu_ao_mask; uint32_t cu_bitmap[4][4]; /* video memory type info*/ uint32_t vram_type; /* video memory bit width*/ uint32_t vram_bit_width; /** constant engine ram size*/ uint32_t ce_ram_size; /* vce harvesting instance */ uint32_t vce_harvest_config; /* PCI revision ID */ uint32_t pci_rev_id; }; /*--------------------------------------------------------------------------*/ /*------------------------- Functions --------------------------------------*/ /*--------------------------------------------------------------------------*/ /* * Initialization / Cleanup * */ /** * * \param fd - \c [in] File descriptor for AMD GPU device * received previously as the result of * e.g. drmOpen() call. * For legacy fd type, the DRI2/DRI3 * authentication should be done before * calling this function. * \param major_version - \c [out] Major version of library. It is assumed * that adding new functionality will cause * increase in major version * \param minor_version - \c [out] Minor version of library * \param device_handle - \c [out] Pointer to opaque context which should * be passed as the first parameter on each * API call * * * \return 0 on success\n * <0 - Negative POSIX Error code * * * \sa amdgpu_device_deinitialize() */ int amdgpu_device_initialize(int fd, uint32_t *major_version, uint32_t *minor_version, amdgpu_device_handle *device_handle); /** * * When access to such library does not needed any more the special * function must be call giving opportunity to clean up any * resources if needed. * * \param device_handle - \c [in] Context associated with file * descriptor for AMD GPU device * received previously as the * result e.g. of drmOpen() call. * * \return 0 on success\n * <0 - Negative POSIX Error code * * \sa amdgpu_device_initialize() * */ int amdgpu_device_deinitialize(amdgpu_device_handle device_handle); /* * Memory Management * */ /** * Allocate memory to be used by UMD for GPU related operations * * \param dev - \c [in] Device handle. * See #amdgpu_device_initialize() * \param alloc_buffer - \c [in] Pointer to the structure describing an * allocation request * \param buf_handle - \c [out] Allocated buffer handle * * \return 0 on success\n * <0 - Negative POSIX Error code * * \sa amdgpu_bo_free() */ int amdgpu_bo_alloc(amdgpu_device_handle dev, struct amdgpu_bo_alloc_request *alloc_buffer, amdgpu_bo_handle *buf_handle); /** * Associate opaque data with buffer to be queried by another UMD * * \param dev - \c [in] Device handle. See #amdgpu_device_initialize() * \param buf_handle - \c [in] Buffer handle * \param info - \c [in] Metadata to associated with buffer * * \return 0 on success\n * <0 - Negative POSIX Error code */ int amdgpu_bo_set_metadata(amdgpu_bo_handle buf_handle, struct amdgpu_bo_metadata *info); /** * Query buffer information including metadata previusly associated with * buffer. * * \param dev - \c [in] Device handle. * See #amdgpu_device_initialize() * \param buf_handle - \c [in] Buffer handle * \param info - \c [out] Structure describing buffer * * \return 0 on success\n * <0 - Negative POSIX Error code * * \sa amdgpu_bo_set_metadata(), amdgpu_bo_alloc() */ int amdgpu_bo_query_info(amdgpu_bo_handle buf_handle, struct amdgpu_bo_info *info); /** * Allow others to get access to buffer * * \param dev - \c [in] Device handle. * See #amdgpu_device_initialize() * \param buf_handle - \c [in] Buffer handle * \param type - \c [in] Type of handle requested * \param shared_handle - \c [out] Special "shared" handle * * \return 0 on success\n * <0 - Negative POSIX Error code * * \sa amdgpu_bo_import() * */ int amdgpu_bo_export(amdgpu_bo_handle buf_handle, enum amdgpu_bo_handle_type type, uint32_t *shared_handle); /** * Request access to "shared" buffer * * \param dev - \c [in] Device handle. * See #amdgpu_device_initialize() * \param type - \c [in] Type of handle requested * \param shared_handle - \c [in] Shared handle received as result "import" * operation * \param output - \c [out] Pointer to structure with information * about imported buffer * * \return 0 on success\n * <0 - Negative POSIX Error code * * \note Buffer must be "imported" only using new "fd" (different from * one used by "exporter"). * * \sa amdgpu_bo_export() * */ int amdgpu_bo_import(amdgpu_device_handle dev, enum amdgpu_bo_handle_type type, uint32_t shared_handle, struct amdgpu_bo_import_result *output); /** * Request GPU access to user allocated memory e.g. via "malloc" * * \param dev - [in] Device handle. See #amdgpu_device_initialize() * \param cpu - [in] CPU address of user allocated memory which we * want to map to GPU address space (make GPU accessible) * (This address must be correctly aligned). * \param size - [in] Size of allocation (must be correctly aligned) * \param buf_handle - [out] Buffer handle for the userptr memory * resource on submission and be used in other operations. * * * \return 0 on success\n * <0 - Negative POSIX Error code * * \note * This call doesn't guarantee that such memory will be persistently * "locked" / make non-pageable. The purpose of this call is to provide * opportunity for GPU get access to this resource during submission. * * The maximum amount of memory which could be mapped in this call depends * if overcommit is disabled or not. If overcommit is disabled than the max. * amount of memory to be pinned will be limited by left "free" size in total * amount of memory which could be locked simultaneously ("GART" size). * * Supported (theoretical) max. size of mapping is restricted only by * "GART" size. * * It is responsibility of caller to correctly specify access rights * on VA assignment. */ int amdgpu_create_bo_from_user_mem(amdgpu_device_handle dev, void *cpu, uint64_t size, amdgpu_bo_handle *buf_handle); /** * Free previosuly allocated memory * * \param dev - \c [in] Device handle. See #amdgpu_device_initialize() * \param buf_handle - \c [in] Buffer handle to free * * \return 0 on success\n * <0 - Negative POSIX Error code * * \note In the case of memory shared between different applications all * resources will be “physically” freed only all such applications * will be terminated * \note If is UMD responsibility to ‘free’ buffer only when there is no * more GPU access * * \sa amdgpu_bo_set_metadata(), amdgpu_bo_alloc() * */ int amdgpu_bo_free(amdgpu_bo_handle buf_handle); /** * Request CPU access to GPU accessible memory * * \param buf_handle - \c [in] Buffer handle * \param cpu - \c [out] CPU address to be used for access * * \return 0 on success\n * <0 - Negative POSIX Error code * * \sa amdgpu_bo_cpu_unmap() * */ int amdgpu_bo_cpu_map(amdgpu_bo_handle buf_handle, void **cpu); /** * Release CPU access to GPU memory * * \param buf_handle - \c [in] Buffer handle * * \return 0 on success\n * <0 - Negative POSIX Error code * * \sa amdgpu_bo_cpu_map() * */ int amdgpu_bo_cpu_unmap(amdgpu_bo_handle buf_handle); /** * Wait until a buffer is not used by the device. * * \param dev - \c [in] Device handle. See #amdgpu_device_initialize() * \param buf_handle - \c [in] Buffer handle. * \param timeout_ns - Timeout in nanoseconds. * \param buffer_busy - 0 if buffer is idle, all GPU access was completed * and no GPU access is scheduled. * 1 GPU access is in fly or scheduled * * \return 0 - on success * <0 - Negative POSIX Error code */ int amdgpu_bo_wait_for_idle(amdgpu_bo_handle buf_handle, uint64_t timeout_ns, bool *buffer_busy); /** * Creates a BO list handle for command submission. * * \param dev - \c [in] Device handle. * See #amdgpu_device_initialize() * \param number_of_resources - \c [in] Number of BOs in the list * \param resources - \c [in] List of BO handles * \param resource_prios - \c [in] Optional priority for each handle * \param result - \c [out] Created BO list handle * * \return 0 on success\n * <0 - Negative POSIX Error code * * \sa amdgpu_bo_list_destroy() */ int amdgpu_bo_list_create(amdgpu_device_handle dev, uint32_t number_of_resources, amdgpu_bo_handle *resources, uint8_t *resource_prios, amdgpu_bo_list_handle *result); /** * Destroys a BO list handle. * * \param handle - \c [in] BO list handle. * * \return 0 on success\n * <0 - Negative POSIX Error code * * \sa amdgpu_bo_list_create() */ int amdgpu_bo_list_destroy(amdgpu_bo_list_handle handle); /** * Update resources for existing BO list * * \param handle - \c [in] BO list handle * \param number_of_resources - \c [in] Number of BOs in the list * \param resources - \c [in] List of BO handles * \param resource_prios - \c [in] Optional priority for each handle * * \return 0 on success\n * <0 - Negative POSIX Error code * * \sa amdgpu_bo_list_update() */ int amdgpu_bo_list_update(amdgpu_bo_list_handle handle, uint32_t number_of_resources, amdgpu_bo_handle *resources, uint8_t *resource_prios); /* * GPU Execution context * */ /** * Create GPU execution Context * * For the purpose of GPU Scheduler and GPU Robustness extensions it is * necessary to have information/identify rendering/compute contexts. * It also may be needed to associate some specific requirements with such * contexts. Kernel driver will guarantee that submission from the same * context will always be executed in order (first come, first serve). * * * \param dev - \c [in] Device handle. See #amdgpu_device_initialize() * \param priority - \c [in] Context creation flags. See AMDGPU_CTX_PRIORITY_* * \param context - \c [out] GPU Context handle * * \return 0 on success\n * <0 - Negative POSIX Error code * * \sa amdgpu_cs_ctx_free() * */ int amdgpu_cs_ctx_create2(amdgpu_device_handle dev, uint32_t priority, amdgpu_context_handle *context); /** * Create GPU execution Context * * Refer to amdgpu_cs_ctx_create2 for full documentation. This call * is missing the priority parameter. * * \sa amdgpu_cs_ctx_create2() * */ int amdgpu_cs_ctx_create(amdgpu_device_handle dev, amdgpu_context_handle *context); /** * * Destroy GPU execution context when not needed any more * * \param context - \c [in] GPU Context handle * * \return 0 on success\n * <0 - Negative POSIX Error code * * \sa amdgpu_cs_ctx_create() * */ int amdgpu_cs_ctx_free(amdgpu_context_handle context); /** * Query reset state for the specific GPU Context * * \param context - \c [in] GPU Context handle * \param state - \c [out] One of AMDGPU_CTX_*_RESET * \param hangs - \c [out] Number of hangs caused by the context. * * \return 0 on success\n * <0 - Negative POSIX Error code * * \sa amdgpu_cs_ctx_create() * */ int amdgpu_cs_query_reset_state(amdgpu_context_handle context, uint32_t *state, uint32_t *hangs); /* * Command Buffers Management * */ /** * Send request to submit command buffers to hardware. * * Kernel driver could use GPU Scheduler to make decision when physically * sent this request to the hardware. Accordingly this request could be put * in queue and sent for execution later. The only guarantee is that request * from the same GPU context to the same ip:ip_instance:ring will be executed in * order. * * The caller can specify the user fence buffer/location with the fence_info in the * cs_request.The sequence number is returned via the 'seq_no' parameter * in ibs_request structure. * * * \param dev - \c [in] Device handle. * See #amdgpu_device_initialize() * \param context - \c [in] GPU Context * \param flags - \c [in] Global submission flags * \param ibs_request - \c [in/out] Pointer to submission requests. * We could submit to the several * engines/rings simulteniously as * 'atomic' operation * \param number_of_requests - \c [in] Number of submission requests * * \return 0 on success\n * <0 - Negative POSIX Error code * * \note It is required to pass correct resource list with buffer handles * which will be accessible by command buffers from submission * This will allow kernel driver to correctly implement "paging". * Failure to do so will have unpredictable results. * * \sa amdgpu_command_buffer_alloc(), amdgpu_command_buffer_free(), * amdgpu_cs_query_fence_status() * */ int amdgpu_cs_submit(amdgpu_context_handle context, uint64_t flags, struct amdgpu_cs_request *ibs_request, uint32_t number_of_requests); /** * Query status of Command Buffer Submission * * \param fence - \c [in] Structure describing fence to query * \param timeout_ns - \c [in] Timeout value to wait * \param flags - \c [in] Flags for the query * \param expired - \c [out] If fence expired or not.\n * 0 – if fence is not expired\n * !0 - otherwise * * \return 0 on success\n * <0 - Negative POSIX Error code * * \note If UMD wants only to check operation status and returned immediately * then timeout value as 0 must be passed. In this case success will be * returned in the case if submission was completed or timeout error * code. * * \sa amdgpu_cs_submit() */ int amdgpu_cs_query_fence_status(struct amdgpu_cs_fence *fence, uint64_t timeout_ns, uint64_t flags, uint32_t *expired); /** * Wait for multiple fences * * \param fences - \c [in] The fence array to wait * \param fence_count - \c [in] The fence count * \param wait_all - \c [in] If true, wait all fences to be signaled, * otherwise, wait at least one fence * \param timeout_ns - \c [in] The timeout to wait, in nanoseconds * \param status - \c [out] '1' for signaled, '0' for timeout * \param first - \c [out] the index of the first signaled fence from @fences * * \return 0 on success * <0 - Negative POSIX Error code * * \note Currently it supports only one amdgpu_device. All fences come from * the same amdgpu_device with the same fd. */ int amdgpu_cs_wait_fences(struct amdgpu_cs_fence *fences, uint32_t fence_count, bool wait_all, uint64_t timeout_ns, uint32_t *status, uint32_t *first); /* * Query / Info API * */ /** * Query allocation size alignments * * UMD should query information about GPU VM MC size alignments requirements * to be able correctly choose required allocation size and implement * internal optimization if needed. * * \param dev - \c [in] Device handle. See #amdgpu_device_initialize() * \param info - \c [out] Pointer to structure to get size alignment * requirements * * \return 0 on success\n * <0 - Negative POSIX Error code * */ int amdgpu_query_buffer_size_alignment(amdgpu_device_handle dev, struct amdgpu_buffer_size_alignments *info); /** * Query firmware versions * * \param dev - \c [in] Device handle. See #amdgpu_device_initialize() * \param fw_type - \c [in] AMDGPU_INFO_FW_* * \param ip_instance - \c [in] Index of the IP block of the same type. * \param index - \c [in] Index of the engine. (for SDMA and MEC) * \param version - \c [out] Pointer to to the "version" return value * \param feature - \c [out] Pointer to to the "feature" return value * * \return 0 on success\n * <0 - Negative POSIX Error code * */ int amdgpu_query_firmware_version(amdgpu_device_handle dev, unsigned fw_type, unsigned ip_instance, unsigned index, uint32_t *version, uint32_t *feature); /** * Query the number of HW IP instances of a certain type. * * \param dev - \c [in] Device handle. See #amdgpu_device_initialize() * \param type - \c [in] Hardware IP block type = AMDGPU_HW_IP_* * \param count - \c [out] Pointer to structure to get information * * \return 0 on success\n * <0 - Negative POSIX Error code */ int amdgpu_query_hw_ip_count(amdgpu_device_handle dev, unsigned type, uint32_t *count); /** * Query engine information * * This query allows UMD to query information different engines and their * capabilities. * * \param dev - \c [in] Device handle. See #amdgpu_device_initialize() * \param type - \c [in] Hardware IP block type = AMDGPU_HW_IP_* * \param ip_instance - \c [in] Index of the IP block of the same type. * \param info - \c [out] Pointer to structure to get information * * \return 0 on success\n * <0 - Negative POSIX Error code */ int amdgpu_query_hw_ip_info(amdgpu_device_handle dev, unsigned type, unsigned ip_instance, struct drm_amdgpu_info_hw_ip *info); /** * Query heap information * * This query allows UMD to query potentially available memory resources and * adjust their logic if necessary. * * \param dev - \c [in] Device handle. See #amdgpu_device_initialize() * \param heap - \c [in] Heap type * \param info - \c [in] Pointer to structure to get needed information * * \return 0 on success\n * <0 - Negative POSIX Error code * */ int amdgpu_query_heap_info(amdgpu_device_handle dev, uint32_t heap, uint32_t flags, struct amdgpu_heap_info *info); /** * Get the CRTC ID from the mode object ID * * \param dev - \c [in] Device handle. See #amdgpu_device_initialize() * \param id - \c [in] Mode object ID * \param result - \c [in] Pointer to the CRTC ID * * \return 0 on success\n * <0 - Negative POSIX Error code * */ int amdgpu_query_crtc_from_id(amdgpu_device_handle dev, unsigned id, int32_t *result); /** * Query GPU H/w Info * * Query hardware specific information * * \param dev - \c [in] Device handle. See #amdgpu_device_initialize() * \param heap - \c [in] Heap type * \param info - \c [in] Pointer to structure to get needed information * * \return 0 on success\n * <0 - Negative POSIX Error code * */ int amdgpu_query_gpu_info(amdgpu_device_handle dev, struct amdgpu_gpu_info *info); /** * Query hardware or driver information. * * The return size is query-specific and depends on the "info_id" parameter. * No more than "size" bytes is returned. * * \param dev - \c [in] Device handle. See #amdgpu_device_initialize() * \param info_id - \c [in] AMDGPU_INFO_* * \param size - \c [in] Size of the returned value. * \param value - \c [out] Pointer to the return value. * * \return 0 on success\n * <0 - Negative POSIX error code * */ int amdgpu_query_info(amdgpu_device_handle dev, unsigned info_id, unsigned size, void *value); /** * Query hardware or driver information. * * The return size is query-specific and depends on the "info_id" parameter. * No more than "size" bytes is returned. * * \param dev - \c [in] Device handle. See #amdgpu_device_initialize() * \param info - \c [in] amdgpu_sw_info_* * \param value - \c [out] Pointer to the return value. * * \return 0 on success\n * <0 - Negative POSIX error code * */ int amdgpu_query_sw_info(amdgpu_device_handle dev, enum amdgpu_sw_info info, void *value); /** * Query information about GDS * * \param dev - \c [in] Device handle. See #amdgpu_device_initialize() * \param gds_info - \c [out] Pointer to structure to get GDS information * * \return 0 on success\n * <0 - Negative POSIX Error code * */ int amdgpu_query_gds_info(amdgpu_device_handle dev, struct amdgpu_gds_resource_info *gds_info); /** * Query information about sensor. * * The return size is query-specific and depends on the "sensor_type" * parameter. No more than "size" bytes is returned. * * \param dev - \c [in] Device handle. See #amdgpu_device_initialize() * \param sensor_type - \c [in] AMDGPU_INFO_SENSOR_* * \param size - \c [in] Size of the returned value. * \param value - \c [out] Pointer to the return value. * * \return 0 on success\n * <0 - Negative POSIX Error code * */ int amdgpu_query_sensor_info(amdgpu_device_handle dev, unsigned sensor_type, unsigned size, void *value); /** * Read a set of consecutive memory-mapped registers. * Not all registers are allowed to be read by userspace. * * \param dev - \c [in] Device handle. See #amdgpu_device_initialize( * \param dword_offset - \c [in] Register offset in dwords * \param count - \c [in] The number of registers to read starting * from the offset * \param instance - \c [in] GRBM_GFX_INDEX selector. It may have other * uses. Set it to 0xffffffff if unsure. * \param flags - \c [in] Flags with additional information. * \param values - \c [out] The pointer to return values. * * \return 0 on success\n * <0 - Negative POSIX error code * */ int amdgpu_read_mm_registers(amdgpu_device_handle dev, unsigned dword_offset, unsigned count, uint32_t instance, uint32_t flags, uint32_t *values); /** * Flag to request VA address range in the 32bit address space */ #define AMDGPU_VA_RANGE_32_BIT 0x1 #define AMDGPU_VA_RANGE_HIGH 0x2 /** * Allocate virtual address range * * \param dev - [in] Device handle. See #amdgpu_device_initialize() * \param va_range_type - \c [in] Type of MC va range from which to allocate * \param size - \c [in] Size of range. Size must be correctly* aligned. * It is client responsibility to correctly aligned size based on the future * usage of allocated range. * \param va_base_alignment - \c [in] Overwrite base address alignment * requirement for GPU VM MC virtual * address assignment. Must be multiple of size alignments received as * 'amdgpu_buffer_size_alignments'. * If 0 use the default one. * \param va_base_required - \c [in] Specified required va base address. * If 0 then library choose available one. * If !0 value will be passed and those value already "in use" then * corresponding error status will be returned. * \param va_base_allocated - \c [out] On return: Allocated VA base to be used * by client. * \param va_range_handle - \c [out] On return: Handle assigned to allocation * \param flags - \c [in] flags for special VA range * * \return 0 on success\n * >0 - AMD specific error code\n * <0 - Negative POSIX Error code * * \notes \n * It is client responsibility to correctly handle VA assignments and usage. * Neither kernel driver nor libdrm_amdpgu are able to prevent and * detect wrong va assignemnt. * * It is client responsibility to correctly handle multi-GPU cases and to pass * the corresponding arrays of all devices handles where corresponding VA will * be used. * */ int amdgpu_va_range_alloc(amdgpu_device_handle dev, enum amdgpu_gpu_va_range va_range_type, uint64_t size, uint64_t va_base_alignment, uint64_t va_base_required, uint64_t *va_base_allocated, amdgpu_va_handle *va_range_handle, uint64_t flags); /** * Free previously allocated virtual address range * * * \param va_range_handle - \c [in] Handle assigned to VA allocation * * \return 0 on success\n * >0 - AMD specific error code\n * <0 - Negative POSIX Error code * */ int amdgpu_va_range_free(amdgpu_va_handle va_range_handle); /** * Query virtual address range * * UMD can query GPU VM range supported by each device * to initialize its own VAM accordingly. * * \param dev - [in] Device handle. See #amdgpu_device_initialize() * \param type - \c [in] Type of virtual address range * \param offset - \c [out] Start offset of virtual address range * \param size - \c [out] Size of virtual address range * * \return 0 on success\n * <0 - Negative POSIX Error code * */ int amdgpu_va_range_query(amdgpu_device_handle dev, enum amdgpu_gpu_va_range type, uint64_t *start, uint64_t *end); /** * VA mapping/unmapping for the buffer object * * \param bo - \c [in] BO handle * \param offset - \c [in] Start offset to map * \param size - \c [in] Size to map * \param addr - \c [in] Start virtual address. * \param flags - \c [in] Supported flags for mapping/unmapping * \param ops - \c [in] AMDGPU_VA_OP_MAP or AMDGPU_VA_OP_UNMAP * * \return 0 on success\n * <0 - Negative POSIX Error code * */ int amdgpu_bo_va_op(amdgpu_bo_handle bo, uint64_t offset, uint64_t size, uint64_t addr, uint64_t flags, uint32_t ops); /** * VA mapping/unmapping for a buffer object or PRT region. * * This is not a simple drop-in extension for amdgpu_bo_va_op; instead, all * parameters are treated "raw", i.e. size is not automatically aligned, and * all flags must be specified explicitly. * * \param dev - \c [in] device handle * \param bo - \c [in] BO handle (may be NULL) * \param offset - \c [in] Start offset to map * \param size - \c [in] Size to map * \param addr - \c [in] Start virtual address. * \param flags - \c [in] Supported flags for mapping/unmapping * \param ops - \c [in] AMDGPU_VA_OP_MAP or AMDGPU_VA_OP_UNMAP * * \return 0 on success\n * <0 - Negative POSIX Error code * */ int amdgpu_bo_va_op_raw(amdgpu_device_handle dev, amdgpu_bo_handle bo, uint64_t offset, uint64_t size, uint64_t addr, uint64_t flags, uint32_t ops); /** * create semaphore * * \param sem - \c [out] semaphore handle * * \return 0 on success\n * <0 - Negative POSIX Error code * */ int amdgpu_cs_create_semaphore(amdgpu_semaphore_handle *sem); /** * signal semaphore * * \param context - \c [in] GPU Context * \param ip_type - \c [in] Hardware IP block type = AMDGPU_HW_IP_* * \param ip_instance - \c [in] Index of the IP block of the same type * \param ring - \c [in] Specify ring index of the IP * \param sem - \c [in] semaphore handle * * \return 0 on success\n * <0 - Negative POSIX Error code * */ int amdgpu_cs_signal_semaphore(amdgpu_context_handle ctx, uint32_t ip_type, uint32_t ip_instance, uint32_t ring, amdgpu_semaphore_handle sem); /** * wait semaphore * * \param context - \c [in] GPU Context * \param ip_type - \c [in] Hardware IP block type = AMDGPU_HW_IP_* * \param ip_instance - \c [in] Index of the IP block of the same type * \param ring - \c [in] Specify ring index of the IP * \param sem - \c [in] semaphore handle * * \return 0 on success\n * <0 - Negative POSIX Error code * */ int amdgpu_cs_wait_semaphore(amdgpu_context_handle ctx, uint32_t ip_type, uint32_t ip_instance, uint32_t ring, amdgpu_semaphore_handle sem); /** * destroy semaphore * * \param sem - \c [in] semaphore handle * * \return 0 on success\n * <0 - Negative POSIX Error code * */ int amdgpu_cs_destroy_semaphore(amdgpu_semaphore_handle sem); /** * Get the ASIC marketing name * * \param dev - \c [in] Device handle. See #amdgpu_device_initialize() * * \return the constant string of the marketing name * "NULL" means the ASIC is not found */ const char *amdgpu_get_marketing_name(amdgpu_device_handle dev); /** * Create kernel sync object * * \param dev - \c [in] device handle * \param flags - \c [in] flags that affect creation * \param syncobj - \c [out] sync object handle * * \return 0 on success\n * <0 - Negative POSIX Error code * */ int amdgpu_cs_create_syncobj2(amdgpu_device_handle dev, uint32_t flags, uint32_t *syncobj); /** * Create kernel sync object * * \param dev - \c [in] device handle * \param syncobj - \c [out] sync object handle * * \return 0 on success\n * <0 - Negative POSIX Error code * */ int amdgpu_cs_create_syncobj(amdgpu_device_handle dev, uint32_t *syncobj); /** * Destroy kernel sync object * * \param dev - \c [in] device handle * \param syncobj - \c [in] sync object handle * * \return 0 on success\n * <0 - Negative POSIX Error code * */ int amdgpu_cs_destroy_syncobj(amdgpu_device_handle dev, uint32_t syncobj); /** * Reset kernel sync objects to unsignalled state. * * \param dev - \c [in] device handle * \param syncobjs - \c [in] array of sync object handles * \param syncobj_count - \c [in] number of handles in syncobjs * * \return 0 on success\n * <0 - Negative POSIX Error code * */ int amdgpu_cs_syncobj_reset(amdgpu_device_handle dev, const uint32_t *syncobjs, uint32_t syncobj_count); /** * Signal kernel sync objects. * * \param dev - \c [in] device handle * \param syncobjs - \c [in] array of sync object handles * \param syncobj_count - \c [in] number of handles in syncobjs * * \return 0 on success\n * <0 - Negative POSIX Error code * */ int amdgpu_cs_syncobj_signal(amdgpu_device_handle dev, const uint32_t *syncobjs, uint32_t syncobj_count); /** * Wait for one or all sync objects to signal. * * \param dev - \c [in] self-explanatory * \param handles - \c [in] array of sync object handles * \param num_handles - \c [in] self-explanatory * \param timeout_nsec - \c [in] self-explanatory * \param flags - \c [in] a bitmask of DRM_SYNCOBJ_WAIT_FLAGS_* * \param first_signaled - \c [in] self-explanatory * * \return 0 on success\n * -ETIME - Timeout * <0 - Negative POSIX Error code * */ int amdgpu_cs_syncobj_wait(amdgpu_device_handle dev, uint32_t *handles, unsigned num_handles, int64_t timeout_nsec, unsigned flags, uint32_t *first_signaled); /** * Export kernel sync object to shareable fd. * * \param dev - \c [in] device handle * \param syncobj - \c [in] sync object handle * \param shared_fd - \c [out] shared file descriptor. * * \return 0 on success\n * <0 - Negative POSIX Error code * */ int amdgpu_cs_export_syncobj(amdgpu_device_handle dev, uint32_t syncobj, int *shared_fd); /** * Import kernel sync object from shareable fd. * * \param dev - \c [in] device handle * \param shared_fd - \c [in] shared file descriptor. * \param syncobj - \c [out] sync object handle * * \return 0 on success\n * <0 - Negative POSIX Error code * */ int amdgpu_cs_import_syncobj(amdgpu_device_handle dev, int shared_fd, uint32_t *syncobj); /** * Export kernel sync object to a sync_file. * * \param dev - \c [in] device handle * \param syncobj - \c [in] sync object handle * \param sync_file_fd - \c [out] sync_file file descriptor. * * \return 0 on success\n * <0 - Negative POSIX Error code * */ int amdgpu_cs_syncobj_export_sync_file(amdgpu_device_handle dev, uint32_t syncobj, int *sync_file_fd); /** * Import kernel sync object from a sync_file. * * \param dev - \c [in] device handle * \param syncobj - \c [in] sync object handle * \param sync_file_fd - \c [in] sync_file file descriptor. * * \return 0 on success\n * <0 - Negative POSIX Error code * */ int amdgpu_cs_syncobj_import_sync_file(amdgpu_device_handle dev, uint32_t syncobj, int sync_file_fd); /** * Export an amdgpu fence as a handle (syncobj or fd). * * \param what AMDGPU_FENCE_TO_HANDLE_GET_{SYNCOBJ, FD} * \param out_handle returned handle * * \return 0 on success\n * <0 - Negative POSIX Error code */ int amdgpu_cs_fence_to_handle(amdgpu_device_handle dev, struct amdgpu_cs_fence *fence, uint32_t what, uint32_t *out_handle); /** * Submit raw command submission to kernel * * \param dev - \c [in] device handle * \param context - \c [in] context handle for context id * \param bo_list_handle - \c [in] request bo list handle (0 for none) * \param num_chunks - \c [in] number of CS chunks to submit * \param chunks - \c [in] array of CS chunks * \param seq_no - \c [out] output sequence number for submission. * * \return 0 on success\n * <0 - Negative POSIX Error code * */ struct drm_amdgpu_cs_chunk; struct drm_amdgpu_cs_chunk_dep; struct drm_amdgpu_cs_chunk_data; int amdgpu_cs_submit_raw(amdgpu_device_handle dev, amdgpu_context_handle context, amdgpu_bo_list_handle bo_list_handle, int num_chunks, struct drm_amdgpu_cs_chunk *chunks, uint64_t *seq_no); void amdgpu_cs_chunk_fence_to_dep(struct amdgpu_cs_fence *fence, struct drm_amdgpu_cs_chunk_dep *dep); void amdgpu_cs_chunk_fence_info_to_data(struct amdgpu_cs_fence_info *fence_info, struct drm_amdgpu_cs_chunk_data *data); /** * Reserve VMID * \param context - \c [in] GPU Context * \param flags - \c [in] TBD * * \return 0 on success otherwise POSIX Error code */ int amdgpu_vm_reserve_vmid(amdgpu_device_handle dev, uint32_t flags); /** * Free reserved VMID * \param context - \c [in] GPU Context * \param flags - \c [in] TBD * * \return 0 on success otherwise POSIX Error code */ int amdgpu_vm_unreserve_vmid(amdgpu_device_handle dev, uint32_t flags); #ifdef __cplusplus } #endif #endif /* #ifdef _AMDGPU_H_ */