/* * Copyright © 2014 Advanced Micro Devices, Inc. * All Rights Reserved. * * Permission is hereby granted, free of charge, to any person obtaining a * copy of this software and associated documentation files (the "Software"), * to deal in the Software without restriction, including without limitation * the rights to use, copy, modify, merge, publish, distribute, sublicense, * and/or sell copies of the Software, and to permit persons to whom the * Software is furnished to do so, subject to the following conditions: * * The above copyright notice and this permission notice shall be included in * all copies or substantial portions of the Software. * * THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR * IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY, * FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN NO EVENT SHALL * THE COPYRIGHT HOLDER(S) OR AUTHOR(S) BE LIABLE FOR ANY CLAIM, DAMAGES OR * OTHER LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, * ARISING FROM, OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE USE OR * OTHER DEALINGS IN THE SOFTWARE. * */ #ifndef _AMDGPU_INTERNAL_H_ #define _AMDGPU_INTERNAL_H_ #ifdef HAVE_CONFIG_H #include "config.h" #endif #include #include #include "libdrm_macros.h" #include "xf86atomic.h" #include "amdgpu.h" #include "util_double_list.h" #define AMDGPU_CS_MAX_RINGS 8 /* do not use below macro if b is not power of 2 aligned value */ #define __round_mask(x, y) ((__typeof__(x))((y)-1)) #define ROUND_UP(x, y) ((((x)-1) | __round_mask(x, y))+1) #define ROUND_DOWN(x, y) ((x) & ~__round_mask(x, y)) #define AMDGPU_INVALID_VA_ADDRESS 0xffffffffffffffff #define AMDGPU_NULL_SUBMIT_SEQ 0 struct amdgpu_bo_va_hole { struct list_head list; uint64_t offset; uint64_t size; }; struct amdgpu_bo_va_mgr { /* the start virtual address */ uint64_t va_offset; uint64_t va_max; struct list_head va_holes; pthread_mutex_t bo_va_mutex; uint32_t va_alignment; }; struct amdgpu_va { amdgpu_device_handle dev; uint64_t address; uint64_t size; enum amdgpu_gpu_va_range range; struct amdgpu_bo_va_mgr *vamgr; }; struct amdgpu_device { atomic_t refcount; int fd; int flink_fd; unsigned major_version; unsigned minor_version; /** List of buffer handles. Protected by bo_table_mutex. */ struct util_hash_table *bo_handles; /** List of buffer GEM flink names. Protected by bo_table_mutex. */ struct util_hash_table *bo_flink_names; /** This protects all hash tables. */ pthread_mutex_t bo_table_mutex; struct drm_amdgpu_info_device dev_info; struct amdgpu_gpu_info info; /** The global VA manager for the whole virtual address space */ struct amdgpu_bo_va_mgr *vamgr; /** The VA manager for the 32bit address space */ struct amdgpu_bo_va_mgr vamgr_32; }; struct amdgpu_bo { atomic_t refcount; struct amdgpu_device *dev; uint64_t alloc_size; uint32_t handle; uint32_t flink_name; pthread_mutex_t cpu_access_mutex; void *cpu_ptr; int cpu_map_count; }; struct amdgpu_bo_list { struct amdgpu_device *dev; uint32_t handle; }; struct amdgpu_context { struct amdgpu_device *dev; /** Mutex for accessing fences and to maintain command submissions in good sequence. */ pthread_mutex_t sequence_mutex; /* context id*/ uint32_t id; uint64_t last_seq[AMDGPU_HW_IP_NUM][AMDGPU_HW_IP_INSTANCE_MAX_COUNT][AMDGPU_CS_MAX_RINGS]; struct list_head sem_list[AMDGPU_HW_IP_NUM][AMDGPU_HW_IP_INSTANCE_MAX_COUNT][AMDGPU_CS_MAX_RINGS]; }; /** * Structure describing sw semaphore based on scheduler * */ struct amdgpu_semaphore { atomic_t refcount; struct list_head list; struct amdgpu_cs_fence signal_fence; }; /** * Functions. */ drm_private void amdgpu_bo_free_internal(amdgpu_bo_handle bo); drm_private void amdgpu_vamgr_init(struct amdgpu_bo_va_mgr *mgr, uint64_t start, uint64_t max, uint64_t alignment); drm_private void amdgpu_vamgr_deinit(struct amdgpu_bo_va_mgr *mgr); drm_private uint64_t amdgpu_vamgr_find_va(struct amdgpu_bo_va_mgr *mgr, uint64_t size, uint64_t alignment, uint64_t base_required); drm_private void amdgpu_vamgr_free_va(struct amdgpu_bo_va_mgr *mgr, uint64_t va, uint64_t size); drm_private int amdgpu_query_gpu_info_init(amdgpu_device_handle dev); drm_private uint64_t amdgpu_cs_calculate_timeout(uint64_t timeout); /** * Inline functions. */ /** * Increment src and decrement dst as if we were updating references * for an assignment between 2 pointers of some objects. * * \return true if dst is 0 */ static inline bool update_references(atomic_t *dst, atomic_t *src) { if (dst != src) { /* bump src first */ if (src) { assert(atomic_read(src) > 0); atomic_inc(src); } if (dst) { assert(atomic_read(dst) > 0); return atomic_dec_and_test(dst); } } return false; } /** * Assignment between two amdgpu_bo pointers with reference counting. * * Usage: * struct amdgpu_bo *dst = ... , *src = ...; * * dst = src; * // No reference counting. Only use this when you need to move * // a reference from one pointer to another. * * amdgpu_bo_reference(&dst, src); * // Reference counters are updated. dst is decremented and src is * // incremented. dst is freed if its reference counter is 0. */ static inline void amdgpu_bo_reference(struct amdgpu_bo **dst, struct amdgpu_bo *src) { if (update_references(&(*dst)->refcount, &src->refcount)) amdgpu_bo_free_internal(*dst); *dst = src; } #endif