/* -*- mode: C; c-file-style: "k&r"; tab-width 4; indent-tabs-mode: t; -*- */ /* * Copyright (C) 2012 Rob Clark * * Permission is hereby granted, free of charge, to any person obtaining a * copy of this software and associated documentation files (the "Software"), * to deal in the Software without restriction, including without limitation * the rights to use, copy, modify, merge, publish, distribute, sublicense, * and/or sell copies of the Software, and to permit persons to whom the * Software is furnished to do so, subject to the following conditions: * * The above copyright notice and this permission notice (including the next * paragraph) shall be included in all copies or substantial portions of the * Software. * * THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR * IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY, * FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN NO EVENT SHALL * THE AUTHORS OR COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER * LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING FROM, * OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS IN THE * SOFTWARE. * * Authors: * Rob Clark */ #ifdef HAVE_CONFIG_H # include #endif #include "freedreno_drmif.h" #include "freedreno_priv.h" drm_private pthread_mutex_t table_lock = PTHREAD_MUTEX_INITIALIZER; drm_private void bo_del(struct fd_bo *bo); /* set buffer name, and add to table, call w/ table_lock held: */ static void set_name(struct fd_bo *bo, uint32_t name) { bo->name = name; /* add ourself into the handle table: */ drmHashInsert(bo->dev->name_table, name, bo); } /* lookup a buffer, call w/ table_lock held: */ static struct fd_bo * lookup_bo(void *tbl, uint32_t key) { struct fd_bo *bo = NULL; if (!drmHashLookup(tbl, key, (void **)&bo)) { /* found, incr refcnt and return: */ bo = fd_bo_ref(bo); /* don't break the bucket if this bo was found in one */ list_delinit(&bo->list); } return bo; } /* allocate a new buffer object, call w/ table_lock held */ static struct fd_bo * bo_from_handle(struct fd_device *dev, uint32_t size, uint32_t handle) { struct fd_bo *bo; bo = dev->funcs->bo_from_handle(dev, size, handle); if (!bo) { struct drm_gem_close req = { .handle = handle, }; drmIoctl(dev->fd, DRM_IOCTL_GEM_CLOSE, &req); return NULL; } bo->dev = fd_device_ref(dev); bo->size = size; bo->handle = handle; atomic_set(&bo->refcnt, 1); list_inithead(&bo->list); /* add ourself into the handle table: */ drmHashInsert(dev->handle_table, handle, bo); return bo; } struct fd_bo * fd_bo_new(struct fd_device *dev, uint32_t size, uint32_t flags) { struct fd_bo *bo = NULL; uint32_t handle; int ret; bo = fd_bo_cache_alloc(&dev->bo_cache, &size, flags); if (bo) return bo; ret = dev->funcs->bo_new_handle(dev, size, flags, &handle); if (ret) return NULL; pthread_mutex_lock(&table_lock); bo = bo_from_handle(dev, size, handle); bo->bo_reuse = TRUE; pthread_mutex_unlock(&table_lock); return bo; } struct fd_bo * fd_bo_from_handle(struct fd_device *dev, uint32_t handle, uint32_t size) { struct fd_bo *bo = NULL; pthread_mutex_lock(&table_lock); bo = lookup_bo(dev->handle_table, handle); if (bo) goto out_unlock; bo = bo_from_handle(dev, size, handle); out_unlock: pthread_mutex_unlock(&table_lock); return bo; } struct fd_bo * fd_bo_from_dmabuf(struct fd_device *dev, int fd) { int ret, size; uint32_t handle; struct fd_bo *bo; pthread_mutex_lock(&table_lock); ret = drmPrimeFDToHandle(dev->fd, fd, &handle); if (ret) { return NULL; } bo = lookup_bo(dev->handle_table, handle); if (bo) goto out_unlock; /* lseek() to get bo size */ size = lseek(fd, 0, SEEK_END); lseek(fd, 0, SEEK_CUR); bo = bo_from_handle(dev, size, handle); out_unlock: pthread_mutex_unlock(&table_lock); return bo; } struct fd_bo * fd_bo_from_name(struct fd_device *dev, uint32_t name) { struct drm_gem_open req = { .name = name, }; struct fd_bo *bo; pthread_mutex_lock(&table_lock); /* check name table first, to see if bo is already open: */ bo = lookup_bo(dev->name_table, name); if (bo) goto out_unlock; if (drmIoctl(dev->fd, DRM_IOCTL_GEM_OPEN, &req)) { ERROR_MSG("gem-open failed: %s", strerror(errno)); goto out_unlock; } bo = lookup_bo(dev->handle_table, req.handle); if (bo) goto out_unlock; bo = bo_from_handle(dev, req.size, req.handle); if (bo) set_name(bo, name); out_unlock: pthread_mutex_unlock(&table_lock); return bo; } struct fd_bo * fd_bo_ref(struct fd_bo *bo) { atomic_inc(&bo->refcnt); return bo; } void fd_bo_del(struct fd_bo *bo) { struct fd_device *dev = bo->dev; if (!atomic_dec_and_test(&bo->refcnt)) return; pthread_mutex_lock(&table_lock); if (bo->bo_reuse && (fd_bo_cache_free(&dev->bo_cache, bo) == 0)) goto out; bo_del(bo); fd_device_del_locked(dev); out: pthread_mutex_unlock(&table_lock); } /* Called under table_lock */ drm_private void bo_del(struct fd_bo *bo) { if (bo->map) drm_munmap(bo->map, bo->size); /* TODO probably bo's in bucket list get removed from * handle table?? */ if (bo->handle) { struct drm_gem_close req = { .handle = bo->handle, }; drmHashDelete(bo->dev->handle_table, bo->handle); if (bo->name) drmHashDelete(bo->dev->name_table, bo->name); drmIoctl(bo->dev->fd, DRM_IOCTL_GEM_CLOSE, &req); } bo->funcs->destroy(bo); } int fd_bo_get_name(struct fd_bo *bo, uint32_t *name) { if (!bo->name) { struct drm_gem_flink req = { .handle = bo->handle, }; int ret; ret = drmIoctl(bo->dev->fd, DRM_IOCTL_GEM_FLINK, &req); if (ret) { return ret; } pthread_mutex_lock(&table_lock); set_name(bo, req.name); pthread_mutex_unlock(&table_lock); bo->bo_reuse = FALSE; } *name = bo->name; return 0; } uint32_t fd_bo_handle(struct fd_bo *bo) { return bo->handle; } int fd_bo_dmabuf(struct fd_bo *bo) { int ret, prime_fd; ret = drmPrimeHandleToFD(bo->dev->fd, bo->handle, DRM_CLOEXEC, &prime_fd); if (ret) { ERROR_MSG("failed to get dmabuf fd: %d", ret); return ret; } bo->bo_reuse = FALSE; return prime_fd; } uint32_t fd_bo_size(struct fd_bo *bo) { return bo->size; } void * fd_bo_map(struct fd_bo *bo) { if (!bo->map) { uint64_t offset; int ret; ret = bo->funcs->offset(bo, &offset); if (ret) { return NULL; } bo->map = drm_mmap(0, bo->size, PROT_READ | PROT_WRITE, MAP_SHARED, bo->dev->fd, offset); if (bo->map == MAP_FAILED) { ERROR_MSG("mmap failed: %s", strerror(errno)); bo->map = NULL; } } return bo->map; } /* a bit odd to take the pipe as an arg, but it's a, umm, quirk of kgsl.. */ int fd_bo_cpu_prep(struct fd_bo *bo, struct fd_pipe *pipe, uint32_t op) { return bo->funcs->cpu_prep(bo, pipe, op); } void fd_bo_cpu_fini(struct fd_bo *bo) { bo->funcs->cpu_fini(bo); } #ifndef HAVE_FREEDRENO_KGSL struct fd_bo * fd_bo_from_fbdev(struct fd_pipe *pipe, int fbfd, uint32_t size) { return NULL; } #endif