/* -*- mode: C; c-file-style: "k&r"; tab-width 4; indent-tabs-mode: t; -*- */ /* * Copyright (C) 2012 Rob Clark * * Permission is hereby granted, free of charge, to any person obtaining a * copy of this software and associated documentation files (the "Software"), * to deal in the Software without restriction, including without limitation * the rights to use, copy, modify, merge, publish, distribute, sublicense, * and/or sell copies of the Software, and to permit persons to whom the * Software is furnished to do so, subject to the following conditions: * * The above copyright notice and this permission notice (including the next * paragraph) shall be included in all copies or substantial portions of the * Software. * * THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR * IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY, * FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN NO EVENT SHALL * THE AUTHORS OR COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER * LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING FROM, * OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS IN THE * SOFTWARE. * * Authors: * Rob Clark */ #ifndef FREEDRENO_RINGBUFFER_H_ #define FREEDRENO_RINGBUFFER_H_ #include /* the ringbuffer object is not opaque so that OUT_RING() type stuff * can be inlined. Note that users should not make assumptions about * the size of this struct.. more stuff will be added when we eventually * have a kernel driver that can deal w/ reloc's.. */ struct fd_ringbuffer_funcs; struct fd_ringmarker; struct fd_ringbuffer { int size; uint32_t *cur, *end, *start, *last_start; struct fd_pipe *pipe; const struct fd_ringbuffer_funcs *funcs; uint32_t last_timestamp; struct fd_ringbuffer *parent; }; struct fd_ringbuffer * fd_ringbuffer_new(struct fd_pipe *pipe, uint32_t size); void fd_ringbuffer_del(struct fd_ringbuffer *ring); void fd_ringbuffer_set_parent(struct fd_ringbuffer *ring, struct fd_ringbuffer *parent); void fd_ringbuffer_reset(struct fd_ringbuffer *ring); int fd_ringbuffer_flush(struct fd_ringbuffer *ring); /* in_fence_fd: -1 for no in-fence, else fence fd * out_fence_fd: NULL for no output-fence requested, else ptr to return out-fence */ int fd_ringbuffer_flush2(struct fd_ringbuffer *ring, int in_fence_fd, int *out_fence_fd); void fd_ringbuffer_grow(struct fd_ringbuffer *ring, uint32_t ndwords); uint32_t fd_ringbuffer_timestamp(struct fd_ringbuffer *ring); static inline void fd_ringbuffer_emit(struct fd_ringbuffer *ring, uint32_t data) { (*ring->cur++) = data; } struct fd_reloc { struct fd_bo *bo; #define FD_RELOC_READ 0x0001 #define FD_RELOC_WRITE 0x0002 uint32_t flags; uint32_t offset; uint32_t or; int32_t shift; uint32_t orhi; /* used for a5xx+ */ }; /* NOTE: relocs are 2 dwords on a5xx+ */ void fd_ringbuffer_reloc2(struct fd_ringbuffer *ring, const struct fd_reloc *reloc); will_be_deprecated void fd_ringbuffer_reloc(struct fd_ringbuffer *ring, const struct fd_reloc *reloc); will_be_deprecated void fd_ringbuffer_emit_reloc_ring(struct fd_ringbuffer *ring, struct fd_ringmarker *target, struct fd_ringmarker *end); uint32_t fd_ringbuffer_cmd_count(struct fd_ringbuffer *ring); uint32_t fd_ringbuffer_emit_reloc_ring_full(struct fd_ringbuffer *ring, struct fd_ringbuffer *target, uint32_t cmd_idx); will_be_deprecated struct fd_ringmarker * fd_ringmarker_new(struct fd_ringbuffer *ring); will_be_deprecated void fd_ringmarker_del(struct fd_ringmarker *marker); will_be_deprecated void fd_ringmarker_mark(struct fd_ringmarker *marker); will_be_deprecated uint32_t fd_ringmarker_dwords(struct fd_ringmarker *start, struct fd_ringmarker *end); will_be_deprecated int fd_ringmarker_flush(struct fd_ringmarker *marker); #endif /* FREEDRENO_RINGBUFFER_H_ */