/* -*- mode: C; c-file-style: "k&r"; tab-width 4; indent-tabs-mode: t; -*- */ /* * Copyright (C) 2013 Rob Clark * * Permission is hereby granted, free of charge, to any person obtaining a * copy of this software and associated documentation files (the "Software"), * to deal in the Software without restriction, including without limitation * the rights to use, copy, modify, merge, publish, distribute, sublicense, * and/or sell copies of the Software, and to permit persons to whom the * Software is furnished to do so, subject to the following conditions: * * The above copyright notice and this permission notice (including the next * paragraph) shall be included in all copies or substantial portions of the * Software. * * THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR * IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY, * FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN NO EVENT SHALL * THE AUTHORS OR COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER * LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING FROM, * OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS IN THE * SOFTWARE. * * Authors: * Rob Clark */ #ifdef HAVE_CONFIG_H # include #endif #include "kgsl_priv.h" #include static int set_memtype(struct fd_device *dev, uint32_t handle, uint32_t flags) { struct drm_kgsl_gem_memtype req = { .handle = handle, .type = flags & DRM_FREEDRENO_GEM_TYPE_MEM_MASK, }; return drmCommandWrite(dev->fd, DRM_KGSL_GEM_SETMEMTYPE, &req, sizeof(req)); } static int bo_alloc(struct kgsl_bo *kgsl_bo) { struct fd_bo *bo = &kgsl_bo->base; if (!kgsl_bo->offset) { struct drm_kgsl_gem_alloc req = { .handle = bo->handle, }; int ret; /* if the buffer is already backed by pages then this * doesn't actually do anything (other than giving us * the offset) */ ret = drmCommandWriteRead(bo->dev->fd, DRM_KGSL_GEM_ALLOC, &req, sizeof(req)); if (ret) { ERROR_MSG("alloc failed: %s", strerror(errno)); return ret; } kgsl_bo->offset = req.offset; } return 0; } static int kgsl_bo_offset(struct fd_bo *bo, uint64_t *offset) { struct kgsl_bo *kgsl_bo = to_kgsl_bo(bo); int ret = bo_alloc(kgsl_bo); if (ret) return ret; *offset = kgsl_bo->offset; return 0; } static int kgsl_bo_cpu_prep(struct fd_bo *bo, struct fd_pipe *pipe, uint32_t op) { uint32_t timestamp = kgsl_bo_get_timestamp(to_kgsl_bo(bo)); if (op & DRM_FREEDRENO_PREP_NOSYNC) { uint32_t current; int ret; /* special case for is_idle().. we can't really handle that * properly in kgsl (perhaps we need a way to just disable * the bo-cache for kgsl?) */ if (!pipe) return -EBUSY; ret = kgsl_pipe_timestamp(to_kgsl_pipe(pipe), ¤t); if (ret) return ret; if (timestamp > current) return -EBUSY; return 0; } if (timestamp) fd_pipe_wait(pipe, timestamp); return 0; } static void kgsl_bo_cpu_fini(struct fd_bo *bo) { } static void kgsl_bo_destroy(struct fd_bo *bo) { struct kgsl_bo *kgsl_bo = to_kgsl_bo(bo); free(kgsl_bo); } static const struct fd_bo_funcs funcs = { .offset = kgsl_bo_offset, .cpu_prep = kgsl_bo_cpu_prep, .cpu_fini = kgsl_bo_cpu_fini, .destroy = kgsl_bo_destroy, }; /* allocate a buffer handle: */ drm_private int kgsl_bo_new_handle(struct fd_device *dev, uint32_t size, uint32_t flags, uint32_t *handle) { struct drm_kgsl_gem_create req = { .size = size, }; int ret; ret = drmCommandWriteRead(dev->fd, DRM_KGSL_GEM_CREATE, &req, sizeof(req)); if (ret) return ret; // TODO make flags match msm driver, since kgsl is legacy.. // translate flags in kgsl.. set_memtype(dev, req.handle, flags); *handle = req.handle; return 0; } /* allocate a new buffer object */ drm_private struct fd_bo * kgsl_bo_from_handle(struct fd_device *dev, uint32_t size, uint32_t handle) { struct kgsl_bo *kgsl_bo; struct fd_bo *bo; unsigned i; kgsl_bo = calloc(1, sizeof(*kgsl_bo)); if (!kgsl_bo) return NULL; bo = &kgsl_bo->base; bo->funcs = &funcs; for (i = 0; i < ARRAY_SIZE(kgsl_bo->list); i++) list_inithead(&kgsl_bo->list[i]); return bo; } struct fd_bo * fd_bo_from_fbdev(struct fd_pipe *pipe, int fbfd, uint32_t size) { struct fd_bo *bo; if (!is_kgsl_pipe(pipe)) return NULL; bo = fd_bo_new(pipe->dev, 1, 0); /* this is fugly, but works around a bug in the kernel.. * priv->memdesc.size never gets set, so getbufinfo ioctl * thinks the buffer hasn't be allocate and fails */ if (bo) { void *fbmem = drm_mmap(NULL, size, PROT_READ | PROT_WRITE, MAP_SHARED, fbfd, 0); struct kgsl_map_user_mem req = { .memtype = KGSL_USER_MEM_TYPE_ADDR, .len = size, .offset = 0, .hostptr = (unsigned long)fbmem, }; struct kgsl_bo *kgsl_bo = to_kgsl_bo(bo); int ret; ret = ioctl(to_kgsl_pipe(pipe)->fd, IOCTL_KGSL_MAP_USER_MEM, &req); if (ret) { ERROR_MSG("mapping user mem failed: %s", strerror(errno)); goto fail; } kgsl_bo->gpuaddr = req.gpuaddr; bo->map = fbmem; } return bo; fail: if (bo) fd_bo_del(bo); return NULL; } drm_private uint32_t kgsl_bo_gpuaddr(struct kgsl_bo *kgsl_bo, uint32_t offset) { struct fd_bo *bo = &kgsl_bo->base; if (!kgsl_bo->gpuaddr) { struct drm_kgsl_gem_bufinfo req = { .handle = bo->handle, }; int ret; ret = bo_alloc(kgsl_bo); if (ret) { return ret; } ret = drmCommandWriteRead(bo->dev->fd, DRM_KGSL_GEM_GET_BUFINFO, &req, sizeof(req)); if (ret) { ERROR_MSG("get bufinfo failed: %s", strerror(errno)); return 0; } kgsl_bo->gpuaddr = req.gpuaddr[0]; } return kgsl_bo->gpuaddr + offset; } /* * Super-cheezy way to synchronization between mesa and ddx.. the * SET_ACTIVE ioctl gives us a way to stash a 32b # w/ a GEM bo, and * GET_BUFINFO gives us a way to retrieve it. We use this to stash * the timestamp of the last ISSUEIBCMDS on the buffer. * * To avoid an obscene amount of syscalls, we: * 1) Only set the timestamp for buffers w/ an flink name, ie. * only buffers shared across processes. This is enough to * catch the DRI2 buffers. * 2) Only set the timestamp for buffers submitted to the 3d ring * and only check the timestamps on buffers submitted to the * 2d ring. This should be enough to handle synchronizing of * presentation blit. We could do synchronization in the other * direction too, but that would be problematic if we are using * the 3d ring from DDX, since client side wouldn't know this. * * The waiting on timestamp happens before flush, and setting of * timestamp happens after flush. It is transparent to the user * of libdrm_freedreno as all the tracking of buffers happens via * _emit_reloc().. */ drm_private void kgsl_bo_set_timestamp(struct kgsl_bo *kgsl_bo, uint32_t timestamp) { struct fd_bo *bo = &kgsl_bo->base; if (bo->name) { struct drm_kgsl_gem_active req = { .handle = bo->handle, .active = timestamp, }; int ret; ret = drmCommandWrite(bo->dev->fd, DRM_KGSL_GEM_SET_ACTIVE, &req, sizeof(req)); if (ret) { ERROR_MSG("set active failed: %s", strerror(errno)); } } } drm_private uint32_t kgsl_bo_get_timestamp(struct kgsl_bo *kgsl_bo) { struct fd_bo *bo = &kgsl_bo->base; uint32_t timestamp = 0; if (bo->name) { struct drm_kgsl_gem_bufinfo req = { .handle = bo->handle, }; int ret; ret = drmCommandWriteRead(bo->dev->fd, DRM_KGSL_GEM_GET_BUFINFO, &req, sizeof(req)); if (ret) { ERROR_MSG("get bufinfo failed: %s", strerror(errno)); return 0; } timestamp = req.active; } return timestamp; }