/* -*- mode: C; c-file-style: "k&r"; tab-width 4; indent-tabs-mode: t; -*- */ /* * Copyright (C) 2013 Rob Clark * * Permission is hereby granted, free of charge, to any person obtaining a * copy of this software and associated documentation files (the "Software"), * to deal in the Software without restriction, including without limitation * the rights to use, copy, modify, merge, publish, distribute, sublicense, * and/or sell copies of the Software, and to permit persons to whom the * Software is furnished to do so, subject to the following conditions: * * The above copyright notice and this permission notice (including the next * paragraph) shall be included in all copies or substantial portions of the * Software. * * THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR * IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY, * FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN NO EVENT SHALL * THE AUTHORS OR COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER * LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING FROM, * OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS IN THE * SOFTWARE. * * Authors: * Rob Clark */ #ifdef HAVE_CONFIG_H # include #endif #include "msm_priv.h" static int query_param(struct fd_pipe *pipe, uint32_t param, uint64_t *value) { struct msm_pipe *msm_pipe = to_msm_pipe(pipe); struct drm_msm_param req = { .pipe = msm_pipe->pipe, .param = param, }; int ret; ret = drmCommandWriteRead(pipe->dev->fd, DRM_MSM_GET_PARAM, &req, sizeof(req)); if (ret) return ret; *value = req.value; return 0; } static int msm_pipe_get_param(struct fd_pipe *pipe, enum fd_param_id param, uint64_t *value) { struct msm_pipe *msm_pipe = to_msm_pipe(pipe); switch(param) { case FD_DEVICE_ID: // XXX probably get rid of this.. case FD_GPU_ID: *value = msm_pipe->gpu_id; return 0; case FD_GMEM_SIZE: *value = msm_pipe->gmem; return 0; case FD_CHIP_ID: *value = msm_pipe->chip_id; return 0; case FD_MAX_FREQ: return query_param(pipe, MSM_PARAM_MAX_FREQ, value); case FD_TIMESTAMP: return query_param(pipe, MSM_PARAM_TIMESTAMP, value); default: ERROR_MSG("invalid param id: %d", param); return -1; } } static int msm_pipe_wait(struct fd_pipe *pipe, uint32_t timestamp, uint64_t timeout) { struct fd_device *dev = pipe->dev; struct drm_msm_wait_fence req = { .fence = timestamp, }; int ret; get_abs_timeout(&req.timeout, timeout); ret = drmCommandWrite(dev->fd, DRM_MSM_WAIT_FENCE, &req, sizeof(req)); if (ret) { ERROR_MSG("wait-fence failed! %d (%s)", ret, strerror(errno)); return ret; } return 0; } static void msm_pipe_destroy(struct fd_pipe *pipe) { struct msm_pipe *msm_pipe = to_msm_pipe(pipe); free(msm_pipe); } static const struct fd_pipe_funcs funcs = { .ringbuffer_new = msm_ringbuffer_new, .get_param = msm_pipe_get_param, .wait = msm_pipe_wait, .destroy = msm_pipe_destroy, }; static uint64_t get_param(struct fd_pipe *pipe, uint32_t param) { uint64_t value; int ret = query_param(pipe, param, &value); if (ret) { ERROR_MSG("get-param failed! %d (%s)", ret, strerror(errno)); return 0; } return value; } drm_private struct fd_pipe * msm_pipe_new(struct fd_device *dev, enum fd_pipe_id id) { static const uint32_t pipe_id[] = { [FD_PIPE_3D] = MSM_PIPE_3D0, [FD_PIPE_2D] = MSM_PIPE_2D0, }; struct msm_pipe *msm_pipe = NULL; struct fd_pipe *pipe = NULL; msm_pipe = calloc(1, sizeof(*msm_pipe)); if (!msm_pipe) { ERROR_MSG("allocation failed"); goto fail; } pipe = &msm_pipe->base; pipe->funcs = &funcs; /* initialize before get_param(): */ pipe->dev = dev; msm_pipe->pipe = pipe_id[id]; /* these params should be supported since the first version of drm/msm: */ msm_pipe->gpu_id = get_param(pipe, MSM_PARAM_GPU_ID); msm_pipe->gmem = get_param(pipe, MSM_PARAM_GMEM_SIZE); msm_pipe->chip_id = get_param(pipe, MSM_PARAM_CHIP_ID); if (! msm_pipe->gpu_id) goto fail; INFO_MSG("Pipe Info:"); INFO_MSG(" GPU-id: %d", msm_pipe->gpu_id); INFO_MSG(" Chip-id: 0x%08x", msm_pipe->chip_id); INFO_MSG(" GMEM size: 0x%08x", msm_pipe->gmem); return pipe; fail: if (pipe) fd_pipe_del(pipe); return NULL; }