aboutsummaryrefslogtreecommitdiffstats
blob: 11a86eff056a03c82d6865e6f9205f5c5b22e58f (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
424
425
426
427
428
429
430
431
432
433
434
435
436
437
438
439
440
441
442
443
444
445
446
447
448
449
450
451
452
453
454
455
456
457
458
459
460
461
462
463
464
465
466
467
468
469
470
471
472
473
474
475
476
477
478
479
480
481
482
483
484
485
486
487
488
489
490
491
492
493
494
495
496
497
498
499
500
501
502
503
504
505
506
507
508
509
510
511
512
513
514
515
516
517
518
519
520
521
522
523
524
525
526
527
528
529
530
531
532
533
534
535
536
537
538
539
540
541
542
543
544
545
546
547
548
549
550
551
552
553
554
555
556
557
558
559
560
561
562
563
564
565
566
567
568
569
570
571
572
573
574
575
576
577
578
579
580
581
582
583
584
585
586
587
588
589
590
591
592
593
594
595
596
597
598
599
600
601
602
603
604
605
606
607
608
609
610
611
612
613
614
615
616
617
618
619
620
621
622
623
624
625
626
627
628
629
630
631
632
633
634
635
636
637
638
639
640
641
642
643
644
645
646
647
648
649
650
651
652
653
654
655
656
657
658
659
660
661
662
663
664
665
666
667
668
669
670
671
672
673
674
675
676
677
678
679
680
681
682
683
684
685
686
687
688
689
690
691
692
693
694
695
696
697
698
699
700
701
702
703
704
705
706
707
708
709
710
711
712
713
714
715
716
717
718
719
720
721
722
723
724
725
726
727
728
729
730
731
732
733
734
735
736
737
738
739
740
741
742
743
744
745
746
747
748
749
750
751
752
753
754
755
756
757
758
759
760
761
762
763
764
765
766
767
768
769
770
771
772
773
774
775
776
777
778
779
780
781
782
783
784
785
786
787
788
789
790
791
792
793
794
795
796
797
798
799
800
801
802
803
804
805
806
807
808
809
810
811
812
813
814
815
816
817
818
819
820
821
822
823
824
825
826
827
828
829
830
831
832
833
834
835
836
837
838
839
840
841
842
843
844
845
846
847
848
849
850
851
852
853
854
855
856
857
858
859
860
861
862
863
864
865
866
867
868
869
870
871
872
873
874
875
876
877
878
879
880
881
882
883
884
885
886
887
888
889
890
891
892
893
894
895
896
897
898
899
900
901
902
903
904
905
906
907
908
909
910
911
912
913
914
915
916
917
918
919
920
921
922
923
924
925
926
927
928
929
930
931
932
933
934
935
936
937
938
939
940
941
942
943
944
945
946
947
948
949
950
951
952
953
954
955
956
957
958
959
960
961
962
963
964
965
966
967
968
969
970
971
972
973
974
975
976
977
978
979
980
981
982
983
984
985
986
987
988
989
990
991
992
993
994
995
996
997
998
999
1000
1001
1002
1003
1004
1005
1006
1007
1008
1009
1010
1011
1012
1013
1014
1015
1016
1017
1018
1019
1020
1021
1022
1023
1024
1025
1026
1027
1028
1029
1030
1031
1032
1033
1034
1035
1036
1037
1038
1039
1040
1041
1042
1043
1044
1045
1046
1047
1048
1049
1050
1051
1052
1053
1054
1055
1056
1057
1058
1059
1060
1061
1062
1063
1064
1065
1066
1067
1068
1069
1070
1071
1072
1073
1074
1075
1076
1077
1078
1079
1080
1081
1082
1083
1084
1085
1086
1087
1088
1089
1090
1091
1092
1093
1094
1095
1096
1097
1098
1099
1100
1101
1102
1103
1104
1105
1106
1107
1108
1109
1110
1111
1112
1113
1114
1115
1116
1117
1118
1119
1120
1121
1122
1123
1124
1125
1126
1127
1128
1129
1130
1131
1132
1133
1134
1135
1136
1137
1138
1139
1140
1141
1142
1143
1144
1145
1146
1147
1148
1149
1150
1151
1152
1153
1154
1155
1156
1157
1158
1159
1160
1161
1162
1163
1164
1165
1166
1167
1168
1169
1170
1171
1172
1173
1174
1175
1176
1177
1178
1179
1180
1181
1182
1183
1184
1185
1186
1187
1188
1189
1190
1191
1192
1193
1194
1195
1196
1197
1198
1199
1200
1201
1202
1203
1204
1205
1206
1207
1208
1209
1210
1211
1212
1213
1214
1215
1216
1217
1218
1219
1220
1221
1222
1223
1224
1225
1226
1227
1228
1229
1230
1231
1232
1233
1234
1235
1236
1237
1238
1239
1240
1241
1242
1243
1244
1245
1246
1247
1248
1249
1250
1251
1252
1253
1254
1255
1256
1257
1258
1259
1260
1261
1262
1263
1264
1265
1266
1267
1268
1269
1270
1271
1272
1273
1274
1275
1276
/*
 * Copyright 2014 Advanced Micro Devices, Inc.
 *
 * Permission is hereby granted, free of charge, to any person obtaining a
 * copy of this software and associated documentation files (the "Software"),
 * to deal in the Software without restriction, including without limitation
 * the rights to use, copy, modify, merge, publish, distribute, sublicense,
 * and/or sell copies of the Software, and to permit persons to whom the
 * Software is furnished to do so, subject to the following conditions:
 *
 * The above copyright notice and this permission notice shall be included in
 * all copies or substantial portions of the Software.
 *
 * THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR
 * IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY,
 * FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT.  IN NO EVENT SHALL
 * THE COPYRIGHT HOLDER(S) OR AUTHOR(S) BE LIABLE FOR ANY CLAIM, DAMAGES OR
 * OTHER LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR OTHERWISE,
 * ARISING FROM, OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE USE OR
 * OTHER DEALINGS IN THE SOFTWARE.
 *
*/

/**
 * \file amdgpu.h
 *
 * Declare public libdrm_amdgpu API
 *
 * This file define API exposed by libdrm_amdgpu library.
 * User wanted to use libdrm_amdgpu functionality must include
 * this file.
 *
 */
#ifndef _AMDGPU_H_
#define _AMDGPU_H_

#include <stdint.h>
#include <stdbool.h>

struct drm_amdgpu_info_hw_ip;

/*--------------------------------------------------------------------------*/
/* --------------------------- Defines ------------------------------------ */
/*--------------------------------------------------------------------------*/

/**
 * Define max. number of Command Buffers (IB) which could be sent to the single
 * hardware IP to accommodate CE/DE requirements
 *
 * \sa amdgpu_cs_ib_info
*/
#define AMDGPU_CS_MAX_IBS_PER_SUBMIT		4

/**
 *
 */
#define AMDGPU_TIMEOUT_INFINITE			0xffffffffffffffffull

/**
 * The special flag for GFX submission to identify that this is CE IB
 * \sa amdgpu_cs_ib_info
*/
#define AMDGPU_CS_GFX_IB_CE			0x1

/**
 * The special flag to mark that this IB will re-used
 * by client and should not be automatically return back
 * to free pool by libdrm_amdgpu when submission is completed.
 *
 * \sa amdgpu_cs_ib_info
*/
#define AMDGPU_CS_REUSE_IB			0x2

/**
 * The special resource flag for IB submission.
 * When VRAM is full, some resources may be moved to GTT to make place
 * for other resources which want to be in VRAM. This flag affects the order
 * in which resources are moved back to VRAM until there is no space there.
 * The resources with the highest priority will be moved first.
 * The value can be between 0 and 15, inclusive.
 */
#define AMDGPU_IB_RESOURCE_PRIORITY(x)		((x) & 0xf)


/*--------------------------------------------------------------------------*/
/* ----------------------------- Enums ------------------------------------ */
/*--------------------------------------------------------------------------*/

/**
 * Enum describing possible handle types
 *
 * \sa amdgpu_bo_import, amdgpu_bo_export
 *
*/
enum amdgpu_bo_handle_type {
	/** GEM flink name (needs DRM authentication, used by DRI2) */
	amdgpu_bo_handle_type_gem_flink_name = 0,

	/** KMS handle which is used by all driver ioctls */
	amdgpu_bo_handle_type_kms = 1,

	/** DMA-buf fd handle */
	amdgpu_bo_handle_type_dma_buf_fd = 2
};

/**
 * Enum describing possible context reset states
 *
 * \sa amdgpu_cs_query_reset_state()
 *
*/
enum amdgpu_cs_ctx_reset_state {
	/** No reset was detected */
	amdgpu_cs_reset_no_error = 0,

	/** Reset/TDR was detected and context caused */
	amdgpu_cs_reset_guilty   = 1,

	/** Reset/TDR was detected caused by other context */
	amdgpu_cs_reset_innocent = 2,

	/** Reset TDR was detected by cause of it unknown */
	amdgpu_cs_reset_unknown  = 3
};

/**
 * For performance reasons and to simplify logic libdrm_amdgpu will handle
 * IBs only some pre-defined sizes.
 *
 * \sa amdgpu_cs_alloc_ib()
 */
enum amdgpu_cs_ib_size {
	amdgpu_cs_ib_size_4K	= 1,
	amdgpu_cs_ib_size_16K	= 2,
	amdgpu_cs_ib_size_32K	= 3,
	amdgpu_cs_ib_size_64K	= 4,
	amdgpu_cs_ib_size_128K	= 5
};

/** The number of different IB sizes */
#define AMDGPU_CS_IB_SIZE_NUM 6


/*--------------------------------------------------------------------------*/
/* -------------------------- Datatypes ----------------------------------- */
/*--------------------------------------------------------------------------*/

/**
 * Define opaque pointer to context associated with fd.
 * This context will be returned as the result of
 * "initialize" function and should be pass as the first
 * parameter to any API call
 */
typedef struct amdgpu_device *amdgpu_device_handle;

/**
 * Define GPU Context type as pointer to opaque structure
 * Example of GPU Context is the "rendering" context associated
 * with OpenGL context (glCreateContext)
 */
typedef struct amdgpu_context *amdgpu_context_handle;

/**
 * Define handle for amdgpu resources: buffer, GDS, etc.
 */
typedef struct amdgpu_bo *amdgpu_bo_handle;

/**
 * Define handle to be used when dealing with command
 * buffers (a.k.a. ibs)
 *
 */
typedef struct amdgpu_ib *amdgpu_ib_handle;


/*--------------------------------------------------------------------------*/
/* -------------------------- Structures ---------------------------------- */
/*--------------------------------------------------------------------------*/

/**
 * Structure describing memory allocation request
 *
 * \sa amdgpu_bo_alloc()
 *
*/
struct amdgpu_bo_alloc_request {
	/** Allocation request. It must be aligned correctly. */
	uint64_t alloc_size;

	/**
	 * It may be required to have some specific alignment requirements
	 * for physical back-up storage (e.g. for displayable surface).
	 * If 0 there is no special alignment requirement
	 */
	uint64_t phys_alignment;

	/**
	 * UMD should specify where to allocate memory and how it
	 * will be accessed by the CPU.
	 */
	uint32_t preferred_heap;

	/** Additional flags passed on allocation */
	uint64_t flags;
};

/**
 * Structure describing memory allocation request
 *
 * \sa amdgpu_bo_alloc()
*/
struct amdgpu_bo_alloc_result {
	/** Assigned virtual MC Base Address */
	uint64_t virtual_mc_base_address;

	/** Handle of allocated memory to be used by the given process only. */
	amdgpu_bo_handle buf_handle;
};

/**
 * Special UMD specific information associated with buffer.
 *
 * It may be need to pass some buffer charactersitic as part
 * of buffer sharing. Such information are defined UMD and
 * opaque for libdrm_amdgpu as well for kernel driver.
 *
 * \sa amdgpu_bo_set_metadata(), amdgpu_bo_query_info,
 *     amdgpu_bo_import(), amdgpu_bo_export
 *
*/
struct amdgpu_bo_metadata {
	/** Special flag associated with surface */
	uint64_t flags;

	/**
	 * ASIC-specific tiling information (also used by DCE).
	 * The encoding is defined by the AMDGPU_TILING_* definitions.
	 */
	uint64_t tiling_info;

	/** Size of metadata associated with the buffer, in bytes. */
	uint32_t size_metadata;

	/** UMD specific metadata. Opaque for kernel */
	uint32_t umd_metadata[64];
};

/**
 * Structure describing allocated buffer. Client may need
 * to query such information as part of 'sharing' buffers mechanism
 *
 * \sa amdgpu_bo_set_metadata(), amdgpu_bo_query_info(),
 *     amdgpu_bo_import(), amdgpu_bo_export()
*/
struct amdgpu_bo_info {
	/** Allocated memory size */
	uint64_t alloc_size;

	/**
	 * It may be required to have some specific alignment requirements
	 * for physical back-up storage.
	 */
	uint64_t phys_alignment;

	/**
	 * Assigned virtual MC Base Address.
	 * \note  This information will be returned only if this buffer was
	 * allocated in the same process otherwise 0 will be returned.
	*/
	uint64_t virtual_mc_base_address;

	/** Heap where to allocate memory. */
	uint32_t preferred_heap;

	/** Additional allocation flags. */
	uint64_t alloc_flags;

	/** Metadata associated with buffer if any. */
	struct amdgpu_bo_metadata metadata;
};

/**
 * Structure with information about "imported" buffer
 *
 * \sa amdgpu_bo_import()
 *
 */
struct amdgpu_bo_import_result {
	/** Handle of memory/buffer to use */
	amdgpu_bo_handle  buf_handle;

	 /** Buffer size */
	uint64_t alloc_size;

	 /** Assigned virtual MC Base Address */
	uint64_t virtual_mc_base_address;
};


/**
 *
 * Structure to describe GDS partitioning information.
 * \note OA and GWS resources are asscoiated with GDS partition
 *
 * \sa amdgpu_gpu_resource_query_gds_info
 *
*/
struct amdgpu_gds_resource_info {
	uint32_t   gds_gfx_partition_size;
	uint32_t   compute_partition_size;
	uint32_t   gds_total_size;
	uint32_t   gws_per_gfx_partition;
	uint32_t   gws_per_compute_partition;
	uint32_t   oa_per_gfx_partition;
	uint32_t   oa_per_compute_partition;
};



/**
 *  Structure describing result of request to allocate GDS
 *
 *  \sa amdgpu_gpu_resource_gds_alloc
 *
*/
struct amdgpu_gds_alloc_info {
	/** Handle assigned to gds allocation */
	amdgpu_bo_handle resource_handle;

	/** How much was really allocated */
	uint32_t   gds_memory_size;

	/** Number of GWS resources allocated */
	uint32_t   gws;

	/** Number of OA resources allocated */
	uint32_t   oa;
};

/**
 * Structure to described allocated command buffer (a.k.a. IB)
 *
 * \sa amdgpu_cs_alloc_ib()
 *
*/
struct amdgpu_cs_ib_alloc_result {
	/** IB allocation handle */
	amdgpu_ib_handle handle;

	/** Assigned GPU VM MC Address of command buffer */
	uint64_t	mc_address;

	/** Address to be used for CPU access */
	void		*cpu;
};

/**
 * Structure describing IB
 *
 * \sa amdgpu_cs_request, amdgpu_cs_submit()
 *
*/
struct amdgpu_cs_ib_info {
	/** Special flags */
	uint64_t      flags;

	/** Handle of command buffer */
	amdgpu_ib_handle ib_handle;

	/**
	 * Size of Command Buffer to be submitted.
	 *   - The size is in units of dwords (4 bytes).
	 *   - Must be less or equal to the size of allocated IB
	 *   - Could be 0
	 */
	uint32_t       size;
};

/**
 * Structure describing submission request
 *
 * \note We could have several IBs as packet. e.g. CE, CE, DE case for gfx
 *
 * \sa amdgpu_cs_submit()
*/
struct amdgpu_cs_request {
	/** Specify flags with additional information */
	uint64_t	flags;

	/** Specify HW IP block type to which to send the IB. */
	unsigned	ip_type;

	/** IP instance index if there are several IPs of the same type. */
	unsigned	ip_instance;

	/**
	 * Specify ring index of the IP. We could have several rings
	 * in the same IP. E.g. 0 for SDMA0 and 1 for SDMA1.
	 */
	uint32_t           ring;

	/**
	 * Specify number of resource handles passed.
	 * Size of 'handles' array
	 *
	 */
	uint32_t number_of_resources;

	/** Array of resources used by submission. */
	amdgpu_bo_handle   *resources;

	/** Array of resources flags. This is optional and can be NULL. */
	uint8_t *resource_flags;

	/** Number of IBs to submit in the field ibs. */
	uint32_t number_of_ibs;

	/**
	 * IBs to submit. Those IBs will be submit together as single entity
	 */
	struct amdgpu_cs_ib_info *ibs;
};

/**
 * Structure describing request to check submission state using fence
 *
 * \sa amdgpu_cs_query_fence_status()
 *
*/
struct amdgpu_cs_query_fence {

	/** In which context IB was sent to execution */
	amdgpu_context_handle  context;

	/** Timeout in nanoseconds. */
	uint64_t  timeout_ns;

	/** To which HW IP type the fence belongs */
	unsigned  ip_type;

	/** IP instance index if there are several IPs of the same type. */
	unsigned ip_instance;

	/** Ring index of the HW IP */
	uint32_t      ring;

	/** Flags */
	uint64_t  flags;

	/** Specify fence for which we need to check
	 * submission status.*/
	uint64_t	fence;
};

/**
 * Structure which provide information about GPU VM MC Address space
 * alignments requirements
 *
 * \sa amdgpu_query_buffer_size_alignment
 */
struct amdgpu_buffer_size_alignments {
	/** Size alignment requirement for allocation in
	 * local memory */
	uint64_t size_local;

	/**
	 * Size alignment requirement for allocation in remote memory
	 */
	uint64_t size_remote;
};


/**
 * Structure which provide information about heap
 *
 * \sa amdgpu_query_heap_info()
 *
 */
struct amdgpu_heap_info {
	/** Theoretical max. available memory in the given heap */
	uint64_t  heap_size;

	/**
	 * Number of bytes allocated in the heap. This includes all processes
	 * and private allocations in the kernel. It changes when new buffers
	 * are allocated, freed, and moved. It cannot be larger than
	 * heap_size.
	 */
	uint64_t  heap_usage;

	/**
	 * Theoretical possible max. size of buffer which
	 * could be allocated in the given heap
	 */
	uint64_t  max_allocation;
};



/**
 * Describe GPU h/w info needed for UMD correct initialization
 *
 * \sa amdgpu_query_gpu_info()
*/
struct amdgpu_gpu_info {
	/** Asic id */
	uint32_t asic_id;
	/**< Chip revision */
	uint32_t chip_rev;
	/** Chip external revision */
	uint32_t chip_external_rev;
	/** Family ID */
	uint32_t family_id;
	/** Special flags */
	uint64_t ids_flags;
	/** max engine clock*/
	uint64_t max_engine_clk;
	/** number of shader engines */
	uint32_t num_shader_engines;
	/** number of shader arrays per engine */
	uint32_t num_shader_arrays_per_engine;
	/**  Number of available good shader pipes */
	uint32_t avail_quad_shader_pipes;
	/**  Max. number of shader pipes.(including good and bad pipes  */
	uint32_t max_quad_shader_pipes;
	/** Number of parameter cache entries per shader quad pipe */
	uint32_t cache_entries_per_quad_pipe;
	/**  Number of available graphics context */
	uint32_t num_hw_gfx_contexts;
	/** Number of render backend pipes */
	uint32_t rb_pipes;
	/** Active render backend pipe number */
	uint32_t active_rb_pipes;
	/**  Enabled render backend pipe mask */
	uint32_t enabled_rb_pipes_mask;
	/** Frequency of GPU Counter */
	uint32_t gpu_counter_freq;
	/** CC_RB_BACKEND_DISABLE.BACKEND_DISABLE per SE */
	uint32_t backend_disable[4];
	/** Value of MC_ARB_RAMCFG register*/
	uint32_t mc_arb_ramcfg;
	/** Value of GB_ADDR_CONFIG */
	uint32_t gb_addr_cfg;
	/** Values of the GB_TILE_MODE0..31 registers */
	uint32_t gb_tile_mode[32];
	/** Values of GB_MACROTILE_MODE0..15 registers */
	uint32_t gb_macro_tile_mode[16];
	/** Value of PA_SC_RASTER_CONFIG register per SE */
	uint32_t pa_sc_raster_cfg[4];
	/** Value of PA_SC_RASTER_CONFIG_1 register per SE */
	uint32_t pa_sc_raster_cfg1[4];
	/* CU info */
	uint32_t cu_active_number;
	uint32_t cu_ao_mask;
	uint32_t cu_bitmap[4][4];
};


/*--------------------------------------------------------------------------*/
/*------------------------- Functions --------------------------------------*/
/*--------------------------------------------------------------------------*/

/*
 * Initialization / Cleanup
 *
*/


/**
 *
 * \param   fd            - \c [in]  File descriptor for AMD GPU device
 *                                   received previously as the result of
 *                                   e.g. drmOpen() call.
 *                                   For legacy fd type, the DRI2/DRI3 authentication
 *                                   should be done before calling this function.
 * \param   major_version - \c [out] Major version of library. It is assumed
 *                                   that adding new functionality will cause
 *                                   increase in major version
 * \param   minor_version - \c [out] Minor version of library
 * \param   device_handle - \c [out] Pointer to opaque context which should
 *                                   be passed as the first parameter on each
 *                                   API call
 *
 *
 * \return   0 on success\n
 *          >0 - AMD specific error code\n
 *          <0 - Negative POSIX Error code
 *
 *
 * \sa amdgpu_device_deinitialize()
*/
int amdgpu_device_initialize(int fd,
			     uint32_t *major_version,
			     uint32_t *minor_version,
			     amdgpu_device_handle *device_handle);



/**
 *
 * When access to such library does not needed any more the special
 * function must be call giving opportunity to clean up any
 * resources if needed.
 *
 * \param   device_handle - \c [in]  Context associated with file
 *                                   descriptor for AMD GPU device
 *                                   received previously as the
 *                                   result e.g. of drmOpen() call.
 *
 * \return  0 on success\n
 *         >0 - AMD specific error code\n
 *         <0 - Negative POSIX Error code
 *
 * \sa amdgpu_device_initialize()
 *
*/
int amdgpu_device_deinitialize(amdgpu_device_handle device_handle);


/*
 * Memory Management
 *
*/

/**
 * Allocate memory to be used by UMD for GPU related operations
 *
 * \param   dev		 - \c [in] Device handle.
 *				   See #amdgpu_device_initialize()
 * \param   alloc_buffer - \c [in] Pointer to the structure describing an
 *				   allocation request
 * \param   info	 - \c [out] Pointer to structure which return
 *				    information about allocated memory
 *
 * \return   0 on success\n
 *          >0 - AMD specific error code\n
 *          <0 - Negative POSIX Error code
 *
 * \sa amdgpu_bo_free()
*/
int amdgpu_bo_alloc(amdgpu_device_handle dev,
		    struct amdgpu_bo_alloc_request *alloc_buffer,
		    struct amdgpu_bo_alloc_result *info);

/**
 * Associate opaque data with buffer to be queried by another UMD
 *
 * \param   dev	       - \c [in] Device handle. See #amdgpu_device_initialize()
 * \param   buf_handle - \c [in] Buffer handle
 * \param   info       - \c [in] Metadata to associated with buffer
 *
 * \return   0 on success\n
 *          >0 - AMD specific error code\n
 *          <0 - Negative POSIX Error code
*/
int amdgpu_bo_set_metadata(amdgpu_bo_handle buf_handle,
			   struct amdgpu_bo_metadata *info);

/**
 * Query buffer information including metadata previusly associated with
 * buffer.
 *
 * \param   dev	       - \c [in] Device handle.
 *				 See #amdgpu_device_initialize()
 * \param   buf_handle - \c [in]   Buffer handle
 * \param   info       - \c [out]  Structure describing buffer
 *
 * \return   0 on success\n
 *          >0 - AMD specific error code\n
 *          <0 - Negative POSIX Error code
 *
 * \sa amdgpu_bo_set_metadata(), amdgpu_bo_alloc()
*/
int amdgpu_bo_query_info(amdgpu_bo_handle buf_handle,
			 struct amdgpu_bo_info *info);

/**
 * Allow others to get access to buffer
 *
 * \param   dev		  - \c [in] Device handle.
 *				    See #amdgpu_device_initialize()
 * \param   buf_handle    - \c [in] Buffer handle
 * \param   type          - \c [in] Type of handle requested
 * \param   shared_handle - \c [out] Special "shared" handle
 *
 * \return   0 on success\n
 *          >0 - AMD specific error code\n
 *          <0 - Negative POSIX Error code
 *
 * \sa amdgpu_bo_import()
 *
*/
int amdgpu_bo_export(amdgpu_bo_handle buf_handle,
		     enum amdgpu_bo_handle_type type,
		     uint32_t *shared_handle);

/**
 * Request access to "shared" buffer
 *
 * \param   dev		  - \c [in] Device handle.
 *				    See #amdgpu_device_initialize()
 * \param   type	  - \c [in] Type of handle requested
 * \param   shared_handle - \c [in] Shared handle received as result "import"
 *				     operation
 * \param   output        - \c [out] Pointer to structure with information
 *				     about imported buffer
 *
 * \return   0 on success\n
 *          >0 - AMD specific error code\n
 *          <0 - Negative POSIX Error code
 *
 * \note  Buffer must be "imported" only using new "fd" (different from
 *	  one used by "exporter").
 *
 * \sa amdgpu_bo_export()
 *
*/
int amdgpu_bo_import(amdgpu_device_handle dev,
		     enum amdgpu_bo_handle_type type,
		     uint32_t shared_handle,
		     struct amdgpu_bo_import_result *output);

/**
 * Free previosuly allocated memory
 *
 * \param   dev	       - \c [in] Device handle. See #amdgpu_device_initialize()
 * \param   buf_handle - \c [in]  Buffer handle to free
 *
 * \return   0 on success\n
 *          >0 - AMD specific error code\n
 *          <0 - Negative POSIX Error code
 *
 * \note In the case of memory shared between different applications all
 *	 resources will be “physically” freed only all such applications
 *	 will be terminated
 * \note If is UMD responsibility to ‘free’ buffer only when there is no
 *	 more GPU access
 *
 * \sa amdgpu_bo_set_metadata(), amdgpu_bo_alloc()
 *
*/
int amdgpu_bo_free(amdgpu_bo_handle buf_handle);

/**
 * Request CPU access to GPU accessable memory
 *
 * \param   buf_handle - \c [in] Buffer handle
 * \param   cpu        - \c [out] CPU address to be used for access
 *
 * \return   0 on success\n
 *          >0 - AMD specific error code\n
 *          <0 - Negative POSIX Error code
 *
 * \sa amdgpu_bo_cpu_unmap()
 *
*/
int amdgpu_bo_cpu_map(amdgpu_bo_handle buf_handle, void **cpu);

/**
 * Release CPU access to GPU memory
 *
 * \param   buf_handle  - \c [in] Buffer handle
 *
 * \return   0 on success\n
 *          >0 - AMD specific error code\n
 *          <0 - Negative POSIX Error code
 *
 * \sa amdgpu_bo_cpu_map()
 *
*/
int amdgpu_bo_cpu_unmap(amdgpu_bo_handle buf_handle);


/**
 * Wait until a buffer is not used by the device.
 *
 * \param   dev           - \c [in] Device handle. See #amdgpu_lib_initialize()
 * \param   buf_handle    - \c [in] Buffer handle.
 * \param   timeout_ns    - Timeout in nanoseconds.
 * \param   buffer_busy   - 0 if buffer is idle, all GPU access was completed
 *                            and no GPU access is scheduled.
 *                          1 GPU access is in fly or scheduled
 *
 * \return   0 - on success
 *          <0 - AMD specific error code
 */
int amdgpu_bo_wait_for_idle(amdgpu_bo_handle buf_handle,
			    uint64_t timeout_ns,
			    bool *buffer_busy);


/*
 * Special GPU Resources
 *
*/



/**
 * Query information about GDS
 *
 * \param   dev	     - \c [in] Device handle. See #amdgpu_device_initialize()
 * \param   gds_info - \c [out] Pointer to structure to get GDS information
 *
 * \return   0 on success\n
 *          >0 - AMD specific error code\n
 *          <0 - Negative POSIX Error code
 *
*/
int amdgpu_gpu_resource_query_gds_info(amdgpu_device_handle dev,
					struct amdgpu_gds_resource_info *
								gds_info);


/**
 * Allocate GDS partitions
 *
 * \param   dev	       - \c [in] Device handle. See #amdgpu_device_initialize()
 * \param   gds_size   - \c [in] Size of gds allocation. Must be aligned
 *				accordingly.
 * \param   alloc_info - \c [out] Pointer to structure to receive information
 *				  about allocation
 *
 * \return   0 on success\n
 *          >0 - AMD specific error code\n
 *          <0 - Negative POSIX Error code
 *
 *
*/
int amdgpu_gpu_resource_gds_alloc(amdgpu_device_handle dev,
				   uint32_t gds_size,
				   struct amdgpu_gds_alloc_info *alloc_info);




/**
 * Release GDS resource. When GDS and associated resources not needed any
 * more UMD should free them
 *
 * \param   dev	   - \c [in] Device handle. See #amdgpu_device_initialize()
 * \param   handle - \c [in] Handle assigned to GDS allocation
 *
 * \return   0 on success\n
 *          >0 - AMD specific error code\n
 *          <0 - Negative POSIX Error code
 *
*/
int amdgpu_gpu_resource_gds_free(amdgpu_bo_handle handle);



/*
 * GPU Execution context
 *
*/

/**
 * Create GPU execution Context
 *
 * For the purpose of GPU Scheduler and GPU Robustness extensions it is
 * necessary to have information/identify rendering/compute contexts.
 * It also may be needed to associate some specific requirements with such
 * contexts.  Kernel driver will guarantee that submission from the same
 * context will always be executed in order (first come, first serve).
 *
 *
 * \param   dev	    - \c [in] Device handle. See #amdgpu_device_initialize()
 * \param   context - \c [out] GPU Context handle
 *
 * \return   0 on success\n
 *          >0 - AMD specific error code\n
 *          <0 - Negative POSIX Error code
 *
 * \sa amdgpu_cs_ctx_free()
 *
*/
int amdgpu_cs_ctx_create(amdgpu_device_handle dev,
			 amdgpu_context_handle *context);

/**
 *
 * Destroy GPU execution context when not needed any more
 *
 * \param   dev	    - \c [in] Device handle. See #amdgpu_device_initialize()
 * \param   context - \c [in] GPU Context handle
 *
 * \return   0 on success\n
 *          >0 - AMD specific error code\n
 *          <0 - Negative POSIX Error code
 *
 * \sa amdgpu_cs_ctx_create()
 *
*/
int amdgpu_cs_ctx_free(amdgpu_device_handle dev,
		       amdgpu_context_handle context);

/**
 * Query reset state for the specific GPU Context
 *
 * \param   dev	    - \c [in] Device handle. See #amdgpu_device_initialize()
 * \param   context - \c [in]  GPU Context handle
 * \param   state   - \c [out] Reset state status
 *
 * \return   0 on success\n
 *          >0 - AMD specific error code\n
 *          <0 - Negative POSIX Error code
 *
 * \sa amdgpu_cs_ctx_create()
 *
*/
int amdgpu_cs_query_reset_state(amdgpu_device_handle dev,
				amdgpu_context_handle context,
				enum amdgpu_cs_ctx_reset_state *state);


/*
 * Command Buffers Management
 *
*/


/**
 * Allocate memory to be filled with PM4 packets and be served as the first
 * entry point of execution (a.k.a. Indirect Buffer)
 *
 * \param   dev	    - \c [in] Device handle. See #amdgpu_device_initialize()
 * \param   context - \c [in]  GPU Context which will use IB
 * \param   ib_size - \c [in]  Size of allocation
 * \param   output  - \c [out] Pointer to structure to get information about
 *				   allocated IB
 *
 * \return   0 on success\n
 *          >0 - AMD specific error code\n
 *          <0 - Negative POSIX Error code
 *
 * \sa amdgpu_cs_free_ib()
 *
*/
int amdgpu_cs_alloc_ib(amdgpu_device_handle dev,
		       amdgpu_context_handle context,
		       enum amdgpu_cs_ib_size ib_size,
		       struct amdgpu_cs_ib_alloc_result *output);

/**
 * If UMD has allocates IBs which doesn’t need any more than those IBs must
 * be explicitly freed
 *
 * \param   dev	    - \c [in] Device handle. See #amdgpu_device_initialize()
 * \param   context - \c [in] GPU Context containing IB
 * \param   handle  - \c [in] IB handle
 *
 * \return   0 on success\n
 *          >0 - AMD specific error code\n
 *          <0 - Negative POSIX Error code
 *
 * \note Libdrm_amdgpu will guarantee that it will correctly detect when it
 *	is safe to return IB to free pool
 *
 * \sa amdgpu_cs_alloc_ib()
 *
*/
int amdgpu_cs_free_ib(amdgpu_device_handle dev,
		      amdgpu_context_handle context,
		      amdgpu_ib_handle handle);

/**
 * Send request to submit command buffers to hardware.
 *
 * Kernel driver could use GPU Scheduler to make decision when physically
 * sent this request to the hardware. Accordingly this request could be put
 * in queue and sent for execution later. The only guarantee is that request
 * from the same GPU context to the same ip:ip_instance:ring will be executed in
 * order.
 *
 *
 * \param   dev		       - \c [in]  Device handle.
 *					  See #amdgpu_device_initialize()
 * \param   context            - \c [in]  GPU Context
 * \param   flags              - \c [in]  Global submission flags
 * \param   ibs_request        - \c [in]  Pointer to submission requests.
 *					  We could submit to the several
 *					  engines/rings simulteniously as
 *					  'atomic' operation
 * \param   number_of_requests - \c [in]  Number of submission requests
 * \param   fences             - \c [out] Pointer to array of data to get
 *					  fences to identify submission
 *					  requests. Timestamps are valid
 *					  in this GPU context and could be used
 *					  to identify/detect completion of
 *					  submission request
 *
 * \return   0 on success\n
 *          >0 - AMD specific error code\n
 *          <0 - Negative POSIX Error code
 *
 * \note It is assumed that by default IB will be returned to free pool
 *	 automatically by libdrm_amdgpu when submission will completed.
 *	 It is possible for UMD to make decision to re-use the same IB in
 *	 this case it should be explicitly freed.\n
 *	 Accordingly, by default, after submission UMD should not touch passed
 *	 IBs. If UMD needs to re-use IB then the special flag AMDGPU_CS_REUSE_IB
 *	 must be passed.
 *
 * \note It is required to pass correct resource list with buffer handles
 *	 which will be accessible by command buffers from submission
 *	 This will allow kernel driver to correctly implement "paging".
 *	 Failure to do so will have unpredictable results.
 *
 * \sa amdgpu_command_buffer_alloc(), amdgpu_command_buffer_free(),
 *     amdgpu_cs_query_fence_status()
 *
*/
int amdgpu_cs_submit(amdgpu_device_handle  dev,
		     amdgpu_context_handle context,
		     uint64_t flags,
		     struct amdgpu_cs_request *ibs_request,
		     uint32_t number_of_requests,
		     uint64_t *fences);

/**
 *  Query status of Command Buffer Submission
 *
 * \param   dev	    - \c [in] Device handle. See #amdgpu_device_initialize()
 * \param   fence   - \c [in] Structure describing fence to query
 * \param   expired - \c [out] If fence expired or not.\n
 *				0  – if fence is not expired\n
 *				!0 - otherwise
 *
 * \return   0 on success\n
 *          >0 - AMD specific error code\n
 *          <0 - Negative POSIX Error code
 *
 * \note If UMD wants only to check operation status and returned immediately
 *	 then timeout value as 0 must be passed. In this case success will be
 *	 returned in the case if submission was completed or timeout error
 *	 code.
 *
 * \sa amdgpu_cs_submit()
*/
int amdgpu_cs_query_fence_status(amdgpu_device_handle dev,
				 struct amdgpu_cs_query_fence *fence,
				 uint32_t *expired);


/*
 * Query / Info API
 *
*/


/**
 * Query allocation size alignments
 *
 * UMD should query information about GPU VM MC size alignments requirements
 * to be able correctly choose required allocation size and implement
 * internal optimization if needed.
 *
 * \param   dev  - \c [in] Device handle. See #amdgpu_device_initialize()
 * \param   info - \c [out] Pointer to structure to get size alignment
 *			  requirements
 *
 * \return   0 on success\n
 *          >0 - AMD specific error code\n
 *          <0 - Negative POSIX Error code
 *
*/
int amdgpu_query_buffer_size_alignment(amdgpu_device_handle dev,
					struct amdgpu_buffer_size_alignments
									*info);



/**
 * Query firmware versions
 *
 * \param   dev	        - \c [in] Device handle. See #amdgpu_device_initialize()
 * \param   fw_type     - \c [in] AMDGPU_INFO_FW_*
 * \param   ip_instance - \c [in] Index of the IP block of the same type.
 * \param   index       - \c [in] Index of the engine. (for SDMA and MEC)
 * \param   version     - \c [out] Pointer to to the "version" return value
 * \param   feature     - \c [out] Pointer to to the "feature" return value
 *
 * \return   0 on success\n
 *          >0 - AMD specific error code\n
 *          <0 - Negative POSIX Error code
 *
*/
int amdgpu_query_firmware_version(amdgpu_device_handle dev, unsigned fw_type,
				  unsigned ip_instance, unsigned index,
				  uint32_t *version, uint32_t *feature);



/**
 * Query the number of HW IP instances of a certain type.
 *
 * \param   dev      - \c [in] Device handle. See #amdgpu_device_initialize()
 * \param   type     - \c [in] Hardware IP block type = AMDGPU_HW_IP_*
 * \param   count    - \c [out] Pointer to structure to get information
 *
 * \return   0 on success\n
 *          >0 - AMD specific error code\n
 *          <0 - Negative POSIX Error code
*/
int amdgpu_query_hw_ip_count(amdgpu_device_handle dev, unsigned type,
			     uint32_t *count);



/**
 * Query engine information
 *
 * This query allows UMD to query information different engines and their
 * capabilities.
 *
 * \param   dev         - \c [in] Device handle. See #amdgpu_device_initialize()
 * \param   type        - \c [in] Hardware IP block type = AMDGPU_HW_IP_*
 * \param   ip_instance - \c [in] Index of the IP block of the same type.
 * \param   info        - \c [out] Pointer to structure to get information
 *
 * \return   0 on success\n
 *          >0 - AMD specific error code\n
 *          <0 - Negative POSIX Error code
*/
int amdgpu_query_hw_ip_info(amdgpu_device_handle dev, unsigned type,
			    unsigned ip_instance,
			    struct drm_amdgpu_info_hw_ip *info);




/**
 * Query heap information
 *
 * This query allows UMD to query potentially available memory resources and
 * adjust their logic if necessary.
 *
 * \param   dev  - \c [in] Device handle. See #amdgpu_device_initialize()
 * \param   heap - \c [in] Heap type
 * \param   info - \c [in] Pointer to structure to get needed information
 *
 * \return   0 on success\n
 *          >0 - AMD specific error code\n
 *          <0 - Negative POSIX Error code
 *
*/
int amdgpu_query_heap_info(amdgpu_device_handle dev,
			    uint32_t heap,
				uint32_t flags,
			    struct amdgpu_heap_info *info);



/**
 * Get the CRTC ID from the mode object ID
 *
 * \param   dev    - \c [in] Device handle. See #amdgpu_device_initialize()
 * \param   id     - \c [in] Mode object ID
 * \param   result - \c [in] Pointer to the CRTC ID
 *
 * \return   0 on success\n
 *          >0 - AMD specific error code\n
 *          <0 - Negative POSIX Error code
 *
*/
int amdgpu_query_crtc_from_id(amdgpu_device_handle dev, unsigned id,
			      int32_t *result);



/**
 * Query GPU H/w Info
 *
 * Query hardware specific information
 *
 * \param   dev  - \c [in] Device handle. See #amdgpu_device_initialize()
 * \param   heap - \c [in] Heap type
 * \param   info - \c [in] Pointer to structure to get needed information
 *
 * \return   0 on success\n
 *          >0 - AMD specific error code\n
 *          <0 - Negative POSIX Error code
 *
*/
int amdgpu_query_gpu_info(amdgpu_device_handle dev,
			   struct amdgpu_gpu_info *info);



/**
 * Query hardware or driver information.
 *
 * The return size is query-specific and depends on the "info_id" parameter.
 * No more than "size" bytes is returned.
 *
 * \param   dev     - \c [in] Device handle. See #amdgpu_device_initialize()
 * \param   info_id - \c [in] AMDGPU_INFO_*
 * \param   size    - \c [in] Size of the returned value.
 * \param   value   - \c [out] Pointer to the return value.
 *
 * \return   0 on success\n
 *          >0 - AMD specific error code\n
 *          <0 - Negative POSIX error code
 *
*/
int amdgpu_query_info(amdgpu_device_handle dev, unsigned info_id,
		      unsigned size, void *value);



/**
 * Read a set of consecutive memory-mapped registers.
 * Not all registers are allowed to be read by userspace.
 *
 * \param   dev          - \c [in] Device handle. See #amdgpu_device_initialize(
 * \param   dword_offset - \c [in] Register offset in dwords
 * \param   count        - \c [in] The number of registers to read starting
 *                                 from the offset
 * \param   instance     - \c [in] GRBM_GFX_INDEX selector. It may have other
 *                                 uses. Set it to 0xffffffff if unsure.
 * \param   flags        - \c [in] Flags with additional information.
 * \param   values       - \c [out] The pointer to return values.
 *
 * \return   0 on success\n
 *          >0 - AMD specific error code\n
 *          <0 - Negative POSIX error code
 *
*/
int amdgpu_read_mm_registers(amdgpu_device_handle dev, unsigned dword_offset,
			     unsigned count, uint32_t instance, uint32_t flags,
			     uint32_t *values);



/**
 * Request GPU access to user allocated memory e.g. via "malloc"
 *
 * \param dev - [in] Device handle. See #amdgpu_device_initialize()
 * \param cpu - [in] CPU address of user allocated memory which we
 * want to map to GPU address space (make GPU accessible)
 * (This address must be correctly aligned).
 * \param size - [in] Size of allocation (must be correctly aligned)
 * \param amdgpu_bo_alloc_result - [out] Handle of allocation to be passed as resource
 * on submission and be used in other operations.(e.g. for VA submission)
 * ( Temporally defined amdgpu_bo_alloc_result as parameter for return mc address. )
 *
 *
 * \return 0 on success
 * >0 - AMD specific error code
 * <0 - Negative POSIX Error code
 *
 *
 * \note
 * This call doesn't guarantee that such memory will be persistently
 * "locked" / make non-pageable. The purpose of this call is to provide
 * opportunity for GPU get access to this resource during submission.
 *
 * The maximum amount of memory which could be mapped in this call depends
 * if overcommit is disabled or not. If overcommit is disabled than the max.
 * amount of memory to be pinned will be limited by left "free" size in total
 * amount of memory which could be locked simultaneously ("GART" size).
 *
 * Supported (theoretical) max. size of mapping is restricted only by
 * "GART" size.
 *
 * It is responsibility of caller to correctly specify access rights
 * on VA assignment.
*/
int amdgpu_create_bo_from_user_mem(amdgpu_device_handle dev,
				    void *cpu,
				    uint64_t size,
				    struct amdgpu_bo_alloc_result *info);


#endif /* #ifdef _AMDGPU_H_ */