aboutsummaryrefslogtreecommitdiffstats
blob: 804f9a75199ca1877a9d04f64abb490a670ab6d7 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
#include "drmP.h"
#include "drm.h"
#include "nouveau_drv.h"

static void
nv04_instmem_determine_amount(struct drm_device *dev)
{
	struct drm_nouveau_private *dev_priv = dev->dev_private;
	int i;

	/* Figure out how much instance memory we need */
	if (dev_priv->card_type >= NV_40) {
		/* We'll want more instance memory than this on some NV4x cards.
		 * There's a 16MB aperture to play with that maps onto the end
		 * of vram.  For now, only reserve a small piece until we know
		 * more about what each chipset requires.
		 */
		dev_priv->ramin_rsvd_vram = (1*1024* 1024);
	} else {
		/*XXX: what *are* the limits on <NV40 cards?, and does RAMIN
		 *     exist in vram on those cards as well?
		 */
		dev_priv->ramin_rsvd_vram = (512*1024);
	}
	DRM_DEBUG("RAMIN size: %dKiB\n", dev_priv->ramin_rsvd_vram>>10);

	/* Clear all of it, except the BIOS image that's in the first 64KiB */
	for (i=(64*1024); i<dev_priv->ramin_rsvd_vram; i+=4)
		NV_WI32(i, 0x00000000);
}

static void
nv04_instmem_configure_fixed_tables(struct drm_device *dev)
{
	struct drm_nouveau_private *dev_priv = dev->dev_private;
	struct nouveau_engine *engine = &dev_priv->Engine;

	/* FIFO hash table (RAMHT)
	 *   use 4k hash table at RAMIN+0x10000
	 *   TODO: extend the hash table
	 */
	dev_priv->ramht_offset = 0x10000;
	dev_priv->ramht_bits   = 9;
	dev_priv->ramht_size   = (1 << dev_priv->ramht_bits);
	DRM_DEBUG("RAMHT offset=0x%x, size=%d\n", dev_priv->ramht_offset,
						  dev_priv->ramht_size);

	/* FIFO runout table (RAMRO) - 512k at 0x11200 */
	dev_priv->ramro_offset = 0x11200;
	dev_priv->ramro_size   = 512;
	DRM_DEBUG("RAMRO offset=0x%x, size=%d\n", dev_priv->ramro_offset,
						  dev_priv->ramro_size);

	/* FIFO context table (RAMFC)
	 *   NV40  : Not sure exactly how to position RAMFC on some cards,
	 *           0x30002 seems to position it at RAMIN+0x20000 on these
	 *           cards.  RAMFC is 4kb (32 fifos, 128byte entries).
	 *   Others: Position RAMFC at RAMIN+0x11400
	 */
	switch(dev_priv->card_type)
	{
		case NV_40:
		case NV_44:
			dev_priv->ramfc_offset = 0x20000;
			dev_priv->ramfc_size   = engine->fifo.channels *
						 nouveau_fifo_ctx_size(dev);
			break;
		case NV_30:
		case NV_20:
		case NV_17:
		case NV_11:
		case NV_10:
		case NV_04:
		default:
			dev_priv->ramfc_offset = 0x11400;
			dev_priv->ramfc_size   = engine->fifo.channels *
						 nouveau_fifo_ctx_size(dev);
			break;
	}
	DRM_DEBUG("RAMFC offset=0x%x, size=%d\n", dev_priv->ramfc_offset,
						  dev_priv->ramfc_size);
}

int nv04_instmem_init(struct drm_device *dev)
{
	struct drm_nouveau_private *dev_priv = dev->dev_private;
	uint32_t offset;
	int ret = 0;

	nv04_instmem_determine_amount(dev);
	nv04_instmem_configure_fixed_tables(dev);

	/* Create a heap to manage RAMIN allocations, we don't allocate
	 * the space that was reserved for RAMHT/FC/RO.
	 */
	offset = dev_priv->ramfc_offset + dev_priv->ramfc_size;

	/* On my NV4E, there's *something* clobbering the 16KiB just after
	 * where we setup these fixed tables.  No idea what it is just yet,
	 * so reserve this space on all NV4X cards for now.
	 */
	if (dev_priv->card_type >= NV_40)
		offset += 16*1024;

	ret = nouveau_mem_init_heap(&dev_priv->ramin_heap,
				    offset, dev_priv->ramin_rsvd_vram - offset);
	if (ret) {
		dev_priv->ramin_heap = NULL;
		DRM_ERROR("Failed to init RAMIN heap\n");
	}

	return ret;
}

void
nv04_instmem_takedown(struct drm_device *dev)
{
}

int
nv04_instmem_populate(struct drm_device *dev, struct nouveau_gpuobj *gpuobj, uint32_t *sz)
{
	if (gpuobj->im_backing)
		return -EINVAL;

	return 0;
}

void
nv04_instmem_clear(struct drm_device *dev, struct nouveau_gpuobj *gpuobj)
{
	struct drm_nouveau_private *dev_priv = dev->dev_private;

	if (gpuobj && gpuobj->im_backing) {
		if (gpuobj->im_bound)
			dev_priv->Engine.instmem.unbind(dev, gpuobj);
		gpuobj->im_backing = NULL;
	}
}

int
nv04_instmem_bind(struct drm_device *dev, struct nouveau_gpuobj *gpuobj)
{
	if (!gpuobj->im_pramin || gpuobj->im_bound)
		return -EINVAL;

	gpuobj->im_bound = 1;
	return 0;
}

int
nv04_instmem_unbind(struct drm_device *dev, struct nouveau_gpuobj *gpuobj)
{
	if (gpuobj->im_bound == 0)
		return -EINVAL;

	gpuobj->im_bound = 0;
	return 0;
}