aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorRob Clark2012-10-07 18:57:31 -0500
committerRob Clark2013-02-14 11:13:15 -0600
commit41fc2cc8a98a8d02ea7d3635d3103f7dd371de10 (patch)
tree10d8aab5a340486a34f00052cb110d3ff3d93208 /.gitignore
parent36d18211b196cad4761ac70c4fd08aba323f5b0d (diff)
downloadexternal-libgbm-41fc2cc8a98a8d02ea7d3635d3103f7dd371de10.tar.gz
external-libgbm-41fc2cc8a98a8d02ea7d3635d3103f7dd371de10.tar.xz
external-libgbm-41fc2cc8a98a8d02ea7d3635d3103f7dd371de10.zip
freedreno: add freedreno DRM
The libdrm_freedreno helper layer for use by xf86-video-freedreno, fdre (freedreno r/e library and tests for driving gpu), and eventual gallium driver for the Adreno GPU. This uses the msm gpu driver from QCOM's android kernel tree. Note that current msm kernel driver is a bit strange. It provides a DRM interface for GEM, which is basically sufficient to have DRI2 working. But it does not provide KMS. And interface to 2d and 3d cores is via different other devices (/dev/kgsl-*). This is not quite how I'd write a DRM driver, but at this stage it is useful for xf86-video-freedreno and fdre (and eventual gallium driver) to be able to work on existing kernel driver from QCOM, to allow to capture cmdstream dumps from the binary blob drivers without having to reboot. So libdrm_freedreno attempts to hide most of the crazy. The intention is that when there is a proper kernel driver, it will be mostly just changes in libdrm_freedreno to adapt the gallium driver and xf86-video-freedreno (ignoring the fbdev->KMS changes). So don't look at freedreno as an example of how to write a libdrm module or a DRM driver.. it is just an attempt to paper over a non- standard kernel driver architecture. v1: original v2: hold ref's to pending bo's (because qcom's kernel driver doesn't), various bug fixes, add ringbuffer markers so we can emit IB's to portion of ringbuffer (so that gallium driver can use a single ringbuffer for both tile cmds and draw cmds. Signed-off-by: Rob Clark <robclark@freedesktop.org>
Diffstat (limited to '.gitignore')
-rw-r--r--.gitignore1
1 files changed, 1 insertions, 0 deletions
diff --git a/.gitignore b/.gitignore
index 225fd801..9f8eabbf 100644
--- a/.gitignore
+++ b/.gitignore
@@ -48,6 +48,7 @@ libdrm_nouveau.pc
48libdrm_radeon.pc 48libdrm_radeon.pc
49libdrm_omap.pc 49libdrm_omap.pc
50libdrm_exynos.pc 50libdrm_exynos.pc
51libdrm_freedreno.pc
51libkms.pc 52libkms.pc
52libtool 53libtool
53ltmain.sh 54ltmain.sh